L-com

Blog

Servo Cables vs. VFD Cables: Key Differences
In industrial automation, robotics and driving systems, choosing the right cable is just as important as selecting the right motor or controller. Two of the most widely used cables in these applications are servo cables and variable frequency drive (VFD) cables. While they might appear similar at first glance, they are engineered for very different purposes. Using the wrong cable can lead to system inefficiencies, electromagnetic interference (EMI) and even premature equipment failure.... Read more
Servo Cables in Robotics and Motion Control
Robotics and modern motion control systems are rapidly evolving fields that demand unparalleled levels of precision, reliability and efficiency. At the heart of these sophisticated systems are servo cables, specialized cables engineered to deliver essential power, feedback and control signals to servo motors, which are critical components in a wide array of applications.... Read more
How to Extend the Lifespan of Servo and VFD Cables
Industrial automation depends on the seamless operation of servo and variable frequency drive (VFD) systems to deliver precise motion control and efficient motor management across a variety of processes. Central to these operations are specialized servo and VFD cables, which are tasked with reliably transmitting power, signals and crucial data between drive components and motors. Their ability to withstand the demanding electrical and environmental stresses of modern manufacturing is essential for maintaining peak productivity.... Read more
How to Choose the Right Servo Cable for Your Application
Servo systems are undeniably the backbone of modern industrial automation, robotics, CNC machinery and a plethora of motion control applications. These systems are designed to provide precise control over movement, making them essential in a wide range of industries, from manufacturing and aerospace to automotive and medical devices. At the heart of these intricate systems lies a crucial yet often overlooked component: the servo cable.... Read more
Do You Always Need Shielding for VFD Cables?
Variable frequency drives (VFDs) have become indispensable components in modern industrial automation, thanks to their ability to precisely control motor speeds, enhance energy efficiency and improve overall operational effectiveness. By adjusting the frequency and voltage supplied to electric motors, VFDs enable smoother starts and stops, reduce mechanical stress and facilitate significant energy savings, particularly in applications that require variable loads.... Read more
Choosing the Correct VFD Cable for Drive Systems
Variable frequency drives (VFDs) are vital components in contemporary industrial applications, providing the ability to fine-tune motor speed and torque to meet specific operational needs. This level of control is crucial across a wide range of sectors, including HVAC systems, conveyor belts and CNC machines, where precise adjustments can lead to enhanced efficiency, energy savings and improved overall performance.... Read more
Can Servo and VFD Cables Be Used Outdoors?
Servo and VFD (variable frequency drive) cables are truly the lifelines of modern automation and industrial operations, delivering precise control to motors in robotics and CNC equipment, while ensuring efficient power transmission with strong EMI protection in drive and motor applications. Their reliability is crucial for keeping automated processes running smoothly.... Read more
Best Practices for Installing Servo and VFD Cables
Servo and variable frequency drive (VFD) cables are the backbone of modern automation, robotics and motion control systems. However, even the most robust and high-quality cables can suffer from premature failure if they are not properly installed and maintained. Factors such as incorrect routing, inadequate shielding practices and exposure to harsh environmental conditions can compromise the integrity of these cables. For instance, improper bending or twisting during installation can cause strain on the wires, leading to potential short circuits. Furthermore, exposure to extreme temperatures, moisture or chemicals can deteriorate the cable’s materials, making them susceptible to electrical faults and operational inefficiencies.... Read more
Test Equipment, Labeling and Maintenance Products for Uptime
For enterprise data centers, uptime is everything. The relentless demand for continuous availability means that even a few minutes of downtime can translate into significant financial losses, disrupted services and lasting damage to a company’s reputation.... Read more
Racks, Cabinets and Cable Management: Designing for Density and Efficiency
Enterprise data centers are the backbone of contemporary IT infrastructure, playing a pivotal role in managing and processing vast amounts of information that organizations rely on for their daily operations. With the exponential growth of data and the increasing demands placed on IT systems, the efficient utilization of space, power and cooling resources has become more critical than ever. Data centers are not just large rooms filled with servers; they are complex ecosystems that require meticulous planning and design.... Read more

Resources

Search Entries