L-com

Can Servo and VFD Cables Be Used Outdoors?

By Eileen Harvey 

Servo and VFD (variable frequency drive) cables are truly the lifelines of modern automation and industrial operations, delivering precise control to motors in robotics and CNC equipment, while ensuring efficient power transmission with strong EMI protection in drive and motor applications. Their reliability is crucial for keeping automated processes running smoothly. 

When considering outdoor use, engineers and installers must be vigilant about cable specification and installation quality. Outdoor environments present challenges such as prolonged UV exposure, fluctuating temperatures, moisture, chemical exposure and physical/mechanical stress. Without suitable cable construction, these factors can rapidly degrade cable jackets and insulation, causing breakdowns and failures that disrupt operations 

Understanding Servo and VFD Cables 

Servo cables are designed for motion control applications. They provide power and feedback to servo motors and are highly flexible for repetitive bending in robotics and automated systems. VFD cables carry power from a VFD to a motor. They are equipped with shielding to minimize EMI and voltage spikes and are built to handle high voltages, thermal stress and electrical noise. 

While Servo cables emphasize flexibility and signal integrity, VFD cables prioritize power handling and EMI suppression. 

Challenges of Outdoor Cable Installation 

When servo and VFD cables are installed outdoors they must withstand a range of harsh environmental conditions. UV radiation can degrade standard PVC jackets, leading to cracking, brittleness and eventual insulation failure. Moisture is another risk since rain, snow and condensation can seep into cables that are not properly sealed, causing short circuits, rust and insulation breakdown. Outdoor systems also face temperature extremes with heat in the summer and sub-zero conditions in the winter. These thermal swings expand and contract cable materials and can weaken insulation over time. Mechanical stress is an added concern because outdoor robotics or long cable runs may be exposed to abrasion, vibration or pulling forces that can damage the jacket and fatigue the conductors. 

Factors That Make Cables Suitable for Outdoor Use 

Not all cables are appropriate for outdoor environments, so outdoor installers of servo or VFD cables should look for specific features that ensure durability and performance. UV-resistant jackets made from PUR or specially formulated PVC protect against sun damage. Moisture protection is critical, and outdoor-rated cables typically use tight jacket constructions or gel-filled or double-jacket designs to block water ingress. The cable’s operating temperature range should also be suitable for the climate, for example −40°C to +90°C, since standard indoor cables with narrow tolerances cannot withstand outdoor extremes. Enhanced shielding using copper tape or braided shields provides added EMI protection in electrically noisy environments. 

Best Practices for Using Servo and VFD Cables Outdoors 

Following best practices helps maximize cable life and system reliability in outdoor settings. Always choose cables that are rated for UV exposure and weather resistance; TKD Kabel’s Kaweflex series is one example engineered for industrial and outdoor use. Proper grounding and shielding are essential to prevent EMI while avoiding ground loops by adhering to the manufacturer’s guidelines. Using conduits or cable trays protects cables from physical damage and moisture and is especially important in areas with heavy foot traffic or moving machinery. Regular maintenance is also necessary, including quarterly inspections for cracks, discoloration or insulation wear, with immediate replacement of damaged sections. Finally, avoid overbending by respecting the specified minimum bend radius, particularly in cold climates where jackets are less flexible. 

Real-World Applications 

  • Wind Turbines: Servo cables manage pitch control systems; VFD cables drive generator motors. 
  • Solar Farms: VFD cables regulate water pumps and tracking systems exposed to the elements. 
  • Outdoor Robotics: Servo cables ensure precise movement even in dusty or wet conditions. 

Outdoor-rated Servo and VFD cables can last three to five times longer than non-rated alternatives when installed correctly. 

Recommendations and Tips 

  • Always buy cables from reputable brands like TKD Kabel. 
  • Match cable specs to environmental conditions don’t assume one size fits all. 
  • If in doubt, consult the manufacturer’s datasheet before installation. 
  • Factor in long-term cost savings: the higher upfront cost of outdoor-rated cables often prevents expensive downtime later. 

These cables must resist UV radiation, temperature swings and moisture while maintaining EMI shielding and mechanical durability. 

If you’re planning an outdoor installation, invest in high-quality cables like TKD Kabel’s Kaweflex series, which are designed to handle industrial and environmental stresses. Proper installation, protection and maintenance will ensure long service life and reduce downtime. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries