L-com

Servo Cables vs. VFD Cables: Key Differences

By Eileen Harvey 

In industrial automation, robotics and driving systems, choosing the right cable is just as important as selecting the right motor or controller. Two of the most widely used cables in these applications are servo cables and variable frequency drive (VFD) cables. While they might appear similar at first glance, they are engineered for very different purposes. Using the wrong cable can lead to system inefficiencies, electromagnetic interference (EMI) and even premature equipment failure.  

At first glance, these cables may seem interchangeable due to their similar appearance and construction; however, they are meticulously engineered to serve distinct purposes within automation systems. Servo cables are specifically designed to facilitate high-performance motion control, ensuring precise communication between the servo motor and the controller. They support the rapid transmission of data and power needed for smooth, accurate movements, which is essential in applications requiring a high degree of precision, such as robotics and CNC machinery.  

On the other hand, VFD cables are tailored for variable frequency drives that control the speed and torque of AC motors. These cables are constructed to withstand the challenges posed by high voltage and the EMI that can occur during operation. Using the incorrect cable in these applications can have serious consequences.  

Understanding Servo Cables 

Servo cables play a crucial role in the operation of servo motors, which are essential components in many automated systems. These cables are meticulously engineered to facilitate the connection between servo motors and their corresponding controllers or drives, ensuring a seamless flow of power and data. Unlike standard power cables, which typically serve a singular function, servo cables are designed to accommodate multiple lines within a single protective sheath.  

This includes not only the power lines necessary for the motor's operation but also the signal and feedback lines that provide real-time communication between the motor and the controller. This integration is vital for achieving precise motion control, allowing for accurate positioning and speed regulation, which are critical in applications such as robotics, CNC machinery and automation systems. 

Key Features and Applications of Servo Cables 

Servo cables are engineered with specific features that allow them to perform reliably in demanding motion control environments. Their high flexibility supports continuous movement in applications such as drag chains and robotic arms, while effective shielding protects signal transmission from electrical noise. Many servo cables use hybrid construction that combines power conductors with signal or feedback wires to simplify installation and maintain precise control. Durable jacket materials add further protection by resisting oil, UV exposure and mechanical stress. 

These characteristics make servo cables suitable for a wide range of applications, including robotics and automated systems, CNC machinery and high-speed packaging or assembly lines. They are essential anywhere accurate positioning and consistent feedback are required to maintain optimal system performance. 

Understanding VFD Cables 

VFD cables play a crucial role in the operation of industrial and commercial motor systems by providing the necessary connection between variable frequency drives (often referred to as inverters) and AC motors. These cables are specifically engineered to accommodate the unique demands of VFD applications, where the frequency and voltage supplied to the motor can be adjusted to control its speed and torque. This adaptability offers significant energy savings and improved performance, making VFDs a popular choice in various industries.  

However, with the capability to alter motor speed comes the potential for generating harmonics and electrical noise, which can adversely affect both the motor and the surrounding electrical environment. Therefore, the selection and design of VFD cables are critical, as they must be able to withstand these challenges while ensuring reliable operation. 

Key Features and Applications of VFD Cables 

VFD cables are built with specific attributes that allow them to perform reliably in drive-controlled motor systems. They use heavy insulation to withstand high voltage spikes generated during switching, and they incorporate foil and braid shielding to control EMI emissions that could affect nearby equipment. Their reduced capacitance supports stable performance over varying cable lengths, and they are optimized strictly for power transmission rather than feedback signals. 

These features make VFD cables well suited for a variety of motor-driven applications. They are commonly used in pumps and compressors, HVAC systems, conveyor belts, cranes and general industrial motor control where consistent power delivery and minimized electrical noise are essential for dependable operation. 

When to Use Servo Cables vs. VFD Cables 

When it comes to industrial automation and control systems, understanding the distinction between servo cables and VFD cables is essential for ensuring optimal performance and reliability of your machinery. Servo cables are specifically designed to connect servo motors to servo drives, providing precise control over position, speed and torque 

These cables typically feature multiple twisted pairs, which help to minimize EMI and maintain signal integrity in high-precision applications. 

Use servo cables when: your system requires position feedback, you need flexible movement in drag chains or robotics, and signal and power must be transmitted together. 

Use VFD cables when: connecting a VFD to a motor, EMI suppression is critical, and high-power loads and longer runs are involved. 

Common Mistakes to Avoid 

  • Using a VFD cable in place of a servo cable, which results in signal transmission issues. 
  • Using a servo cable for high-power drives, which causes overheating and EMI leaks. 
  • Poor grounding of shields, which lead to electrical noise and equipment malfunctions. 

Best Practices for Selection and Installation 

Selection Tips: 

  • Match cable type to the application (servo for precision, VFD for power). 
  • Check voltage and current ratings. 
  • Choose cables with oil, UV or chemical resistance if operating in harsh environments. 

Installation Tips: 

  • Maintain separation between power and signal cables. 
  • Ground shields at one or both ends (depending on manufacturer guidance). 
  • Avoid tight bends that could strain conductors. 
  • Perform regular visual inspections for jacket damage. 

While both servo cables and VFD cables are essential in modern automation, they serve very different purposes. Servo cables are built for precision, flexibility and hybrid transmission of power + signals, while VFD cables are designed for robust power delivery with superior EMI suppression. Choosing the right one not only enhances performance but also extends the lifespan of your equipment. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries