L-com

How to Extend the Lifespan of Servo and VFD Cables

By Eileen Harvey 

Industrial automation depends on the seamless operation of servo and variable frequency drive (VFD) systems to deliver precise motion control and efficient motor management across a variety of processes. Central to these operations are specialized servo and VFD cables, which are tasked with reliably transmitting power, signals and crucial data between drive components and motors. Their ability to withstand the demanding electrical and environmental stresses of modern manufacturing is essential for maintaining peak productivity. 

Premature cable failure, however, can have far-reaching consequences. Not only does it result in costly operational downtime and expensive repair cycles, but it can also compromise the safety of equipment and personnel within the plant. Common causes of failure include overheating, electrical surges, loose connections, improper grounding and contamination from dust, moisture or chemicals.  

Why Cable Lifespan Matters 

In an increasingly interconnected world, the longevity of cable infrastructure plays a pivotal role in maintaining the efficiency and reliability of various technological systems. Whether in telecommunications, data centers or residential networks, the lifespan of cables directly impacts performance, operational costs and overall system integrity. 

Cables are not merely conduits for transferring data; they are critical components that affect bandwidth, speed and signal quality. Brands like TKD Kabel offer industrial-grade solutions specifically designed to withstand harsh conditions and dynamic applications. Choosing high-quality cables is the first step toward long-term performance. 

Factors Affecting Cable Lifespan 

Several conditions influence how long a cable will perform reliably. 

Mechanical stress is a major factor since frequent bending, twisting and abrasion gradually degrade both the insulation and the conductors. Systems with moving parts, such as robotic arms or conveyors, place added strain on servo cables and can accelerate wear. 

Electrical stress also plays a role; high voltages, harmonics and electrical noise can shorten a cable’s life, and VFD cables are especially vulnerable to electromagnetic interference when shielding is insufficient. 

Environmental conditions further affect longevity because moisture, UV radiation, oils and chemicals can break down cable jackets, making outdoor applications dependent on cables rated specifically for industrial outdoor use.  

Installation errors can also lead to premature failure. Incorrect bend radius, over-tightened clamps or running signal cables parallel to power cables can all create mechanical or electrical issues that reduce overall lifespan. 

Best Practices for Installation 

  • Maintain the minimum bend radius (usually 7–12x cable diameter). 
  • Avoid sharp edges and cable pinching during routing. 
  • Separate power and signal cables to minimize EMI. 
  • Use shielded cables for environments with heavy electrical noise. 
  • Ensure grounding and bonding are properly executed. 

Example: The Kaweflex EMC-Optimized VFD Cables offer superior shielding to reduce EMI, extending system reliability. 

Preventive Maintenance Tips 

  1. Visual Inspections: Look for cracks, cuts, discoloration or insulation wear. 
  1. Check Connections: Loose or corroded terminations cause overheating. 
  1. Grounding Integrity: Ensure shield connections remain intact. 
  1. Strain Relief: Use proper clamps and cable carriers to prevent pulling stress. 
  1. Cleanliness: Keep connectors free from dust, oil and metal shavings. 

Diagnosing and Solving Problems with Servo and VFD Cables 

Servo and VFD cables can exhibit different symptoms when issues arise, and understanding these signs helps pinpoint the root cause. 

Servo cable problems often appear as loss of motor precision, erratic movements or encoder feedback errors. These issues typically stem from damaged signal conductors or degradation of the shielding that protects sensitive data lines. 

VFD cable failures present differently, with symptoms such as overheating drives, EMI interference affecting nearby equipment or nuisance tripping of breakers. These problems are usually linked to poor shielding, insulation breakdown or improper grounding. 

Diagnosing these issues requires reliable testing methods. Continuity testing helps verify conductor integrity, insulation resistance testing identifies breakdowns in protective layers and thermal imaging can uncover hot spots that indicate electrical or mechanical stress. Improving cable durability begins with selecting designs that match the application. High flex cables are essential for moving systems that rely on drag chains. Jackets with UV, oil or chemical resistance are necessary for outdoor or factory floor environments, and double-shielded constructions help prevent EMI. UL and CSA flame retardant certifications also ensure the cable meets safety and compliance requirements. 

Advanced solutions can further extend cable lifespan. Cable carriers or drag chains protect moving cables from abrasion and strain. Surge protection reduces stress caused by transient voltages. Predictive maintenance systems monitor insulation or shield degradation and identify early signs of failure before downtime occurs. Heat management is equally important, and keeping cables away from high temperature zones prevents thermal damage and prolongs service life. 

Facts About Servo and VFD Cables 

  • A high-quality VFD cable can last over 10 years with proper installation and care. 
  • 80% of premature failures are due to improper installation, not manufacturing defects. 
  • Shielding effectiveness can degrade by 30% if grounding is not correctly maintained. 

FAQs About Extending Lifespan of Servo and VFD Cables 

Q1: How often should servo and VFD cables be inspected? 
A: At least every three to six months in demanding environments. 

Q2: Can I repair a damaged cable? 
A: Minor outer jacket cuts can be repaired with proper sealing, but conductor or shielding damage requires replacement. 

Q3: What is the average lifespan of these cables? 
A: With proper installation, 5 to 15 years, depending on the environment and stress. 

Q4: Do I always need outdoor-rated cables for outdoor use? 
A: Yes, unless fully enclosed in conduits. For example, TKD Kabel industrial outdoor cables are designed for long-term UV and moisture resistance. 

Extending the lifespan of servo and VFD cables requires a mix of correct installation, preventive maintenance and choosing the right cable type for your application. By reducing mechanical, electrical and environmental stresses, you’ll ensure reliable performance, minimize downtime and save costs over time. With solutions from TKD Kabel including shielded, high-flex and outdoor-rated VFD cables you can optimize your industrial systems for long-term success. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries