Your drive can give you precise motor control, but the wrong cable can undermine that performance. Electrical noise may disrupt nearby sensors, while undersized conductors or unsuitable insulation can lead to overheating and premature failure. Knowing how to choose a VFD cable helps you avoid those problems before they turn into downtime and repairs.
Variable frequency drives (VFDs) adjust motor speed and torque in equipment such as HVAC systems, conveyors and CNC machines. That control can improve efficiency, save energy and reduce wear, but the cable connecting the drive to the motor needs to suit the job. A fixed installation, a moving assembly and a long cable run each place different demands on it.
So what should you look for? Let's work through voltage rating, conductor size, shielding and cable materials, then connect those choices to your application and the installation practices that help keep it running reliably.
Key Takeaways
- VFD cables need shielding and insulation rated for the high-frequency switching noise variable frequency drives generate.
- Cable selection should be matched to the specific application (fixed installation vs. continuous motion) not treated as one-size-fits-all.
- Common mistakes include undersizing conductors and skipping shielding on longer cable runs.
- Correct grounding and termination practices are as important as the cable specification itself.
What are VFD Cables?
VFD cables are specially designed power and control cables used to connect a VFD to a motor. Unlike standard power cables, they are built to handle high voltage spikes generated by drives, EMI suppression, and thermal and mechanical stresses in industrial environments. Key differences include shielding (foil/braid) to reduce EMI, robust insulation materials like XLPE or PVC, and flexibility for dynamic and moving applications.
Those features give you a starting point. The next step is checking which specifications your drive, motor and installation actually need.
Key Factors in Choosing the Correct VFD Cable
Voltage Rating
Start by matching the VFD cable voltage rating to your drive and motor system. Common ratings include 600V, 1kV and higher. A rating that's too low increases the risk of insulation breakdown. Check current carrying capacity against the motor's full load current as well. Oversizing the conductor can help reduce voltage drop and improve cooling. For instance, 14 AWG cables typically work for smaller drives, while 6 AWG cables are better suited for heavy-duty high current motors.
Shielding
Once you've checked voltage and conductor size, consider the electrical noise the drive generates. Its high-frequency switching creates EMI that can interfere with nearby equipment. Read more on VFD cable shielding options: foil for lightweight basic protection, braid for more durable high-performance shielding, and a combination of foil and braid that is ideal for industrial automation.
Insulation and Jacket Material
With shielding covered, look at the materials that protect the cable. PVC offers general purpose performance at an affordable cost, XLPE provides high temperature resistance, and PUR delivers superior resistance to oil, chemicals and abrasion. For environments exposed to oil, UV or chemicals, a PUR jacket is recommended. If the cable will move with robotics or CNC equipment, check its flexibility and the manufacturer's minimum bend radius before installation.
Alongside those material and movement requirements, check the temperatures the cable will face.
Temperature Rating
Temperature rating is the final key factor. Many VFD cables operate from −40°C to +90°C, while some are designed for continuous duty at temperatures as high as +105°C or +125°C. Choosing a cable with an appropriate temperature range helps ensure long-term reliability.
VFD Cable Selection at a Glance
With those factors in mind, use this quick comparison to connect your application type to the recommended cable specifications:
| Application Type | Recommended Cable Spec | Why |
|---|---|---|
| Fixed installation | Standard shielded VFD cable, PVC or XLPE jacket | Minimal movement means flexibility matters less than voltage rating and shielding |
| Continuous motion (robotics, CNC) | Flexible shielded cable, PUR jacket, tight bend radius rating | Withstands repeated flexing without cracking insulation or breaking shielding |
| Long cable runs | Larger conductor gauge, combination foil + braid shielding | Reduces voltage drop and maintains EMI suppression over distance |
| Oil, UV or chemical exposure | PUR jacket, UL/CSA-rated for outdoor or washdown use | Resists environmental degradation that PVC or XLPE can't handle long-term |
VFD Cable Selection by Application
The table gives you a starting point, but the details of your setup determine which features matter most. Industrial automation and robotics need flexible shielded cables that can withstand constant motion in moving assemblies. HVAC systems benefit from strong EMI suppression to protect sensitive sensors, while CNC machines need robust shielding and low capacitance to maintain precision. In oil, gas and mining operations, rugged jackets that resist oil, UV and chemicals are essential for long-term reliability.
Before you settle on a cable, check for these common selection mistakes that can undo an otherwise suitable choice.
Common Mistakes to Avoid
Using standard power cables without the EMI suppression required for drive applications is a common mistake. Undersizing conductors can also lead to overheating. Other installations miss the need for shielding near sensitive equipment or overlook resistance to oil, UV and chemicals. These mistakes can cause premature failure. See common causes of servo and VFD cable failure for a fuller breakdown.
Choosing a suitable cable is only part of the job. How you ground, route and inspect it matters too.
Best Practices for VFD Cable Installation
- Ground properly: Ensure shield termination at both ends.
- Route carefully: Avoid running parallel with sensitive signal cables.
- Follow standards: NEC, UL, IEEE recommendations.
- Inspect regularly: Look for insulation cracks or EMI issues.
Still have questions about cable size, shielding or suitability? These answers can help you check your choice.
FAQs (Frequently Asked Questions)
Can I use standard power cables for VFDs?
No. Standard cables lack shielding and insulation strength, leading to EMI issues and premature failure.
What size cable should I use for a VFD?
It depends on the motor's current rating. Always check AWG charts and manufacturer recommendations.
Why is shielding so important in VFD cables?
Shielding reduces EMI, preventing interference with nearby electronics and ensuring system stability.
Are VFD cables suitable for outdoor use?
Yes, if they have UV and weather-resistant jackets like PUR.
What is a VFD cable and how is it different from standard power cable?
A VFD cable is purpose-built with shielding and insulation rated for the high-frequency switching noise a drive generates, whereas standard power cable has neither. Using standard cable on a VFD circuit risks EMI interference and early insulation failure.
Do I need shielded cable for a variable frequency drive?
In almost all cases, yes. Shielded VFD cable is the standard recommendation, especially for longer runs or installations near sensitive electronics, since it contains the EMI that unshielded drive cabling would otherwise radiate.
How do I size a VFD cable for my drive system?
Size the conductor to the motor's full load current with margin for voltage drop, and confirm the cable's voltage rating meets or exceeds the drive's output. Manufacturer AWG and ampacity charts, cross-checked against your run length, are the fastest way to land on the right VFD cable sizing.
What happens if I use the wrong cable with a VFD?
The wrong cable, whether undersized, unshielded or rated for the wrong voltage, can overheat, radiate EMI into nearby equipment, and suffer insulation breakdown far sooner than a correctly specified cable, leading to unplanned downtime and repair costs.
Before you order, check the cable's voltage rating, conductor size, shielding and materials against your drive system and operating conditions. Then plan for the flexibility, grounding and routing the installation needs. Getting those details right helps protect the system and reduce costly downtime.
Explore the full range of TKD Kabel through L-com. We'll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com.