L-com

DAC vs AOC vs Fiber: Choosing Short-Reach Data Center Links

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Choosing the right cable for a data center link is not simply a matter of selecting the highest available speed. For short server-to-switch, switch-to-switch, and rack-to-rack connections, engineers commonly evaluate three options: Direct Attach Copper (DAC), Active Optical Cable (AOC), and fiber with separate optical transceivers. All three can support high-speed networking, but they have different characteristics. 

DAC generally makes sense when the connection is short and cost, simplicity, and low power are priorities. AOC uses fiber with integrated optical components and can provide a thinner, lighter alternative as the distance and cable-management requirements increase. Separate transceivers with fiber provide the greatest flexibility when links need to extend farther or connect through structured cabling. 

The right decision therefore depends on more than distance. Reach, cost, power consumption, cable weight, density, latency, flexibility, serviceability, and equipment compatibility should all be considered. For example, Cisco describes passive DAC as a short-reach option, while AOCs extend the practical range and reduce cable bulk in higher-density environments. 

 

Key Takeaways 

  • DAC, AOC, and fiber can all support high-speed data center connectivity, but they serve different deployment needs. 
  • DAC is generally the most attractive option for very short links when low cost, low power, and simple installation are priorities. 
  • AOC uses fiber with integrated active components and can provide greater reach with a lighter and smaller cable than many copper DAC solutions. 
  • Fiber with separate transceivers provides the greatest flexibility for longer links, structured cabling, and future network changes. 
  • Distance is a useful first filter, but it should not be the only selection criterion. Cost, power, cable weight, density, latency, compatibility, and serviceability also matter. 
  • Passive DAC is commonly used for very short connections, while active DAC can extend reach on supported platforms. 
  • AOC reach varies considerably by product and interface. Some Intel-listed AOCs support up to 100 meters, while individual product families may specify shorter ranges. 
  • Copper DAC can become physically bulky in high-density racks, making AOC or fiber attractive when cable weight, airflow, and routing become concerns. 
  • Do not treat generic distance ranges as hard standards. Always verify the exact manufacturer's specification for the selected speed, interface, cable, and equipment. 
  • For 1–5 meter links, DAC is often worth evaluating first. For longer fixed optical connections, AOC can be considered; for flexible or longer infrastructure, fiber with pluggable optics is often more appropriate. 
  • The best media choice is the one that meets the required reach and performance while fitting the rack's physical and operational constraints. 

 

What Are DAC, AOC, and Fiber? 

Before comparing them, it helps to understand what each option actually includes. 

 

Direct Attach Copper (DAC) 

A DAC is a fixed-length cable assembly with connector/transceiver components integrated at both ends. Passive DACs typically use twinax copper, while active DACs add electronics for signal conditioning. 

DAC is commonly used for: 

  • Server-to-ToR switch connections 
  • Short switch-to-switch links 
  • In-rack connections 
  • Adjacent-rack connections 
  • High-density short-reach applications 

Cisco documentation identifies passive DAC as a short-reach copper solution and active DAC as an option for additional reach on supported platforms. 

 

Active Optical Cable (AOC) 

An active optical cable combines optical fiber with active electronics integrated into the connectors. Instead of using separate optical transceivers and a fiber patch cable, an AOC provides an integrated fixed-length assembly. Intel's Ethernet cable guide lists AOC configurations supporting distances up to 100 meters for several SFP/QSFP form factors, although actual reach depends on the specific product and standard. 

AOCs are useful when you want: 

  • Longer reach than many DAC deployments 
  • Lower cable weight 
  • Smaller cable diameter 
  • High-density rack connectivity 
  • A fixed-length optical connection without separate transceivers 

 

Fiber With Separate Transceivers 

The third option uses pluggable optical transceivers connected to separate fiber cabling. 

A simplified link looks like: 

Switch 

  │ 

Optical Transceiver 

  │ 

Fiber Cable 

  │ 

Optical Transceiver 

  │ 

Server / Switch 

This approach separates the optical electronics from the cable. 

That makes it particularly useful when you need: 

  • Longer reach 
  • Structured fiber infrastructure 
  • Replaceable transceivers 
  • Different fiber types 
  • Patch-panel connectivity 
  • Greater deployment flexibility 
  • Future network upgrades 

The tradeoff is that a transceiver-plus-fiber solution typically involves more components than a fixed DAC or AOC assembly. 

 

1. DAC: The Short-Link Cost and Power Option 

DAC is often the first option to consider when two compatible ports are close together. 

For example: 

Server NIC 

    │ 

    │  3 m DAC 

    │ 

    ▼ 

┌──────────────┐ 

│ ToR Switch   │ 

└──────────────┘ 

A passive DAC can provide a direct electrical connection without separate optical transceivers. 

Cisco's 25G documentation, for example, lists passive copper DACs in fixed lengths from 1 to 5 meters for supported 25G applications. 

 

Advantages of DAC 

  • Low initial cost for short links 
  • Low power consumption 
  • Simple installation 
  • Low latency 
  • No separate fiber patch cable 
  • Useful for ToR server connections 
  • Available in multiple SFP and QSFP configurations 

 

Limitations of DAC 

The biggest limitation is reach. Copper DAC also tends to be thicker and heavier than fiber-based alternatives. As cable count and length increase, cable weight and bulk can become important considerations for rack management and airflow. Cisco has specifically noted that copper cable bulk and weight can become significant as density increases. 

2. AOC: When You Need More Reach Without Separate Optics 

AOC combines the cable and optical components into one fixed assembly. 

Server 

  │ 

  │ 

[AOC] 

  │ 

  │ 

ToR / Aggregation Switch 

The optical transmission medium makes AOC substantially lighter and thinner than many copper DAC designs. That can be valuable in high-density environments. Cisco documentation notes that AOCs can reduce space requirements compared with copper and can help with airflow and cable management. Intel's guide lists AOC configurations up to 100 meters for several high-speed Ethernet interfaces. 

 

Advantages of AOC 

  • Longer reach than many DAC configurations 
  • Lower cable weight 
  • Smaller cable diameter 
  • Good for dense racks 
  • Optical transmission 
  • Integrated connectors 
  • No separate transceiver installation 

 

Limitations of AOC 

An AOC is still a fixed-length assembly. If one component fails, the complete assembly normally needs to be replaced rather than replacing only a transceiver or patch cable. AOC also does not provide the same structured-cabling flexibility as separate transceivers and fiber. 

3. Fiber + Transceivers: Maximum Flexibility 

When a network requires flexibility, separate transceivers and fiber become increasingly attractive. 

A typical design is: 

Switch 

  │ 

[Transceiver] 

  │ 

  │ Fiber 

  │ 

[Patch Panel] 

  │ 

  │ Fiber 

  │ 

[Transceiver] 

  │ 

Server / Switch 

This approach allows the optical transceiver and fiber cable to be selected independently. 

You can select different: 

  • Fiber types 
  • Connector configurations 
  • Cable lengths 
  • Optical transceivers 
  • Wavelengths 
  • Reach classes 
  • Patch-panel systems 

This makes fiber particularly useful for structured cabling and links that may change over time. For example, Cisco's 25G documentation identifies 25G SR optical modules supporting 70 meters over OM3 and 100 meters over OM4, while other optical modules support substantially longer distances. 

 

DAC vs AOC: What Is the Difference? 

The most common comparison is DAC vs AOC. The main difference is the transmission medium. 

DAC uses copper. AOC uses optical fiber. That difference affects physical characteristics. 

DAC 

  • Copper conductors 
  • Generally heavier 
  • Generally thicker 
  • Very low power for passive versions 
  • Excellent for short links 
  • Often lowest cost for short connections 

AOC 

  • Fiber inside the cable 
  • Lighter and thinner 
  • Optical transmission 
  • Generally supports greater reach than passive DAC 
  • Useful in high-density environments 
  • Fixed-length assembly 

Cisco's published 25G examples show passive DAC at 1–5 meters and AOC at 1–10 meters, while other AOC products support substantially longer distances. This illustrates why the actual product specification matters more than a generic DAC or AOC range. 

 

DAC vs Fiber: When Does Fiber Make More Sense? 

DAC is attractive when two devices are physically close. Fiber becomes increasingly useful when the link: 

  • Crosses racks or rows 
  • Requires patch panels 
  • Needs more reach 
  • Requires low cable weight 
  • Must support structured cabling 
  • May need future changes 
  • Requires different optical reach options 

For example, a 2-meter server-to-ToR link may be an excellent candidate for DAC. A link running from one network cabinet to another across a data hall is more likely to benefit from fiber. The exact decision should always be based on the required interface and supported optical or copper specification. 

 

Choosing by Distance 

Around 1–5 Meters: Start With DAC 

For very short server-to-switch connections, passive DAC is often a practical option when supported by the equipment. Cisco's 25G documentation specifically identifies 1–5 meter passive DAC as a low-cost solution for ToR applications. 

Consider: 

  • Passive DAC 
  • Active DAC if required by the specific reach 
  • Cable gauge 
  • Port compatibility 
  • Bend radius 
  • Rack density 

 

Around 5–15 Meters: Compare DAC and AOC 

At this distance, the choice becomes more application-specific. 

Ask: 

  • Is cable weight becoming an issue? 
  • Is the rack highly populated? 
  • Is airflow important? 
  • Is the additional cost of AOC justified? 
  • Does the selected DAC support the required distance? 

Active DAC can support longer distances than passive DAC in some product families, while AOC may provide a lighter physical solution. Cisco's documentation includes examples of active DAC reaching up to 15 meters and AOC extending farther, although exact limits vary by product. 

 

Around 15–30 Meters: AOC or Fiber 

At this range, AOC becomes increasingly attractive when you want a fixed-length optical connection without separate transceivers. Fiber with pluggable transceivers becomes more attractive when structured cabling or future flexibility is important. 

 

Beyond 30 Meters: Evaluate Fiber First 

Once the link moves beyond typical short-reach DAC territory, fiber deserves serious consideration. Depending on the transceiver and fiber type, optical links can support tens, hundreds, or even thousands of meters. The correct optical solution depends on: 

  • Data rate 
  • MMF vs SMF 
  • Transceiver type 
  • Connector 
  • Required reach 
  • Fiber infrastructure 
  • Budget 

Cost vs. Power vs. Weight 

There is no single metric that determines the right cable. Instead, think about the tradeoff. 

DAC 

Strength: Cost and power 

Tradeoff: Weight, bulk, and reach 

AOC 

Strength: Weight, density, and fixed optical connectivity 

Tradeoff: Fixed assembly and higher cost than many short DACs 

Fiber + Transceivers 

Strength: Reach and flexibility 

Tradeoff: More components and potentially higher deployment complexity 

This distinction becomes increasingly important as data center density increases. Cisco notes that copper cable weight and bulk can become significant in dense deployments, while AOC or pluggable optics can reduce physical cable burden. 

 

Latency Considerations 

Latency can matter in applications such as: 

  • High-performance computing 
  • Financial systems 
  • Storage 
  • Distributed databases 
  • AI/accelerated computing 
  • Real-time data processing 

DAC can provide very low latency over short distances because the link is a direct copper connection. AOC and fiber also provide very low latency, and the difference in a real deployment may be much smaller than the impact of network equipment, switching, processing, and topology. 

Therefore, do not choose DAC solely because “copper is faster.” Instead, evaluate the complete link latency and application requirements. For short links, DAC can be an excellent low-latency option. For longer links, fiber can provide the necessary reach without creating an unacceptable latency penalty. 

 

Cable Management and Rack Density 

Cable management can change the decision even when multiple media types meet the electrical requirements. Imagine a rack with dozens or hundreds of connections. A collection of thick copper DAC cables can: 

  • Increase bundle size 
  • Add weight to ports 
  • Restrict airflow 
  • Make access more difficult 
  • Complicate service work 

AOCs and fiber assemblies are generally smaller and lighter. Cisco has highlighted these physical considerations when comparing copper with AOC and pluggable optical solutions in dense data center environments. However, fiber also requires proper bend-radius management and connector handling. The goal is not simply to choose the smallest cable. It is to choose a media type that supports performance, reliability, serviceability, and airflow. 

 

Common Mistakes When Choosing DAC, AOC, or Fiber 

1. Choosing Based Only on Price 

The cheapest cable may not provide the best total deployment value if it creates cable-management or reach problems. 

2. Ignoring Port Compatibility 

Always verify the actual switch, NIC, server, and transceiver requirements. 

3. Assuming Every DAC Reaches the Same Distance 

Passive and active DACs have different reach capabilities, and product families vary. 

4. Treating AOC as Interchangeable With Any Fiber Cable 

AOC is an integrated fixed-length assembly. It is not the same as a pluggable transceiver connected to separate fiber. 

5. Forgetting Cable Weight 

Large numbers of copper cables can create significant rack-management challenges. 

6. Using Fiber When a Simple DAC Would Work 

For very short links, separate transceivers and fiber may add unnecessary components and cost. 

7. Using DAC Beyond Its Specified Reach 

Always follow the manufacturer's maximum supported distance. 

 

How to Select the Right Data Center Link 

Before ordering, work through this checklist: 

  1. Identify the ports. Determine whether the equipment uses SFP+, SFP28, QSFP+, QSFP28, QSFP-DD, or another interface. 
  1. Confirm the speed. Match the cable or optics to the required 10G, 25G, 40G, 100G, 200G, 400G, or other data rate. 
  1. Measure the actual path. Include rack routing, vertical managers, and cable-management paths. 
  1. Determine the required reach. 
  1. Evaluate DAC first for very short links. 
  1. Compare AOC when lower cable weight or additional fixed-link reach is needed. 
  1. Consider fiber and pluggable optics when flexibility or longer reach is important. 
  1. Check compatibility and coding requirements. 
  1. Review cable diameter and bend characteristics. 
  1. Consider rack density and airflow. 
  1. Compare total deployment cost rather than cable price alone. 
  1. Test representative connections before large-scale deployment. 

 

Benefits of Choosing the Right Short-Reach Media 

Lower Deployment Cost 

Using DAC where appropriate can reduce the number of separate components required for short connections. 

 

Lower Power Consumption 

Passive DAC can have very low power requirements compared with solutions using active electronics. 

 

Better Rack Density 

AOC and fiber can reduce cable bulk and weight in high-density deployments. 

 

Greater Reach 

AOC and fiber can support longer links than many passive DAC implementations. 

 

Improved Flexibility 

Separate fiber and transceiver systems allow components to be changed independently. 

 

Easier Standardization 

A clearly defined media-selection strategy can simplify network design, procurement, installation, and maintenance. 

 

Choosing the Right Short-Reach Link with L-com 
DAC, AOC, and fiber with pluggable optics each have a place in the data center. The right choice depends on required reach, port compatibility, cable weight, rack density, and total deployment cost. L-com offers DAC cables and active optical cables for short in-rack and row-level links, along with fiber optic cable assemblies and transceivers for longer or more flexible connections. For the complete build, explore L-com’s data center solutions. 

 

Frequently Asked Questions (FAQs) 

 

What is the difference between DAC and AOC? 

DAC uses copper, generally twinax, while AOC uses optical fiber with active electronics integrated into the cable ends. DAC is commonly favored for shorter links, while AOC can provide greater reach and lower cable weight. 

Is DAC cheaper than AOC? 

For many short-reach applications, DAC is generally less expensive than AOC. However, pricing varies by speed, connector type, length, coding, and manufacturer. 

Is AOC faster than DAC? 

Not inherently. Both DAC and AOC can support high data rates. The appropriate choice depends on the specific interface, standard, distance, and equipment. 

When should you use DAC instead of fiber? 

DAC is attractive when two devices are physically close, such as a server-to-ToR link of around 1 to 5 meters. Fiber becomes more useful when the link crosses racks or rows, requires patch panels, needs more reach, or must support structured cabling and future changes. 

How far can DAC, AOC, and fiber reach? 

Passive DAC is commonly used for very short links of around 1 to 5 meters, and active DAC can extend reach on supported platforms. AOC reach varies by product, with some listed configurations supporting up to 100 meters. Fiber with pluggable transceivers can support tens, hundreds, or even thousands of meters depending on the transceiver and fiber type. Always verify the manufacturer's specification for the selected product. 

Why choose AOC or fiber over DAC in dense racks? 

Copper DAC tends to be thicker and heavier than fiber-based alternatives, so large numbers of DAC cables can increase bundle size, add weight to ports, and restrict airflow. AOC and fiber assemblies are generally smaller and lighter, which can make cable management easier in high-density racks.

Resources

Search Entries