By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics
Twinax cable is often mentioned alongside DAC cable specifications, but the relationship between the two can be confusing. Is twinax the same thing as DAC? What makes twinax different from ordinary Ethernet copper? And why is it commonly used for short, high-speed connections inside data centers?
The answer starts with the physical construction.
Twinax, short for twinaxial cable, is a balanced copper cable designed around two inner conductors that carry differential signals. In data center applications, twinax is commonly used inside direct attach copper assemblies, where fixed transceiver-style connectors are attached to the cable ends.
This combination provides a practical way to connect servers, storage systems, switches, and other network equipment over short distances. Intel describes DAC as Twinax copper cable with SFP or QSFP transceiver components at the ends, with passive and active versions available for different reach requirements. For engineers, understanding twinax is useful because cable construction, gauge, length, connector form factor, and equipment compatibility all affect whether a DAC link is appropriate.
Key Takeaways
- Twinax is a copper cable technology commonly used inside DAC assemblies for short, high-speed network connections.
- DAC and twinax are related but not identical terms: twinax describes the copper media, while DAC generally refers to the complete direct-attach cable assembly.
- Passive Twinax DAC is designed for short-reach connections, while active Twinax can provide additional supported reach through signal-conditioning electronics.
- Cable gauge affects physical characteristics such as diameter, flexibility, weight, and routing, but AWG alone does not determine maximum transmission distance.
- Higher data rates and longer cable runs require careful signal-integrity consideration, making manufacturer-specified reach limits important.
- Twinax DAC can provide low-latency, low-power connectivity for suitable short server-to-switch and switch-to-switch links.
- HPC and other latency-sensitive environments can benefit from short, direct interconnects, provided the selected cable meets the application's speed, reach, and compatibility requirements.
- DAC is generally better suited to short connections than long-distance infrastructure. AOC or fiber can be considered when greater reach is required.
- Compatibility should be checked before deployment, including port type, network speed, cable coding, supported distance, and equipment requirements.
- The shortest practical cable is usually preferable because it reduces excess slack and simplifies rack-level cable management.
- Cable gauge should be selected alongside density and routing requirements, rather than used as a standalone indicator of performance.
- For data center connectivity planning, evaluate twinax, DAC, AOC, and fiber based on distance, speed, latency, power, density, compatibility, and deployment requirements.
What Is Twinax Cable?
Twinax cable is a type of shielded copper cable that uses two conductors to carry differential high-speed signals. Unlike conventional coaxial cable, which typically has one central conductor surrounded by a shield, twinax uses a pair of signal conductors. The conductors are surrounded by insulation and shielding designed to control electromagnetic interference and maintain signal integrity.
A simplified construction looks like this:
Outer Jacket → Shield → Insulation → Twin Signal Conductors
The exact construction varies by cable design, speed, manufacturer, and application. Twinax is particularly useful for high-speed data transmission because differential signaling helps reject common-mode noise. Shielding also helps control electromagnetic interference in environments where many cables and electronic devices operate close together.
Twinax vs. Ordinary Ethernet Copper
Twinax should not be confused with standard twisted-pair Ethernet cabling such as Cat6A or Cat8. Twisted-pair Ethernet cables use pairs of individually twisted conductors and are designed for connection through interfaces such as RJ45. Twinax DAC assemblies, by contrast, normally terminate in high-speed transceiver-style interfaces such as SFP+, SFP28, QSFP+, or QSFP28. The physical interfaces and supported transmission standards are therefore different.
How Twinax Relates to DAC Cables
The simplest way to understand the relationship is: Twinax = the copper cable medium
DAC = the complete direct-attach cable assembly. A DAC assembly combines the twinax copper cable with connector/transceiver assemblies at the ends. Those ends are designed to plug directly into compatible switch, server, storage, or network-device ports.
For example:
Server NIC → SFP+ DAC → Top-of-Rack Switch
or:
Switch → QSFP DAC → Switch
The connector form factor determines how the cable interfaces with the equipment.
Common DAC configurations include:
- SFP+ for 10GbE
- SFP28 for 25GbE
- QSFP+ for 40GbE
- QSFP28 for 100GbE
- Breakout configurations such as QSFP-to-multiple SFP connections
The supported reach depends on the cable type, speed, construction, and equipment. Intel's published guidance, for example, lists different maximum distances for passive and active DAC configurations across several form factors.
Why Twinax Is Used in Data Centers
Twinax is particularly useful when a network connection needs to be:
- High speed
- Short distance
- Low power
- Low latency
- Physically compact
- Cost-conscious
Cisco documentation describes SFP+ direct-attach Twinax copper as a solution for in-rack and adjacent-rack connections, combining low power consumption, low cost, and low latency.
Passive vs. Active Twinax
Twinax DAC assemblies are commonly available in passive and active configurations.
Passive Twinax
A passive DAC does not use active signal-conditioning electronics within the cable assembly. It is generally intended for shorter connections where the host equipment can drive the link successfully without additional signal conditioning.
Advantages include:
- Lower power consumption
- Simple construction
- Short-reach suitability
- Lower deployment cost
- Low latency
For example, Cisco lists passive SFP+ Twinax cables in several short lengths, including 1, 1.5, 2, 2.5, 3, and 5 meters for supported platforms.
Active Twinax
Active Twinax incorporates electronics into the connector assemblies to improve signal performance over a longer supported distance. This can allow a Twinax-based DAC to reach farther than a comparable passive design. However, active does not mean unlimited reach. The maximum distance remains dependent on the specific cable, interface, speed, and equipment. For example, Cisco documentation identifies active SFP+ Twinax options at 7 and 10 meters on certain platforms.
Twinax Cable Gauge: Why AWG Matters
Cable gauge is another factor engineers encounter when comparing twinax assemblies. AWG, or American Wire Gauge, describes conductor size. A lower AWG number generally indicates a larger conductor.
For data center DAC assemblies, gauge can influence:
- Cable diameter
- Flexibility
- Weight
- Current-carrying characteristics
- Thermal behavior
- Routing difficulty
- Bend characteristics
- Signal performance
However, AWG does not provide a universal reach rating.
A common mistake is to assume that a specific AWG automatically determines how many meters a cable can support. Actual reach depends on the complete electrical design, data rate, cable construction, connectors, shielding, and host equipment.
Twinax Cable Length and Signal Performance
As cable length increases, maintaining signal integrity becomes more challenging. Higher data rates generally place greater demands on the cable and connector system. This is one reason DAC deployments are concentrated around short server-to-switch and switch-to-switch connections.
A practical approach is to:
- Measure the actual cable path.
- Determine the required interface speed.
- Check the DAC's supported maximum length.
- Confirm passive or active construction.
- Verify switch and NIC compatibility.
- Select the shortest practical cable.
Avoid choosing a cable that is significantly longer than necessary simply to provide extra slack. Excess cable can increase congestion inside the rack and make service work more difficult.
Why Twinax Can Deliver Low Latency
One reason twinax-based DAC is attractive for certain data center applications is its short electrical path and direct connection architecture. There are no separate optical modules and fiber spans in a passive copper DAC link. The result can be a very low-latency connection for short distances.
Cisco has published examples showing approximately 0.1 microsecond of link latency for supported passive SFP+ Twinax configurations on specific platforms. Actual latency varies by equipment, cable, interface, and architecture, so a vendor's published specification should always take precedence over generic assumptions. Twinax for HPC and Low-Latency Workloads High-performance computing (HPC), financial systems, storage infrastructure, and other latency-sensitive environments can place strong emphasis on fast interconnects.
In these applications, the goal is not simply maximum cable speed. Engineers may also consider:
- Link latency
- Port density
- Cable length
- Power consumption
- Thermal load
- Network topology
- Equipment compatibility
- Total cost
Twinax DAC can be appropriate for short links when these requirements align with its supported distance and interface specifications. For broader HPC connectivity planning, the internal “High-Performance Computing (HPC) Interconnects and Cabling” article can provide additional context.
When Should You Choose Twinax DAC?
Twinax DAC is worth considering when:
1. The connection is short
DAC is designed around short-reach connectivity. If the cable must travel across a large facility or between distant network rooms, fiber may be more appropriate.
2. You need a direct connection
DAC connects directly into compatible SFP or QSFP ports without requiring separate optical transceivers and patch cables.
3. Low power is important
Passive copper DAC assemblies can have low power requirements compared with solutions that use separate active optical components.
4. Rack density is high
Selecting an appropriate cable gauge can help with routing and cable management, although very high-density deployments still require careful consideration of cable diameter and airflow.
5. You want a practical short-link solution
For supported applications, DAC can provide a straightforward connection between servers and switches without unnecessary components.
Benefits of Twinax-Based DAC Cabling
Low-Latency Connectivity
Short copper links can provide very low latency for appropriate data center applications.
Low Power Requirements
Passive DAC designs can avoid some of the power requirements associated with separate optical components.
Simple Deployment
Integrated connector assemblies can reduce the number of components required for short connections.
High-Speed Support
Twinax-based assemblies are available for several high-speed interface families, depending on the specific standard and product.
Efficient Rack Connectivity
DAC is particularly useful for server-to-switch and switch-to-switch connections within and around equipment racks.
Practical Cost Structure
For supported short-reach applications, DAC can be a cost-effective alternative to separate transceiver-and-fiber configurations.
Specifying Twinax DAC Cables for the Data Center
Twinax-based DAC assemblies offer a practical way to connect servers and switches over short distances when speed, reach, latency, and compatibility requirements align. When the link is longer, AOC or fiber may be more appropriate. L-com’s DAC cables cover SFP and QSFP form factors for in-rack server and switch links, and L-com’s data center solutions provide connectivity options for the wider build.
Frequently Asked Questions (FAQs)
What is a twinax cable?
Twinax is a shielded copper cable that uses two signal conductors for differential high-speed data transmission. It is commonly used as the copper medium inside DAC assemblies.
Is twinax the same as DAC?
No. Twinax describes the cable medium, while DAC generally refers to a complete direct-attach cable assembly with integrated connector/transceiver ends.
What is a twinax DAC cable used for?
Twinax DAC cables are commonly used for short server-to-switch, switch-to-switch, and storage-to-switch connections in data centers.
What is the difference between passive and active twinax DAC?
A passive DAC has no active signal-conditioning electronics and is intended for shorter connections, with lower power consumption and lower cost. Active twinax incorporates electronics into the connector assemblies to improve signal performance over a longer supported distance. Active does not mean unlimited reach, so the maximum distance still depends on the specific cable, interface, speed, and equipment.
Does AWG determine how far a twinax cable can reach?
No. AWG describes conductor size and influences cable diameter, flexibility, weight, and routing, but it is not a universal reach rating. Actual reach depends on the complete electrical design, data rate, cable construction, connectors, shielding, and host equipment.
When should you choose twinax DAC over AOC or fiber?
Twinax DAC is worth considering when the connection is short, direct, and low power, and when rack density is high. If the cable must travel across a large facility or between distant network rooms, AOC or fiber may be more appropriate.