L-com

Blog

GigE Vision – A Clear Standard
As big data has gotten bigger and bigger, so have vision applications. GigE Vision is a global interface standard designed to support the transmission of high-speed video and related control data over Ethernet networks that include GigE, 10 GigE and 802.11 wireless networks.... Read more
Embedded Antennas and the IoT
In the not so distant future, the world will be fully automated with machines being able to communicate with little or no interaction from humans, thanks to the arrival of the Internet of Things (IoT) and ....... Read more
Video Blog: Ruggedized Connectivity Solutions
In harsh industrial and military settings, standard commercial connectivity components will fail causing expensive downtime and even danger to lives in some ....... Read more
Futureproofing with Cat6a Cable Assemblies
There is no telling what technological breakthroughs await us in the future. But one thing no one wants, is to have to re-cable an entire network because the existing cabling can’t meet the speed and bandwidth needed to support future technology....... Read more
What is the 12G-SDI Serial Digital Interface?
Serial Digital Interface (SDI) is a digital video interface that provides a range of advantages for transmitting video and audio. This long-lived standard has been ....... Read more
What Are USB Active Optical Cables (AOC)?
USB has long been proven to be a dependable, flexible and simple-to-use interface that is a staple for a multitude of applications. Along the way, USB has adapted to offer a variety of formats to fit today’s technology needs. From power delivery to SuperSpeed USB 3.1 Gen 1 and Gen 2, USB has got you covered. Now the interface is taking things to another level with the introduction of USB 3.0 active optical cables (AOC).... Read more
M12 Connector Coding Demystified
When you need to ensure that you have a reliable connection, even in the harshest conditions, you need an M12 connector. These rugged ....... Read more
Antenna Downtilt: A Practical Overview
When managing cellular networks with multiple base stations, one of the toughest challenges for operators is mitigating inter-cell interference. As 5G implementation ramps up....... Read more
OM5 Fiber – Inside and Out
Multimode fiber cable has long been a versatile connectivity solution with high capability and reliability for local area networks and voice, video, and data applications...... Read more
DisplayPort 2.0 - Just the Facts
HDMI might be the most popular connection standard for TVs and monitors, but DisplayPort comes in a close second place. This high-quality alternative is similar to HDMI in many ways including smaller connectors... Read more

Resources

Search Entries