For many telecommunications and networking infrastructure, cables are generally chosen for their throughput, frequency, longevity, ruggedness, ease-of-installation, power handling, and for other electrical or mechanical parameters. These are not the only considerations, however, when telecommunications and networking cables are used in medical, food, or other applications where harmful bacteria and other pathogens may take the cables for a ride and dangerously expose patients or otherwise contaminate the surrounding environments and objects. There are strict codes in virtually every country for maintaining a clean environment that is optimally free of bacteria and other dangerous microbes where rigorous testing is used to ensure a high standard of cleanliness.... Read more
Blog
Wednesday, May 5, 2021
Applications for Antibacterial/Antimicrobial Cables
Wednesday, April 21, 2021
Small Cells Defined
A small cell is just a cellular radio access point with lower RF power output, range, footprint, and size than the typical homogenous macrocell. Small cell is also a blanket term for a wide range of cell types that are smaller than traditional macrocells.... Read more
Wednesday, April 7, 2021
Benefits of POE++ 802.3bt
Power over Ethernet (POE) has been a huge boon in factory automation, building automation, security, and a host of new applications made more cost effective by delivering ethernet connectivity as well as power to edge devices. POE (IEEE 802.3af) was first standardized in 2003 and has grown explosively in the past many years. This growth has also come with an evolution to the original standard, and the creation of a few varieties of POE, namely POE, POE+ (IEEE 802.3at-2009), and POE++ (IEEE 802.3bt-2013). These standards have also been reclassified as Type 1, Type 2, Type 3, and Type 4, to better capture the specifications and capabilities of each type of POE.... Read more
Wednesday, March 24, 2021
All About Coarse Wavelength Division Multiplexing (CWDM) For Fiber Networking
Passive coarse wavelength division multiplexing (CWDM) is a method of multiplexing (mux) and de-multiplexing (demux) optical signals over fiber optic transmission cables. It is considered a cost effective method for scaling connections over existing fiber infrastructure for point-to-point (P2P) or point-to-multipoint (P2M) connections for add/drop or fiber ring applications. Both passive CWDM cassettes and barrel filters are useful in a wide range of applications that benefit from the aggregation and separation of fiber channels. These applications include telecommunications, R&D< test lab, research and mil/aero installations, among other applications that require extensions of existing fiber infrastructure.... Read more
Wednesday, March 10, 2021
Single Pair Ethernet
Internet connected devices with advanced sensor and control features are becoming increasingly common in industrial applications. The rise of the Industrial Internet-of-Things (IIoT) is being driven by the availability of more capable wired and wireless connectivity technologies and the need for manufacturers to enhance efficiency, reliability, and productivity through automation. The results of these trends are increased focus of edge-computing and more advanced sensor/control technologies integrated into industrial processes. Realizing a dramatic increase in density of connectivity devices naturally results in the increase in interconnect. Though industrial wireless networks can offset some of interconnect challenges, industrial wireless networks generally need some type of physical connection and wireless is not serviceable in all industrial environments.... Read more
Wednesday, February 24, 2021
5G Infrastructure Focus – Industrial Networks
5G services are beginning to rollout at a dizzying pace, which is likely many times that of the original 4G rollout. Most major carriers in the US, and several other countries, have deployed low-band (sub-1 GHz), mid-band (sub-6 GHz), and high-band (millimeter-wave frequencies beyond 6 GHz) services. Along with these services is a wide range of consumer 5G handsets that can make use of the new mid-band frequencies, as well as select models capable of using low-band and high-band frequencies. Though the user experience for consumer 5G is not significantly different at this stage, the wheels are in motion for 5G to fully develop beyond the initial rushed consumer use case.... Read more
Wednesday, February 10, 2021
PROFINET Primer
PROFINET is one of the world’s leading Industrial Ethernet-based communication solutions widely used in industrial automation applications. The modifications to the Ethernet standard used by PROFINET enable deterministic communication and ensure real-time data transmission even in harsh operating conditions.... Read more
Thursday, September 5, 2019
An Inside (and Outside) Look at Fiber Active Optical Cables
An Inside (and Outside) Look at Fiber Active Optical Cables... Read more
Thursday, March 1, 2018
The Full Spectrum of Wireless Communications Protocols and Standards
The Full Spectrum of Wireless Communications Protocols and Standards... Read more
Thursday, February 22, 2018
The IIoT and Manufacturing
The IIoT and Manufacturing... Read more
Resources
- Application Overviews
- Blog: Engineering Hub
- Case Studies
- Credit Application
- Connector Charts
- Custom Cable Configurators
- Featured Products
-
Frequently Asked Questions
- How do I change my password?
- What is the difference between simplex and duplex fiber optic cable?
- How do I update my personal and company details?
- How do I add or edit my address information?
- How do I view my order history?
- How do I reorder?
- How can I change my communication preferences?
- How do I sign up for your newsletter?
- What does RG316/U mean?
- What is a Distributed Antenna System (DAS)?
- What is plenum rated cable, and why is plenum cable more expensive than PVC cable?
- What is the difference between male and female connectors?
- What is the difference between 75 Ohm and 50 Ohm coaxial cable and when should each one be used?
- What is the difference between VGA, SVGA and UXGA, and does L-com sell cables for each?
- What are some popular Fiber Optic connector types?
- What do the fiber terms 9/125, 50/125 and 62.5/125 refer to?
- Why Use Shielded Cat 6 Cable vs. Unshielded Cat 6 cable?
- Is your website secure?
- How do I return a purchase?
- What are your shipping and processing fees?
- What is the difference between VGA, SVGA and UXGA?
- What are common WiFi Antenna FAQs?
- How do I check my order status?
- What does IP67 mean? I need waterproof cables, connectors, and adapters
- How do I request your product guide?
- What is your Privacy Policy?
- How can I follow L-com on social media?
- What are your Terms and Conditions?
- What is your contact information?
- What is Coaxial Cable?
- What is a USB Cable?
- What is a DB9 Connector?
- Can Too Much Gain Be A Bad Thing?
- What is the Difference between Stranded and Solid Conductors?
- What are the Advantages and Disadvantages of ISM Band Frequencies?
- Industry Application Brochures
- Industrial Solutions
- Product Brochures
- Product Guide Downloads
- Technical Briefs and Articles
- White Papers
- Wireless Calculators