In the world of industrial Ethernet and building automation, there is a bountiful opportunity for very harsh environments and challenging installation situations. In these cases, industrial Ethernet rated cables are often used. These ruggedized Ethernet cables tend to have additional shielding thickness, thick and hard outer jackets, strain relief members built in, and other protections for the delicate copper wiring... Read more
Blog
Wednesday, September 8, 2021
High-flex Ethernet Cables: Applications & Overview
Wednesday, September 22, 2021
What is Low Power Wide Area Network (LPWAN) Technology?
In these times of rapid technological acceleration, people, processes and technologies are integrating with each other via connectable devices and battery-powered sensors that enable remote monitoring and manipulation of M2M and IoT devices. However, industries including consumer, commercial, industrial and infrastructure are all wrestling to achieve the reliable and scalable connectivity required for successful implementation of these devices. This is where LPWAN technology comes into play.... Read more
Tags:
Wednesday, August 25, 2021
The Mighty MPO Connector
A Multi-fiber Push On (MPO) connector is a fiber optic connector that contains multiple fiber-optic lines internally. MPO connectors are used for high-speed telecommunication and data communication networks. The standards governing the design and use of MPO connectors are the IEC 61754-7 and TIA 604-5. Originally, MPO connectors were predominantly used in the Central and Branch offices but have also seen wide adoption in high performance computing (HPC) applications and in enterprise datacenters.... Read more
Wednesday, August 11, 2021
What is RFoG ? Radio Frequency Over Glass Primer
In many cases the losses and potential interference with sending RF signals over long runs of coaxial cable results in inadequate hybrid fiber-coax (HFC) network performance. The reason is that the losses and interference susceptibility for RF coaxial cables used to keep network infrastructure costs reasonable are much greater than fiber or even higher quality coaxial cables.... Read more
Wednesday, July 28, 2021
The Counterfeit Cable Problem
Counterfeit currency, travel papers, and professional certifications are almost as old as the official paperwork or coinage that counterfeiters are attempting to duplicate. Unfortunately for the safety and reliability of Ethernet and other data communication, counterfeit cabling is now a growing trend.... Read more
Wednesday, July 14, 2021
What Is The Difference Between Cat 6, Cat 6a, and Cat 7
Even with many consumer, commercial, industrial, and even automotive electronics moving to wireless technology for networking, many local area networks (LANs) are still wired using physical cabling and applications with reliability concerns still heavily use physical cabling. As there are a wide range of application requirements for Ethernet cabling, there are also a wide range of cabling types at different performance and price points to accommodate these various needs.... Read more
Wednesday, June 30, 2021
What is Wi-Fi 6E?
Wi-Fi 6e is an enhancement of Wi-Fi 6 (802.11ax) and builds on that standard to provide higher performance using extended frequency capability. Like Wi-Fi 6, Wi-Fi 6e uses Orthogonal Frequency-Division Multiple Access (OFDMA) to use available bandwidth more efficiently. Wi-Fi 6e is also capable of multi-user multi-input multi-output (MU-MIMO) for up to eight streams, as is Wi-Fi 6. Both standards allow for very high order modulation to 1024 quadrature amplitude modulation (1024-QAM). There are also battery and energy efficiency aspects built into both standards, such as Target Wake Time (TWT) that allows for devices to sleep until a given target time.... Read more
Wednesday, June 16, 2021
What’s The Difference: Passive Optical Networks PON, GPON, EPON, 10G-PON?
Optical networks, relying on optical fiber and other optical hardware, make up the networks that are the nerves of the internet. Outside of a home or office, the electrical cables typically connect to optical cables, which provide the interconnect among data centers and optical line terminals (OLT) at user locations. There are a variety of optical fiber network technologies, including several passive optical networks (PONs).... Read more
Wednesday, June 2, 2021
HDMI 2.1 Overview
HDMI 2.1 is an update of the HDMI specifications that boosts the video resolution and refresh rate capability of the HDMI standard. HDMI 2.1 specifications are able to support throughput to 48 Gbps, which can provide 8k refresh rates to 60 hertz, 4k refresh rates to 120 hertz, and resolutions to 10k. A new Ultra High Speed HDMI Cable is needed to hit 48 Gbps of bandwidth, and this new cable enables ultra-high bandwidth dependent features, such as uncompressed 8k video with high-dynamic range (HDR) capability.... Read more
Wednesday, May 19, 2021
All about DWDM (Dense Wavelength Division Multiplexing)
Information network technology developers continually strive to enhance the throughput and quality of the network data lines, while also reducing the cost-per-bit (CPB) of the networks. One such technology is, Dense Wavelength Division Multiplexing (DWDM). DWDM is a method of creating several virtual fiber optic lines, which effectively multiplies the capacity of the physical fiber optic line. Wavelength division multiplexing (WDM) uses optical multiplexing that results in increasing bandwidth over existing fiber optic cabling without needing to add additional cabling. Optical multiplexing involves combining several transmitted and received signals of different wavelengths simultaneously. The term “dense” in DWDM implies that the new method of WDM uses more densely packed frequency channels than previous “coarse” WDM (CWDM) technology.... Read more
Resources
- Application Overviews
- Blog: Engineering Hub
- Case Studies
- Credit Application
- Connector Charts
- Custom Cable Configurators
- Featured Products
-
Frequently Asked Questions
- How do I change my password?
- What is the difference between simplex and duplex fiber optic cable?
- How do I update my personal and company details?
- How do I add or edit my address information?
- How do I view my order history?
- How do I reorder?
- How can I change my communication preferences?
- How do I sign up for your newsletter?
- What does RG316/U mean?
- What is a Distributed Antenna System (DAS)?
- What is plenum rated cable, and why is plenum cable more expensive than PVC cable?
- What is the difference between male and female connectors?
- What is the difference between 75 Ohm and 50 Ohm coaxial cable and when should each one be used?
- What is the difference between VGA, SVGA and UXGA, and does L-com sell cables for each?
- What are some popular Fiber Optic connector types?
- What do the fiber terms 9/125, 50/125 and 62.5/125 refer to?
- Why Use Shielded Cat 6 Cable vs. Unshielded Cat 6 cable?
- Is your website secure?
- How do I return a purchase?
- What are your shipping and processing fees?
- What is the difference between VGA, SVGA and UXGA?
- What are common WiFi Antenna FAQs?
- How do I check my order status?
- What does IP67 mean? I need waterproof cables, connectors, and adapters
- How do I request your product guide?
- What is your Privacy Policy?
- How can I follow L-com on social media?
- What are your Terms and Conditions?
- What is your contact information?
- What is Coaxial Cable?
- What is a USB Cable?
- What is a DB9 Connector?
- Can Too Much Gain Be A Bad Thing?
- What is the Difference between Stranded and Solid Conductors?
- What are the Advantages and Disadvantages of ISM Band Frequencies?
- Industry Application Brochures
- Industrial Solutions
- Product Brochures
- Product Guide Downloads
- Technical Briefs and Articles
- White Papers
- Wireless Calculators