By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics
What makes a robot cable different from a standard cable?
A robot cable is designed to twist and bend at the same time, for millions of cycles, without its conductors, shield or jacket fatiguing. A standard installation cable is meant to be pulled into place once and left alone. A drag-chain cable bends back and forth in one plane all day, but it isn't built to twist. On a typical 6-axis arm from FANUC, ABB, KUKA or Yaskawa, axes 1 to 3 move the arm through space and put mostly bending motion on the cables. Axes 4, 5 and 6 form the wrist. Axes 4 and 6 rotate the forearm and the tool flange, so every cable that crosses them gets twisted along its length on every cycle, usually while axis 5 bends it too.
Twist loads a cable very differently from a bend. In a bend, the inside of the cable compresses and the outside stretches. In torsion, every layer winds tighter or looser around the cable center, so the conductors try to change length relative to each other while the shield and jacket take shear. That's why a cable that lasts years in a cable track can fail in weeks on a robot wrist.
Making the cable thicker doesn't help. Construction does: finer stranding, shorter lay lengths, low-friction layers between the core and the shield, and shields and jackets chosen to tolerate twist.
Key Takeaways
- Robot cable is built to twist (torsion) and bend at the same time, which is exactly what a 6-axis arm does to cables at axes 4, 5 and 6. Standard and drag-chain cables are not designed for that combination.
- Torsion is rated in degrees of twist per meter of cable, for example ±180°/m or ±360°/m. The free length you leave between clamps decides how much twist each meter sees.
- Five specs decide service life: torsion rating, flex-cycle rating, fine-stranded conductors (IEC 60228 Class 5 or 6), a shield designed for twist, and a PUR jacket for oil and abrasion.
- Most wrist failures, like intermittent Ethernet on axis 6 or a cracked jacket, trace back to a cable that was never torsion-rated or a clamp that locks the twist into a few centimeters.
- When a wrist cable fails, change the cable type and routing together. A like-for-like swap usually gets you the same failure on the same schedule.
How do torsion, bending, and continuous flex differ?
Each type of motion needs its own cable construction, and a rating for one doesn't carry over to the next. Match the cable to what it does in service, not to where it's mounted.
|
Motion type |
Where you see it |
What the cable must handle |
Typical construction |
Spec to check |
|
Static |
Cabinet wiring, fixed runs to the robot base |
Installation bends only |
IEC 60228 Class 1–2 conductors, PVC jacket |
Installation bend radius |
|
Flexing (occasional) |
Machine guards, doors, adjustable fixtures |
Occasional bending, no fixed cycle count |
Class 5 stranded conductors |
Flexible bend radius |
|
Continuous flex |
Cable track (drag chain) on linear axes and gantries |
Millions of bend cycles in one plane |
Class 5/6 conductors, short lay length, PUR or TPE jacket |
Flex cycles at a stated bend radius, travel length and speed |
|
Torsion |
Robot arm axes 4–6, rotary tables, dress packs |
Twisting combined with bending |
Class 6 conductors, torsion-rated shield, low-friction separators, PUR jacket |
Torsion rating (±°/m) plus flex cycles |
Torsion ratings are written as degrees of twist per meter, such as ±180°/m or ±360°/m. The per-meter part matters more than most people expect. If axis 6 rotates the tool ±270° and only 0.5 m of cable is free between the last two clamps, that cable sees ±540°/m. Give it 1.5 m of free length and the same rotation drops to ±180°/m.
Flex-cycle numbers need the same scrutiny. "Millions of cycles" means little without the test conditions behind it: bend radius, travel length, speed and acceleration. Test methods vary from one manufacturer to the next, so compare datasheets at matching conditions rather than by the headline number.
What's inside a robot cable?
A robot cable has four layers that decide how long it survives: the conductors, the binders and fillers that hold the core together, the shield, and the jacket. Each one is chosen so the layers can slide over each other as the cable twists, instead of grinding.
Conductors
Robot cables use fine-stranded copper to IEC 60228 Class 5 (flexible) or Class 6 (extra flexible). Class 6 uses thinner individual wires, so each strand takes less strain when the cable twists. The conductors are cabled in bundles with short lay lengths, which makes them move together under torsion instead of one conductor taking all the stretch. Tinned copper helps in wet or oily cells.
Binders, fillers and separators
Tape wraps, fleece and soft fillers keep the core round and let the layers slip past each other. Leave them out and conductors slowly wear through their own insulation from the inside. You won't see that damage until the circuit opens.
Shields
The shield is usually the first layer to give up under torsion, and each shield type is a trade-off:
- Braid shields give the best EMI coverage and are standard on high-flex Ethernet. Under heavy twist, individual braid wires can fatigue and snap, so on a wrist the braid has to be designed for torsion.
- Spiral (served) shields wind wires helically in one direction. They handle twists well, but their effectiveness drops at higher frequencies, so they suit power and low-speed signals better than data.
- Foil shields are thin and cheap, and they crack under repeated motion. Avoid foil-only constructions in moving sections unless the cable is rated for that motion.
Jackets
PUR (polyurethane) is the default jacket on robot arms because it resists abrasion, cutting oils and coolants and stays flexible. Weld cells and wash down lines sometimes call for something else.
What is a robot dress pack and how does it route cables?
A robot dress pack is the complete set of cables and hoses, plus the hardware that carries them, running along the arm to the end-of-arm tooling (EOAT). It usually includes a corrugated protective conduit, mounting brackets and swivel clamps at each axis, and often a spring or retraction system that pulls slack back as the arm extends. Dress packs come in two forms. External dress packs run along the outside of the arm and are easy to inspect and service. Internal, or through-arm, dress packs route through a hollow forearm and wrist on robots built for it. That keeps cables away from spatter and fixtures but makes inspection and replacement slower.
Either way, the dress pack's real job is to control where the cables bend and twist. Swivel clamps let the conduit rotate instead of winding up. The retraction system keeps slack from snagging on fixtures or whipping around on fast moves. When those parts are set up properly, the cable inside only sees motion it was rated for. When they aren't, even a torsion-rated cable dies early. A typical dress pack carries tool power, a high-flex Ethernet line for a vision camera or tool changer, M8 or M12 sensor cables, discrete I/O, air lines and, on weld cells, the welding power lead.
How should you manage cables on a robot arm?
Good robotic cable management comes down to two things: giving twist enough length to spread out and keeping clamps from pinning it into one spot. These practices prevent most early failures:
- Spread torsion over length. Leave enough free cable between fixation points that the twist per meter stays inside the cable's rating.
- Avoid fixed-point twisting. Don't clamp a cable rigidly on both sides of a rotating joint with only a few centimeters between the clamps. The twist has nowhere to go, so it focuses on one spot, and that's where the conductor breaks.
- Clamp firmly without crushing. A fixation point should hold the cable without deforming the jacket, because a flattened jacket passes stress straight to the conductors.
- Size service loops for the full range of motion. Run the robot through its extreme poses in teach mode at low speed and watch the cables. A loop that goes tight at full reach is too short, and one that sags into fixtures is too long.
- Keep power away from data. Route motor and weld power on the opposite side of the dress pack from Ethernet and sensor lines where you can.
- Don't tie cables of different stiffness tightly together. A stiff hose and a thin sensor cable zip-tied into one bundle move differently, and the thin cable loses. Use the dress pack's separators instead.
Which Ethernet, sensor and power cables should you use on a robot arm?
Choose each cable for the motion it sees at its position on the arm. A cable that stops at the robot base can be standard or flexible in construction. Anything that crosses axes 4 to 6 needs a torsion rating.
Ethernet
For EtherNet/IP, PROFINET or EtherCAT running to a camera or tool changer, use high-flex Cat5e with stranded conductors and a braid shield, such as L-com's high-flex Ethernet patch cords. Because 100 Mbps industrial protocols only use two pairs, 2-pair cable built to PROFINET Type C, the cable class intended for special applications such as torsion and continuous flex, is also common on robot wrists.
Sensors
Proximity, presence, and vacuum sensors on the tooling typically use M8 or M12 connectors. Compact M8 cable assemblies, including M8 Ethernet versions, save space at the tool flange. Choose overmolded assemblies with a PUR cable and make sure the connector strain relief isn't sitting right at a twist point.
Power and I/O
Tool power, solenoid valves and discrete I/O run on multi-conductor cable. L-com's flexible multi-conductor control cable covers these runs. Check the torsion rating before you route it through the wrist.
One rule we'd push on any maintenance floor: if a cable has already failed at the wrist, don't reorder the same part number until you've confirmed it was ever rated for torsion. Repeat failures on the same joint are often a good cable used in the wrong motion class.
Why do robot cables fail, and how do you fix them?
Robot cable failures usually show up as intermittent faults long before the cable opens completely, and they cluster at the wrist and at clamp points. The table maps the symptoms we see most often to their usual cause and fix.
|
Symptom |
Likely cause |
Fix |
|
Intermittent Ethernet drops or CRC errors on axis 6, worse at certain poses |
Conductor or shield fatigue in a cable not rated for torsion, or twist concentrated near a clamp |
Replace with torsion-rated high-flex Ethernet, lengthen the free cable between clamps, check connector strain relief |
|
Cracked or split jacket at the wrist |
PVC jacket, bend radius too tight, or abrasion against tooling |
Switch to PUR, add a protective sleeve or conduit, reroute away from contact points |
|
Rising noise or EMI-related faults after months of running |
Broken braid wires from torsion fatigue |
Use a shield rated for torsion, separate power from data, verify shield termination at both connectors |
|
Cable corkscrews into a spiral between clamps |
Cable clamped at both ends of a rotating section with no room to twist |
Change to a swivel clamp or add free length so the twist spreads out |
|
Sensor drops out at one robot position only |
Broken conductor inside an intact jacket, usually at a fixation point |
Replace with Class 6 conductor cable, then move or soften the clamp |
|
Connector pulls loose or the overmold cracks |
No strain relief, or service loop too short at full reach |
Lengthen the service loop and add a strain relief clamp behind the connector |
|
Weld cell cables fail faster than the rest of the plant |
Spatter, heat and high current near data lines |
See welding robot cell cabling for weld-specific routing and jacket choices |
A practical debugging tip: pull the switch port counters or PLC diagnostics and line up the error timestamps with the robot program. If errors spike on the same program step every cycle, you've found the pose, and usually the exact cable section, that's failing.
How often should you inspect and replace robot cables?
Inspect the dress pack and cables at every scheduled preventive maintenance (PM) stop, using the robot OEM's PM interval as your baseline. Replace on condition, unless the cable will reach its rated cycle life before the next planned shutdown.
At each inspection, check:
- Jacket wear, cuts, flat spots and discoloration at the wrist and at clamp points
- Corkscrewing or kinks between fixation points
- Connector condition, coupling nuts and strain relief
- Clamp tightness, and whether any clamp has slipped along the cable
- Network error counters and intermittent I/O faults logged since the last PM
It also helps to estimate how fast a cable uses up its rated life. A robot running 1,200 cycles an hour across two 8-hour shifts, 250 days a year, puts about 4.8 million cycles on its wrist cables every year. Compare that with the datasheet rating and you'll know whether a planned replacement belongs in this year's shutdown or next year's.
Keep pre-terminated spares on the shelf for every cable that crosses axes 4 to 6. Those are the cables that stop a line, and they're the ones you don't want to be building at 2 a.m.
Sourcing Robot Cables and Dress Pack Components from L-com
Once you know the motion each cable sees, choosing the right part comes down to matching its torsion rating, flex-cycle rating and jacket to its position on the arm. L-com carries high-flex Ethernet patch cords, M8 cable assemblies and flexible multi-conductor control cable for robot wrists, dress packs and other moving applications.
Frequently Asked Questions (FAQs)
What is a robot cable?
A robot cable is a cable built to survive torsion and bending at the same time over millions of cycles, which is the motion a robot arm's wrist puts on it. It uses fine-stranded IEC 60228 Class 5 or 6 conductors, a shield designed for twist and usually a PUR jacket. Standard and drag-chain cables lack the torsion rating these applications need.
Can I use a drag chain cable on a robot arm?
You can use a drag chain cable on axes 1 to 3 if it only bends there, but not across the wrist. Drag chain cables are rated for bending in one plane, not twisting. On axes 4 to 6, use a cable with a stated torsion rating.
What is the difference between a robot dress pack and a cable track?
A robot dress pack routes cables and hoses along a multi-axis robot arm, using swivel clamps and retraction to manage twist and slack. A cable track (drag chain) guides cables along a linear path, where the motion is bending in one plane. The two need different cable constructions.
What does a torsion rating on a robot cable mean?
A torsion rating is the amount of twist a cable can handle, written in degrees per meter, such as ±180°/m or ±360°/m. The free length between clamps decides how much twist each meter sees. If axis 6 rotates the tool ±270° with 0.5 m of free cable, the cable sees ±540°/m. With 1.5 m of free length, the same rotation drops to ±180°/m.
Why do robot cables fail at the wrist?
Every cable that crosses axes 4 to 6 is twisted along its length on each cycle, usually while axis 5 bends it too. Most failures trace back to a cable that was never torsion-rated or a clamp that locks the twist into a few centimeters. They often show up first as intermittent Ethernet drops or sensor dropouts. Changing the cable type and the routing together prevents a repeat failure.