L-com

Industrial Ethernet Protocols Compared: PROFINET vs EtherNet/IP vs EtherCAT vs Modbus TCP

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics 

 

Industrial Ethernet uses the same physical layers as office networks (IEEE 802.3 copper and fiber) but runs protocols designed for predictable, repeatable control traffic. Four dominate the plant floor: PROFINET, EtherNet/IP, EtherCAT and Modbus TCP. They differ far more in how they move data and who governs them than in the cable they ride on. 

 

Key Takeaways 

  • PROFINET (PI), EtherNet/IP (ODVA), EtherCAT (ETG) and Modbus TCP all run over standard Ethernet cabling, so the protocol decision rarely changes the cable category, only the jacket, shielding and connector you choose for the environment. 
  • EtherCAT is the fastest of the four, with cycle times that can drop below 100 microseconds, because slaves process the frame on the fly instead of receiving it into a buffer first. 
  • PROFINET and EtherNet/IP sit in the middle: both deliver cycle times of roughly 1 to 10 ms on standard hardware, and both are usually chosen because of the PLC brand already on site. 
  • Modbus TCP is the simplest and most open option, but it has no real-time mechanism, so it suits monitoring and slow supervisory data better than motion or tight I/O loops. 
  • M12 D-coded connectors carry 100 Mb/s over four pins, while M12 X-coded connectors carry Gigabit and faster over eight pins. Pick based on the speed your devices need, not on the protocol name. 

 

What Is Industrial Ethernet, and How Is It Different from Office Ethernet? 

Industrial Ethernet is standard Ethernet adapted for control networks: the same frames, the same RJ45 and M12 interfaces, but with protocols, hardware and cabling chosen for determinism and survival on a factory floor. Determinism means a packet arrives within a known, repeatable window, which matters when a drive or valve is waiting on it. 

Office Ethernet is built for throughput and tolerates delays. If a web page loads 200 ms late, nobody notices. In a motion application, a late packet can mean a missed position or a stopped line. Industrial protocols address this with scheduled or prioritized traffic, and industrial hardware addresses the environment with sealed connectors, tougher jackets, shielding against electrical noise and wider temperature ratings. The protocols below are all described as "industrial Ethernet protocols," but they are not interchangeable. Each one is a different answer to the same question: how do you get control data across Ethernet reliably? 

 

PROFINET: The Siemens-Backed Standard 

PROFINET is governed by PROFIBUS & PROFINET International (PI) and is the dominant industrial Ethernet protocol in Europe, with strong adoption in automotive and discrete manufacturing. It is most closely tied to the Siemens ecosystem, though many vendors build conformant devices. 

It comes in two main real-time flavors. PROFINET RT is software-based and works on standard Ethernet hardware, typically with cycle times in the 1 to 10 ms range. PROFINET IRT (isochronous real-time) reserves time slots for critical traffic and can reach cycle times well under 1 ms, but it needs switches with dedicated hardware support. Devices are grouped into conformance classes (A, B and C) that define which features they support. 

PROFINET also has the clearest cable conventions of the four. Jackets are green, and cable types A, B and C describe the mechanical load: fixed installation, occasional flexing and continuous flexing. 

 

EtherNet/IP: CIP Over Standard Ethernet 

EtherNet/IP is managed by ODVA and carries the Common Industrial Protocol (CIP) over standard TCP/IP and UDP/IP. The name is a frequent source of confusion: the "IP" stands for "Industrial Protocol," not Internet Protocol, even though it does run on IP networks. It is the dominant protocol in North America and is closely associated with the Rockwell Automation ecosystem. 

Because EtherNet/IP uses unmodified Ethernet and standard switching, it is easy to integrate with IT infrastructure. Cyclic I/O data travels as UDP multicast or unicast, with typical update intervals of 2 to 10 ms, and CIP Motion and CIP Sync extend it toward coordinated motion. The tradeoff is that determinism depends on network design. Managed switches with IGMP snooping and sensible VLAN or QoS settings are strongly recommended, since unmanaged switches flood multicast traffic to every port. 

EtherNet/IP also supports a Device Level Ring (DLR) topology, which gives single-fault ring redundancy without a managed-switch core. In searches for ethernet/ip you will find plenty of vendor material, but the physical layer is the same standard Ethernet used elsewhere. 

 

EtherCAT: Built for Motion 

EtherCAT is managed by the EtherCAT Technology Group (ETG) and is designed for speed. A single frame from the master passes through every device in turn, and each device reads its outputs and inserts its inputs while the frame is still moving. This "processing on the fly" approach is why cycle times of 100 microseconds or less are practical, and why EtherCAT is common in CNC, robotics, packaging and semiconductor equipment. 

It is strongest in Europe and Asia and is closely associated with Beckhoff. In practice, EtherCAT networks are usually daisy-chained or tree-structured using devices with two ports and no standard switches in the cyclic path. The cable is still standard Ethernet at 100 Mb/s.  

 

Modbus TCP: Open, Simple and Everywhere 

Modbus TCP wraps the classic Modbus request/response model in a TCP packet on port 502. It is maintained by the Modbus Organization, is royalty-free, and is among the easiest protocols to implement. Nearly every drive, meter, sensor gateway and PLC supports it, which makes it a common lowest-common-denominator link between systems from different vendors. 

The simplicity comes with limits. Modbus TCP has no real-time class, no built-in prioritization and no standard device profile, and update times usually fall in the tens to hundreds of milliseconds depending on network load. It performs well for energy metering, building systems, SCADA polling, and HMI data. It is a poor fit for synchronized motion. Any standard managed or unmanaged switch will carry it. 

 

Industrial Ethernet Protocols Side by Side 

The table below summarizes how the four compare governance, real-time behavior and topology. Cycle times are typical figures for common hardware; actual performance depends on device count, payload size, and network design. 

Protocol 

Governing body 

Real-time approach 

Typical cycle time 

Common topologies 

PROFINET 

PI (PROFIBUS & PROFINET International) 

RT (software) and IRT (hardware-scheduled) 

1-10 ms (RT); under 1 ms (IRT) 

Star, line, ring (MRP) 

EtherNet/IP 

ODVA 

CIP over UDP/TCP, prioritized with QoS 

2-10 ms typical; lower on tuned networks 

Star, linear, DLR ring 

EtherCAT 

ETG 

On-the-fly frame processing 

100 microseconds or less; up to 1 ms common 

Line, tree, ring (with redundancy) 

Modbus TCP 

Modbus Organization 

None (request/response) 

Tens to hundreds of ms 

Star, any IP topology 

 

The second view matters more for purchasing. It shows what each protocol asks of your switches and cabling. 

Protocol 

Switch requirements 

Cable and connector conventions 

Dominant regions and vendors 

PROFINET 

Managed switches; IRT needs hardware-supported switches 

Green jacket, Type A/B/C; RJ45 IP20/IP67, M12 D-coded 

Europe; Siemens ecosystem 

EtherNet/IP 

Managed switches with IGMP snooping advised 

Standard Cat5e/Cat6; RJ45 or M12 D-coded 

North America; Rockwell ecosystem 

EtherCAT 

Often none in the cyclic path; devices daisy-chain 

Standard Cat5e at 100 Mb/s; RJ45 or M12 D-coded 

Europe and Asia; Beckhoff and motion vendors 

Modbus TCP 

Any standard switch 

Any Ethernet cabling 

Global; vendor-neutral 

 

 

What Changes in the Physical Layer? 

Very little changes in the physical layer between protocols, and a lot changes between the office and the plant. The cable still carries Ethernet; what differs is how well it resists noise, heat, oil, vibration and repeated movement. 

  • Shielding. Drives, motors and welders produce electrical noise. Shielded cable (foil, braid or both) with properly terminated connectors is the norm for industrial runs. 
  • Jacket material. PVC is common for fixed indoor runs. Polyurethane (PUR) resists oil, abrasion and flexing, which is why it dominates drag-chain and robotic applications. 
  • Conductor type. Solid copper suits fixed runs, while stranded conductors handle repeated bending. 
  • Standards. ANSI/TIA-1005 defines structured cabling for industrial premises, including the MICE environmental classification.  

 

M12 D-Coded vs X-Coded vs RJ45 

The connector you choose depends on speed and ingress protection, not on protocol. A device that needs only 100 Mb/s, which covers most PROFINET, EtherNet/IP and EtherCAT I/O devices, can use M12 D-coded. A device that needs Gigabit needs X-coded. 

Connector 

Pins 

Speed 

Typical use 

M12 D-coded 

4 

100 Mb/s 

I/O blocks, sensors and drives in IP67 environments 

M12 X-coded 

8 

Gigabit and above 

Vision systems, backbone links and Gigabit devices in IP67 environments 

RJ45 (IP20) 

8 

Up to Gigabit and above 

Control cabinets and protected enclosures 

RJ45 (IP67) 

8 

Up to Gigabit and above 

Industrial RJ45 in sealed housings, where devices use RJ45 ports 

 

L-com offers both M12 D-coded Ethernet cable and M12 X-coded to RJ45 assemblies built for these environments. 

 

Choosing Cabling for Your Protocol 

The cabling decision comes after the protocol decision, but it is the one that decides whether the network stays up. Industrial Ethernet performs as well as its weakest connector, so match the jacket, shielding and connector coding to the environment and the speed.  

 

Industrial Ethernet Cables from L-com 

Whichever protocol you choose, match the cable and connector to the speed and the environment. L-com offers M12 D-coded Ethernet cable for 100 Mb/s devices and M12 X-coded to RJ45 assemblies for Gigabit links in IP67 environments. 

 

Frequently Asked Questions (FAQs) 

 

Can PROFINET, EtherNet/IP and Modbus TCP run on the same network? 

Yes, physically they can share cabling and switches, since all use standard Ethernet frames. In practice, mixed traffic needs managed switches, VLANs and QoS to protect real-time traffic from bulk traffic. Many plants keep protocols on separate VLANs or segments. 

Do I need special switches for EtherCAT? 

Generally, no, since EtherCAT devices daisy-chain and pass the frame along themselves, so standard switches are not part of the cyclic path. A standard switch can connect EtherCAT segments to a standard network, but it cannot sit inside the real-time chain. 

Is Modbus TCP a real-time protocol? 

No. Modbus TCP uses a request/response model with no scheduling or prioritization, so response times vary with network load. It is dependable for monitoring and supervisory data but should not be used for synchronized motion control. 

Which industrial Ethernet protocol is fastest? 

EtherCAT is the fastest of the four, with cycle times that can drop below 100 microseconds because each device processes the frame on the fly. PROFINET and EtherNet/IP typically run at roughly 1 to 10 ms, and Modbus TCP updates in the tens to hundreds of milliseconds. 

What is the difference between PROFINET RT and IRT? 

PROFINET RT is software-based, runs on standard Ethernet hardware and typically has cycle times of 1 to 10 ms. PROFINET IRT (isochronous real-time) reserves time slots for critical traffic and can reach cycle times well under 1 ms, but it needs switches with dedicated hardware support. 

What is the difference between M12 D-coded and X-coded connectors? 

M12 D-coded connectors have four pins and carry 100 Mb/s, which covers most PROFINET, EtherNet/IP and EtherCAT I/O devices. M12 X-coded connectors have eight pins and carry Gigabit and faster. Choose by the speed your devices need, not by the protocol. 

Resources

Search Entries