L-com

Industrial Control Panel Design: DIN Rail, Enclosure and Cabling Best Practices

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics 

 

Good control panel design starts with the enclosure rating (NEMA or IP), followed by a layout that keeps power wiring away from signal wiring, standard DIN rail mounting, and a thermal plan that holds every component inside its rated temperature. Where your customer, machine type or local inspector requires it, the finished panel also has to follow UL 508A or NFPA 79. 

This puts the decisions in the order you make on a real build: enclosure, DIN rail, layout, wiring, in-panel networking, surge protection and a pre-energization check. 

 

Key Takeaways 

  • Pick the enclosure from the environment first: NEMA 12 suits clean indoor areas, while NEMA 4 or 4X (roughly IP66) suits wash-down, dust and outdoor exposure. 
  • Standard 35 mm (about 1.38 in) top-hat DIN rail (EN 60715) comes in 7.5 mm (about 0.3 in) and 15 mm depths, and the 15 mm (about 0.59 in) version is the safer choice for heavy drives and contactors. 
  • Divide the back panel into a power zone, a control zone and a network zone, and keep parallel power and signal running roughly 150 mm (6 in) apart or cross them at 90 degrees. 
  • Add the heat every component dissipates before choosing a fan, heat exchanger, air conditioner or heater, because most industrial devices are rated for about 0 to 55 or 60 °C inside the cabinet. 
  • Finish with surge protection on field-wired circuits and a written pre-energization checklist, so the first power-up is a verification and not an experiment. 

 

What Is an Industrial Control Panel? 

An industrial control panel is an assembly of power distribution, protection, control and communication devices mounted in an enclosure and wired together to run a machine or process. You will also hear it called an electrical control panel or a control cabinet. The names mean the same thing in practice: a box that holds breakers, power supplies, a PLC or controller, I/O, terminal blocks and, increasingly, network gear. 

Two standards come up most often. UL 508A is the North American listing standard for industrial control panels, and it drives choices such as component ratings and the short-circuit current rating (SCCR) marking. NFPA 79 covers the electrical equipment of industrial machinery. Which one applies depends on the machine, the customer specification and the authority having jurisdiction, so confirm that before you finalize the bill of materials. 

 

Choosing the Enclosure: NEMA, IP Rating, Material and Climate 

The enclosure rating should match the worst condition the panel will see, not the average one. Water, dust and corrosive wash-down chemicals are the usual reasons panels fail early. 

 

NEMA Types and IP Equivalents 

NEMA and IP ratings are not a one-to-one match, because NEMA tests include items such as corrosion and icing that IP codes do not cover. The table below gives practical starting points. 

Environment 

Typical NEMA Type 

Approximate IP Level 

Notes 

Clean indoor, dust and dripping water 

NEMA 12 

IP52 

Gasketed, no outside openings for knockouts 

Indoor or outdoor, hose-directed water 

NEMA 4 

IP66 

Watertight and dust-tight 

Wash-down, chemicals, coastal air 

NEMA 4X 

IP66 

Adds corrosion resistance 

Hazardous locations 

Separate classification 

Varies 

Needs a purpose-built enclosure, not a standard one 

 

 

Fiberglass vs Steel 

Fiberglass does not rust, handles chemicals and salt air well, and is non-conductive, which makes it popular for outdoor and wash-down installs. Painted steel costs less for large sizes and gives some shielding against electromagnetic interference. Stainless steel is the usual pick for food, beverage, and pharmaceutical areas. Whichever you choose, ground the back panel and the door to the protective earth bar. A fiberglass box does not bond itself. For lighter-duty panels that need corrosion resistance and a factory-mounted rail, DIN rail fiberglass enclosures are a common starting point. 

 

Heating and Cooling 

Heat is what shortens the life of drives, power supplies, and PLC modules. Add up the watts each device dissipates (the datasheets list it), compare that with what the enclosure can shed on its own, and choose cooling only if there is a gap. Filtered fans work in clean, cool rooms. Heat exchangers and air conditioners suit sealed NEMA 4 and 4X boxes, since they do not bring in outside air. In cold locations, a small thermostat-controlled heater keeps condensation off the electronics. If your calculation shows a gap, look at cooled and heated industrial enclosures before you add fans to a sealed box and give up its rating. 

 

What Is DIN Rail? Types and Sizes 

DIN rail is a standardized metal mounting rail that lets modules clip on without drilling or tapping the back panel. The common top-hat profile is defined in EN 60715 (formerly DIN EN 50022), and it is what most breakers, terminal blocks, relays, power supplies and industrial switches are designed to snap onto. If you are comparing DIN rail types and DIN rail sizes, these are the profiles you will meet: 

Rail Type 

Dimensions (Width x Depth) 

Typical Use 

TS35 x 7.5 (top-hat) 

35 x 7.5 mm (about 0.3 in) 

Most terminal blocks, breakers, relays, I/O and switches 

TS35 x 15 (deep top-hat) 

35 x 15 mm (about 0.59 in) 

Heavier loads such as contactors, drives and large power supplies 

G-rail 

35 mm (about 1.38 in) wide, 15 mm (about 0.59 in) deep, asymmetric profile 

Older equipment and some European designs 

Mini rail (TS15) 

15 mm (about 0.59 in) wide, about 5.5 mm (about 0.22 in) deep 

Compact devices in space-limited enclosures 

 

For most new builds, the 35 x 7.5 mm (about 0.3 in) rail is the default, and the 35 x 15 mm (about 0.59 in) rail is the upgrade when weight or leverage matters. Network gear follows the same pattern: DIN-rail mounted switches are built for standard 35 mm DIN rail, so you can place them next to the terminals and breakers they serve. 

 

Laying Out the Panel: Power, Control and Network Zones 

A clean layout separates what is noisy and hot from what is sensitive. Plan it on paper before you drill anything, with the back panel divided into three zones. An annotated layout drawing is the fastest way to see this, so mark each zone and the wire duct runs on your panel drawing: 

  • Power zone. Disconnect, circuit protection, contactors, power supplies and any drives. Keep this zone at one side, usually the top or the left, where the incoming power enters. 
  • Control zone. The PLC or controller, I/O modules, relays and safety devices. Keep these away from the drives and power supplies, with the clearance each datasheet asks for. 
  • Network zone. Switches, media converters and the patch cords that connect them, kept near the controller and away from motor and drive wiring. 

Run wire duct between the rows of rail so conductors reach each device by the shortest path, and keep the duct below about 40 percent fill so heat can escape and you can add wires later. Put terminal blocks for field wiring along the bottom or the side nearest to the cable's entry, so field conductors do not cross the whole panel. Mount heavy parts low and keep labels visible from the front of the device after the duct covers are on. 

 

Control Panel Wiring Practices 

Most intermittent faults in a finished panel trace back to wiring habits, not device failures. These practices prevent the common ones. 

  • Segregate power and signal. Keep AC power, motor and drive cables away from DC control, analog and Ethernet cables. A common practice is roughly 150 mm (6 in) of separation on parallel runs, with any crossing made at 90 degrees. Use separate ducts where you can. 
  • Use ferrules on stranded wire. Crimped wire-end ferrules give a repeatable connection in spring-clamp and screw terminals and stop stray strands from shorting to the next terminal. 
  • Label both ends. Print wire numbers that match the schematic at both ends of every conductor, and label devices to match the bill of materials. Future troubleshooting time is mostly a function of this step. 
  • Use a grounding bar. Bond the protective earth bar to the enclosure and back panel with a short, heavy conductor, and take every device ground to the bar in a star pattern, not a daisy chain. 
  • Terminate shields properly. Clamp the shield of drive and sensor cables to the grounding bar at the point where the cable enters the panel, with a 360-degree clamp and not a long pigtail, because a pigtail adds the inductance that lets noise through. 

Shield and ground practices matter most near variable frequency drives. 

 

How Do You Wire Networking Inside the Panel? 

Treat the network zone like any other part of the panel: short runs, strain relief and separation from power. Ethernet is limited to 100 m per channel, but inside a panel most links are well under 2 m, so the real concerns are bend radius, vibration and noise. 

 

DIN-Rail Switches and Patch Cords 

Mount the switch on rail close to the controller and use factory-molded patch cords with a snagless or locking boot, kept as short as the layout allows. Do not coil excess cord next to a drive or contactor. Unmanaged switches are enough for a simple machine with a few devices, while managed models add diagnostics, VLANs and ring redundancy. 

 

Bulkhead Connections and Field-Terminated Cable 

A bulkhead M12 or RJ45 feed-through on the enclosure wall lets technicians connect a laptop or a field device without opening the door, and it keeps the enclosure rating intact because the connector is sealed at the panel. Where a cable must be cut to length inside the cabinet, an industrial RJ45 plug kit allows field termination for permanent runs. Use solid-conductor cable for permanent installs and stranded patch cords for anything that moves. 

 

HMI and Door-Mounted Devices 

Door-mounted HMIs and pilot devices need slack in their cables, routed on the hinge side with a service loop so the cable is not pulled when the door swings. Keep these cables in their own duct, away from the power zone. 

 

Surge Protection for Field-Wired Circuits 

Any conductor that leaves the building or runs a long distance outdoors can carry a surge into the panel, and the 24 V DC sensor and control lines are the ones most often left unprotected. Install a surge protector on the field side of each affected circuit at the point of entry, and bond it to the grounding bar with the shortest conductor you can manage, because the length of that ground lead sets how well it clamps. Match the protector to the circuit voltage, signal type and current. DC control-line surge protectors are made for exactly these 24 V and low-voltage control and sensor lines. Protect Ethernet lines that leave the building as well, using devices rated for the data rate you run. 

 

Pre-Energization Checklist 

Run through these checks with the power locked out and tagged. Each takes only minutes and prevents the most common first-power-up failures. 

  1. Compare every wire to the schematic and check that every wire number is present at both ends. 
  1. Pull-test terminated conductors and re-torque screw terminals to the values printed on the device or in its datasheet. 
  1. Measure continuity of the protective earth path from the grounding bar to the door, the back panel and each device. 
  1. Check insulation resistance and look for shorts between power rails and ground before closing breakers. 
  1. Verify that the supply voltage, breaker ratings and power supply output settings match the drawings. 
  1. Confirm the clearance around heat-producing devices and that vents, fans and filters are installed and unblocked. 
  1. Inspect network cables for bend radius, strain relief and separation from power conductors. 
  1. Close breakers one at a time, from the main down to each branch, and check the voltage at each stage. 

 

Solid control panel design comes down to a handful of decisions made in the right order: match the enclosure to the environment, mount everything on the right DIN rail, divide the layout into power, control and network zones, wire with ferrules, labels and clean grounding, and protect field circuits before you energize. Before you order parts, write your heat load and spare capacity on the drawing, and use the checklist above as the sign-off for every panel you ship. 

 

Control Panel Components from L-com 

L-com supplies the enclosure, networking and protection parts covered above, including DIN rail fiberglass enclosures, cooled and heated industrial enclosures, DIN rail Ethernet switches, an industrial RJ45 plug kit and DC control-line surge protectors. 

 

Frequently Asked Questions (FAQs) 

 

Do I need UL 508A for my control panel? 

Not always. UL 508A applies when the panel must be listed for the US or Canadian market, and many customers and inspectors require it. NFPA 79 may apply as well when the panel runs industrial machinery. Ask the end customer and the local authority having jurisdiction before you build. 

How much spare space should I leave in a control cabinet? 

Plan for 20 to 30 percent spare panel space and spare wire duct capacity. Devices get added later, and a panel that is full on day one is hard to service and runs hot. 

Can I use standard patch cords inside a control panel? 

Yes, for short links in a clean, low-vibration panel, provided the cord is rated for the temperature range inside the cabinet. For panels near drives or in high-vibration machines, industrial patch cords with shielding and locking connectors are the safer choice. 

What NEMA rating does a control panel need? 

Match the enclosure to the worst condition it will see. NEMA 12 suits clean indoor areas, NEMA 4 suits indoor or outdoor areas with hose-directed water, and NEMA 4X adds corrosion resistance for wash-down, chemicals and coastal air. 

What is the difference between 7.5 mm and 15 mm DIN rail? 

Both are 35 mm wide top-hat rail (EN 60715). The 7.5 mm depth is the default for most terminal blocks, breakers, relays, I/O and switches. The 15 mm deep rail is the upgrade for heavier loads such as contactors, drives and large power supplies. 

How far apart should power and signal wiring be in a control panel? 

A common practice is roughly 150 mm (6 in) of separation on parallel runs, with any crossing made at 90 degrees. Use separate ducts where you can. 

Resources

Search Entries