L-com

Blog

Can Bus Cables Be Used Outdoors?
In control systems, bus communication protocols such as PROFIBUS and CAN-Bus are vital for connecting sensors, controllers and actuators. However, a common concern for engineers and system integrators is whether these cables can withstand outdoor environments. Using the right cables outdoors is essential to ensure system reliability, safety and compliance with environmental standards.... Read more
Cable Jacket Materials: PVC vs. PUR vs. TPE for Bus Applications
In process control, robotics, and automotive systems, bus cables serve as vital connectors that reliably transmit data and power. While the focus often centers on the conductors and shielding, the cable jacket material is equally important. The jacket safeguards the cable against mechanical damage, exposure to chemicals and oils, UV radiation and temperature fluctuations, ensuring durability and safety over time.... Read more
Bus Cables in Industrial Automation and Process Control
Industrial automation and process control systems have become the backbone of modern manufacturing and production facilities, relying heavily on precise, real-time communication between a diverse array of devices. At the core of this intricate communication network are bus cables, which are specialized cables designed to efficiently transmit signals between controllers, sensors, actuators and various machines. These cables stand apart from standard wiring due to their unique engineering, which allows them to withstand high levels of electromagnetic interference, maintain consistent impedance and ensure data integrity even in the harshest industrial environments. With the increasing complexity of automated processes, the importance of reliable signal transmission has never been more critical.... Read more
Anatomy of a Bus Cable: Conductors, Shielding, Impedance, Jacket Materials
Conductors, the core of any cable, determine the efficiency of signal transmission, while shielding plays a critical role in minimizing electromagnetic interference that can degrade performance. Additionally, impedance is a crucial parameter that influences signal integrity and compatibility among connected devices. Whether in automotive systems, industrial automation or consumer electronics, the knowledge of bus cable anatomy is indispensable for ensuring optimal functionality and longevity in electronic communication networks.... Read more
Products that Can Help Edge Data Centers Power Your Company’s Performance
As the demand for real-time data processing grows, edge computing has become a foundation of modern digital infrastructure. From smart cities to autonomous vehicles and industrial automation, edge data centers are enabling faster, localized computing closer to where data is generated. This shift allows businesses to respond instantly to critical information, but it also introduces new challenges that traditional data centers were never designed to face.... Read more
What’s the Difference Between Industrial and Commercial RJ45?
In Ethernet networking, RJ45 connectors are the standard interface for twisted-pair cables, enabling everything from office internet connections to complex industrial automation systems. But not all RJ45 connectors are created equal.... Read more
Are Industrial Ethernet Cables Flame-Retardant?
In industries where heavy machinery, high electrical loads and combustible substances are the norm, fire safety is essential. Industrial Ethernet cables, the backbone of modern automation networks, must often endure extreme heat, mechanical stress and potential fire hazards. But are they flame-retardant?... Read more
How Long Can an Industrial Ethernet Cable Be?
Industrial Ethernet cables are the backbone of modern automation systems, connecting programmable logic controllers (PLCs), sensors, human-machine interfaces (HMIs) and industrial PCs. But when it comes to designing or troubleshooting an Ethernet network in a factory, oil rig or processing plant, one question comes up repeatedly: “How long can an industrial Ethernet cable be before it affects performance?”... Read more
Do You Need Shielded Cables for Industrial Ethernet?
Industrial Ethernet networks are the nervous system of modern manufacturing plants, automation lines, oil and gas facilities, and other mission-critical environments. In these high-stakes applications, reliable data transmission is non-negotiable. Even a brief disruption can cause production downtime, safety risks or expensive equipment failures.... Read more
Can Industrial Ethernet Cables Be Used Outdoors?
Industrial Ethernet cables are engineered to handle the rigorous conditions found in manufacturing plants, outdoor facilities and other challenging environments. Unlike standard Ethernet cables, industrial versions offer enhanced durability, better shielding against interference and materials designed to resist environmental damage.... Read more

Resources

Search Entries