L-com

Bus Cables in Industrial Automation and Process Control

By Eileen Harvey 

Industrial automation and process control systems have become the backbone of modern manufacturing and production facilities, relying heavily on precise, real-time communication between a diverse array of devices. At the core of this intricate communication network are bus cables, which are specialized cables designed to efficiently transmit signals between controllers, sensors, actuators and various machines. These cables stand apart from standard wiring due to their unique engineering, which allows them to withstand high levels of electromagnetic interference, maintain consistent impedance and ensure data integrity even in the harshest industrial environments. With the increasing complexity of automated processes, the importance of reliable signal transmission has never been more critical. 

Brands like TKD Kabel have emerged as key players in providing industrial-grade cables that rise to the challenges presented by automation and process industries. Their products are designed to meet rigorous industry standards, ensuring that they can operate effectively in environments characterized by extreme temperatures, vibrations and exposure to chemicals. 

Role of Bus Cables in Industrial Automation 

Industrial automation involves interconnected machines, controllers and sensors that must exchange data seamlessly. Bus cables play a critical role in: ensuring real-time communication between PLCs, HMIs and field devices; reducing wiring complexity by connecting multiple devices over a single cable; and enhancing reliability through shielding and impedance control. For example, PROFIBUS cables are widely used in factory automation to interconnect devices with high accuracy and minimal signal loss. 

Applications of Bus Cables in Industrial Automation 

In factory automation, bus cables play a crucial role in connecting robotic arms and conveyor sensors, ensuring synchronized movements across the production line. They also enable machine-to-machine communication with CAN-Bus cables proving especially useful in assembly lines where rapid communication is essential. 

In process automation, PROFIBUS and Fieldbus cables are widely used in chemical, food and pharmaceutical plants to enable precise monitoring of batch processes. Shielded bus cables also support continuous monitoring by transmitting data from sensors measuring temperature, flow and pressure. 

In energy and power systems, CAN-Bus cables facilitate data collection from remote substations within smart grids and power distribution networks. Fieldbus connections are commonly used in SCADA systems allowing operators to control high-voltage systems from central hubs. 

In automotive and manufacturing applications, bus cables are relied upon for automated welding where reliable CAN-Bus cables can withstand electromagnetic interference (EMI) generated by welding equipment. They are also integral to quality control processes, transmitting real-time inspection data to central monitoring systems. 

Applications of Bus Cables in Process Control 

The oil and gas industry uses bus cables in pipeline monitoring systems where reliability is vital. These cables are built to withstand harsh environments including exposure to oil, gas and chemicals. 

In water and wastewater treatment facilities, bus cables connect pumps, valves and sensors within SCADA systems. This enables real-time monitoring that helps prevent downtime and ensures compliance with regulatory requirements. 

In HVAC and building automation, bus cables support climate control, lighting and access systems, helping to ensure energy-efficient building operations. 

In the pharmaceutical and food industries, bus cables are commonly used in batch processing systems where data accuracy is critical. Specialized cable jackets also help these cables meet strict safety and hygiene compliance standards. 

Benefits of Using Bus Cables in Automation and Process Control 

Bus cables offer several benefits to industrial automation and process control systems. High-speed data transfer ensures there is no lag in communication across networks. Reduced wiring complexity saves both installation time and costs. Scalability makes it possible to expand factory systems without the need for major rewiring. In addition, improved safety is achieved because EMI-shielded bus cables help prevent malfunctions in sensitive environments. 

Tips for Selecting the Right Bus Cable 

When selecting the right bus cable, it is important to match the protocol whether PROFIBUS, CAN-Bus, Fieldbus or ASi-Bus. Shielding should be chosen carefully with foil or braid selected depending on the level of EMI exposure. Environmental considerations are also essential; for example, UV resistance, oil resistance or chemical resistance may be required for certain applications. Impedance compatibility must be ensured with typical requirements including 150 ohms for PROFIBUS and 120 ohms for CAN-Bus. Finally, it is best to choose trusted brands with TKD Kabel recognized for reliable industrial-grade bus cables. 

Recommendations 

  • Use double-shielded cables in high EMI environments such as welding shops. 

  • Select UV-resistant and oil-resistant jackets for outdoor or harsh environments. 

  • Standardize one bus system per application for ease of maintenance. 

  • Always source from reliable suppliers like L-com to ensure compliance and durability. 

Interesting Facts About Bus Cables 

  • PROFIBUS is used in over 56 million devices worldwide. 

  • CAN-Bus was originally developed for the automotive industry but is now used across industries. 

  • ASi-Bus cables are flat, making installation easier in tight industrial spaces. 

  • Proper shielding can reduce EMI-related errors by up to 90%. 

 

FAQs (Frequently Asked Questions) 

Q1: What makes bus cables different from standard cables?  
A: Bus cables are designed with controlled impedance, shielding and insulation to maintain reliable data transmission in noisy industrial environments. 

Q2: Can I use PROFIBUS cables for CAN-Bus applications?  
A: No. Each bus system requires a cable with specific impedance (e.g., a PROFIBUS cable should be 150 ohms, a CAN-Bus is 120 ohms). 

Q3: Are bus cables suitable for outdoor installations?  
A: Yes, but ensure the cable is UV-resistant and oil-resistant, such as PVC or TPE jacketed bus cables. 

Q4: Which brand is recommended for industrial-grade bus cables?  
A: TKD Kabel is a trusted brand for automation-grade bus cables. 

Bus cables are the backbone of industrial automation and process control systems. Whether in manufacturing, energy, oil and gas, or water treatment, these cables ensure uninterrupted data transmission, system efficiency and safety. Choosing the right cable such as PROFIBUS, CAN-Bus or Fieldbus can significantly enhance productivity and reduce downtime. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries