L-com

Industrial Bus Cables vs. Standard Communication Cables

By Eileen Harvey 

From manufacturing plants to home entertainment systems, the choice of communication cables plays a crucial role in determining the overall reliability, safety and performance of various systems. In the modern world, where technology is deeply integrated into our daily lives, the right cable can make all the difference. For instance, in a home entertainment system, a high-quality HDMI or optical audio cable can significantly enhance the audio-visual experience, ensuring that signals are transmitted without loss or distortion. Conversely, using subpar cables can lead to frustrating glitches, interruptions and generally poor performance.  

In industrial settings, the stakes are considerably higher. Communication cables are not just conduits for data; they are lifelines that support critical operations and processes, making the selection of the appropriate type of cable is paramount. 

What Are Bus Cables? 

Bus cables are specialized, robust cables engineered for reliable data transmission between multiple devices in complex control systems, automation networks and industrial machinery. Unlike standard communication cables, bus cables are built to withstand demanding industrial environments where electrical noise, mechanical stress and environmental hazards are common. 

In industrial automation, bus cables connect devices in daisy-chain or star topologies, enabling efficient data sharing, diagnostics and system control. They are designed to ensure high data integrity, low latency and strong resilience against electromagnetic interference (EMI), which is critical in settings with motors, transformers and other electrical equipment. 

Common Types of Industrial Bus Cables 

Industrial bus cables include PROFIBUS cables, which are used in factory automation for real-time data exchange. CAN bus cables are widely applied in automotive systems, industrial control and instrumentation. EtherCAT and DeviceNet cables are designed for high-speed real-time industrial networks. Examples from TKD Kabel include the PROFIBUS Process Fieldbus Cable and CAN Bus Controller Area Network Cables. 

Construction and Materials 

Industrial bus cables are built with robust insulation and shielding, using materials that resist oils, chemicals, UV radiation and mechanical stress to ensure durability in harsh environments. 

What Are Standard Communication Cables? 

Standard communication cables are the everyday tools used to transfer data across a wide variety of electronic devices and systems. They are designed for controlled environments such as homes, offices and commercial spaces where the need for durability and environmental resistance is lower. Their primary purpose is to provide seamless and reliable connectivity between devices, making them essential for digital communication. 

One of the most common types of standard communication cables is the Ethernet cable, such as Cat5e, Cat6 and higher categories, which are used to build wired networks. These cables provide stable internet and local network connections for computers, servers, routers and other network devices. 

Common Types of Standard Cables 

Examples include Ethernet cables for local area networks, USB cables for connecting peripherals, HDMI cables for audio and video transmission, and serial cables such as RS-232 or RS-485 for serial communication. 

Construction and Materials 

Standard communication cables are designed for flexibility, cost-effectiveness and ease of installation. They often use PVC jackets or similar materials and may have limited shielding, which makes them less suitable for industrial or harsh environments. 

Key Differences Between Industrial Bus Cables and Standard Communication Cables 

Construction and Materials 

Industrial bus cables are heavily shielded with foil, braid or a combination of both to prevent EMI. Their insulation is made of durable, oil- and UV-resistant materials such as PVC, TPE or specialized polymers, and they often include reinforced armor or robust jackets for added mechanical protection. For example, PROFIBUS cables are constructed with double shielding and oil-resistant PVC jackets. Standard communication cables, on the other hand, usually include minimal shielding such as a single foil or braid, and their jackets are typically flexible PVC or TPE. They are not built to withstand chemicals, UV radiation or heavy mechanical stress. 

Electrical Characteristics 

Industrial bus cables are designed to minimize noise and EMI to ensure data integrity in noisy environments. They often use twisted pairs with impedance matching, such as 120Ω for CAN bus, and they support high data rates with low latency, which is essential for real-time control. Standard communication cables are optimized for speed and convenience in low-noise settings. While they support high data rates, they are more vulnerable to interference and are not suitable for real-time critical systems. 

Environmental Resistance 

Industrial bus cables offer strong resistance to oils, chemicals, moisture, UV radiation and extreme temperatures. This makes them suitable for outdoor use, underground installations or hazardous environments. Many of these cables are built with TPE or specialized PVC jackets for added resilience. Standard communication cables have limited environmental resistance and are generally restricted to indoor or protected spaces, where harsh conditions would otherwise cause deterioration or failure. 

Connectivity and Compatibility 

Industrial bus cables connect specialized industrial devices and use connectors and protocols designed to meet strict standards and certifications such as UL and IEC. Standard communication cables are built for consumer electronics and use common interfaces and connectors such as RJ45, USB, HDMI and serial ports. 

Tips for Selecting the Right Cable 

  • Always verify environmental ratings: oil, chemical, UV and temperature resistance. 
  • Use shielded cables for noisy industrial environments. 
  • Match impedance and connector types to the device specifications. 
  • If in doubt, consult with manufacturers like TKD Kabel for durable, industrial-grade solutions. 
  • Ensure the cable’s certification aligns with your region’s safety standards. 

FAQs (Frequently Asked Questions) 

Q1: Can I use standard Ethernet cables for industrial automation?  
A: Generally, no. Standard Ethernet cables are not designed to withstand harsh industrial environments. For automation, use industrial-grade Ethernet cables with appropriate shielding and environmental resistance. 

Q2: What certifications should I look for in industrial cables?  
A: Look for UL, IEC, CE and other regional safety standards to ensure durability and compliance. 

Q3: How do I know if a cable is suitable for outdoor use?  
A: Check for UV-resistant jackets, waterproofing and certifications indicating outdoor suitability.  

 

Understanding the fundamental differences between industrial bus cables and standard communication cables is crucial for optimal system design and operational reliability. While standard cables excel in cost-effective, controlled environments, industrial bus cables are engineered to withstand the rigors of harsh settings, ensuring data integrity and safety. 

Selecting the right communication cable is vital to ensure system longevity, safety and efficiency. Whether you’re designing a new factory automation system or upgrading existing infrastructure, understanding the core differences outlined here will guide you toward the best choice. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

 

Resources

Search Entries