L-com

Securing Wireless IIoT Devices: A Complete Field Guide

Securing Wireless IIoT Devices: A Complete Field Guide

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics

 

Key Takeaway 

•   Wireless IIoT security requires more than protocol configuration — it requires a 6-layer approach that starts with the RF physical environment and ends with physical device protection, because an unsecured antenna feed or an unlocked gateway enclosure can bypass every logical control in between. 

•   The most common wireless IIoT vulnerabilities are not exotic: WPA2 KRACK attacks on industrial WiFi, LoRaWAN 1.0 replay attacks on sensor networks, default join keys on WirelessHART gateways, and BLE pairing vulnerabilities on asset tracking devices. All are addressed by specific, available mitigations. 

•   Protocol selection determines your security floor — WPA3-Enterprise, LoRaWAN 1.1, Zigbee 3.0, and WirelessHART with changed join keys provide substantially better security than their predecessors, and migrating to them is the highest-impact single decision in a wireless IIoT hardening project. 

•   RF lightning protection on outdoor antenna coax connections is the physical security control most often missing from wireless IIoT deployments. A lightning strike on an outdoor gateway antenna follows the coax into the enclosure and can destroy the gateway, the connected switch, and anything else on the same network segment — regardless of firmware version or firewall configuration. 

  

Why is wireless IIoT security different from enterprise wireless security? 

Wireless in enterprise environments connects laptops, phones, and conference room equipment — devices that are routinely replaced, can run security agents, and operate in controlled indoor environments. Wireless in industrial environments connects sensors bolted to outdoor tanks, gateways mounted on utility poles, and edge devices embedded in equipment that runs continuously for years. 

The differences that matter for security are device lifespan (enterprise devices are replaced every 3–5 years; industrial wireless devices may run for 10–15 years without replacement), physical exposure (outdoor antennas are exposed to lightning, temperature extremes, and physical access), update constraints (many IIoT devices can't receive OTA updates without a maintenance window or physical access), and protocol diversity (industrial wireless includes LoRaWAN, Zigbee, WirelessHART, and ISA-100.11a in addition to WiFi and Bluetooth). 

The attack surface is also larger than most wireless security guides acknowledge. Protocol vulnerabilities, RF physical attacks, and supply chain compromises all apply — and the physical layer vulnerabilities unique to outdoor industrial deployments are almost absent from enterprise wireless guidance.  

 

What is the wireless IIoT attack surface? 

Eight attack vectors account for the majority of documented wireless IIoT security incidents and vulnerability disclosures. 

  

Attack vector 

How it works 

Protocols most affected 

Primary mitigation 

Rogue access point 

Attacker deploys AP with matching SSID; devices connect to it instead of legitimate AP 

WiFi 

RSSI-based rogue AP detection; 802.1X mutual authentication; WPA3-Enterprise 

WPA2 KRACK (Key Reinstallation) 

Nonce reuse in the 4-way handshake allows decryption of encrypted traffic 

WiFi (WPA2) 

Migrate to WPA3; patch all WPA2 endpoints; WPA2-Enterprise with mutual auth reduces impact 

BLE man-in-the-middle 

Attacker intercepts pairing exchange; captures keys; decrypts session 

BLE 4.1 and earlier 

Require LE Secure Connections (BLE 4.2+); numeric comparison or passkey pairing 

RF jamming 

High-power RF noise on the device frequency disrupts communication 

All wireless 

Frequency hopping (802.15.4, WirelessHART, ISA-100); redundant wired backup for critical control 

RF spoofing 

Replay or fabrication of valid-format RF packets 

LoRaWAN 1.0, older Zigbee 

Message integrity codes; sequence counters; LoRaWAN 1.1 replay protection 

Insecure OTA firmware update 

Unsigned or unencrypted firmware delivered over the air; attacker injects malicious image 

All 

Code-signed firmware; TLS-encrypted update channel; version rollback prevention 

Physical device tampering 

Device removed, cloned, or debugged; key material extracted 

All 

Tamper-evident hardware; secure enclave/HSM; physical lockdown; tamper-detection alerts 

Lightning / surge on antenna feed 

Surge energy enters network via coax; damages gateway or network equipment 

All (outdoor deployments) 

RF lightning protectors on all outdoor antenna coax connections; proper grounding per IEC 61643-11 

  

The last row — lightning and surge on antenna feeds — is absent from most wireless security frameworks because it is categorized as an electrical problem rather than a security problem. The security consequence is the same regardless of categorization: a single surge event can destroy gateway hardware and create a network outage that, in a poorly monitored environment, could be exploited as a cover for other activity. It also represents a physical path from outside the facility directly into network equipment — a path that no firewall can see. 

 

What is the 6-layer wireless IIoT security model? 

The six layers below represent a defense-in-depth approach to wireless IIoT security. They're ordered by dependency: the lower layers are prerequisites for the upper layers to function correctly. Configuring Layer 3 (authentication and encryption) on a device with a compromised physical environment (Layer 1 or Layer 6) is incomplete — an attacker who can access the physical hardware or intercept the RF path has options that authentication alone doesn't close. 

  

# 

Layer 

What it protects 

Key controls 

Physical dependency 

1 

RF environment 

Airspace from rogue APs, jamming, spoofing 

RSSI monitoring; rogue AP detection; directional antennas; RF shielding where needed 

Antenna placement; cable path from AP to network 

2 

Protocol selection 

Devices from protocol-level vulnerabilities 

WPA3 for WiFi; BLE 4.2+ pairing; LoRaWAN 1.1 with AppSKey; avoid open Zigbee networks 

Antenna type determines protocol range and exposure 

3 

Authentication & encryption 

Sessions from eavesdropping and credential attacks 

WPA3-Enterprise; EAP-TLS; device certificates; VPN for backhaul; TLS 1.3 for application layer 

Certificate provisioning at commissioning 

4 

Device certificate management 

Device identity integrity over time 

PKI; automated certificate renewal; SCEP or EST; revocation via OCSP or CRL 

HSM or secure enclave on device; physical access for initial provisioning 

5 

Network segmentation 

Lateral movement from compromised wireless devices 

Dedicated OT wireless VLAN; deny-by-default firewall; wireless IDS; no bridge to wired OT 

Wireless AP in locked enclosure; fiber backhaul to wired network 

6 

Physical protection 

Hardware from tampering, theft, environmental damage, and surge 

Locked enclosures; tamper switches; RF lightning protectors; NEMA-rated housings 

This layer is the foundation — software controls depend on hardware integrity 

  

The physical protection layer (Layer 6) is placed last in the numbering but first in the implementation sequence — secure the hardware before configuring the software. This inversion is common in security frameworks that list logical controls before physical ones, and it produces the gap that industrial deployments most often expose. 

 

Layer 1: How do you harden the RF environment? 

RF environment hardening addresses threats that operate below the protocol layer — rogue access points, jamming, and unauthorized RF devices that can intercept or disrupt wireless communication before encryption is even relevant. 

 

Rogue access point detection 

A rogue access point broadcasting a matching SSID can convince IIoT devices — particularly those using PSK authentication — to connect to it instead of the legitimate network. Industrial WiFi devices that auto-reconnect to any matching SSID are particularly vulnerable. The mitigation is twofold: 802.1X mutual authentication (so the device verifies the AP's identity, not just the network name) and wireless IDS monitoring for unauthorized APs on the industrial SSID. Cisco Catalyst 9800, Fortinet FortiAP, and Aruba Clear Pass all support rogue AP containment in OT-segmented deployments. 

 

RF site survey as a security baseline 

An RF site survey before deployment establishes the expected signal environment: legitimate AP coverage maps, interference sources, signal bleed outside the facility boundary, and baseline RSSI levels for each device location. This baseline serves a security function: significant changes in the RF environment — new high-power sources, unexpected signal patterns — can indicate interference equipment or rogue APs and are detectable against the baseline. 

The survey also identifies locations where antenna placement creates unintended coverage outside the physical perimeter. An outdoor antenna that covers the parking lot is extending the wireless network attack surface beyond the fence line. Directional antennas pointed inward and cardioid antenna patterns reduce this exposure without reducing indoor coverage. 

 

RF jamming and frequency hopping 

RF jamming — deliberate high-power interference on the operating frequency — can deny service to wireless IIoT devices. For WiFi, the primary mitigation is moving to 5 GHz or 6 GHz bands, which are less crowded and harder to jam without expensive equipment. For sub-GHz protocols like LoRaWAN, frequency hopping in regulations-compliant implementations provides some resilience. 

For control functions where wireless communication is on the critical path — process control feedback loops, emergency shutoff triggers — the correct design is wired backup, not jamming resistance. Wireless should carry monitoring and non-critical data; safety-critical and time-sensitive control commands should have wired paths that function even when wireless is unavailable. 

 

Layer 2: How do you select and configure wireless protocols for security? 

Protocol selection is the highest-impact single decision in a wireless IIoT security project because it determines the security ceiling for everything that runs on top of it. A device running LoRaWAN 1.0 cannot be fully secured by configuration — the protocol itself has replay vulnerabilities that configuration cannot fix. 

  

Protocol 

Frequency 

Range 

Data rate 

Security model 

IIoT fit 

Key security consideration 

WiFi 6 (802.11ax) 

2.4/5/6 GHz 

30–100 m indoor 

Up to 9.6 Gbps 

WPA3-Enterprise + EAP-TLS 

HMIs, gateways, high-bandwidth edge devices 

KRACK vulnerability affects WPA2; migrate to WPA3. Rogue AP risk is the highest of all listed protocols. Backhaul requires RF lightning protection on outdoor antenna runs. 

BLE 5.x 

2.4 GHz 

~100m (PHY-dependent) 

2 Mbps 

LE Secure Connections (ECDH) 

Low-power sensors, asset tracking, wearables 

BLE 4.1 and earlier pairing is is vulnerable to MITM. Require LE Secure Connections (BLE 4.2+). BLE beacons with no pairing are passive and unauthenticated — treat their data as untrusted. 

LoRaWAN 1.1 

Sub-GHz (868/915 MHz) 

2–15 km 

250 bps–50 kbps 

AppSKey + NwkSKey (AES-128) 

Remote sensors, metering, and environmental monitoring 

LoRaWAN 1.0 has known replay attack vulnerabilities; require 1.1. Join server security is the weak point — compromise of the join server exposes all device keys. Outdoor gateway antennas require RF lightning protection. 

Zigbee 3.0 

2.4 GHz 

10–100m 

250 kbps 

AES-128 CCM; Trust Center key distribution 

Building automation, smart metering, mesh sensor networks 

Pre-3.0 Zigbee (HA, ZLL profiles) had insecure touchlink commissioning. Zigbee 3.0 requires install code-based commissioning. The Trust Center is a single point of failure — compromise of the coordinator key compromises the entire network. 

WirelessHART 

2.4 GHz 

~250m with mesh 

250 kbps 

AES-128; network and session keys; join key 

Process sensors in hazardous areas; certified instruments 

Strongest security model of the listed protocols by design. Key risk: default join keys left at factory default. Change all join keys at commissioning. Physical security of the gateway is critical — it holds all network keys. 

ISA-100.11a 

2.4 GHz 

~150m with mesh 

250 kbps 

AES-128 CCM*; PKI-based device identity 

Critical process control; ISA/IEC 62443 environments 

PKI infrastructure is required for full security model — significant operational overhead. Physical device identity (device certificates) at commissioning. Most secure general-purpose IIoT wireless protocol. 

  

 

WiFi: migrate from WPA2 to WPA3 

The KRACK vulnerability (CVE-2017-13077 and related) demonstrated that WPA2's 4-way handshake could be exploited to force nonce reuse, allowing an attacker in RF range to decrypt traffic without knowing the password. The vulnerability affects WPA2-Personal and WPA2-Enterprise differently — WPA2-Enterprise with EAP-TLS mutual authentication significantly reduces the practical impact because the attacker can't easily complete the handshake — but the correct resolution is migration to WPA3. 

WPA3-Enterprise with EAP-TLS and device certificates is the target configuration for industrial WiFi. It provides forward secrecy (each session uses a unique key), strong mutual authentication (both device and AP verify each other's identity), and protection against offline dictionary attacks on captured handshakes. For environments where device replacement isn't immediate, WPA2-Enterprise with EAP-TLS is an acceptable interim configuration with significantly better security than WPA2-PSK. 

 

LoRaWAN: requires version 1.1 

LoRaWAN 1.0 has documented replay attack vulnerabilities — an attacker who captures a valid uplink frame can retransmit it, and the network server may accept it. LoRaWAN 1.1 addresses this with frame counter anti-replay protection and improved key derivation. Deploying LoRaWAN 1.0 devices in a new installation is a security decision, not just a procurement decision. 

LoRaWAN gateways with outdoor antennas are frequently mounted on rooftops, utility poles, or towers — locations with high lightning exposure.RF lightning protectors on the coax feed between the outdoor antenna and the indoor gateway are required at these positions. A lightning event on an unprotected outdoor antenna follows the coax directly into the gateway's RF input, which has essentially no surge tolerance, and from there into whatever switch or network equipment the gateway is connected to. 

 

Zigbee: requires version 3.0 with install code commissioning 

Pre-Zigbee 3.0 profiles (Home Automation, ZigBee Light Link) used a touch link commissioning process that had no authentication — any device in RF range could join a network during commissioning. ZigBee 3.0 requires install code-based commissioning: each device has a unique commissioning key printed on a label, and only devices with a known install code can join. For existing ZigBee HA or ZLL deployments, the mitigation is replacing the Trust Center key and disabling touch link permanently. 

 

WirelessHART: change all factory default join keys 

Wireless HART has one of the strongest security models among IIoT wireless protocols — AES-128 encryption, network and session key architecture, and join key provisioning. The most common deployment vulnerability is straightforward: the factory default join key is left unchanged. Factory default keys for major Wireless HART device manufacturers are documented publicly. Every Wireless HART installation should change the join key on every device at commissioning before the device is placed in a network reachable from any external connection. 

 

Layers 3–4: How do you implement authentication, encryption, and certificate management for wireless IIoT devices? 

Authentication and encryption for wireless IIoT follow the same principles as wired OT, but with additional complexity introduced by the diversity of wireless protocols and the operational challenges of managing certificates on field-deployed devices. 

 

EAP-TLS for industrial WiFi 

EAP-TLS is the authentication method that eliminates shared secrets from WiFi: each device has a certificate issued by an internal PKI, and the AP verifies the certificate at connection time. No password is stored on the device; no shared secret exists that a compromised device can expose. The operational overhead is the certificate lifecycle — provisioning certificates at manufacturing or commissioning, monitoring expiry, and replacing expired certificates without physical access. 

Automated certificate renewal using SCEP (Simple Certificate Enrolment Protocol) or EST (Enrolment over Secure Transport) is the operational answer to certificate lifecycle at scale. Both protocols allow a device to request and receive a new certificate over the network before the current one expires, without human intervention. For devices that can't run SCEP or EST clients, maintaining a certificate expiry calendar and scheduling maintenance visits before expiry is a manual alternative that works on a small scale. 

 

Application-layer encryption for non-WiFi protocols 

LoRaWAN, Zigbee 3.0, and Wireless HART all provide link-layer encryption — the RF transmission is encrypted. What they don't natively provide is end-to-end encryption of the application data from sensor to cloud or SCADA. In architectures where data passes through a gateway that terminates the wireless link-layer encryption, the data is decrypted at the gateway and re-encrypted for the backhaul link. If the gateway is compromised, the data at that gateway is accessible in plaintext. 

The mitigation is application-layer encryption (TLS 1.3 for cloud-connected devices, VPN for locally connected gateways) that maintains data confidentiality end-to-end, independent of the link-layer encryption provided by the wireless protocol. This adds processing overhead that some resource-constrained devices can't support — in those cases, the gateway security becomes more important, which reinforces the physical protection requirements at Layer 6. 

 

Layer 5: How should wireless IIoT devices be segmented from wired OT networks? 

A wireless IIoT device that connects directly to the same network segment as wired PLCs and SCADA servers is a lateral movement path. A compromised wireless sensor doesn't just expose its own data — it provides a foothold in the OT network segment from which an attacker can reach every other device on the same subnet. 

The correct architecture places wireless IIoT devices on a dedicated wireless OT VLAN that is isolated from both the wired OT network and the enterprise network. Traffic from wireless devices crosses a firewall before reaching any wired OT system. The firewall rules define exactly what a wireless sensor is permitted to communicate — typically a specific protocol and port to a specific data historian or gateway IP, and nothing else. 

Three specific segmentation controls for wireless IIoT: 

  • No wireless-to-wired OT bridging: APs configured in bridge mode — connecting wireless clients directly to the wired network — should not exist in OT environments. Every wireless device should be on a VLAN that routes through a firewall before reaching any wired OT segment 
  • Wireless IDS in passive monitoring mode: a dedicated wireless IDS (or the IDS features of industrial-grade APs) monitors the wireless spectrum for rogue devices, protocol anomalies, and DE authentication attacks without affecting wireless performance 
  • AP management plane isolation: the VLAN used to manage APs (configure, monitor, update) should be separate from the OT data VLAN and unreachable from wireless client devices — a compromised wireless device should not be able to reach AP management interfaces 

 

Layer 6: What physical controls are required for wireless IIoT devices? 

Physical protection is the layer that the other five depend on. Firmware integrity, certificate security, and network segmentation all assume that the hardware executing those controls hasn't been tampered with and is functioning correctly. Physical access to a device can bypass all of them: key material can be extracted from unprotected hardware, firmware can be replaced via debug interfaces, and a device can be cloned. 

 

RF lightning protection for outdoor wireless deployments 

Outdoor wireless gateways and access points are connected to antennas via coaxial cable. The antenna is, by design, a metallic structure exposed to the outdoor environment, which makes it an effective collector of transient energy from lightning strikes. A strike on or near the antenna induces voltage on the coax that can reach kilovolts within nanoseconds. The gateway's RF input has a typical surge rating of a few volts. Without protection, the surge travels through the coax, destroys the gateway's RF front end, and continues into whatever switch or network equipment the gateway connects to. RF lightning protectors installed in-line on the coax, close to the outdoor antenna entry point, clamp this surge to ground before it reaches indoor equipment. 

Grounding is the factor that determines whether the protector works. A gas-discharge protector that isn't bonded to a low-impedance ground will not conduct the surge energy away effectively — it will simply pass the energy through. The protector ground lug must connect to a building ground point or dedicated ground rod with a short, large-gauge conductor (6 AWG or heavier). In deployments with multiple outdoor antenna runs, all protector grounds must bond to the same ground reference to prevent ground potential differences between cable shields. 

For the hardware the coax connects to — gateways, APs, and the switches they connect to —secure industrial enclosures rated NEMA 4X for outdoor use provide weather protection, limit physical access, and provide the mounting surface for the protector ground bonding. The enclosure's ground lug connects to the building ground; the RF protector ground lug connects to the enclosure — ensuring the entire assembly shares a common ground reference. 

 

Device tamper protection 

IIoT devices deployed in accessible locations — on the outside of tanks, in open process areas, on utility poles — are physically accessible to anyone who can reach them. Tamper-evident seals on enclosure screws and cable connectors provide visible evidence of physical access without requiring active monitoring. For higher-consequence devices, tamper switches that generate alerts when the enclosure is opened provide the same function as the tamper switches described in the network segmentation guide — physical access becomes a logged, alertable event. 

For devices that hold key material — Wireless HART gateways, LoRa network servers, PKI infrastructure — hardware security modules (HSMs) or secure enclaves that prevent key extraction from a physically accessed device are the correct control. A gateway whose join key can be extracted by connecting a debug probe is not a gateway whose key management is secure, regardless of what network controls surround it. 

 

 Wireless IIoT Security Deployment Checklist 

This 21-item checklist covers the deployment sequence from pre-installation RF survey through ongoing operations. It's designed for field use — each item is specific enough to verify on-site, not just in documentation. 

  1. RF site survey completed — coverage, interference, and rogue AP baseline established 
    Category: RF 
    Notes: Know the RF environment before deploying. 
  1. Antenna placement optimized — minimize unintended coverage outside the facility boundary 
    Category: RF 
    Notes: Reduces external attack surface. 
  1. RF lightning protectors on all outdoor antenna coax connections 
    Category: RF 
    Notes: Gas-discharge or solid-state; rated for frequency band. 
  1. Antenna coax grounded at both ends — RF protector bonded to building/cabinet ground 
    Category: RF 
    Notes: Per IEC 61643-11, protector only works with a low-impedance ground. 
  1. WPA3-Enterprise deployed — WPA2 migrated or isolated on separate SSID 
    Category: Protocol 
    Notes: WPA2 KRACK risk eliminated. 
  1. LoRaWAN 1.1 required — LoRaWAN 1.0 devices isolated or replaced 
    Category: Protocol 
    Notes: Replay attack protection. 
  1. Zigbee 3.0 with install code commissioning — no touchlink 
    Category: Protocol 
    Notes: Prevents rogue device joining. 
  1. WirelessHART join keys changed from the factory default 
    Category: Protocol 
    Notes: Default keys are published. 
  1. EAP-TLS configured on WiFi — device certificates, not PSK 
    Category: Auth 
    Notes: No shared credentials. 
  1. BLE requires LE Secure Connections — legacy pairing disabled 
    Category: Auth 
    Notes: Eliminates BLE MITM vulnerability. 
  1. All device certificates issued from internal PKI — expiry monitored 
    Category: Auth 
    Notes: Expired certificates cause outages. 
  1. MFA enforced on all management interfaces of APs and gateways 
    Category: Auth 
    Notes: Admin access hardening. 
  1. OTA updates require valid code signature — unsigned firmware rejected 
    Category: Firmware 
    Notes: Malicious firmware prevention. 
  1. Firmware version rollback prevention enabled 
    Category: Firmware 
    Notes: Prevents downgrade attacks. 
  1. Firmware inventory tracked — CISA ICS-CERT alerts subscribed for deployed devices 
    Category: Firmware 
    Notes: Patch awareness. 
  1. Wireless OT devices on isolated VLAN — no bridge to wired OT or enterprise 
    Category: Segmentation 
    Notes: Contains wireless breach impact. 
  1. Wireless IDS/IPS active — rogue AP and anomalous protocol detection enabled 
    Category: Segmentation 
    Notes: Rogue AP and protocol anomaly visibility. 
  1. AP management VLAN is separate from OT data VLAN 
    Category: Segmentation 
    Notes: Management plane isolation. 
  1. All APs and gateways in rated, locked enclosures — tamper switches wired to alarm 
    Category: Physical 
    Notes: Walk-up access elimination. 
  1. Device tamper-evident seals applied — seal check in site visit log 
    Category: Physical 
    Notes: Physical integrity audit. 
  1. NEMA 4X enclosures are used for outdoor wireless hardware 
    Category: Physical 
    Notes: Weather and dust protection 

  

The control that most wireless IIoT deployments are missing 

Most wireless IIoT security checklists end at the protocol configuration layer — WPA3, certificates, segmentation. They don't address the coax running from an outdoor antenna into a gateway enclosure or what happens to the gateway when a summer thunderstorm hits the rooftop mount it's bolted to. 

A single lightning event on an unprotected outdoor antenna can destroy a gateway and the connected switch and create a network outage that takes hours to diagnose and replace. The fix — an inline RF protector and a proper ground bond — costs a fraction of the equipment it protects and takes 15 minutes to install. 

L-com'sRF lightning protectors are specified for industrial outdoor deployments — available in N-type, TNC, SMA, and other connector formats to match the coax termination on your gateway or AP.Secure industrial enclosures rated NEMA 4X provide the mounting and grounding surface that makes the protector work. If your wireless IIoT deployment includes outdoor antennas, these two items belong in the bill of materials before the project closes. 

  

Frequently Asked Questions 

Q1: What are the main security risks of wireless IIoT devices? 

A: The main wireless IIoT security risks are rogue access points that intercept device connections (WiFi); protocol-level vulnerabilities including WPA2 KRACK (WiFi), replay attacks on LoRaWAN 1.0, and insecure touchline commissioning on pre-ZigBee 3.0 devices; RF jamming that denies communication service; insecure over-the-air firmware updates that allow firmware replacement with malicious images; physical device tampering enabling key extraction or hardware cloning; and lightning/surge damage on outdoor antenna feeds that destroys gateway hardware.  

Q2: Is WiFi 6 secure enough for industrial IIoT? 

A: WiFi 6 (802.11ax) with WPA3. Enterprise and EAP-TLS are secure for industrial IIoT applications that require higher bandwidth — HMIs, edge computing gateways, video inspection systems, and similar devices. WPA3's key improvements over WPA2 are: Simultaneous Authentication of Equals (SAE) replacing PSK, which eliminates offline dictionary attacks on captured handshakes; protected management frames (PMF) mandatory by default, which blocks deauthentication attacks; and forward secrecy per session.  

Q3: What wireless protocol is most secure for IIoT sensors? 

A: For process sensors in industrial control environments, WirelessHART and ISA-100.11a have the strongest security models by design — both were developed specifically for industrial process automation with security as a first-class requirement. WirelessHART is the more widely deployed of the two. LoRaWAN 1.1 is appropriate for remote monitoring applications where the low data rate is acceptable and where the network server and join server are properly secured.  

Q4: Do outdoor wireless gateways need lightning protection? 

A: Yes. Any wireless gateway or access point connected to an outdoor antenna via coaxial cable requires an RF lightning protector on the coax, installed at the point where the cable enters the building or enclosure. The antenna is a metallic structure with a direct path to the outdoors — it collects transient energy from lightning and from induced surges on nearby structures.

Resources

Search Entries