As an automation system grows, giving every device its own dedicated connection can make wiring complicated and expensive. Bus cables simplify that setup by letting multiple devices share a communication line. The result is less wiring to install and maintain, with room to expand as the system changes.
PROFIBUS, CAN-Bus, DeviceNet and Modbus serve different communication needs, from process automation and vehicle electronics to building systems. The right choice depends on the protocol, the devices you're connecting and the conditions around the cable.
So how do bus cables work, and what should you look for when choosing one? Let's start with their construction and working principle, then compare common types, applications and practical selection checks.
Key Takeaways
- A bus cable connects multiple devices along one shared communication line, reducing wiring cost and complexity versus point-to-point wiring.
- Construction typically uses copper conductors (solid or stranded), PVC/PE/TPE insulation and foil or braided EMI shielding.
- Common types include PROFIBUS, CAN-Bus, DeviceNet and Modbus, each suited to different automation protocols.
- Selection factors include impedance matching, shielding, flex requirements and environmental exposure.
What Are Bus Cables?
A bus cable connects multiple devices along a shared communication pathway, known as the bus. It carries signals, power or a combination of both, depending on the system. Unlike point-to-point wiring, where every device needs a dedicated connection, a shared bus reduces the amount of wiring required. That makes complex industrial networks and building systems easier to install, expand or modify.
Bus cables carry electrical signals that let computers, printers and other peripherals share information. In manufacturing plants, data centers and office networks, that communication needs to be fast and reliable.
To keep those connections reliable, the cable needs the right conductors, insulation and protection. Here's what goes into its construction.
Construction of Bus Cables
Bus cables typically use copper conductors, either solid or stranded depending on how much flexibility is needed. PVC, PE or TPE insulation keeps the conductors electrically separated, while foil or braided shielding protects against electromagnetic interference (EMI). The outer jacket often resists oil, UV exposure or flames to suit industrial conditions. For a closer look, see choosing the right jacket material for bus cables.
Those layers protect the cable and its signals. The next question is how several devices use the same communication line.
Working Principle of Bus Cables
In a bus topology, a single communication line connects devices such as controllers, sensors and actuators. Data travels in packets, and each device checks the address to see whether a message is intended for it. Shielding helps prevent crosstalk and signal loss, supporting reliable data transfer with less complicated wiring.
That shared-line approach supports several protocols. Each has different requirements, which is why bus cables come in a range of types.
Types of Bus Cables
Several types of bus cables are used in industrial and commercial applications. PROFIBUS cables are commonly employed in process automation and manufacturing environments because of their robust shielding and ability to maintain stable data transfer over long distances. CAN-Bus cables were originally developed for automotive applications but are now widely used in industrial systems that require fast real-time communication. DeviceNet cables are designed for industrial automation, connecting sensors and actuators to PLCs with reliability in rugged environments. AS-Interface (AS-i) cables provide a simple and cost-effective networking solution for sensors and actuators in factory automation. Ethernet-based bus cables support high-speed communication and are essential for Industry 4.0 applications, robotics and real-time control.
Bus Cable Types at a Glance
Here's a side-by-side reference for common bus cable types and the systems where they're used.
| Bus Cable Type | Protocol / Standard | Typical Use Case |
|---|---|---|
| PROFIBUS | Process Field Bus (DP/FMS/FIP) | Process automation in chemical, food processing and energy plants |
| CAN-Bus | Controller Area Network | Automotive ECUs and industrial real-time control |
| DeviceNet | CIP over CAN | Connecting sensors and actuators to PLCs in rugged environments |
| Modbus | Serial / TCP communication protocol | Building automation, SCADA and general industrial monitoring |
Those differences become clearer when you look at the equipment and industries that rely on each type.
Applications of Bus Cables
Bus cables are used across industries to power modern automation and connectivity. In industrial automation and robotics they provide real-time communication between PLCs, drives and sensors. In the automotive sector CAN-Bus enables reliable communication between vehicle electronic control units. In process control PROFIBUS supports critical operations in chemical plants, food processing facilities and energy systems. Building automation also depends on bus cables for managing lighting, HVAC and security systems. In energy management bus cables are used in power plants and renewable energy facilities to ensure efficient system operation.
Across these applications, the same advantages keep coming up: simpler wiring, reliable communication and easier expansion.
Benefits of Bus Cables
Bus cables help information move reliably between networked devices, supporting performance and bandwidth. A bus topology reduces installation costs, simplifies maintenance and makes future expansion easier. Minimizing signal interference also helps keep communication clear and reduces the risk of data loss.
Getting those benefits starts with matching the cable to the system. These practical checks will help you narrow down the options.
Tips for Choosing the Right Bus Cable
- Start with impedance: the cable needs to match the system, such as 120 ohms for CAN-Bus or 150 ohms for PROFIBUS. Next, check the electrical environment. Shielding is essential near high-frequency equipment, where inadequate protection is a common cause of signal loss in bus cables, especially over longer runs. Choose a jacket that can handle the oil, UV exposure or chemicals around it, and size the conductors (AWG) for the distance and current requirements. Finally, verify compliance with the relevant UL, CSA or IEC standards.
- The choice comes down to the application: PROFIBUS for process control, CAN-Bus for automotive systems or AS-i for factory automation. Matching the cable to the protocol and environment helps keep communication reliable as the system grows.
TKD Kabel's industrial-grade solutions offer durable, standards-compliant cabling for these systems. Here's where you can explore the range and get help with selection.
About L-com
Explore the full range of TKD Kabel through L-com. We'll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com.
Still have questions about how bus cables differ or which one you need? Here are the ones that come up most often.
FAQs About Bus Cables
What is the difference between a bus cable and a standard data cable?
A standard data cable is typically wired point-to-point between two devices, while a bus cable is built to carry data along a single shared line that multiple devices tap into, each reading only the packets addressed to it. This shared-bus approach is what cuts down on wiring compared to individually connecting every device.
What types of bus cables are used in industrial automation?
The most common types are PROFIBUS, CAN-Bus, DeviceNet, AS-Interface (AS-i) and Ethernet-based bus cables, along with protocols like Modbus. Each is suited to a different mix of speed, distance and environment, from process automation to real-time robotics control.
How do I choose the right bus cable for my application?
Match the cable's impedance to your protocol (120 ohms for CAN-Bus, 150 ohms for PROFIBUS, for example), confirm shielding is adequate for the EMI environment, size the conductor for your run length and current, and verify compliance with the relevant UL, CSA or IEC standards.
Are bus cables shielded?
Most industrial bus cables include foil or braided shielding to prevent crosstalk and signal loss, and shielding becomes especially important near high-frequency equipment or on longer cable runs. Lower-EMI, short-run applications can sometimes get by with less shielding, but it's rarely worth skipping in an industrial setting.
Read Next
• Voltage and Temperature Ratings for Flexible Control Cables