L-com

Types of Industrial Bus Cables

By Eileen Harvey 

Automation is a complex interplay of various components, where seamless communication between controllers, sensors, actuators and machines is paramount. This intricate network relies on industrial bus cables, which are designed to facilitate fast, interference-free and reliable data transmission, even in the harshest of environments. These cables must withstand extreme temperatures, vibrations and exposure to chemicals, making their construction and materials crucial for maintaining signal integrity. The proper selection of bus cables not only ensures efficient operation but also minimizes the risk of equipment failures, which can lead to costly downtimes and safety hazards in industrial settings. 

Different applications within industrial automation require specific types of bus cables to meet their unique demands. For instance, PROFIBUS is widely used in process automation due to its ability to support complex network topologies and high-speed data transfer, enabling real-time monitoring and control of processes. On the other hand, CAN-Bus is predominantly utilized in automotive systems, where robust communication between different vehicle components is essential for safety and performance. Selecting the right bus cable is critical, as it can significantly impact the overall efficiency, safety and long-term performance of the automation system. 

What Are Industrial Bus Cables? 

Industrial bus cables are specialized communication cables designed to facilitate the transmission of data signals between devices within a networked automation system. These cables are essential in industrial environments where multiple components such as sensors, controllers, and actuators must communicate effectively to ensure seamless operation. Their design often incorporates robust insulation and shielding to protect against electromagnetic interference, which is common in facilities that rely on heavy machinery and electrical equipment. 

Working Principle 

Industrial bus cables function as the communication backbone of automation systems by connecting controllers, programmable logic controllers (PLCs), sensors, actuators, robots and drives. They transmit digital data signals while minimizing electrical interference. Thanks to their shielding and insulation, these cables can withstand harsh industrial environments where they may be exposed to oil, UV radiation, chemicals and mechanical stress. 

Major Types of Industrial Bus Cables 

PROFIBUS Cables 

PROFIBUS, or Process Field Bus, is one of the most widely used fieldbus systems for automation. These cables are typically constructed as one-pair shielded twisted pairs with 150-ohm or 100-ohm impedance. They are used extensively in process automation for industries such as chemical production, oil and gas, and water treatment, as well as in factory automation for applications like assembly lines and robotics. 

CAN-Bus Cables 

CAN-Bus, or Controller Area Network, is designed for robust communication in both automotive and industrial environments. These cables are usually made with one or two pairs of shielded conductors and have a standard impedance of 120 ohms. They are applied in automotive systems for engine control and diagnostics, in industrial robots, and in equipment such as elevators and conveyors. 

DeviceNet Cables 

DeviceNet is a communication protocol based on CAN-Bus but optimized for industrial automation. These cables are typically constructed with two twisted pairs, one for signal and one for power, using 24 AWG conductors for signal and 18 AWG for power. DeviceNet cables are often used to connect motor controllers, industrial sensors, actuators, and other components of factory networks. 

Fieldbus Cables 

Fieldbus is a general term used to describe digital industrial networks that replace traditional point-to-point wiring. The construction of fieldbus cables varies depending on the standard, such as FOUNDATION Fieldbus or AS-Interface. These cables are commonly found in oil and gas plants, power plants, and other large-scale process industries. 

Other Industrial Bus Cable Types 

In addition to the major categories, other bus cable types are widely used in automation. Modbus cables are common in supervisory control and data acquisition (SCADA) systems and PLC networks. EtherCAT cables support real-time Ethernet-based automation, while PROFINET cables are designed for high-speed Ethernet communication in industrial applications. 

How to Choose the Right Bus Cable 

Choosing the correct bus cable depends on several factors. The first consideration is application needs: PROFIBUS is often the best choice for large-scale industrial automation, CAN-Bus is ideal for automotive and robotics, and DeviceNet is well suited for connecting sensors and actuators. The second factor is the environment. Outdoor or chemically intensive settings require UV- and oil-resistant cables, while shielded cables are essential in areas with heavy electromagnetic interference. Finally, data rate and distance requirements must be evaluated. Higher transmission speeds require shorter distances, while longer cable runs demand cables optimized for low attenuation. 

Tips for Reliable Bus Cable Installation 

  • Avoid tight bends—follow the manufacturer’s bend radius. 
  • Ensure proper grounding to minimize EMI. 
  • Use connectors rated for industrial use. 
  • Keep power and data cables separated where possible. 
  • Regularly inspect for wear, cracks or insulation damage. 

FAQs About Industrial Bus Cables 

Q1: What is the difference between PROFIBUS and PROFINET? 
A: PROFIBUS is a fieldbus (serial communication), while PROFINET is Ethernet-based, supporting higher speeds and real-time data. 

Q2: Can I use CAN-Bus cables in place of Device Net cables? 
A: No. Although Device Net is based on CAN-Bus, it includes power conductors and follows stricter standards. 

Q3: How long can PROFIBUS cables run? 
A: Up to 1,200 meters at lower speeds (9.6 kbps), but distance decreases with higher data rates. 

Q4: Which bus cable is best for automotive applications? 
A: CAN-Bus cables are the global standard in vehicles. 

Q5: Do bus cables require special connectors? 
A: Yes, using protocol-specific connectors ensures proper impedance matching and reduces data loss. 

 

Industrial bus cables are the lifelines of modern automation. Whether it’s PROFIBUS in process plants, CAN-Bus in vehicles or Device Net in robotics, each bus cable type has unique advantages tailored to specific industries. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

 

Resources

Search Entries