By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics
Key Takeaways
- Wi-Fi 6/6E, private 5G/CBRS, LoRaWAN, ISA100.11a, and WirelessHART each solve a different problem — running one technology plant-wide usually means compromising somewhere.
- ISM-band interference is the most common reason wireless projects fail after deployment — a proper RF site survey before installation is not optional.
- The physical layer — antenna placement, RF cable quality, weatherproofing, and lightning protection — determines real-world reliability more than the wireless standard you choose.
- Private 5G on CBRS spectrum gives you lightly licensed spectrum and predictable QoS for latency-sensitive automation, but at higher upfront cost than Wi-Fi.
- LoRaWAN is the right call for low-power, low-data-rate sensor networks — not for video or control traffic.
Plant network architects are getting pressured from two directions at once. On one side: OT teams want wireless so they can move AGVs, connect handheld scanners, and stop running cable to every sensor. On the other: IT teams want something that integrates cleanly with enterprise Wi-Fi infrastructure and doesn't turn the 2.4 GHz band into a disaster. Meanwhile, vendors are pushing private 5G like it solves everything.
Here's what actually helps: understanding what each wireless technology is built for, where it breaks down, and which physical-layer details separate the plants that get reliable wireless from the ones that spend six months troubleshooting drops.
Which wireless technology is right for which factory application?
The short answer: there isn't one. Most large plants run two or three wireless technologies in parallel because the requirements for machine vision cameras, forklift tracking, and loop instrument data are just too different to satisfy with one radio standard.
|
Technology |
Typical Range |
Throughput |
Latency |
Spectrum |
Best Fit |
|
Wi-Fi 6 (802.11ax) |
Up to 300 ft indoors |
Up to 9.6 Gbps |
< 5 ms |
2.4 / 5 GHz (unlicensed) |
Machine vision, MES, mobile carts |
|
Wi-Fi 6E |
Up to 200 ft indoors |
Up to 9.6 Gbps |
< 2 ms |
6 GHz (unlicensed) |
High-density lines, AR/VR |
|
Private 5G / CBRS |
Up to 1,500 ft outdoor |
100–1,000 Mbps |
1–10 ms |
3.5 GHz (CBRS, lightly licensed) |
AGVs, wide-area coverage, SLAs |
|
LoRaWAN |
Up to 3 miles (outdoor) |
0.3–50 Kbps |
Seconds |
915 MHz ISM (unlicensed) |
Sensors, asset tracking, meter reads |
|
ISA100.11a / WirelessHART |
100–300 ft per hop (mesh) |
< 250 Kbps |
100 ms–1 s |
2.4 GHz (unlicensed) |
Process instrumentation, loop data |
These numbers are directional — actual throughput, range, and latency depend on antenna configuration, interference levels, and how many clients are sharing the spectrum. Take vendor spec sheets at face value and you'll overestimate coverage on a real factory floor by 30–50%.
What makes each technology tick?
Wi-Fi 6 and Wi-Fi 6E
Wi-Fi 6 (802.11ax) is the natural upgrade path for plants already running Wi-Fi 5. The big improvements are OFDMA, which lets a single access point serve multiple clients simultaneously instead of sequentially, and BSS Coloring, which reduces airtime wasted on collision avoidance in dense deployments. In a warehouse with dozens of scanners or a line with multiple HMI tablets, those improvements add up fast.
Wi-Fi 6E adds the 6 GHz band. That's meaningful because 6 GHz is currently uncongested — no legacy devices, no microwave interference, no Bluetooth crosstalk. The downside is shorter range and worse penetration through walls and metal equipment. For high-density production lines with short AP-to-client distances, 6E is excellent. For wide-area coverage in a large plant, it's not the right call.
Industrial access points for factory environments need IP66 or IP67 ratings at minimum, M12 connectors rather than RJ45 (which corrode), and wide operating temperature ranges. See industrial Ethernet cable assemblies and M12 industrial connectors for the physical-layer components that keep APs running in harsh conditions.
Private 5G and CBRS
Private 5G on CBRS (Citizens Broadband Radio Service, 3.5 GHz) is the option that gets the most hype and the most confusion. CBRS is a lightly licensed spectrum band in the US — you don't pay for a broadcast license, but Spectrum Access System (SAS) databases coordinate usage to protect incumbent federal users. That matters for factories: you get more predictable interference management than you do on unlicensed ISM bands.
The real advantages of private 5G over Wi-Fi are deterministic latency, built-in QoS at the radio layer, and native support for device authentication via SIM-based credentials rather than PSK or 802.1X. For AGVs on safety-critical paths or robotics that need guaranteed sub-10ms round trips, 5G NR with network slicing delivers something Wi-Fi just can't promise.
The honest downsides: upfront cost is significantly higher than Wi-Fi, you need a 5G core (which can be on-premises or cloud-hosted), and the ecosystem of 5G-connected industrial devices is still maturing. Most plants piloting private 5G today are running it alongside Wi-Fi, not replacing it.
LoRaWAN
LoRaWAN is built for one thing: connecting large numbers of low-power sensors over long distances without expensive infrastructure. A single LoRaWAN gateway can cover an entire large facility or outdoor yard. Battery-powered sensors — temperature nodes, fill-level monitors, asset trackers, vibration loggers — can run for years without a swap.
What LoRaWAN cannot do: stream data fast or handle anything time-critical. Payloads are tiny (typically under 250 bytes), duty-cycle limits on the 915 MHz ISM band mean you can't transmit continuously, and latency is measured in seconds, not milliseconds. If you're reading a thermocouple every 30 minutes, LoRaWAN is a great fit. If you're monitoring a servo motor in real time, it isn't.
ISA100.11a and WirelessHART
These are the process automation standards, and they're worth understanding separately from IT-centric wireless. WirelessHART is an extension of the HART protocol — if your plant runs HART-enabled field instruments, WirelessHART is often the path of least resistance for wireless process data. ISA100.11a (also known as ISA100 Wireless) covers similar territory with more flexibility in network design.
Both use 2.4 GHz with mesh networking and frequency hopping to work around interference. Both prioritize reliability over throughput — a WirelessHART network will retry transmissions to ensure delivery rather than drop packets and move on. That's the right tradeoff for process loop data where a missed value matters.
How do you handle spectrum conflicts and ISM-band interference?
This is where most wireless projects run into trouble. The 2.4 GHz ISM band is genuinely crowded in most industrial facilities: Wi-Fi, Bluetooth, WirelessHART, ISA100, and ZigBee all share it, plus interference from arc welders, induction heaters, and variable-frequency drives. The result, if you don't plan for it, is intermittent dropouts that are nearly impossible to diagnose without a spectrum analyzer.
A few things actually help here. First: do an RF site survey before you design the network. Walk the floor with a spectrum analyzer or a Wi-Fi analysis tool and map the interference sources. You'll find that certain areas — near welding stations, near large motors, near HVAC equipment — have noise floors that will kill 2.4 GHz performance reliably. Design around those.
Coexistence tactics worth implementing:
- Push Wi-Fi 6 clients to 5 GHz or 6 GHz where possible — leave 2.4 GHz for the legacy devices that need it.
- For WirelessHART / ISA100, verify that your gateway channels don't overlap with your Wi-Fi APs. Tools like WirelessHART network managers can help coordinate frequency hopping schedules.
- Set up CBRS / private 5G on 3.5 GHz if you have latency-sensitive automation — it keeps the critical traffic off the congested ISM bands entirely.
- For LoRaWAN at 915 MHz, check for interference from older industrial radios and point-to-point links in that band. Less common, but not zero.
Why does the physical layer make or break wireless reliability?
Wireless infrastructure fails at the physical layer more often than at the radio protocol level. A well-designed 802.11ax network with corroded connectors, improperly grounded antennas, and cheap LMR coax will underperform a mediocre 802.11ac network with solid physical installation.
Antenna selection and placement
Omnidirectional antennas are common and convenient, but they're the wrong choice in long, narrow environments like conveyor galleries or warehouse aisles. Directional antennas — sector antennas for wide-angle coverage, Yagis for point-to-point links — can dramatically improve link budget in specific geometries. Antenna gain doesn't violate EIRP limits if you reduce transmit power accordingly.
Antenna placement matters as much as type. Antennas mounted inside metal enclosures, behind steel columns, or below the level of moving equipment will underperform. Budget time during installation for antenna placement testing — walk the coverage area with a RSSI tool before you finalize positions.
RF cabling and connectors
Every foot of coaxial cable and every connector adds insertion loss. In a factory environment, that loss accumulates: water intrusion at a poorly sealed N-type connector, oxidation on an SMA fitting, a kinked run of LMR-195 between an AP and a remote antenna. Use rated industrial RF cable assemblies, weatherproof your outdoor connections, and keep cable runs as short as the installation allows.
For anything going to an outdoor antenna or across a rooftop, use rugged fiber optic cable assemblies for the backhaul run and keep RF cable segments short and sheltered. Mixing RF and fiber at the right points in the infrastructure significantly reduces signal degradation.
Lightning and surge protection
Outdoor antennas and rooftop wireless equipment need lightning protection — full stop. A single surge through an unprotected antenna feed line will take out the AP, the switch port, and potentially more downstream. Gas discharge tube arrestors inline on the coax, proper bonding of the antenna mount to building ground, and isolation of the lightning protection ground from the signal ground all matter. This is not the place to cut costs.
What should you check before buying wireless gear for a plant floor?
Industrial wireless hardware sold as 'industrial' varies more than the label implies. These are the specs worth verifying, not just scanning:
- IP Rating: IP66 minimum for dusty or washdown environments; IP67 or IP68 if any submersion risk. Check that the rating applies to the full housing, not just the chassis without connectors attached.
- Operating Temperature: Many 'industrial' APs are rated to 50°C or 60°C. If your plant has high ambient temperatures near furnaces or in outdoor enclosures, verify the actual thermal spec — and check whether that rating includes the backplane temperature under full load.
- Vibration and Shock: IEC 60068-2-6 (sinusoidal vibration) and IEC 60068-2-27 (mechanical shock) are the relevant standards. Gear near heavy stamping presses or on mobile equipment needs this verified.
- Connector Type: M12 D-coded for Ethernet in industrial environments — not RJ45. RJ45 doesn't seal against moisture and vibration loosens the connection over time.
- Power Input: PoE (802.3at or 802.3bt) is convenient, but verify your switches can source sufficient power to APs under full radio load. Some multi-radio industrial APs draw more than standard PoE+ provides.
- Radio Certifications: FCC Part 15 for unlicensed bands, FCC Part 96 for CBRS equipment. For hazardous locations (Class I Div 2 or ATEX Zone 2), verify the hazloc rating separately — it's not implied by IP rating.
- Management and Security: Check whether the AP supports WPA3, 802.1X with EAP-TLS, and whether it can be centrally managed. Isolated APs with no management plane are a security and maintenance liability.
For a broader look at when wired Ethernet is still the better call, see our comparison of Ethernet vs wireless for automation.
How L-com Helps
L-com supports Industrial Internet of Things (IIoT) infrastructure with rugged connectivity solutions designed for demanding industrial environments. From industrial Ethernet components and ruggedized cabling to fiber connectivity and edge networking support, L-com helps organizations build reliable physical-layer networks that support long-term industrial system performance and uptime.
Frequently Asked Questions (FAQs)
What is CBRS and why does it matter for private 5G?
CBRS (Citizens Broadband Radio Service) is a 150 MHz band at 3.5 GHz that the FCC opened for shared use in 2020. Unlike Wi-Fi, CBRS uses a Spectrum Access System (SAS) to coordinate users and protect federal incumbents. For factories, that means you can run private 5G on CBRS without a full licensed spectrum purchase, but with significantly better interference management than unlicensed ISM bands. Most US private 5G deployments today use CBRS.
When should I choose private 5G over Wi-Fi 6 for industrial wireless?
Private 5G makes sense when you need guaranteed, deterministic latency for safety-critical automation — AGVs, robotic arms, or remote-controlled equipment where a missed packet has real consequences. It also fits large campuses or outdoor yards where Wi-Fi's shorter range requires too many APs for cost-effective deployment. For everything else — mobile terminals, tablets, cameras, handheld scanners — Wi-Fi 6 is less expensive and easier to integrate with enterprise IT infrastructure.
Can LoRaWAN coexist with Wi-Fi in the same facility?
Yes, with some planning. LoRaWAN in North America uses 915 MHz, which doesn't overlap with Wi-Fi frequencies (2.4, 5, or 6 GHz), so there's no direct RF interference between them. The coexistence consideration is gateway placement and backhaul — LoRaWAN gateways connect to the network via Ethernet or cellular and need IP connectivity. They don't compete with Wi-Fi clients for airtime, so running both in the same building is straightforward.
What IP rating do industrial wireless access points need?
IP66 is the practical minimum for most factory floor deployments — it's rated for powerful water jets and total dust ingress protection. For outdoor mounting, washdown areas, or anywhere with pressure cleaning, IP67 or IP67 is more appropriate. IP67 means temporary immersion to 1 meter for 30 minutes, which handles most incidental water exposure. Check that the IP rating applies with the antenna connectors and cable entries sealed; an unsealed N-type port drops the effective rating.
Why do wireless projects fail after deployment?
The most common culprit is ISM-band interference that wasn't characterized before installation. A spectrum survey done during a quiet period (weekend, overnight) will miss interference from welders, induction furnaces, and other intermittent industrial sources that only run during production. Do the survey during normal production hours. The second most common failure mode is physical-layer issues: loose or corroded connectors, cable damage from forklift traffic, and antennas that were never properly aligned or sited for actual coverage in the space.