L-com

How Sensors Enable Predictive Maintenance in Manufacturing

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Predictive maintenance has become one of the most practical and measurable applications of Industrial Internet of Things (IIoT) technology. By using sensors to continuously monitor equipment condition, manufacturers can identify developing problems before they result in costly downtime, emergency repairs, or production disruptions. From vibration analysis and thermal monitoring to power quality and ultrasonic sensing, modern predictive maintenance programs provide real-time visibility into asset health, helping maintenance teams make more informed decisions and improve overall equipment reliability. 

 

 

Key Takeaways 

•   Predictive maintenance uses real-time data from industrial IoT sensors — vibration, temperature, acoustic, and current — to detect equipment degradation before it becomes an unplanned failure. 

•   Vibration analysis is the most widely deployed technique: bearing faults produce distinctive frequency signatures days or weeks before a mechanical failure stops the line. 

•   The signal chain runs from sensor to industrial wireless gateway to edge computing hardware — each layer has industrial-grade requirements that standard commercial equipment doesn't meet. 

•   A well-implemented predictive maintenance program can reduce unplanned downtime and extend equipment service life. 

•   L-com industrial IoT sensors, wireless gateways, fiber optic connectivity, and edge networking hardware provide the physical data pipeline that predictive maintenance algorithms depend on. 

  

 

Why Does Predictive Maintenance Matter in Manufacturing? 

Unplanned equipment failure is expensive in a way that scheduled downtime is not. When a motor fails mid-shift, production stops, maintenance scrambles, and the cost clock starts immediately — lost output, expedited parts, overtime labor, and sometimes downstream delays that ripple through the supply chain. [CONFIRM: industry-average unplanned downtime cost per hour — commonly cited at $260,000/hour for automotive, varies significantly by sector.] 

  

Predictive maintenance changes the economics. Instead of reacting after a failure or replacing parts on a fixed schedule regardless of actual condition, it uses continuous sensor data to detect the early signatures of degradation — and schedule repairs at a time that minimizes disruption. The maintenance team knows the bearing is failing two weeks before it does. They order the part, schedule a planned outage, and replace it before it takes the line down. 

  

This is not a new idea. Condition monitoring has existed for decades in industries like power generation and aerospace, where the cost of failure is extreme. What has changed is the cost and accessibility of the sensors, the wireless infrastructure to transmit data from the plant floor, and the analytics software to make sense of it at scale. Predictive maintenance is now practical for mid-size manufacturing facilities that could not have justified it ten years ago. 

  

 

What Is the Difference Between Predictive, Preventive, and Reactive Maintenance? 

These three approaches represent different positions on the information-cost trade-off: 

  

Approach 

Trigger 

Basis 

Typical Cost Driver 

Risk 

Reactive (run-to-failure) 

Equipment breaks 

No monitoring 

Emergency repair, downtime, collateral damage 

High — unpredictable failure timing 

Preventive (time-based) 

Fixed schedule 

Manufacturer intervals or elapsed time 

Unnecessary replacements, planned downtime 

Medium — parts replaced before failure; some over-maintained 

Predictive (condition-based) 

Sensor threshold or model alert 

Actual equipment condition 

Sensor infrastructure, analytics platform 

Low — repair when needed, before failure 

Prescriptive (AI-recommended) 

Automated recommendation 

AI analysis of sensor + operational data 

AI platform, data quality investment 

Very low — system recommends optimal action 

  

Most manufacturers operate somewhere between reactive and preventive today. Predictive maintenance is the step that requires investment in sensing infrastructure — but the ROI case is straightforward when you have cost data on a single unplanned outage. 

 

What Sensors Are Used for Predictive Maintenance? 

Different failure modes produce different physical signatures. The sensors used in predictive maintenance programs are chosen to detect those specific signatures early, before they become visible to human inspection or audible on the plant floor. 

  

Vibration Sensors 

Vibration is the most widely used measurement in rotating equipment predictive maintenance. Bearing wear, shaft imbalance, misalignment, looseness, and gear tooth damage all produce characteristic changes in vibration frequency and amplitude — often weeks before the equipment fails visibly. Accelerometers measure vibration in one, two, or three axes depending on the application. 

  

Placement matters as much as sensor selection. A vibration sensor mounted on a motor housing near the bearing captures bearing signals well; the same sensor mounted further from the bearing point picks up structural noise that obscures the signal. Industrial accelerometers are rated for temperature ranges, shock levels, and IP protection appropriate to the installation environment.  

 

Temperature Sensors 

Abnormal heat is a symptom of friction, electrical resistance, cooling failure, and overloading — all of which precede equipment failure. RTDs (resistance temperature detectors) and thermocouples measure contact temperature at specific points; infrared sensors measure surface temperature without contact, useful for electrical panels, conveyor bearings, and rotating equipment where wired connections are impractical. 

  

Temperature monitoring is particularly effective for electrical systems — motors drawing excess current heat up predictably before they fail. Thermal imaging cameras, used in periodic walk-down surveys or mounted at fixed points, identify hot spots in switchgear, transformers, and drive cabinets that precede insulation failure. 

 

Current and Power Quality Sensors 

Motor current signature analysis (MCSA) detects mechanical and electrical faults through the current waveform drawn by the motor. A motor with a developing bearing fault, rotor bar damage, or mechanical load increase draws current with a specific frequency signature that differs from healthy operation. Current transducers installed on the motor supply leads capture this data non-invasively — no mechanical attachment to the motor required. 

  

This makes current-based monitoring particularly practical for retrofitting existing equipment: the sensor goes on the cable, not on the machine. 

 

Ultrasonic Sensors 

Ultrasonic detection identifies the high-frequency sound signatures produced by air/gas leaks, cavitation in pumps, arcing in electrical equipment, and bearing lubrication problems. Healthy bearings produce a consistent ultrasonic signature; under-lubricated or worn bearings produce detectable changes. Ultrasonic monitoring can identify bearing lubrication problems before they progress to temperature increases — making it an earlier warning than thermal monitoring for this specific failure mode. 

 

Pressure and Flow Sensors 

In fluid systems — hydraulics, compressed air, cooling water, and process fluids — pressure and flow monitoring detects leaks, blockages, pump wear, and valve degradation. A pump losing efficiency shows in a declining flow rate at the same drive speed; a developing leak shows in falling system pressure. These sensors are particularly valuable in facilities where fluid system failures affect multiple downstream processes. 

 

Oil Quality Sensors 

For gearboxes, compressors, and hydraulic systems, in-line oil quality sensors monitor viscosity, water contamination, particle count, and acid number — all indicators of lubricant breakdown or internal wear. Oil analysis has traditionally required sending samples to a lab; inline sensors make it continuous and real-time. 

  

How Does Vibration Analysis Actually Predict Equipment Failure? 

A healthy rotating component produces a consistent vibration pattern. When something changes — a bearing race starts to pit, a shaft develops a slight imbalance, or a gear tooth chips the vibration pattern changes in specific, measurable ways. Vibration analysis works by capturing that pattern continuously and comparing it to a baseline. 

  

The analysis techniques build on each other in complexity: 

  

•   Overall vibration level (RMS): the simplest measure; rising overall vibration indicates something is changing, but does not identify what 

•   Frequency spectrum analysis (FFT) breaks the vibration signal into its component frequencies; different faults produce characteristic frequency signatures (e.g., bearing outer race defects produce signals at a calculable frequency based on bearing geometry and rotation speed) 

•   Time waveform analysis  looks at the vibration signal over time rather than as a frequency snapshot; it is useful for identifying impacting, looseness, and cavitation 

•   Envelope analysis  filters the vibration signal to isolate high-frequency impacts from bearing defects, which is particularly effective for early-stage bearing damage 

•   Machine learning models  trained on historical vibration data labeled with known failure events identify complex multi-variable patterns that rule-based thresholds miss 

  

The progression from overall level monitoring to ML-based analysis represents increasing sophistication — and increasing dependence on data quality. A machine learning model trained on vibration data from sensors with high electrical noise, poor mounting, or inconsistent sampling rates will produce unreliable predictions. The hardware foundation determines the ceiling for analytical sophistication. 

 

What Physical Infrastructure Does Predictive Maintenance Require? 

This is the part most predictive maintenance guides skip over. Software platforms and analytics dashboards get the attention, but the infrastructure that delivers sensor data reliably to those systems is what actually determines whether a predictive maintenance program works. 

  

Industrial-Grade Sensors 

The operating environment dictates sensor specifications. A vibration sensor on a motor in a washdown area needs IP67 or IP68 protection. A temperature sensor near a furnace needs a high-temperature rating. A sensor in a motor control cabinet needs EMI shielding rated for the electrical noise environment. Using commercial-grade sensors in industrial conditions produces faster calibration drift, higher failure rates, and noisier data, each of which degrades prediction accuracy. L-com's industrial IoT sensor catalogue covers these environmental requirements: temperature, IP rating, vibration resistance, and electromagnetic compatibility appropriate for plant floor deployment. 

  

Wireless Gateways and Network Infrastructure 

Sensors generate data continuously. That data needs a reliable path to an edge computing device or cloud analytics platform. Industrial wireless gateways aggregate signals from multiple sensors, often using legacy field protocols like Modbus RTU, HART, or 4-20mA – translate them to IP – and transmit over Wi-Fi or cellular. In environments with heavy electromagnetic interference from motors and drives, the gateway's EMI tolerance and antenna design determine whether data transmission is reliable or intermittent. 

  

Intermittent data is a specific problem for predictive maintenance: a model that misses 15% of readings due to network dropout cannot reliably distinguish a developing fault from a data gap. Industrial wireless gateways designed for plant floor environments maintain transmission reliability in conditions where consumer-grade Wi-Fi fails consistently. 

  

Cabling and Physical Connectivity 

For wired sensor installations, which remain preferable in high-noise environments or for high-sample-rate vibration sensors, shielded industrial cabling prevents electrical interference from corrupting analogue signals. For high-bandwidth applications like continuous vibration analysis across many sensors, fibre optic backbone connections between plant zones provide interference-free, high-capacity data transport. 

  

The cable routing and grounding practices in the installation matter as much as the cable specification. A shielded cable grounded at both ends in a motor-heavy environment can actually pick up more noise than one grounded at one end. Industrial connectivity design is a discipline, not an afterthought. 

  

How Do You Build a Sensor-Based Predictive Maintenance Program? 

Most failed predictive maintenance programs tried to instrument everything at once, collected enormous volumes of mediocre data, and found the analytics platform couldn't extract reliable predictions from it. A practical approach starts narrow. 

 

Step 1: Identify the highest-cost failure target 

Start with one asset where unplanned failure is expensive: a critical motor, a pump with a history of failures, or a compressor where downtime halts multiple downstream processes. Calculate what an unplanned outage on that asset actually costs — parts, labor, lost production, and expedited shipping. That number is the ROI denominator. 

 

Step 2: Identify the failure modes and matching sensors 

For a motor-driven pump, the relevant failure modes are bearing wear, shaft imbalance, coupling misalignment, seal failure, and impeller cavitation. Each has a matching sensor: vibration for bearing and imbalance issues, temperature for seal and overload indicators, pressure and flow for cavitation. You do not need every sensor from day one — start with the failure modes most common in your specific equipment. 

 

Step 3: Assess and build the connectivity path 

Before installing sensors, verify the network can carry the data. Is there industrial Wi-Fi coverage at the sensor locations? Is there a gateway nearby, or does one need to be installed? Is the bandwidth sufficient for the planned sensor sample rates? Addressing connectivity gaps before sensor installation avoids the common situation where sensors are installed, but data transmission is unreliable. 

 

Step 4: Establish a baseline under known-good conditions 

Run the sensor system for 4–8 weeks before attempting any predictions. The baseline — the vibration signature, temperature range, and current draw — under normal operating conditions is the reference point for everything that follows. An alert threshold set without a baseline is a guess; a threshold set relative to a well-established baseline is a decision. 

 

Step 5: Set alert thresholds and then refine them 

Initial thresholds based on the baseline will generate false positives. That is expected. The goal in the first three months is not perfect prediction — it is learning which sensor signatures in your specific equipment correlate with actual problems. Each false positive and each confirmed fault is training data for more accurate thresholds. 

 

Step 6: Measure and document outcomes 

Track: alerts generated, alerts that led to planned maintenance, alerts that were false positives, unplanned failures that were not predicted, planned versus unplanned maintenance hours, and parts cost. This data is the ROI case for expanding the program — and the diagnostic information for improving sensor placement or threshold calibration. 

  

Step 7: Scale from evidence 

Once the pilot asset shows measurable improvement in maintenance outcomes, the business case for expansion is concrete rather than theoretical. The lessons from the first installation — sensor placement, gateway configuration, threshold tuning — accelerate every subsequent deployment. 

  

What ROI Can Manufacturers Expect from Predictive Maintenance? 

The categories of return are consistent across industries: 

  

•   Unplanned downtime reduction is the highest-value category; a single avoided failure on a critical asset frequently pays for the entire sensor installation 

•   Planned maintenance optimization — maintenance is performed when the equipment needs it, not on a calendar; parts that would have been replaced prematurely are not, and parts that were being run too long are caught 

•   Maintenance labor efficiency technicians work on identified problems with parts on hand, rather than responding to emergencies with uncertain diagnosis and parts availability 

•   Equipment life extension, catching and correcting developing problems before they cause secondary damage (a failed bearing that damages a shaft, for example) extends asset life 

•   Energy efficiency  equipment running with developing faults often draws more current; correcting mechanical problems reduces energy consumption 

  

The payback period for sensor infrastructure on a well-chosen target asset is typically measured in months, not years. The asset selection matters: predictive maintenance on a $500/day asset with infrequent failures has a very different payback than on a $50,000/hour production bottleneck. 

  

How Do You Choose the Right Sensors for Your Predictive Maintenance Program? 

Sensor selection is a specification exercise, not a catalogue exercise. The right sensor for a given application depends on five factors: 

  

•   The failure mode: what physical phenomenon are you measuring? Vibration sensors for rotating equipment faults, temperature sensors for thermal anomalies, and current sensors for electrical and mechanical load changes. 

•   The operating environment temperature range, moisture exposure, chemical exposure, electromagnetic interference, and physical vibration all constrain which sensor designs are appropriate. An IP67 enclosure rating for washdown areas, a temperature specification that covers the operating range plus 20% margin. 

•   The mounting location where the sensor attaches relative to the failure source affects signal quality significantly. A vibration sensor on a rigid, flat surface on the bearing housing captures bearing signals far better than one on a flexible bracket several inches away. 

•   The sample rate and data volume for high-frequency vibration analysis for early bearing fault detection require sample rates of 5–20 kHz. Slower-changing measurements like temperature or flow can be sampled far less frequently. Sample rate affects sensor cost, data storage requirements, and network bandwidth. 

•   The connectivity path wireless sensors require sufficient network coverage at the mounting location; wired sensors require cable routing that avoids interference sources. 

  

When in doubt on specifications, err toward industrial-grade ratings rather than the minimum that covers current conditions. Sensors in manufacturing environments face years of thermal cycling, vibration, cleaning chemicals, and airborne contamination. A sensor rated for the conditions with a margin lasts significantly longer than one rated exactly to the edge of the operating envelope. 

  

  

What makes industrial IoT sensors different from standard sensors?  

A factory floor has vibration that loosens standard connections. Temperature swings that drift commercial sensor calibration. Coolant and cutting fluid that ingress through inadequate seals. Electromagnetic interference from variable-frequency drives, welders, and motors that corrupts sensor output on inadequately shielded hardware. Physical impact from forklifts and dropped tooling. 

  

Commercial sensors survive office environments. Industrial IoT sensors are specified for: 

•   IP67 or IP69K ingress protection — sealed against dust and high-pressure washdown 

•   Operating temperature ranges of -40°C to +85°C or beyond 

•   EMC ratings that maintain accuracy in the presence of industrial electromagnetic interference 

•   Vibration and shock resistance to IEC 60068 standards 

•   MTBF specifications measured in years, not months, under continuous industrial operation 

  

A sensor that drifts in six months or fails in eighteen doesn't pay back the predictive maintenance investment, and worse, a sensor that gives inaccurate readings without failing visibly destroys operator trust in the entire system. L-com's Industrial IoT Sensors are built to the specifications that industrial deployments require, not commercial hardware with an 'industrial' label. 

  

How does wireless connectivity fit into the sensor data pipeline? 

Most predictive maintenance sensors communicate wirelessly — running cable to every monitored bearing, motor, and pump in a large facility isn't practical. But standard Wi-Fi infrastructure fails in factory environments in ways that aren't always obvious until data gaps start appearing in the monitoring platform. The problems are predictable: The 2.4GHz and 5GHz bands are congested by motor drives and welding equipment. Steel structures and dense machinery create multipath propagation and dead zones. Access points not rated for operating temperatures near furnaces or in outdoor yard equipment areas. Sensors on moving equipment, conveyors, AGVs, and robotic arms create constantly changing signal paths. 

  

Industrial wireless gateways address these conditions directly: hardened radios, industrial antenna designs, interference mitigation, and operating temperature ratings that match the environment rather than the IT closet. A data gap in a predictive maintenance feed is exactly when you might miss the anomaly that precedes a failure — the gateway is not the place to accept consumer-grade specifications. 

For backbone connectivity between monitoring nodes, control rooms, and analytics platforms, Fiber Optic Connectivity Solutions provide EMI-immune, high-bandwidth runs that copper cabling picks up noise on near welders and large motor drives. Fiber is the right choice for any run that crosses electrical equipment or runs longer than standard Ethernet distances. 

 

Building Resilient Industrial Networks 

Reliable industrial security depends on more than firewall rules and network segmentation. The underlying physical infrastructure must be designed to support continuous operation in demanding environments. From industrial Ethernet and fiber connectivity to wireless networking and ruggedized connectivity solutions, L-com helps organizations build resilient industrial networks that support security, reliability, and long-term operational performance. 

  

 

Frequently Asked Questions (FAQs) 

What is predictive maintenance in manufacturing? 
Predictive maintenance uses sensor data to monitor equipment condition and identify signs of degradation before a failure occurs. The goal is to schedule maintenance based on actual equipment health rather than fixed service intervals or unexpected breakdowns. 

 

What sensors are commonly used for predictive maintenance? 
The most common predictive maintenance sensors include vibration sensors, temperature sensors, current and power monitoring sensors, ultrasonic sensors, and pressure or flow sensors. The right sensor depends on the equipment being monitored and the failure modes being targeted. 

 

How does predictive maintenance reduce downtime? 
By detecting early warning signs of equipment problems, predictive maintenance allows maintenance teams to plan repairs before failures occur. This helps avoid unplanned outages, reduces emergency maintenance activity, and minimizes disruptions to production schedules. 

 

Can predictive maintenance be added to existing equipment? 
Yes. Many predictive maintenance programs begin by retrofitting sensors onto existing motors, pumps, gearboxes, compressors, and other critical assets. This allows manufacturers to improve visibility into equipment health without replacing existing machinery. 

 

Resources

Search Entries