L-com

How to Secure Remote Industrial Sites

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

   

Key Takeaway 

• Remote industrial sites — substations, pumping stations, remote manufacturing cells, oil and gas facilities — are harder to secure than main facilities because physical access is limited and IT support is often absent. 

• The most exploited weaknesses at remote sites are flat (unsegmented) networks, default credentials on field devices, unencrypted remote access, and hardware not rated for the physical environment. 

• Effective security at remote sites requires both OT-specific software controls (network segmentation, secure remote access, and anomaly detection) and the right physical hardware (ruggedised gateways, hardened enclosures, and cellular failover). 

• Industrial wireless gateways with built-in firewall and VPN capabilities are the single most impactful hardware investment for most remote OT sites. 

• A security posture that works fine at a main facility will often fail at a remote site — the implementation assumptions are different. 

  

Remote industrial sites are a different problem from securing a main plant or a corporate office. There's no IT team on site. Physical access is infrequent — sometimes monthly, sometimes less. The equipment running those sites was often installed years before anyone started worrying about OT cybersecurity. And the consequences of a failure aren't just data loss: they're production stoppages, safety incidents, and, in critical infrastructure, potentially much worse.  

 

Why Are Remote Industrial Sites Harder to Secure Than Main Facilities? 

Remote sites concentrate every challenge that makes OT security difficult — and add a few more. 

 

No Permanent IT or OT Staff On-Site 

At a main facility, someone notices when a device behaves strangely. At a remote pumping station or substation, anomalies can persist for weeks before anyone visits. The detection window for breaches at remote sites is substantially longer than at staffed facilities. This matters because dwell time — the period between initial compromise and detection — is what allows attackers to escalate privileges, move laterally, and establish persistence. A short dwell time limits the damage a breach can do. A long one doesn't. 

  

Legacy Equipment With No Security Baseline 

Remote industrial sites often run equipment that was installed before industrial cybersecurity was a design consideration. PLCs, RTUs, and HMIs from the 1990s and early 2000s were designed for reliability and operator accessibility — not for defense against networked threats. Default credentials. Unencrypted protocols. No patch mechanism. No logging. 

You can't always replace this equipment on a short timeline. A remote substation might run 20-year-old RTUs that control critical infrastructure. The answer isn't always 'rip and replace' – it's layering compensating controls around the legacy equipment. 

 

 Connectivity That Creates Exposure 

Remote sites need to communicate. Operators need to monitor them. Maintenance teams need to access them remotely. That connectivity — cellular links, satellite, MPLS, VPN tunnels — is also an attack surface. Every remote access path is a potential entry point if it isn't properly controlled. 

The common failure mode is an IT team that sets up a VPN tunnel to a remote site for operational convenience, without considering what OT devices that tunnel now exposes. A properly segmented remote site with controlled remote access is very different from a flat network with a wide-open tunnel. 

 

Physical Security Is Often Minimal 

Remote sites typically have a locked enclosure and not much else. No security cameras. No badge access control. In some cases, physical access is easier than you'd expect — especially for sites in rural or industrial areas where the 'security' is geographic isolation rather than engineered controls. 

Physical access to a device is often the most direct path to compromise. Someone with physical access to a cellular gateway or an RTU can reset it, replace firmware, or install a hardware implant. Physical security isn't a soft requirement at remote sites — it's part of the OT security stack.  

 

What Are the Most Common Security Weaknesses at Remote Industrial Sites? 

Based on OT security incident reports from ICS-CERT and industry researchers, the same weaknesses appear repeatedly at remote sites: 

  

Weakness 

Why It Matters at Remote Sites 

Default or shared credentials on field devices 

No one on site to notice unauthorized access; default credentials are widely known and rarely changed after deployment 

Flat network topology (no OT/IT segmentation) 

A single breach can traverse the entire site network; there's no boundary between control systems and internet-connected equipment 

Unencrypted remote access (Telnet, HTTP, RDP without MFA) 

Remote access is necessary for operations; unencrypted or unauthenticated access is an open door 

No anomaly detection or logging 

Without logs, breaches go undetected; without baselines, anomalies aren't visible 

Hardware not rated for the physical environment 

Equipment failures cause forced remote access or site visits, which expand the attack surface and increase response time 

Missing firmware patches on PLCs and RTUs 

Legacy OT devices often have known vulnerabilities; patch cycles are long and patching is operationally disruptive 

No physical access controls beyond a padlock 

Physical access to a device defeats most software-layer security controls 

  

How Do You Segment an OT Network at a Remote Site? 

Network segmentation is the most impactful security control you can implement at a remote industrial site. It means separating OT devices (PLCs, RTUs, sensors, HMIs) from IT systems (corporate WAN, internet access, business applications) with a defined, monitored boundary. 

At a remote site, the architecture typically looks like this: 

The Three Zones of a Segmented Remote OT Site 

•       Zone 1 — OT/Control Network: PLCs, RTUs, SCADA servers, HMIs, field devices. No direct internet connectivity. Communication out of this zone goes only through the DMZ. 

•       Zone 2 — DMZ (Demilitarized Zone): The buffer between OT and IT. Historian servers, data diodes, and the industrial wireless gateway with firewall capability live here. Data flows in defined directions — not freely between zones. 

•       Zone 3 — IT/WAN: Corporate network, internet, remote access infrastructure. This zone does not directly communicate with Zone 1. 

  

The industrial wireless gateway at the OT/IT boundary is where the security controls are enforced. It needs to support VLAN segmentation, stateful packet inspection, and VPN termination. A consumer-grade router in a weatherproof box does not meet this requirement. An industrial-rated gateway with the right feature set does. L-com's industrial wireless gateways are designed for exactly this boundary role — ruggedized for harsh environments, with built-in firewall and VPN capabilities appropriate for OT network segmentation. 

 

How Do You Implement Secure Remote Access for OT? 

Remote access to OT systems is operationally necessary and one of the most exploited attack vectors in industrial incidents. The two aren't in conflict — but the implementation requirements are specific. 

 

What Secure Remote Access for OT Actually Requires 

•       Multi-factor authentication (MFA) on every remote access session — not just username and password. Hardware tokens or authenticator apps are standard; SMS-based MFA is better than nothing but considered weak. 

•       Role-based access control. A field technician doing routine maintenance doesn't need the same access level as a controls engineer modifying logic. Separate credentials, separate permissions. 

•       Session recording and logging. Every remote session into an OT environment should be logged — who accessed, when, what commands were executed, what changed. This is both a security control and an audit requirement in many regulated industries. 

•       Just-in-time access (JIT). Rather than leaving remote access paths open continuously, JIT systems activate access only when a request is approved, then close it afterward. This shrinks the window of exposure to minutes rather than months. 

•       Dedicated OT remote access infrastructure. General-purpose IT VPN solutions aren't designed for OT protocols or for environments where a session drop causes a control problem. Purpose-built OT remote access platforms (Claroty xDome, Tosibox, Secomea) handle OT-specific requirements better. 

 

 

Cellular Failover and Out-of-Band Management 

Primary WAN connectivity at remote sites can fail — and when it does, you lose both visibility and control. Cellular failover provides a secondary path for monitoring and emergency access when the primary link is down. Out-of-band management — a separate, dedicated management network for accessing devices when the production network is unavailable or compromised — is standard practice at well-secured remote sites. Industrial gateways with dual-SIM cellular support are common for this purpose. 

One practical note: cellular bands vary by geography. A gateway specified for a North American site won't necessarily work for a facility in another region without verifying band compatibility. This is a hardware selection detail that gets missed when purchasing is driven by IT rather than operations. 

What Hardware Does a Secure Remote Industrial Site Need? 

Software controls without the right hardware don't hold up in industrial environments. Here's what a well-secured remote site typically requires: 

  

Hardware Category 

Security Function 

Key Specification Requirements 

Industrial wireless gateway 

OT/IT boundary enforcement, firewall, VPN termination, VLAN segmentation 

Ruggedized (wide temp range, IP-rated enclosure), firewall + VPN support, dual-WAN or cellular failover, DIN-rail mount 

Cellular router / modem 

Primary or failover WAN connectivity; out-of-band management path 

Multi-band LTE/5G, dual-SIM support, industrial temp rating, watchdog/auto-recovery 

Industrial IoT sensors 

Environmental monitoring, tamper detection, physical security alerting 

Rated for ambient conditions (temperature, humidity, IP67/IP68 for outdoor), tamper-evident housing 

Fiber optic cabling 

High-speed, interference-immune backbone for inter-enclosure runs 

Single mode for longer runs; rated for burial or conduit; armored jacket for physical durability 

Hardened enclosures 

Physical protection for electronics in harsh environments 

NEMA 4/4X for outdoor/wet environments; locking hardware; ventilation or cooling if needed 

Managed industrial switch 

Network segmentation within the OT zone; VLAN support; port security 

DIN-rail, wide temp rating, VLAN/802.1X support, port-disable capability 

UPS / power conditioning 

Maintains operation through power events; prevents hardware damage 

Industrial-rated, wide input voltage range, battery backup sized for site response time 

  

How Do You Monitor a Remote Industrial Site for Security Threats? 

You can't respond to threats you can't see. Monitoring a remote OT site is harder than monitoring a main facility — but it's not impossible with the right architecture. 

 

Passive Network Monitoring for OT 

Passive OT network monitoring tools (Claroty, Nozomi Networks, and Dragos) analyze network traffic without actively probing devices — important in OT environments where active scanning can disrupt control systems. They establish a baseline of normal communication patterns and alert on deviations: a PLC that suddenly starts communicating with an unknown IP address, a device sending traffic at unusual hours, or a protocol used on a port it shouldn't be on. 

At remote sites, a lightweight sensor deployed on a SPAN port of the industrial switch sends traffic copies to a centralized analysis platform. The sensor itself has no active presence on the OT network. 

 

Syslog and Event Forwarding 

Every device at the remote site that can generate logs should be configured to forward them to a centralized SIEM or log management platform. Industrial gateways, managed switches, and any Windows-based HMIs all support syslog or Windows Event Forwarding. This creates the audit trail needed to detect and investigate incidents. 

The challenge at remote sites is bandwidth. Sending raw syslog from every device over a cellular link is expensive and slow. Edge filtering — forwarding only events above a threshold, or pre-processing logs at a local aggregator before forwarding summaries — is the standard approach. 

  

Physical Intrusion Detection 

Door contacts, motion sensors, and tamper-evident hardware are the physical layer of remote site monitoring. When a door contact on an enclosure trigger, or a tamper seal on a device is broken, that event should flow into the same alerting system as network anomalies. 

Industrial-rated sensors for environmental monitoring and physical intrusion detection are available in configurations suitable for outdoor enclosures, harsh temperatures, and low-power installations typical of remote sites. 

 

What Does a Remote Site Security Implementation Look Like in Practice? 

A mid-size energy company manages 40 remote pumping stations spread across a 500-mile pipeline corridor. Each station has a PLC, an HMI, and a cellular connection to the SCADA system at the main operations center. Before a security hardening project, the architecture looked like this: flat network, default PLC credentials unchanged from installation, RDP open to the corporate VPN, no logging, consumer-grade cellular routers in weatherproof boxes. 

After the project: 

•       Industrial gateways with firewall capability replaced consumer routers at each station, enforcing a defined OT/IT boundary. 

•       All remote access moved to a purpose-built OT remote access platform with MFA and session recording. 

•       PLC credentials were updated and documented in a privileged access management (PAM) system. 

•       Passive network monitoring sensors were deployed at each station, forwarding alerts to the central SOC. 

•       Cellular failover was added for out-of-band management access. 

The project took 14 months across 40 sites. The first incident caught by the new monitoring system — an unauthorized login attempt on an HMI at a remote station — was detected within 20 minutes of occurrence. Previously, it would have gone unnoticed.  

 

Building Resilient Industrial Networks 

Reliable industrial security depends on more than firewall rules and network segmentation. The underlying physical infrastructure must be designed to support continuous operation in demanding environments. From industrial Ethernet and fiber connectivity to wireless networking and ruggedized connectivity solutions, L-com helps organizations build resilient industrial networks that support security, reliability, and long-term operational performance. 

 

Frequently Asked Questions (FAQs) 

 

What is OT security? 

OT security (operational technology security) is the practice of protecting the hardware and software that monitors and controls physical industrial processes — PLCs, RTUs, SCADA systems, DCS, HMIs, and the networks that connect them.  

 

How is securing a remote industrial site different from securing a main facility? 

A: Main facilities have IT staff on site, physical security infrastructure, and network infrastructure designed for scale. Remote sites have none of these. The security architecture has to work without on-site staff, survive harsh physical conditions, operate over constrained WAN links, and support remote management without creating the vulnerabilities that remote access typically introduces.  

 

What happens when a remote industrial site is breached? 

The consequences depend on what the site controls. At a minimum, an attacker with access to a remote OT network can disrupt production, steal process data, or use the site as a pivot point to reach the main facility.

Resources

Search Entries