L-com

How PROFIBUS Cables Power Smart Factories

By Eileen Harvey 

The rise of Industry 4.0 has ushered in a new era of manufacturing, transforming traditional production methods into highly interconnected and intelligent environments, often referred to as smart factories. In these modern facilities, advanced technologies such as the Internet of Things (IoT), artificial intelligence and big data analytics converge to create a seamless flow of information. This interconnectedness allows machines, sensors and control systems to communicate effortlessly, resulting in heightened efficiency, increased productivity and enhanced flexibility.  

At the core of this extensive connectivity are PROFIBUS cables, which play a crucial role in the communication networks that underpin industrial automation systems. These specialized bus cables are designed to facilitate real-time data exchange between various devices, ensuring that information flows smoothly and reliably throughout the manufacturing process.  

What Are PROFIBUS Cables? 

PROFIBUS (Process Field Bus) is an international communication standard (IEC 61158/61784) widely used in automation systems. PROFIBUS cables are the physical medium that connects controllers, sensors and actuators in distributed industrial networks. 

There are two main types. First, there is PROFIBUS DP (Decentralized Peripherals), which is high-speed data communication for factory automation. For example, TKD Kabel’s PROFIBUS DP cable offers 150-ohm impedance, double shielding and high durability, making it ideal for robust factory environments. 

Second, there is PROFIBUS PA (Process Automation), designed for hazardous environments and often used in industries like oil, gas and chemicals. 

Why PROFIBUS Is Vital for Smart Factories 

Smart factories rely on real-time communication, seamless interoperability and fault-free signal integrity. PROFIBUS cables deliver these benefits in several ways. They ensure seamless communication between controllers, PLCs, HMIs and sensors. They provide reliability even in harsh industrial conditions like EMI-heavy environments. They enable real-time monitoring, predictive maintenance and faster decision-making. And finally, they support scalable systems, from small production lines to complex manufacturing plants. 

Anatomy of a PROFIBUS Cable 

PROFIBUS cable is carefully engineered to ensure high signal integrity and strong noise immunity. At its core are the conductors typically made of solid or stranded copper which provide efficient data transfer. These are surrounded by insulation which keeps the conductors separated and reduces crosstalk. To further enhance performance shielding is applied—usually in the form of foil or braided shields that protect the signal from electromagnetic interference (EMI). In particularly noisy environments double-shielded PROFIBUS DP cables are often recommended. An example is Double-shielded PROFIBUS DP cable. 

Another critical aspect is impedance control with typical values of 150 Ω for DP networks and 100 Ω for PA networks which helps maintain signal quality. Finally, jacket materials such as PVC, PE or PUR provide durability, flexibility, resistance to oils and protection from UV exposure depending on the application environment. 

Key Benefits of PROFIBUS in Smart Factories 

One of the biggest advantages of PROFIBUS is its scalability as it can support thousands of devices within a single network, making it suitable for both small operations and large-scale automation systems. Another key strength is interoperability since the protocol is vendor-independent and allows devices from different manufacturers to communicate seamlessly. PROFIBUS also delivers high efficiency with fast data transmission speeds that minimize downtime and improve throughput. Additionally, it offers strong cost-effectiveness thanks to durable cable designs such as UV- and oil-resistant variants which help reduce maintenance and replacement costs.  

Applications of PROFIBUS Cables in Smart Factories 

PROFIBUS is widely used across diverse industries. In automotive manufacturing PROFIBUS DP connects robots, sensors and PLCs to enable precise and efficient assembly. Within process industries such as oil and gas, chemicals and pharmaceuticals, PROFIBUS PA is especially valued for safe communication in hazardous and potentially explosive environments. In the food and beverage sector PROFIBUS supports hygienic automation systems where downtime could significantly disrupt production and supply chains. Meanwhile, in packaging and logistics PROFIBUS-powered conveyors and sorting systems ensure efficient warehouse operations. In many smart factories PROFIBUS operates alongside CAN-Bus and other Fieldbus cables integrating into multi-network environments. For example, CAN-Bus and Fieldbus cables often integrate alongside PROFIBUS in multi-network smart factories. 

Challenges and Considerations 

Despite its advantages, using PROFIBUS requires attention to certain challenges. Cable length and signal loss can become issues as PROFIBUS DP supports distances of up to 1,200 meters depending on baud rate, after which repeaters may be required. Shielding and grounding are also critical—improper shielding can lead to EMI problems making double-shielded cables the preferred choice in high-noise environments. Environmental conditions must be considered as well; facilities exposed to sunlight, oil or harsh chemicals should select UV- and oil-resistant cables for long-term reliability. Finally, integration with industrial Ethernet is an ongoing consideration: while PROFINET and Ethernet are increasingly common, PROFIBUS remains essential for legacy systems and hybrid networks. 

The Future of PROFIBUS in Smart Manufacturing 

Although newer protocols such as PROFINET and Industrial Ethernet are gaining traction, PROFIBUS continues to play a vital role in modern factories. Its established global infrastructure, compatibility in hybrid networks and relevance in predictive maintenance and Industrial IoT ensure its continued use. As smart factories evolve, PROFIBUS will act as a bridge technology helping integrate legacy systems with next-generation networks. 

Tips for Choosing the Right PROFIBUS Cable 

When selecting a PROFIBUS cable, it is important to match impedance with the network type—150 Ω for DP or 100 Ω for PA. In high-EMI zones, shielding should be prioritized with double-shielded cables offering the best protection. The environment must also guide selection: UV- and oil-resistant jackets are necessary for outdoor or industrial applications. Finally, sourcing cables from trusted brands ensures long-term reliability and proven performance in demanding conditions. 

Interesting Facts About PROFIBUS 

Today more than 60 million devices operate on PROFIBUS networks worldwide. Each segment supports up to 32 devices without repeaters, making it both versatile and robust. Interestingly, around 80% of PROFIBUS failures are traced back to improper cable termination, which highlights the importance of correct installation practices. Despite being over 30 years old, PROFIBUS remains an integral technology in smart factories across industries such as automotive, food and energy. 

Recommendations 

If you are designing or upgrading a smart factory network: 

  1. Use PROFIBUS DP for high-speed automation. 
  1. Choose PROFIBUS PA for hazardous environments. 
  1. Combine PROFIBUS with PROFINET for future-ready hybrid systems. 
  1. Always invest in premium industrial-grade cables such as TKD Kabel to minimize downtime. 

 

FAQs (Frequently Asked Questions) 

Q1: What is the maximum cable length for PROFIBUS?  
A: Up to 1,200 meters, depending on baud rate. 

Q2: Can PROFIBUS work with Ethernet-based systems?  
A: Yes, hybrid systems integrate PROFIBUS with PROFINET. 

Q3: Why is shielding important in PROFIBUS cables?  
A: To prevent EMI from affecting signal quality, especially in heavy industrial environments. 

Q4: How do I choose between PROFIBUS DP and PA?  
A:  Use DP for factory automation (fast speed) and PA for hazardous process industries. 

Q5: Are TKD Kabel PROFIBUS cables suitable for harsh environments?  
A: Yes, many come with oil, UV and chemical resistance for industrial durability. 

 

PROFIBUS cables are the backbone of smart factories, enabling reliable, high-speed and real-time communication across industrial automation systems. From automotive to pharmaceuticals, they ensure efficiency, scalability and safety. 

By choosing trusted solutions like TKD Kabel’s industrial-grade PROFIBUS cables, factories can future-proof their networks and stay competitive in the era of Industry 4.0. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries