By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics
Power over Ethernet (PoE) sends DC power and data down the same twisted-pair cable, so an access point, camera or sensor needs one cable run instead of a data drop plus a nearby outlet. In a data center, the power side is what causes trouble: higher-wattage PoE pushes more current through thin copper, and hundreds of those cables sharing a tray get warm.
This guide walks through the IEEE 802.3af, 802.3at and 802.3bt power classes, then the cabling decisions that follow from them: conductor gauge, bundle heat and derating, Cat6 vs Cat6a, distance, connectors, and whether a PoE injector or a PoE switch should supply the power. If you are scoping a larger build, start with L-com data center connectivity.
Key Takeaways
- 802.3af (PoE) delivers up to 15.4 W per switch port, 802.3at (PoE+) up to 30 W, and 802.3bt (PoE++) up to 60 W for Type 3 or 90 W for Type 4.
- The device always receives less than the port sends. On a worst-case 100 m Type 4 link, close to 19 W is lost as heat in the cable.
- 23 AWG copper has about 20% lower DC resistance than 24 AWG, which means less heat per cable and more headroom in large bundles.
- For new runs that will carry Type 3 or Type 4 power, Cat6a is the better buy: it is usually 23 AWG, sheds heat better than Cat5e or Cat6, and supports 10GBASE-T to 100 m.
- Default to a PoE switch when a rack feeds many devices. Use a PoE injector for a few devices, a non-PoE switch, or a single high-power load the switch budget cannot cover.
What Is Power over Ethernet?
Power over Ethernet is the IEEE 802.3 method for delivering DC power over the same twisted pairs that carry Ethernet data. The device supplying power is called the power sourcing equipment (PSE), usually a PoE switch or injector. The device drawing power is the powered device (PD).
A standards-based PSE checks for a signature resistance in the PD and classifies its power needs before sending anything. With no valid signature, it supplies no power.
802.3af and 802.3at use two of the four pairs for power. 802.3bt, often called 4-pair PoE or PoE++, can energize all four. Spreading current over four pairs lowers the loss on each pair, but it also means every conductor in the cable now carries current and generates heat.
PoE, PoE+ and PoE++ Power Classes
IEEE 802.3 defines nine power classes, numbered 0 through 8. Each class has a maximum at the switch port and a smaller amount guaranteed at the device, and the gap between them is the allowance for loss in a full 100 m channel.
|
Class |
Standard (common name) |
Max at PSE |
Max at PD |
Typical loads |
|
0 |
802.3af (PoE), Type 1 |
15.4 W |
12.95 W |
Default when a device reports no class |
|
1 |
802.3af (PoE), Type 1 |
4.0 W |
3.84 W |
Environmental sensors, small IoT nodes |
|
2 |
802.3af (PoE), Type 1 |
7.0 W |
6.49 W |
IP phones, badge readers |
|
3 |
802.3af (PoE), Type 1 |
15.4 W |
12.95 W |
Fixed cameras, older access points |
|
4 |
802.3at (PoE+), Type 2 |
30 W |
25.5 W |
Wi-Fi 5 and Wi-Fi 6 APs, PTZ cameras |
|
5 |
802.3bt (PoE++), Type 3 |
45 W |
40 W |
Multi-radio APs, video phones |
|
6 |
802.3bt (PoE++), Type 3 |
60 W |
51 W |
Wi-Fi 6E and Wi-Fi 7 APs, thin clients |
|
7 |
802.3bt (PoE++), Type 4 |
75 W |
62 W |
Heated PTZ cameras, small displays |
|
8 |
802.3bt (PoE++), Type 4 |
90 W |
71.3 W |
Digital signage, LED lighting, kiosks |
For the cable, current per pair matters more than watts. Type 1 runs up to 350 mA per pair, Types 2 and 3 up to 600 mA, and Type 4 close to 1 A. Resistive heating rises with the square of current, so the thermal step from basic PoE to Type 4 PoE++ is far larger than the wattage column suggests: roughly seven times the heat per conductor.
What Does PoE Power in a Data Center?
Most PoE loads sit around the white space rather than inside server racks:
- Wireless access points in the NOC, staging rooms and office areas. Many are PoE+ today, and newer Wi-Fi 7 models often need 802.3bt.
- IP cameras at entrances, cage rows and loading docks. PTZ units with heaters or IR illuminators can need Class 6 or higher.
- Access control hardware such as badge readers and door controllers.
- Environmental sensors for temperature, humidity, leak detection and airflow, mostly Class 1 or 2.
- Operations gear in the monitoring room, including displays, thin clients and KVM endpoints.
No single camera is a cabling problem. The rack where 48 or 96 of these runs land together is.
Conductor Gauge: 23 AWG vs 24 AWG
For PoE, a thicker conductor is better. Solid 23 AWG copper has about 6.7 ohms of DC resistance per 100 m, while 24 AWG has about 8.4 ohms. That difference of roughly 20% means less voltage drop, less wasted power and less heat at the same current.
|
Gauge |
DC resistance per 100 m (approx.) |
Where you usually see it |
PoE notes |
|
22 AWG |
5.3 ohms |
Some Cat6a and Cat7 designs, industrial cable |
Lowest heat; larger, stiffer cable |
|
23 AWG |
6.7 ohms |
Most Cat6a, many Cat6 cables |
Good default for 802.3bt runs |
|
24 AWG |
8.4 ohms |
Cat5e, some Cat6 |
Fine for PoE and PoE+; watch big Type 4 bundles |
|
26 AWG |
13.4 ohms |
Slim patch cords |
Keep cords short |
|
28 AWG |
21.3 ohms |
Ultra-thin patch cords |
In-rack cords only; heat builds in dense patch fields |
Values are per conductor for solid copper at 20 °C; stranded cords run a little higher. Thin patch cords matter less because they are short, but TIA-568.2-D reduces the allowed cord length for 26 and 28 AWG, and hundreds of them in a patch field add real heat behind a switch.
Tip: Keep copper-clad aluminum (CCA) cable out of any PoE pathway. It does not meet TIA-568 conductor requirements, its resistance is well above solid copper, and it runs hotter under the same load.
How Much Heat Does a PoE Cable Bundle Produce?
A single PoE cable in open air barely warms up. Bundles are different: cables in the middle of a tight bundle cannot shed heat, so they run well above room temperature while the cables on the outside stay cooler.
On a Type 4 link, the port can send 90 W while the device is only guaranteed 71.3 W, so up to about 19 W can be lost in the cable on a long run. Real links are usually shorter, but a few watts per cable across a 96-cable bundle is a small heater running around the clock.
Two documents give bundle-size guidance by cable category and current: TIA TSB-184-A and ISO/IEC TS 29125. In the US, the National Electrical Code (Section 725.144, added in the 2017 edition) also limits bundle size by conductor gauge and cable temperature rating once conductors carry more than 0.3 A, unless the cable is listed with a limited-power (LP) marking such as CMP-LP.
Heat hurts a link in two ways. It can push cable past its temperature rating, commonly 60 °C or 75 °C, and it raises insertion loss, which eats the margin the data signal needs.
Recommendation: For Type 3 and Type 4 PoE, split large bundles into several smaller ones, use open cable tray or ladder rack where possible, and dress cables loosely with hook-and-loop rather than cinching them. Avoid routing PoE++ bundles through thermal insulation or long sealed conduit.
Is Cat6 Enough for PoE, or Do You Need Cat6a?
Cat6 handles 802.3af and 802.3at comfortably and can carry 802.3bt, but Cat6a is the better choice for new runs that will see Type 3 or Type 4 power. Cat6a is usually 23 AWG, its larger diameter spreads heat over more surface, and it supports 10GBASE-T to 100 m, which multi-gig access points increasingly want.
Shielded F/UTP and S/FTP constructions dissipate heat better still, because the foil carries heat out toward the tray. They only work as intended in a properly bonded and grounded channel with shielded jacks and panels.
|
PoE load |
IEEE minimum |
Recommended for new installs |
Bundle guidance |
|
PoE (802.3af), up to 15.4 W |
Cat5e |
Cat6 |
Standard bundling practice |
|
PoE+ (802.3at), up to 30 W |
Cat5e |
Cat6, 23 AWG |
Watch very large bundles in warm spaces |
|
PoE++ Type 3, up to 60 W |
Cat5e |
Cat6a, 23 AWG |
Smaller bundles, open pathways |
|
PoE++ Type 4, up to 90 W |
Cat5e |
Cat6a, 23 AWG or shielded |
Smallest bundles; check NEC 725.144 or use LP-rated cable |
PoE Distance Limits and Temperature Derating
PoE uses the same 100 m channel limit as Ethernet: up to 90 m of horizontal cable plus 10 m of patch cords. The class table above already assumes a full 100 m channel, so a standards-based device gets its rated power anywhere inside that limit.
Temperature changes the math. TIA-568.2-D raises insertion loss for unshielded cable by about 0.4% per °C from 20 to 40 °C, and 0.6% per °C from 40 to 60 °C. A UTP link sitting at 60 °C has roughly 20% more loss than the same link at 20 °C, which can mean trimming the horizontal run from 90 m to around 75 m to stay in spec. Screened cable derates at about 0.2% per °C, one reason shielded Cat6a shows up in hot, dense PoE pathways.
To go past 100 m, add a PoE extender or a remote switch. Overlong warm runs tend to show up as link flaps, or cameras that reboot when their IR illuminators switch on.
Connectors, Patch Cords and Panels Under PoE Load
Connectors on PoE links have to survive being unplugged while live. When a plug is pulled under load, a small arc forms as the contacts separate, and over many cycles it can pit the contact surface right where the contacts rest when mated. Look for jacks and plugs tested to IEC 60512-99-001 for 2-pair PoE or IEC 60512-99-002 for 4-pair PoE, both of which check contact performance after unmating under load.
On the panel and work-area side, that means Cat6 or Cat6a data connectors & keystone jacks rated for 802.3bt, terminated with care. A poorly seated IDC contact adds resistance, and resistance under current becomes a hot spot. At the rack, Cat6 and Cat6a patch panels with rear cable management let you dress PoE cables in loose groups instead of one tight bundle behind the panel.
PoE Injector vs PoE Switch: When to Use Each
A PoE switch (endspan) powers every port from one chassis and one shared power budget. A PoE injector (midspan) sits between a non-PoE switch port and the device and adds power to that single link. Both are standards-compliant when they are rated for 802.3af, at or bt, so the choice comes down to scale and where the load sits.
|
Factor |
PoE switch |
PoE injector |
|
Best fit |
Many PoE devices fed from one rack or IDF |
One to a few devices, or a non-PoE switch |
|
Power budget |
Shared; often less than every port at full class |
Dedicated to one port |
|
Management |
Per-port power monitoring, scheduling, remote power cycling |
Usually none |
|
Backup power |
One UPS feed covers every device |
Each unit needs its own outlet |
|
Channel impact |
No extra connections |
Adds a patch cord and a connection point |
|
Upgrade path |
Replace or add a switch for higher classes |
Swap in a higher-class injector on one port |
Check the switch's total PoE budget, not only its per-port class. All 48 ports of a PoE+ switch at 30 W need 1,440 W, and many 48-port models ship with far less.
Recommendation: Treat the PoE switch as the default for data center and IDF builds, and keep a few 802.3bt injectors on hand for the occasional high-power device, such as a heated PTZ camera or a display, that the switch cannot cover without a budget upgrade.
PoE Cabling Checklist for Dense Racks
Run each planned PoE pathway through these questions before you order cable:
|
Question |
If yes |
If no |
|
Will any link carry 802.3bt Type 3 or Type 4 power? |
Specify Cat6a, 23 AWG |
Cat6 is usually sufficient |
|
Will dozens of PoE cables share one bundle or tray? |
Split bundles, open pathways, check TSB-184-A |
Standard bundling is fine |
|
Does the pathway run warm (hot aisle, ceiling space, near exhaust)? |
Derate channel length or use shielded cable |
Plan for the full 90 m permanent link |
|
Are you reusing existing Cat5e? |
Limit it to PoE and PoE+ or small bundles; test first |
Install Cat6a for new PoE++ runs |
|
Does total device power exceed the switch budget? |
Add an injector, a midspan panel or a larger supply |
Power everything from the switch |
|
Is any run longer than 100 m? |
Add a PoE extender or a remote switch |
Single run is fine |
|
Is the site in the US with more than 0.3 A per conductor? |
Check NEC 725.144 bundle limits or use LP-rated cable |
Follow local code |
Building PoE Links with L-com
Most PoE cabling plans need the same few parts: solid 23 AWG Cat6 or Cat6a for horizontal runs, jacks rated for 4-pair power, and patch cords short enough to keep heat down in the rack. L-com's Ethernet cable assemblies cover Cat6 through Cat8 in factory-terminated lengths for switch-to-panel and panel-to-device links. For copper, fiber and rack hardware in one place, browse L-com's data center solutions.
Power over Ethernet adds very little to a cabling plan when gauge and bundle size are decided up front. Fixing a hot tray after the cameras are already mounted is a much bigger job.
Frequently Asked Questions (FAQs)
Does PoE slow down Ethernet data speeds?
PoE sends DC power and data over the same twisted-pair cable, and the main effect on data performance is indirect. Heat from PoE current, especially in large bundles and warm pathways, raises insertion loss and reduces the margin the data signal needs. Keeping bundles small and using 23 AWG cable helps limit heat.
Can you run PoE++ over Cat5e?
Yes. IEEE 802.3bt lists Cat5e as the minimum, so Type 3 and Type 4 power will work over a compliant Cat5e channel. The concern is heat in large bundles of 24 AWG cable, which is why Cat6a is the better buy for new PoE++ runs.
Can a PoE switch damage a device that does not support PoE?
Not if the port is standards-based. A PoE switch that follows 802.3af, at or bt checks for a signature resistance in the powered device and classifies its power needs before sending anything. With no valid signature, it supplies no power.
How many watts does a PoE switch need?
Add up the class maximum for every device you plan to connect, then compare it with the switch's total PoE budget, not only its per-port class. For example, all 48 ports of a PoE+ switch at 30 W need 1,440 W, and many 48-port models ship with far less.
Do you need special patch cords for PoE?
There is no separate PoE cord type, but quality matters. Use copper conductors (never CCA), keep 26 and 28 AWG cords short, and choose plugs rated for the PoE type on the link.
What is the difference between a PoE injector and a PoE switch?
A PoE switch (endspan) powers every port from one chassis and one shared power budget, while a PoE injector (midspan) sits between a non-PoE switch port and the device and adds power to that single link. Use a PoE switch when a rack feeds many devices, and an injector for a few devices, a non-PoE switch, or a single high-power load the switch budget cannot cover.