L-com

How to Select the Right Industrial Ethernet Cable for Your Application

By Eileen Harvey

Selecting the right industrial Ethernet cable is essential for ensuring consistent performance and long-term reliability in demanding environments. Unlike standard office networking, industrial applications often involve extreme temperatures, oil, chemicals, moisture and high levels of electromagnetic interference (EMI).

From factory automation and robotics to process control systems and outdoor installations, the right cable can prevent costly downtime and maintain seamless data transmission. For high-quality, rugged cables, L-com partners with trusted brands such as TKD Kabel.

What is an Industrial Ethernet Cable?

An Industrial Ethernet Cable is specifically designed to handle harsh conditions while maintaining high-speed, reliable network communication.

Industrial vs. Standard Ethernet Cables

There are several important differences between industrial and standard Ethernet cables. Industrial have more rugged construction for mechanical stress resistance, and advanced shielding to combat EMI. Industrial cables are also resistant to oil, chemicals, UV light and temperature extremes.

Common Standards and Categories

Let’s look at the three main types of industrial Ethernet cable. Cat5e is cost-effective and achieves data transmission speeds of up to 1 Gbps and with a maximum signal frequency (bandwidth) of 100 MHz. Cat6 industrial Ethernet cable gets up to 10 Gbps (shorter runs) and 250 MHz and has better EMI resistance than Cat5e. Cat6a brings 10 Gbps at up to 100 meters, and bandwidth of 500 MHz, which is great for high-speed needs.

Factors to Consider When Choosing an Industrial Ethernet Cable

When choosing an industrial Ethernet cable, consider several important factors to ensure reliable performance in demanding environments. One of the first considerations is environmental conditions. The cable’s temperature range should match the expected high and low extremes of the installation area. In manufacturing and processing environments, chemical and oil resistance is critical to protect against damage from exposure. For outdoor applications, it is best to select cables designed with UV and moisture resistance.

Shielding and noise protection also play a key role. Shielded twisted pair (STP) cables are recommended for areas with high EMI, such as near motors or welders. In contrast, unshielded twisted pair (UTP) cables are suitable for low-interference environments. For maximum resistance to EMI, cables with foil or braided shielding provide the strongest protection.

Cable construction and jacket type determine both durability and flexibility. PVC jackets are affordable and perform well in indoor fixed installations. PUR jackets are flexible and resistant to abrasion and oil, making them a strong choice for robotics and other moving equipment. TPE jackets offer resistance to both chemicals and temperature extremes, making them suitable for harsher environments.

It is also important to match the cable’s Category rating to the required data speed and bandwidth of the network. Avoid over-specifying and under-specifying to balance performance with cost. Distance and installation route further influence the decision. Copper cables are effective for shorter to medium-length runs, while fiber is preferred for very long distances. Flexible cable designs are particularly beneficial for machinery that moves.

Finally, compliance with recognized standards ensures safety and interoperability. Look for cables that meet TIA/EIA, ISO/IEC, UL and IEEE 802.3 requirements, along with any relevant industry-specific standards.

Matching the Cable to Your Application

For factory automation and robotics, choose high-flex, oil-resistant, EMI-shielded cables like the Cat5e High Flex PUR Jacket Cable or Cat6 High Flex PUR Jacket Cable.

For outdoor and harsh environments, use UV-resistant, weatherproof options like the Cat6a High Flex PUR Jacket Cable.

For indoor industrial networks, cost-effective and shielded runs, use the Cat5e Double Shielded PVC Jacket Cable.

For High-Speed Data Transfer, opt for the Cat6 Double Shielded PVC Jacket Cable for Gigabit and 10-Gigabit Ethernet applications.

Choosing the right industrial Ethernet cable ensures optimal performance, durability and reliability. Whether you need flexibility for robotics, UV protection for outdoor use or high shielding for EMI-heavy environments, L-com and TKD Kabel offer industry-leading solutions.

Explore the full range of Industrial Ethernet Cables or contact our technical experts to find the perfect cable for your project.

Installation Best Practices

We offer three tips. First, avoid sharp bends or excessive pulling during installation. Second, ground shielded cables properly. And third, use connectors rated for the application (RJ45, M12, field-terminable).

L-com offers a wide selection of rugged, high-performance industrial Ethernet cables. They include Cat5e, Cat6 and Cat6a options that are shielded for EMI resistance. There are also flexible, high-durability designs for robotics and moving machinery.

Browse the full range on our Industrial Ethernet Cable page or explore premium options from TKD Kabel.

Resources

Search Entries