L-com

Fiber Optic Splicing vs Connectorization in the Data Center

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Fiber optic splicing permanently joins two fibers, usually with a fusion splicer, and loses almost no light at the joint. Connectorization ends a fiber in a removable connector so it can be plugged, unplugged and moved. In most data centers, splicing wins on backbone and building entrance runs where low loss and permanence matter, and connectors win inside the rack, where links get patched and changed constantly. Most facilities use both. The real decision is where the line between them falls on each run. 

This guide compares splice loss and connector loss, durability, labor time and tooling cost, then gives you a checklist for making the call on a specific link. If you're planning a larger build, L-com's data center fiber solutions cover the connectorized side of the job. 

 

Key Takeaways 

  • A good fusion splice typically loses 0.02 to 0.05 dB. A mated connector pair usually loses 0.15 to 0.5 dB, depending on connector grade and termination method. 
  • Splicing fits backbone runs, outside plant (OSP) entrances, very high fiber counts and repairs to installed cable. 
  • Connectors, whether field-installed or pre-terminated, fit in-rack patching and any link that will be moved, added or changed. 
  • A fusion splicer and precision cleaver cost thousands of dollars up front. Field termination kits cost far less, but each connector costs more and adds more loss. 
  • Pigtail splicing and splice-on connectors combine factory connector quality with splice-level loss, which is why many installers default to them for permanent links. 

 

Splicing vs Connectorization at a Glance 

Factor 

Fusion splicing 

Field-installed connectors 

Pre-terminated assemblies 

Typical loss per joint 

0.02-0.05 dB 

0.2-0.5 dB 

0.15-0.35 dB 

TIA-568 maximum 

0.3 dB per splice 

0.75 dB per mated pair 

0.75 dB per mated pair 

Hands-on time per fiber 

2-4 min, plus enclosure prep 

2-5 min (quick-term) 

Plug in and test 

Reconfigurable 

No 

Yes 

Yes 

Upfront tooling 

High 

Low to moderate 

Minimal 

Best fit 

Backbone, OSP entrance, repairs 

Small jobs, odd lengths, quick fixes 

New builds, MPO trunks, in-rack 

 

 

What Is Fiber Optic Splicing? 

Fiber optic splicing joins two bare fiber ends so light passes from one core into the next with very little loss or reflection. There are two methods, and only one of them belongs in a permanent data center link. 

 

Fusion Splicing 

Fusion splicing melts two cleaved fiber ends together with an electric arc, creating one continuous strand of glass. The splicer aligns the fibers (by core on better units, by cladding on cheaper ones), fires the arc and gives you an estimated loss reading. You then slide a heat-shrink sleeve over the joint and store it in a splice tray. 

Because the glass is continuous, back reflection is negligible. Ribbon (mass fusion) splicers join 12 fibers in one pass, which is how hyperscale facilities splice 864- and 1,728-fiber trunks without spending weeks on it. 

 

Mechanical Splicing 

A mechanical splice holds two cleaved ends together in an alignment sleeve filled with index-matching gel. It needs no splicer, but loss is higher (up to the 0.3 dB TIA limit) and the gel can change over the years. In a data center, treat it as an emergency repair, not a design choice. 

 

What Does Connectorization Involve? 

Connectorization is the fiber optic termination method that ends each fiber in a connector such as LC, SC or MPO instead of fusing it to another fiber. The term covers four quite different approaches: 

  • Epoxy and polish. The cheapest connectors and the slowest, most skill-dependent process. You'll rarely see it in modern data centers. 
  • Pre-polished mechanical (quick-term). A factory-polished ferrule with a short internal fiber stub. You cleave your fiber and push it in. It's fast and easy to learn, though there's a mechanical splice hiding inside, so loss runs higher. 
  • Splice-on connectors. A factory-polished connector fused directly onto your field fiber. Loss is low, but you still need a fusion splicer. 
  • Pre-terminated assemblies. Trunks, jumpers and cassettes terminated and tested at the factory. You do no field termination at all, but you have to get lengths right before ordering. 

 

Splice Loss vs Connector Loss 

A fusion splice usually loses about a tenth of what a mated connector pair does. On a single link that difference sounds small. It stops being small once you look at high-speed multimode budgets. 

Take 100GBASE-SR4 over OM4. The standard allows about 1.9 dB of total channel insertion loss at 100 m, and only 1.5 dB of that is set aside for connections and splices. Four standard mated pairs at 0.5 dB each come to 2.0 dB, which is already over the limit. Four low-loss pairs at 0.35 dB come to 1.4 dB, which fits, barely. Add a few fusion splices at 0.05 dB and the budget hardly moves. 

Reflection matters too. A UPC connector typically has return loss of 50 dB or better and an APC connector 60 dB or better, while a good fusion splice reflects almost nothing. On single-mode links with reflection-sensitive optics, every connector you remove is one less reflection point. 

Tip: Build your loss budget from the manufacturer's maximum values, not its typical values. Then verify the finished link with an optical loss test set (OLTS) before you hand it over. 

 

Durability and Long-Term Reliability 

A protected fusion splice in a closed tray is about as permanent as fiber gets. There are no mating faces to get dirty and nothing to unplug by mistake. The weak points are handling during installation and poor tray management, especially tight bends on the fiber loops. 

Connectors are the opposite. Dirty or damaged endfaces are among the most common causes of fiber link problems, and every mating cycle is another chance to introduce contamination. Most connectors are rated for roughly 500 to 1,000 matings. The upside is that a bad connector is easy to clean, inspect or replace. A damaged splice means opening the enclosure and splicing again. 

 

How Long Does Each Method Take? 

An experienced technician can strip, clean, cleave, fuse and sleeve a single fiber in about two to four minutes. That number hides the real time cost: opening the cable sheath, routing buffer tubes, setting up the splice enclosure and dressing trays often takes longer than the splicing itself. On a 144-fiber trunk, single-fiber splicing can easily run past seven hours per end. Ribbon splicing cuts that dramatically. 

Quick-term connectors take two to five minutes each with no splicer warm-up, so they make sense when you're terminating a handful of fibers. Pre-terminated assemblies are the fastest on site by a wide margin, since you pull, plug and test. The trade-off is lead time and the risk of ordering the wrong length. 

 

Recommendation: Measure pathways twice before ordering pre-terminated trunks, and add enough slack for a service loop at each end. Running short on a pre-term trunk costs more time than splicing would have. 

 

Tooling Cost: Fusion Splicer vs Field Termination Kits 

Tool 

Approximate cost 

Notes 

Core-alignment fusion splicer 

$4,000-$15,000+ 

Lowest loss, needed for single-mode backbones 

Cladding-alignment splicer 

$1,000-$4,000 

Adequate for many multimode jobs 

Precision cleaver 

$300-$1,500 

Cleave quality drives splice loss 

Quick-term termination kit 

$300-$1,500 

Includes cleaver, strippers, visual fault locator 

Quick-term connector (each) 

$10-$25 

Roughly 3 to 5 times a standard connector 

Inspection scope 

$300-$2,000+ 

Needed for every method 

 

Prices vary by brand and region, so treat these as rough ranges. Splicers also carry ongoing costs such as electrode replacement and periodic servicing. If you only splice a few times a year, renting a splicer or bringing in a splicing contractor is often cheaper than owning one. 

 

Where Fiber Optic Splicing Makes the Most Sense 

Splicing earns its tooling cost in a few specific places: 

  • Building entrance facilities. Under the NEC, unlisted OSP cable generally can't run more than 50 ft (15 m) inside a building unless it's in conduit, so OSP cable is usually spliced to indoor-rated cable near the entry point. 
  • Long single-mode backbones between halls or campus buildings, where every tenth of a dB counts. 
  • Very high fiber counts. Ribbon cables with hundreds of fibers are impractical to pre-terminate and difficult to pull with connectors attached. 
  • Repairs. A cut mid-span on installed cable is fixed with a splice, not a new run. 
  • Tight pathways that won't fit a pulling grip over pre-terminated connector ends. 

 

Where Connectorization Makes the Most Sense 

Connectors are the better choice wherever flexibility outweighs a few tenths of a dB: 

  • Inside the rack and at cross-connects, where patching between panels and switches changes regularly. 
  • New builds with MPO trunks between rows, where factory test reports and short install windows matter. 
  • Short runs that don't justify a splice enclosure. 
  • Teams without a splicer or a trained splicing technician on staff. 
  • Temporary, lab and staging links that will be torn down later. 

 

Pigtails and Splice-On Connectors: The Middle Ground 

Plenty of data center installers don't choose one method at all. With pigtail splicing, you fuse a factory-terminated pigtail onto each trunk fiber inside a patch panel or cassette. You get a factory-polished connector at the face of the panel and a 0.05 dB splice behind it. Splice-on connectors deliver a similar result without the separate pigtail. 

For permanent backbone links that you terminate on site, this hybrid usually gives the best performance per dollar. The catches are that you still need a splicer, and your panels need room for splice trays. 

 

Decision Checklist for a Specific Run 

Work through these questions for each link before choosing a method: 

Question 

If yes 

If no 

Is the cable OSP-rated and entering the building? 

Splice to indoor cable 

Either method works 

Will the link be reconfigured during its life? 

Put connectors at that point 

Splice or pre-term 

Is the loss budget tight (100G/400G multimode)? 

Minimize mated pairs; use splices or low-loss pre-term 

Standard connectors are fine 

More than roughly 24 to 48 fibers on the run? 

Ribbon splicing or pre-terminated trunks 

Quick-term may be fastest 

Do you have a splicer and a trained tech? 

Splicing and splice-on are open to you 

Pre-term or quick-term 

Are exact lengths known, with time for lead time? 

Pre-terminated assemblies 

Field termination 

Can the pathway fit connectorized ends? 

Pre-term is an option 

Splice or field-terminate 

 

 

Tips for Better Results with Either Method 

  • Inspect and clean every connector before mating it, including brand-new ones straight out of the bag. Use IEC 61300-3-35 as your pass/fail reference. 
  • Keep the cleaver blade clean and rotate it on schedule. A poor cleave is the most common cause of a bad splice. 
  • Don't rely on the splicer's loss estimate. Confirm with a bidirectional OTDR test, because a one-direction reading can show a misleading "gain" or exaggerated loss. 
  • Label every splice tray and record which fiber went where. Whoever opens that enclosure in five years will need that record. 
  • Leave a service loop at each enclosure so you can re-splice without pulling new cable. 

 

Building the Connectorized Path with L-com 

For in-rack patching, field termination and pre-terminated builds, start with the right components. L-com carries fiber optic connectors in LC, SC and MPO styles, along with bulk fiber optic cable in single-mode and multimode for custom-length runs. If you'd rather skip field termination, factory-built fiber optic patch cables and cable assemblies handle the rack-level connections. You can browse the full lineup through the L-com Data Center hub. 

 

Frequently Asked Questions (FAQs) 

 

1. Is fusion splicing better than using connectors? 

 

For loss and permanence, yes. A fusion splice loses far less light and has no mating surface to contaminate. Connectors are better wherever a link needs to be patched, moved or tested, which describes most of what happens inside a rack. 

 

2. How much loss does a fiber splice add? 

 

A good fusion splice typically adds 0.02 to 0.05 dB. TIA-568 allows up to 0.3 dB per splice, which is the figure to use in a conservative loss budget. Mechanical splices usually land closer to that 0.3 dB limit. 

 

3. When should I use fusion splicing instead of connectors in a data center? 

 

Splicing fits backbone runs, outside plant (OSP) entrances, very high fiber counts, repairs to installed cable, and tight pathways that won't fit connectorized ends. Connectors fit in-rack patching, cross-connects, and any link that will be moved, added, or changed. 

 

4. What is pigtail splicing, and when is it used? 

 

Pigtail splicing fuses a factory-terminated pigtail onto each trunk fiber inside a patch panel or cassette, giving a factory-polished connector at the panel face and a low-loss splice behind it. Splice-on connectors deliver a similar result without a separate pigtail. This hybrid is often used for permanent backbone links terminated on site, though it still requires a fusion splicer. 

 

5. Do pre-terminated fiber cables ever need splicing? 

 

Not under normal conditions. You'd only splice a pre-terminated cable to repair damage or to transition from OSP to indoor cable at the building entrance. 

 

6. What tools do you need for fiber optic termination in the field? 

 

For quick-term connectors, you need a cleaver, strippers, a visual fault locator, an inspection scope, and cleaning supplies. Splice-on connectors add a fusion splicer to that list. 

Resources

Search Entries