L-com

Fiber Optic Cable Assemblies: How to Spec the Right One

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Specifying a fiber optic cable assembly comes down to six decisions: the connector on each end, the fiber type, the end-face polish, the jacket rating, the length, and the testing you expect before it ships. Miss one and you usually find out at install, with a technician holding a cord that won't fit the port. 

This guide turns those decisions into a workflow you can repeat on every order, with a fill-in spec sheet and two worked examples: a top-of-rack uplink and a data center interconnect (DCI) run. If the assembly is part of a larger build, start with L-com data center solutions for the full connectivity lineup. 

 

Key Takeaways 

  • A complete spec covers Connector A, Connector B, fiber type, polish, jacket rating and length, plus the test report you want shipped with the cable. 
  • MPO/MTP gender has to be stated: transceiver ports are pinned (male), so a cord that plugs straight into them needs unpinned (female) connectors. 
  • Never plug an APC connector (green, 8-degree angled end face) into a UPC port (blue); the air gap adds loss and can damage both end faces. 
  • Pick the jacket by the space the cable passes through: OFNP for plenum air-handling spaces, OFNR for risers. Plenum can always replace riser, never the reverse. 
  • Ask for a serialized factory report with insertion loss and return loss for every fiber, then check the total against the optic's channel loss budget. 

 

What Is a Fiber Optic Cable Assembly? 

A fiber optic cable assembly is a length of fiber cable that is terminated, polished and tested at the factory before it ships. The most common type is the fiber optic patch cable (or jumper), a short simplex or duplex cord that connects equipment to a panel or to other equipment. Trunk assemblies carry 12 to 144 or more fibers between panels, and breakout or harness assemblies fan an MPO connector out to several duplex LC ends. 

Because the end faces are machine polished and measured, you know the loss before the cable reaches the rack. Browse L-com's fiber optic cable assemblies for standard configurations, and use the steps below to narrow the options. 

 

The Six-Step Spec Workflow 

Work through the steps in order, because each choice narrows the next. 

 

Step 1: Choose Fiber Optic Connector Types for Each End 

The port at each end decides the connector. The two don't have to match: an LC-to-SC cord is a routine order when a new switch connects to an older patch panel. 

Connector 

Ferrule / fibers 

Where you'll see it 

LC 

1.25 mm, simplex or duplex 

SFP, SFP+, SFP28 and duplex QSFP optics; high-density panels 

SC 

2.5 mm, simplex or duplex 

Older panels, carrier ODFs, PON; often APC 

ST 

2.5 mm, bayonet latch 

Legacy multimode and industrial equipment 

MPO/MTP 

12, 16 or 24 positions in one ferrule 

Parallel optics (SR4, SR8, DR4) and trunks 

 

With MPO/MTP, state the gender on both ends. Transceiver ports are pinned, so a cord going straight into an optic needs unpinned (female) connectors. Two pinned connectors can't mate through an adapter, and two unpinned ones won't align. State polarity as well: duplex cords are normally A-to-B so transmit lands on receive, and MPO cords follow TIA-568 Type A, B or C. Type B is the usual choice for a direct optic-to-optic parallel link. 

 

Step 2: Which Fiber Type Does the Link Need? 

Choose the fiber grade from the optic and the distance. Single-mode OS2 reaches kilometers; multimode pairs with cheaper short-reach optics but tops out at a few hundred meters, less at higher speeds. 

Fiber grade 

Typical jacket color 

Example reach (IEEE optics) 

OS2 single-mode 

Yellow 

400GBASE-DR4: 500 m; 400GBASE-FR4: 2 km; 100GBASE-LR4: 10 km 

OM3 multimode 

Aqua 

10GBASE-SR: 300 m; 100GBASE-SR4: 70 m 

OM4 multimode 

Aqua or violet 

10GBASE-SR: 400 m; 100GBASE-SR4: 100 m 

OM5 multimode 

Lime green 

Matches OM4 for SR optics; longer reach with SWDM and BiDi optics 

 

Count fibers at the same time. Duplex links need two, SR4 and DR4 links use eight fibers in a 12-position MPO, and SR8 needs sixteen. 

 

Recommendation: OM4 is a sensible multimode default for new builds. For runs longer than about 100 meters, or links you expect to outlive the current optics, OS2 is usually the better bet. 

 

Step 3: UPC or APC Polish? 

UPC is the default for most data center links, and APC is used wherever the equipment or panel calls for it. UPC end faces are polished flat with a slight dome and typically reach 50 dB return loss or better. APC end faces are angled at 8 degrees, which sends reflected light into the cladding and pushes return loss to 60 dB or more. 

You'll find APC on single-mode PON, RF-over-fiber, many carrier ODFs and some 400G single-mode optics such as DR4, which use MPO/APC. Multimode connectors are almost always non-angled.  

Tip: Color codes help on the floor: green housings are APC, blue are single-mode UPC, and beige or aqua are multimode. A hybrid cord with APC on one end and UPC on the other is a valid order, as long as each end matches the port it plugs into. 

 

Step 4: Jacket Rating and Cable Construction 

Match the jacket to the space the cable runs through. Under the US National Electrical Code, nonconductive fiber is rated OFNP (plenum), OFNR (riser) or OFN (general purpose), and a higher rating can always stand in for a lower one. LSZH (low smoke zero halogen) jackets cut toxic smoke and are common outside North America, but LSZH on its own doesn't make a cable plenum rated. 

For construction, duplex zip cord is standard for patch cords, round jackets dress more neatly in crowded managers, and armored jackets suit under-floor runs. Bend-insensitive fiber is worth the small premium for cords routed tight to the rails. 

 

Step 5: How Long Should the Assembly Be? 

Measure the real cable path, then add slack for dressing and service. Trace the route through the vertical manager, up into the tray, across and down; the straight-line distance between racks is always short. Trunks need enough at each end for a service loop inside the panel. 

Excess length ends up coiled in the manager, blocking airflow. Ask the supplier to state length tolerance on the quote, and use stock lengths where they fit, since they generally ship faster than custom ones. 

 

Step 6: Testing and Documentation 

Every fiber optic cable assembly should arrive with a factory test report listing insertion loss and return loss for each fiber, tied to a serial number on the cable label. On critical single-mode links, it's reasonable to also request end-face geometry by interferometry and end-face inspection results to IEC 61300-3-35. 

Recommendation: Put the test report on the spec as a line item rather than a note, so it ships with the order and gives you a baseline for later troubleshooting. 

 

Fill-In Spec Sheet for a Fiber Optic Cable Assembly 

Copy this table into your RFQ or purchase request. If you can fill in every row, you're ready to order. 

Field 

What to specify 

Your spec 

Application 

Optic or port type, data rate 

______ 

Connector A 

Type, gender (MPO), polish 

______ 

Connector B 

Type, gender (MPO), polish 

______ 

Fiber count 

2, 8, 12, 16, 24 or more 

______ 

Fiber grade 

OS2, OM3, OM4, OM5 

______ 

Polarity 

A-to-B duplex; MPO Type A, B or C 

______ 

Construction 

Simplex, duplex zip, round, breakout, armored 

______ 

Jacket rating 

OFNP, OFNR, OFN, LSZH 

______ 

Jacket color 

Standard by grade or custom 

______ 

Length and tolerance 

Measured path plus slack 

______ 

Labeling 

Serial number, ID labels on both ends 

______ 

Test report 

IL and RL per fiber; geometry for single-mode 

______ 

Quantity 

Including spares 

______ 

 

 

Worked Example 1: 100G Top-of-Rack Uplink 

A leaf switch at the top of rack 4 uplinks to a spine switch in rack 7 with 100GBASE-SR4 QSFP28 optics. The tray path measures 11 meters including the drops at each end, and the tray runs through a ceiling return-air space. 

Field 

Spec 

Why 

Connector A / B 

MPO-12 female / MPO-12 female 

QSFP28 SR4 ports are pinned 

Polarity 

Type B 

Direct optic-to-optic link 

Fiber 

OM4, 8 active fibers 

SR4 reaches 100 m on OM4 

Polish 

Multimode, non-angled 

Standard for multimode MPO 

Jacket 

OFNP 

Route passes through plenum air space 

Length 

12 m 

11 m path plus 1 m slack 

Testing 

IL per fiber, serialized report 

Baseline for the loss budget 

 

With one cord and no intermediate panels, this link sits comfortably inside the SR4 channel budget (about 1.9 dB on OM4 under IEEE 802.3bm). Route it through two MPO panels instead and each mated pair adds loss, which is when low-loss MPO connectors earn their price. If you still need the optics, pair the cord with matching fiber optic transceivers. 

 

Worked Example 2: Campus DCI Run 

Two data halls in separate buildings, 1.2 km apart, connect with 400GBASE-FR4 optics. The inter-building backbone is armored OS2 cable spliced into an optical distribution frame (ODF) at each end, and the ODF ports are SC/APC. The assemblies you order are the jumpers from each switch to its ODF. 

Field 

Spec 

Why 

Connector A 

Duplex LC/UPC 

FR4 optic has a duplex LC port 

Connector B 

2x SC/APC (hybrid cord) 

ODF adapters are SC/APC 

Fiber 

OS2, duplex 

FR4 is single-mode, 2 km reach 

Polarity 

A-to-B, checked against ODF mapping 

Tx must land on far-end Rx 

Jacket 

OFNR 

Riser route from ODF room to switch row 

Length 

8 m 

Measured route plus slack 

Testing 

IL and RL per fiber 

APC return loss matters at the ODF 

 

At roughly 0.4 dB/km for OS2 at 1310 nm, 1.2 km of backbone adds about 0.5 dB. Two mated connector pairs at the ODFs add around 0.3 dB each, and two fusion splices about 0.05 dB each, for a total near 1.2 dB. That's well under the roughly 4 dB channel budget for 400GBASE-FR4. Treat these as planning figures and confirm them against the optic datasheet. 

If the ODF needs new bulkhead adapters for the APC side, add matching fiber optic adapters to the same order. 

 

Ordering Fiber Optic Cable Assemblies from L-com 

Once the spec sheet is complete, compare it against L-com's standard fiber optic cable assembly configurations by connector, fiber grade and length. If nothing standard fits, send the completed sheet with your custom request so every detail is already answered. For the optics, adapters and patch panels around the link, see L-com's data center connectivity lineup. 

 

Frequently Asked Questions (FAQs) 

 

Is a fiber optic patch cable the same as a fiber optic cable assembly? 

A fiber optic patch cable is one kind of fiber optic cable assembly. "Assembly" covers any factory-terminated fiber cable, including trunks, breakouts and harnesses, while "patch cable" usually means a short simplex or duplex jumper used at the rack or panel. 

Which fiber type does a data center link need? 

Choose the fiber grade from the optic and the distance. Single-mode OS2 reaches kilometers, while multimode pairs with cheaper short-reach optics but tops out at a few hundred meters, less at higher speeds. OM4 is a sensible multimode default for new builds, and OS2 is usually the better bet for runs longer than about 100 meters. 

Which fiber optic connector types should a data center standardize on? 

Most data centers standardize on LC for duplex links and MPO/MTP for parallel optics and trunks. SC tends to stay only where legacy panels or carrier ODFs require it. 

How long does a custom fiber optic cable assembly take? 

Lead time depends on the supplier and the configuration, so ask for it on the quote. Stock lengths and common connector pairs generally ship faster than custom lengths, hybrid connector combinations or high fiber count trunks. 

What is the difference between OFNP and OFNR jacket ratings? 

OFNP is the plenum rating, for cable that runs through air-handling spaces, and OFNR is the riser rating. A higher rating can always stand in for a lower one, so plenum can replace riser but never the reverse.

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Specifying a fiber optic cable assembly comes down to six decisions: the connector on each end, the fiber type, the end-face polish, the jacket rating, the length, and the testing you expect before it ships. Miss one and you usually find out at install, with a technician holding a cord that won't fit the port. 

This guide turns those decisions into a workflow you can repeat on every order, with a fill-in spec sheet and two worked examples: a top-of-rack uplink and a data center interconnect (DCI) run. If the assembly is part of a larger build, start with L-com data center solutions for the full connectivity lineup. 

 

Key Takeaways 

  • A complete spec covers Connector A, Connector B, fiber type, polish, jacket rating and length, plus the test report you want shipped with the cable. 
  • MPO/MTP gender has to be stated: transceiver ports are pinned (male), so a cord that plugs straight into them needs unpinned (female) connectors. 
  • Never plug an APC connector (green, 8-degree angled end face) into a UPC port (blue); the air gap adds loss and can damage both end faces. 
  • Pick the jacket by the space the cable passes through: OFNP for plenum air-handling spaces, OFNR for risers. Plenum can always replace riser, never the reverse. 
  • Ask for a serialized factory report with insertion loss and return loss for every fiber, then check the total against the optic's channel loss budget. 

 

What Is a Fiber Optic Cable Assembly? 

A fiber optic cable assembly is a length of fiber cable that is terminated, polished and tested at the factory before it ships. The most common type is the fiber optic patch cable (or jumper), a short simplex or duplex cord that connects equipment to a panel or to other equipment. Trunk assemblies carry 12 to 144 or more fibers between panels, and breakout or harness assemblies fan an MPO connector out to several duplex LC ends. 

Because the end faces are machine polished and measured, you know the loss before the cable reaches the rack. Browse L-com's fiber optic cable assemblies for standard configurations, and use the steps below to narrow the options. 

 

The Six-Step Spec Workflow 

Work through the steps in order, because each choice narrows the next. 

 

Step 1: Choose Fiber Optic Connector Types for Each End 

The port at each end decides the connector. The two don't have to match: an LC-to-SC cord is a routine order when a new switch connects to an older patch panel. 

Connector 

Ferrule / fibers 

Where you'll see it 

LC 

1.25 mm, simplex or duplex 

SFP, SFP+, SFP28 and duplex QSFP optics; high-density panels 

SC 

2.5 mm, simplex or duplex 

Older panels, carrier ODFs, PON; often APC 

ST 

2.5 mm, bayonet latch 

Legacy multimode and industrial equipment 

MPO/MTP 

12, 16 or 24 positions in one ferrule 

Parallel optics (SR4, SR8, DR4) and trunks 

 

With MPO/MTP, state the gender on both ends. Transceiver ports are pinned, so a cord going straight into an optic needs unpinned (female) connectors. Two pinned connectors can't mate through an adapter, and two unpinned ones won't align. State polarity as well: duplex cords are normally A-to-B so transmit lands on receive, and MPO cords follow TIA-568 Type A, B or C. Type B is the usual choice for a direct optic-to-optic parallel link. 

 

Step 2: Which Fiber Type Does the Link Need? 

Choose the fiber grade from the optic and the distance. Single-mode OS2 reaches kilometers; multimode pairs with cheaper short-reach optics but tops out at a few hundred meters, less at higher speeds. 

Fiber grade 

Typical jacket color 

Example reach (IEEE optics) 

OS2 single-mode 

Yellow 

400GBASE-DR4: 500 m; 400GBASE-FR4: 2 km; 100GBASE-LR4: 10 km 

OM3 multimode 

Aqua 

10GBASE-SR: 300 m; 100GBASE-SR4: 70 m 

OM4 multimode 

Aqua or violet 

10GBASE-SR: 400 m; 100GBASE-SR4: 100 m 

OM5 multimode 

Lime green 

Matches OM4 for SR optics; longer reach with SWDM and BiDi optics 

 

Count fibers at the same time. Duplex links need two, SR4 and DR4 links use eight fibers in a 12-position MPO, and SR8 needs sixteen. 

 

Recommendation: OM4 is a sensible multimode default for new builds. For runs longer than about 100 meters, or links you expect to outlive the current optics, OS2 is usually the better bet. 

 

Step 3: UPC or APC Polish? 

UPC is the default for most data center links, and APC is used wherever the equipment or panel calls for it. UPC end faces are polished flat with a slight dome and typically reach 50 dB return loss or better. APC end faces are angled at 8 degrees, which sends reflected light into the cladding and pushes return loss to 60 dB or more. 

You'll find APC on single-mode PON, RF-over-fiber, many carrier ODFs and some 400G single-mode optics such as DR4, which use MPO/APC. Multimode connectors are almost always non-angled.  

Tip: Color codes help on the floor: green housings are APC, blue are single-mode UPC, and beige or aqua are multimode. A hybrid cord with APC on one end and UPC on the other is a valid order, as long as each end matches the port it plugs into. 

 

Step 4: Jacket Rating and Cable Construction 

Match the jacket to the space the cable runs through. Under the US National Electrical Code, nonconductive fiber is rated OFNP (plenum), OFNR (riser) or OFN (general purpose), and a higher rating can always stand in for a lower one. LSZH (low smoke zero halogen) jackets cut toxic smoke and are common outside North America, but LSZH on its own doesn't make a cable plenum rated. 

For construction, duplex zip cord is standard for patch cords, round jackets dress more neatly in crowded managers, and armored jackets suit under-floor runs. Bend-insensitive fiber is worth the small premium for cords routed tight to the rails. 

 

Step 5: How Long Should the Assembly Be? 

Measure the real cable path, then add slack for dressing and service. Trace the route through the vertical manager, up into the tray, across and down; the straight-line distance between racks is always short. Trunks need enough at each end for a service loop inside the panel. 

Excess length ends up coiled in the manager, blocking airflow. Ask the supplier to state length tolerance on the quote, and use stock lengths where they fit, since they generally ship faster than custom ones. 

 

Step 6: Testing and Documentation 

Every fiber optic cable assembly should arrive with a factory test report listing insertion loss and return loss for each fiber, tied to a serial number on the cable label. On critical single-mode links, it's reasonable to also request end-face geometry by interferometry and end-face inspection results to IEC 61300-3-35. 

Recommendation: Put the test report on the spec as a line item rather than a note, so it ships with the order and gives you a baseline for later troubleshooting. 

 

Fill-In Spec Sheet for a Fiber Optic Cable Assembly 

Copy this table into your RFQ or purchase request. If you can fill in every row, you're ready to order. 

Field 

What to specify 

Your spec 

Application 

Optic or port type, data rate 

______ 

Connector A 

Type, gender (MPO), polish 

______ 

Connector B 

Type, gender (MPO), polish 

______ 

Fiber count 

2, 8, 12, 16, 24 or more 

______ 

Fiber grade 

OS2, OM3, OM4, OM5 

______ 

Polarity 

A-to-B duplex; MPO Type A, B or C 

______ 

Construction 

Simplex, duplex zip, round, breakout, armored 

______ 

Jacket rating 

OFNP, OFNR, OFN, LSZH 

______ 

Jacket color 

Standard by grade or custom 

______ 

Length and tolerance 

Measured path plus slack 

______ 

Labeling 

Serial number, ID labels on both ends 

______ 

Test report 

IL and RL per fiber; geometry for single-mode 

______ 

Quantity 

Including spares 

______ 

 

 

Worked Example 1: 100G Top-of-Rack Uplink 

A leaf switch at the top of rack 4 uplinks to a spine switch in rack 7 with 100GBASE-SR4 QSFP28 optics. The tray path measures 11 meters including the drops at each end, and the tray runs through a ceiling return-air space. 

Field 

Spec 

Why 

Connector A / B 

MPO-12 female / MPO-12 female 

QSFP28 SR4 ports are pinned 

Polarity 

Type B 

Direct optic-to-optic link 

Fiber 

OM4, 8 active fibers 

SR4 reaches 100 m on OM4 

Polish 

Multimode, non-angled 

Standard for multimode MPO 

Jacket 

OFNP 

Route passes through plenum air space 

Length 

12 m 

11 m path plus 1 m slack 

Testing 

IL per fiber, serialized report 

Baseline for the loss budget 

 

With one cord and no intermediate panels, this link sits comfortably inside the SR4 channel budget (about 1.9 dB on OM4 under IEEE 802.3bm). Route it through two MPO panels instead and each mated pair adds loss, which is when low-loss MPO connectors earn their price. If you still need the optics, pair the cord with matching fiber optic transceivers. 

 

Worked Example 2: Campus DCI Run 

Two data halls in separate buildings, 1.2 km apart, connect with 400GBASE-FR4 optics. The inter-building backbone is armored OS2 cable spliced into an optical distribution frame (ODF) at each end, and the ODF ports are SC/APC. The assemblies you order are the jumpers from each switch to its ODF. 

Field 

Spec 

Why 

Connector A 

Duplex LC/UPC 

FR4 optic has a duplex LC port 

Connector B 

2x SC/APC (hybrid cord) 

ODF adapters are SC/APC 

Fiber 

OS2, duplex 

FR4 is single-mode, 2 km reach 

Polarity 

A-to-B, checked against ODF mapping 

Tx must land on far-end Rx 

Jacket 

OFNR 

Riser route from ODF room to switch row 

Length 

8 m 

Measured route plus slack 

Testing 

IL and RL per fiber 

APC return loss matters at the ODF 

 

At roughly 0.4 dB/km for OS2 at 1310 nm, 1.2 km of backbone adds about 0.5 dB. Two mated connector pairs at the ODFs add around 0.3 dB each, and two fusion splices about 0.05 dB each, for a total near 1.2 dB. That's well under the roughly 4 dB channel budget for 400GBASE-FR4. Treat these as planning figures and confirm them against the optic datasheet. 

If the ODF needs new bulkhead adapters for the APC side, add matching fiber optic adapters to the same order. 

 

Ordering Fiber Optic Cable Assemblies from L-com 

Once the spec sheet is complete, compare it against L-com's standard fiber optic cable assembly configurations by connector, fiber grade and length. If nothing standard fits, send the completed sheet with your custom request so every detail is already answered. For the optics, adapters and patch panels around the link, see L-com's data center connectivity lineup. 

 

Frequently Asked Questions (FAQs) 

 

Is a fiber optic patch cable the same as a fiber optic cable assembly? 

A fiber optic patch cable is one kind of fiber optic cable assembly. "Assembly" covers any factory-terminated fiber cable, including trunks, breakouts and harnesses, while "patch cable" usually means a short simplex or duplex jumper used at the rack or panel. 

Which fiber type does a data center link need? 

Choose the fiber grade from the optic and the distance. Single-mode OS2 reaches kilometers, while multimode pairs with cheaper short-reach optics but tops out at a few hundred meters, less at higher speeds. OM4 is a sensible multimode default for new builds, and OS2 is usually the better bet for runs longer than about 100 meters. 

Which fiber optic connector types should a data center standardize on? 

Most data centers standardize on LC for duplex links and MPO/MTP for parallel optics and trunks. SC tends to stay only where legacy panels or carrier ODFs require it. 

How long does a custom fiber optic cable assembly take? 

Lead time depends on the supplier and the configuration, so ask for it on the quote. Stock lengths and common connector pairs generally ship faster than custom lengths, hybrid connector combinations or high fiber count trunks. 

What is the difference between OFNP and OFNR jacket ratings? 

OFNP is the plenum rating, for cable that runs through air-handling spaces, and OFNR is the riser rating. A higher rating can always stand in for a lower one, so plenum can replace riser but never the reverse.

Resources

Search Entries