L-com

Cat7 vs Cat8: Do You Need Cat7 in a Modern Data Center?

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

When comparing Cat7 vs Cat8, it is easy to assume that Cat8 is simply a newer and faster version of Cat7. That is not the whole story. The bigger difference is how these categories fit into cabling standards and data-center deployment requirements. Cat7 is associated with the ISO/IEC Class F cabling system and was designed for high-performance copper connectivity, while Category 8 is defined within the ANSI/TIA balanced twisted-pair cabling framework for high-speed applications. TIA incorporated Category 8 specifications into its structured cabling standard and developed it for applications beyond 10 Gb/s. 

For data-center buyers, this distinction matters. Choosing a cable based only on the number printed on the jacket can create unnecessary complexity, compatibility questions, or additional installation requirements. So, do you actually need Cat7 in a modern data center? 

For most new standards-based deployments where high-speed copper is required, the answer is usually to evaluate Cat8 Ethernet cable rather than choosing Cat7 simply because it has a higher category number than Cat6A. 

 

Key Takeaways 

  • Cat7 is associated with ISO/IEC Class F cabling, while Cat8 is defined within the ANSI/TIA structured cabling framework. 
  • Cat8 was developed for applications beyond 10 Gb/s, with testing extending to 2000 MHz. 
  • Cat8 supports 25GBASE-T and 40GBASE-T over channels up to 30 m, with a maximum permanent-link length of 24 m. 
  • Cat7 systems have traditionally used GG45 or TERA connectors, while Cat8 maintains the familiar RJ45-style 8-position modular connector. 
  • A higher category number does not automatically mean better performance for a data center deployment. 
  • For most new standards-based deployments requiring high-speed copper, Cat8 is the category to evaluate first. 
  • Cat7/Class F can make sense when a project specifically follows an ISO/IEC Class F architecture. 
  • The complete channel, including cable, connectors, patch panels, and testing, should be specified rather than just the cable category. 

 

Cat7 vs Cat8: What Is the Difference? 

Cat7 and Cat8 are both high-performance copper cabling categories, but they belong to different standards frameworks and target somewhat different deployment scenarios. Cat7 is associated with ISO/IEC Class F cabling. Cat7 systems have traditionally used high-performance shielded construction and connector systems such as GG45 or TERA rather than treating conventional RJ45 connectivity as the defining interface. 

Cat8, by contrast, is included in the ANSI/TIA structured-cabling framework. TIA's Category 8 specification was developed for applications beyond 10GBASE-T, with testing extending to 2000 MHz. Category 8 also maintains compatibility with the familiar 8-position modular connector format commonly referred to as RJ45. This makes Cat8 easier to integrate with modern equipment that uses conventional Ethernet interfaces. 

 

Why Cat8 Was Developed 

Traditional structured copper cabling was designed around longer channel lengths and applications such as 1G and 10G Ethernet. As data-center equipment moved toward higher bandwidth, the industry needed copper cabling capable of supporting applications above 10 Gb/s over short distances. TIA's work on Category 8 specifically addressed these high-performance data-center requirements. Category 8 operates at a much higher frequency than Cat6A. TIA documentation identifies testing requirements extending to 2000 MHz, while Category 8 is intended for high-speed applications including 25GBASE-T and 40GBASE-T. 

This makes Cat8 particularly relevant for short connections between equipment in data-center environments. For buyers, the important point is simple: Cat8 was not created just to provide a bigger category number. It was created to address specific high-speed copper applications. 

 

Cat7 vs Cat8: Does Cat7 Offer Better Performance? 

This is one of the most common misconceptions. A Cat7 label does not automatically mean that a cable is a better choice than Cat8 for a new data-center deployment. Cat7 has a higher nominal frequency rating than Cat6A and is associated with ISO Class F cabling. However, frequency rating alone does not determine whether a cabling system is the right choice for a particular network. 

Data-center buyers should consider: 

  1. Which cabling standard the project follows. 
  1. Which connectors and components are being used. 
  1. What Ethernet application the network must support. 
  1. Required channel length. 
  1. Equipment interface compatibility. 
  1. Testing and certification requirements. 
  1. Installation space, bend radius, and cable management. 
  1. Future upgrade requirements. 

A cable marketed as “Cat7” may look attractive on a product page, but that does not automatically make it the preferred option for a standards-based TIA deployment. 

 

Is Cat7 Compatible With RJ45? 

This question needs careful wording. Cat7 is associated with ISO/IEC Class F systems and was designed around connector systems capable of supporting its performance requirements. GG45 and TERA are commonly associated with Cat7/Class F installations. At the same time, RJ45-style connectivity is widely used with Ethernet equipment, and some products marketed as Cat7 use RJ45 connectors. 

That creates an important distinction between a cable's marketing label and the performance of a complete standards-compliant channel. If an installation requires specific Category 7/Class F performance, the cable, connectors, patch panels, and testing methodology should be evaluated as a complete system rather than assuming that any cable labeled Cat7 provides the required performance. 

 

Why Cat8 Makes Sense for Some Data Centers 

Cat8 is designed specifically for high-performance copper applications where short-reach 25G and 40G connectivity is required. Category 8 has a maximum permanent-link length of 24 m and a maximum channel length of 30 m for 25/40G applications. It can also support lower-speed applications over longer channel configurations, depending on the application and installation. This short-reach design makes Cat8 particularly relevant for connections inside data-center racks and between nearby equipment. 

For example, a data-center deployment may use Cat8 for: 

  • Server-to-switch connections 
  • Switch-to-switch connections where supported 
  • High-speed copper links inside racks 
  • Short equipment interconnects 
  • Applications requiring 25GBASE-T or 40GBASE-T copper 

The physical infrastructure still needs to be planned carefully. Category 8 cabling operates at higher frequencies and can have stricter installation and testing considerations than lower-category copper systems. 

 

Cat8 Ethernet Cable: What Buyers Should Check 

If you are considering a Cat8 Ethernet cable, do not evaluate it only by its category designation. Check the complete product specification. 

1. Verify the application 

Determine whether the network actually requires 25GBASE-T or 40GBASE-T copper. If the equipment only requires 1G or 10G connectivity, Cat8 may provide more capability than necessary. 

2. Check channel length 

Cat8's high-speed 25G/40G application is intended for short channels. TIA-related guidance and testing information place the maximum Category 8 channel at 30 m for these applications. Measure the complete channel rather than looking only at the patch-cable length. 

3. Check connector compatibility 

Make sure the cable assembly and connector interface match the equipment and other components in the channel. Cat8 was designed around the widely used 8-position modular connector format, which helps support compatibility with modern Ethernet equipment. 

4. Consider shielding 

High-performance copper cabling commonly requires careful attention to shielding, grounding and installation practices. Do not assume that installing a shielded cable automatically creates a properly bonded shielded channel. The complete system needs to be installed according to the applicable requirements. 

5. Check cable management requirements 

Higher-performance copper cables can have construction characteristics that affect routing, bend radius, and cable density. In a high-density rack, poor cable management can make installation and maintenance more difficult even when the cable itself meets its specifications. 

 

Cat7 vs Cat8: Which Should You Choose? 

For a new data-center deployment, start with the network requirement and applicable cabling standard. 

Choose Cat7/Class F when: 

  • The project specifically follows an ISO/IEC Class F architecture. 
  • The existing infrastructure is designed around Cat7/Class F components. 
  • The connector and channel requirements are already defined for that system. 
  • The installation has a specific technical reason to use the Class F approach. 

Consider Cat8 when: 

  • The deployment requires high-speed copper connectivity. 
  • 25GBASE-T or 40GBASE-T is part of the design. 
  • Connections are within the short-reach limits of Category 8. 
  • The project follows a TIA-based structured-cabling approach. 
  • RJ45-style connectivity is important for equipment compatibility. 
  • The network needs a copper option for high-bandwidth data-center connections. 

The key is to specify the complete channel, not just the cable category. 

 

Do You Need Cat7 in a Modern Data Center? 

For most buyers, do not specify Cat7 simply because it appears to be a higher-performance option than Cat6A. Instead, determine whether your project requires ISO Class F cabling or whether a TIA Category 8 solution is better aligned with the network architecture. 

If you need 25G/40G copper over short data-center distances, Cat8 is the category specifically developed for that type of high-performance application. TIA's Category 8 work was created to address applications beyond 10 Gb/s, including 40GBASE-T. For broader infrastructure planning, review L-com data center solutions to evaluate connectivity options across the data-center environment. 

When the project calls for Cat8, evaluate the available Cat8 cable assemblies based on connector type, construction, shielding, length, and application requirements. Cat7 is associated with ISO/IEC Class F cabling and can make sense in installations designed around that standards framework. Cat8 is part of the TIA Category 8 ecosystem and was developed for high-performance copper applications, including 25GBASE-T and 40GBASE-T over short channels. 

For a new standards-based data-center deployment, buyers should avoid selecting Cat7 because of its “premium” marketing position. Define the Ethernet application, required speed, channel length, connector interface, installation environment, and applicable standard first. If the requirement is high-speed 25G/40G copper over short data-center links, Cat8 is the category worth evaluating first. 

 

Benefits of Choosing the Right Category 

Selecting the appropriate copper category can provide several practical benefits: 

  • Better standards alignment: The cabling system can be specified around the applicable industry standard rather than marketing terminology. 
  • Application-specific performance: Cable selection can match the actual Ethernet speed and distance requirements. 
  • Improved equipment compatibility: Connector selection can be coordinated with switches, servers and patching hardware. 
  • Simpler infrastructure planning: Understanding channel limits helps avoid unsuitable cable runs. 
  • Better upgrade planning: Cabling can be selected with future bandwidth requirements in mind. 
  • Reduced unnecessary spending: Buyers can avoid paying for capabilities that the network does not require. 
  • More predictable testing: A complete standards-based channel can be specified and tested consistently. 

 

Specifying Cat8 Cable Assemblies for the Data Center 

Selecting the right copper category starts with the application, the applicable standard, and the required channel length. For short-reach 25GBASE-T and 40GBASE-T links, L-com’s Cat8 Ethernet cable assemblies can be evaluated by connector type, construction, shielding, and length. L-com’s data center solutions also provide connectivity options across the wider data center environment. 

 

Frequently Asked Questions (FAQs) 

 

Is Cat7 better than Cat8? 
Not automatically. Cat7 and Cat8 are associated with different standards frameworks and deployment considerations. Cat8 is specifically designed for high-speed copper applications such as 25GBASE-T and 40GBASE-T over short channels. 

 

Is Cat7 compatible with RJ45? 
Some Cat7-marketed products use RJ45 connectors, but Cat7/Class F should not be treated as simply an RJ45 category. Cat7 is associated with ISO/IEC Class F systems and connector configurations such as GG45 and TERA. The complete channel should be evaluated for the required standard and performance. 

 

Is Cat8 Ethernet cable good for data centers? 
Yes, Cat8 is designed for high-performance copper applications and is particularly relevant to short data center links requiring 25GBASE-T or 40GBASE-T. Category 8 supports up to a 30 m channel for these applications. 

 

Do you need Cat7 in a modern data center? 
For most new standards-based deployments where high-speed copper is required, Cat8 should be evaluated rather than choosing Cat7 simply because it has a higher category number than Cat6A. Cat7 can make sense when the project specifically follows an ISO/IEC Class F architecture or the existing infrastructure is built around Cat7/Class F components. 

 

What is the maximum channel length for Cat8? 
Category 8 has a maximum permanent-link length of 24 m and a maximum channel length of 30 m for 25/40G applications. The complete channel should be measured rather than only the patch-cable length. 

Resources

Search Entries