L-com

CAN-Bus vs. Ethernet Cables in Automation Systems

By Eileen Harvey 

Modern automation systems are increasingly dependent on robust and reliable communication networks to facilitate seamless data transfer between various devices and components. In this context, two of the most widely used cabling systems in industrial automation are CAN-Bus cables and Ethernet cables. Each type is designed to excel in different applications. CAN-Bus cables, for instance, are particularly favored in automotive and robotics industries due to their ability to handle real-time data transmission with minimal delays, making them ideal for control systems that require quick responses.  

When it comes to sourcing reliable industrial-grade cables, TKD Kabel stands out as a leading provider, offering premium bus cables engineered for demanding environments. These cables are built to withstand harsh conditions typically found in factories, including extreme temperatures, moisture and mechanical stress, ensuring long-term performance and durability. 

What is CAN-Bus? 

CAN-Bus (Controller Area Network) is widely used in robotics, manufacturing and process automation. As automobiles became increasingly sophisticated, manufacturers faced the challenge of integrating numerous electronic control units (ECUs) without overwhelming the existing wiring systems. The introduction of CAN-Bus revolutionized this landscape by allowing multiple devices to communicate over a single two-wire bus, reducing the complexity and weight of wiring harnesses. 

Technical Characteristics 

CAN-Bus typically has an impedance of 120 Ohms. It uses twisted-pair conductors for noise immunity and shielding, often foil or braid, which is applied to reduce electromagnetic interference (EMI). Transmission speeds can reach up to 1 Mbps. 

Advantages of CAN-Bus 

The system provides real-time communication, ensuring that devices communicate instantly, which is particularly valuable for robotics and automotive safety systems. It also offers excellent noise immunity, making it suitable for noisy factory environments. CAN-Bus is cost-effective because it uses more affordable cabling compared to Ethernet and its simplicity makes it easy to implement in distributed control systems. An example of this technology is the CAN-Bus Fieldbus Cable, 120 Ohm, 24AWG Stranded, Shielded (100ft). 

What is Industrial Ethernet? 

Ethernet is the backbone of modern IT and increasingly Industrial Ethernet is being adopted in automation. Designed for high-speed communication, industrial Ethernet integrates easily with Industry 4.0 and Industrial Internet of Things (IIoT) systems. 

Technical Characteristics 

Industrial Ethernet includes cable types such as Cat5e, Cat6, Cat6a and industrial-grade Ethernet cables. It can support bandwidths of up to 10 Gbps. Typical network topologies include star or ring networks and transmission distances can reach up to 100 meters without repeaters. 

Advantages of Ethernet 

Ethernet offers high bandwidth to support massive data flow, making it ideal for smart factories. It is scalable, allowing for easy expansion and integration with cloud and IoT systems. Compatibility with existing IT infrastructure makes it straightforward to adopt and its future-proof nature ensures it supports advanced automation and predictive maintenance. 

Applications in Automation Systems 

CAN-Bus is best suited for automotive electronics and in-vehicle communication, robotics requiring low-latency responses, simple machine-to-machine (M2M) communications and compact networks with a limited number of devices. 

When to Use Ethernet 

Ethernet should be used in smart factories and Industry 4.0 environments, IIoT and big data monitoring applications, predictive maintenance systems and cases requiring integration with IT systems. 

Factors to Consider When Choosing Between CAN-Bus and Ethernet 

When making a choice, several factors should be evaluated. For network size, small and simple setups often benefit from CAN-Bus while large distributed systems typically require Ethernet. Regarding data requirements, if a system needs to transmit large datasets, Ethernet is the better option. For real-time needs, CAN-Bus excels in providing instantaneous control loops. In terms of environmental considerations, harsh conditions involving oil, UV exposure or chemicals call for rugged solutions such as TKD Kabel industrial-grade bus cables. Finally, when considering future scalability, Ethernet is generally more future-proof, especially with its ability to integrate seamlessly into IIoT systems. 

Tips and Recommendations 

  • For robotics and automotive, choose CAN-Bus for real-time precision. 
  • For smart factories, choose Ethernet for high-speed, scalable communication. 
  • Always select double-shielded cables in noisy industrial environments to prevent EMI. 
  • For outdoor and harsh conditions, pick UV- and oil-resistant jackets like those offered in TKD Kabel. 
  • Consider hybrid networks. Many industries run CAN-Bus at the machine level and Ethernet for plant-wide communication. 

FAQs (Frequently Asked Questions) 

Q1: Can I use CAN-Bus and Ethernet together in the same system?  
A: Yes. Many factories use CAN-Bus for local control and Ethernet for higher-level communication. Gateways can integrate both. 

Q2: Which is more cost-effective, CAN-Bus or Ethernet? 
A: CAN-Bus is cheaper in terms of both cable and implementation, but Ethernet provides long-term scalability. 

Q3: What is the maximum length for CAN-Bus cables? 
A: Up to 40 meters at 1 Mbps, but with lower speeds, it can extend up to 1000 meters. 

Q4: Are industrial Ethernet cables different from office Ethernet?  
A: Yes. Industrial Ethernet cables are ruggedized, with shielding, UV/oil resistance and temperature tolerance for harsh environments. 

Both CAN-Bus and Ethernet cables play vital roles in automation systems. Choose CAN-Bus if you need real-time, low-cost, noise-immune communication. Choose Ethernet if your system requires high-speed, scalable and data-heavy networking. 

For industries aiming to balance cost, speed and reliability, a hybrid approach often works best. If you’re looking for rugged, high-quality industrial cables, explore TKD Kabel Industrial-Grade Solutions for PROFIBUS, CAN-Bus, Ethernet and ASI Bus applications. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries