L-com

Armored Fiber Optic Cable for Harsh and High-Traffic Data Center Runs

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Fiber infrastructure in a data center does not always run through protected, low-traffic spaces. Fiber cables may travel beneath raised floors, above racks, through crowded overhead pathways, inside equipment rooms, or along routes where cables are exposed to accidental impact, crushing forces, rodents, or repeated maintenance activity. In these environments, standard fiber optic cable may require additional pathway protection. An armored fiber optic cable provides an additional mechanical protection layer around the fiber cable, helping protect the optical fibers from physical damage during installation and operation. 

Armored construction can be particularly useful where cables share pathways with power, equipment, or other infrastructure, or where maintaining an innerduct system is impractical. However, armor is not automatically the right choice for every data center run. It can increase cable weight, affect bend radius, complicate termination, and increase material cost. The decision should therefore be based on the pathway, physical risks, installation method, and maintenance requirements. 

 

Key Takeaways 

  • Armored fiber optic cable provides integrated mechanical protection around the fiber. 
  • Armor can help protect fiber from crushing, impact, maintenance activity, and rodent damage. 
  • Interlocking and corrugated armor have different construction characteristics and should be evaluated using manufacturer specifications. 
  • Armored fiber can be an alternative to standard fiber installed inside an innerduct in some applications. 
  • Armor adds weight, diameter, bend-radius considerations, and potentially cost. 
  • Metallic armored cable requires appropriate grounding and bonding considerations. 
  • Dielectric armored cable can be considered where a nonconductive construction is needed. 
  • Raised floors, overhead trays, high-traffic areas, and rodent-risk pathways are common situations where armor may warrant evaluation. 
  • Bulk fiber cable and pre-terminated fiber optic cable assemblies serve different installation needs. 
  • Cable selection should consider the entire pathway, not just the cable's mechanical rating. 

 

What Is an Armored Fiber Optic Cable? 

An armored fiber optic cable contains an additional protective layer designed to improve resistance to mechanical damage. Depending on the cable construction, the armor may be made from metallic or nonmetallic materials. Metallic armor can provide strong protection against crushing, impact, and rodent damage, while dielectric constructions can provide mechanical protection without introducing a conductive metallic layer. 

A typical armored cable may include: 

  1. Optical fibers 
  1. Fiber coating and buffer structure 
  1. Strength members 
  1. Inner jacket or subunit construction 
  1. Armor layer 
  1. Outer jacket 

The exact construction varies by cable design and application. For data center engineers, the important question is not simply whether a cable is labeled "armored." The cable should be evaluated according to the physical hazards present along the route and the installation requirements. 

 

Why Specify Armored Fiber in a Data Center? 

Fiber optic cables are relatively lightweight and immune to electromagnetic interference, but the optical fibers themselves still need protection from mechanical stress. 

Potential hazards include: 

  • Cable crushing 
  • Impact from tools or equipment 
  • Rodent damage 
  • Repeated maintenance activity 
  • Heavy cable bundles 
  • Foot traffic around raised floors 
  • Sharp pathway edges 
  • Tight or poorly controlled routing 
  • Construction activity near the cable pathway 

An armored cable can provide an additional mechanical barrier against these risks. This can be particularly valuable in high-traffic areas where technicians frequently access equipment or pathways. Instead of relying entirely on an external conduit or innerduct, the cable itself incorporates additional protection. 

 

Interlocking vs. Corrugated Armor 

Not all armored fiber optic cables use the same armor construction. Two common approaches are interlocking armor and corrugated armor. 

 

Interlocking Armor 

Interlocking armor is constructed using a helically formed metallic layer that surrounds the cable. Its design can provide strong mechanical protection while allowing the cable to retain a degree of flexibility. 

Interlocking armor may be considered for applications where: 

  • Mechanical protection is important 
  • The cable will be routed through exposed pathways 
  • Rodent resistance is a concern 
  • Technicians need to route the cable without installing a rigid conduit 
  • The pathway includes frequent access or maintenance activity 

One consideration is that interlocking armored cable can be heavier and larger than an equivalent unarmored cable. The additional construction may also increase minimum bend radius and affect handling. 

 

Corrugated Armor 

Corrugated armor generally uses a continuous metallic layer formed around the cable. The construction provides mechanical protection while maintaining flexibility suitable for many structured cabling applications. Corrugated designs can offer strong crush and impact resistance while providing a relatively continuous protective barrier. The appropriate construction depends on the cable's mechanical ratings, installation environment, termination method, and pathway design. Rather than selecting armor based only on construction name, engineers should compare the manufacturer's specifications for crush resistance, tensile strength, minimum bend radius, weight, temperature range, and installation requirements. 

 

When Armored Fiber Can Be Preferable 

Armored cable may be attractive when the pathway is already established but does not provide sufficient mechanical protection, and installing a separate innerduct would be difficult. For example, an overhead cable tray with frequent technician activity may benefit from a mechanically protected cable construction. 

 

When Innerduct May Be Preferable 

Innerduct can make more sense when the pathway is designed for future cable additions and removals. A replaceable innerduct can provide a controlled route for multiple cable installations over time. The decision should therefore consider the entire pathway strategy, rather than comparing the cable products alone. 

 

Where Armored Fiber Makes Sense 

Armored fiber is most useful where physical exposure is part of the installation environment. 

 

Under Raised Floors 

Under-floor spaces can contain dense cable pathways, power infrastructure, HVAC components, and areas that may be accessed during maintenance. If the cable route is exposed to foot traffic, equipment movement, or other physical hazards, additional mechanical protection may be appropriate. 

 

Overhead Cable Trays 

Overhead pathways can become crowded as a data center expands. Maintenance activity may also increase the risk of cables being pulled, stepped on, or struck. Armored construction can provide additional protection where the cable is exposed. 

 

High-Traffic Equipment Areas 

Fiber routes near racks and equipment can experience repeated maintenance activity. An armored cable can help reduce the risk of mechanical damage where cables are exposed to technicians, carts, tools, or other equipment. 

 

Rodent-Risk Areas 

Where facility conditions create a known rodent risk, armored construction can provide an additional physical barrier. The exact resistance depends on the armor and cable construction, so engineers should verify the manufacturer's rodent-resistance claims and applicable ratings rather than assuming all armored cables provide the same protection. 

 

Grounding and Bonding Metallic Armor 

Metallic armored fiber requires an additional consideration that does not apply in the same way to dielectric cable: grounding and bonding. If the cable includes conductive metallic armor, the installation should follow the applicable electrical, telecommunications, and facility bonding requirements. The armor may need to be bonded using appropriate hardware at designated termination points. The exact bonding method depends on the cable construction and facility grounding architecture. 

Engineers should verify: 

  • Whether the armor is electrically continuous 
  • Where bonding is required 
  • Which bonding hardware is specified 
  • How the cable termination connects to the bonding system 
  • Applicable local electrical and telecommunications codes 
  • Manufacturer installation instructions 

A key point is that metallic armor should not simply be installed and left electrically unaddressed. If the installation requires a nonconductive construction, a dielectric armored cable may be considered where appropriate. 

 

Armored Fiber Cable and Bend Radius 

One of the most important trade-offs when specifying armored fiber is bend radius. Additional protective layers can make a cable heavier, thicker, and less flexible than an equivalent unarmored cable. 

This matters in: 

  • Rack entrances 
  • Vertical transitions 
  • Patch panels 
  • Tight overhead pathways 
  • Under-floor transitions 
  • Equipment cabinets 

Engineers should always check both the minimum installation bend radius and the minimum long-term/static bend radius specified for the cable. A cable should never be forced into a bend tighter than its rated limit simply because the pathway has limited space. 

 

Armored Fiber Cable and High-Density Data Centers 

High-density environments require careful cable management because pathways may contain hundreds or thousands of connections. Adding armored cable can increase: 

  • Cable diameter 
  • Weight 
  • Tray loading 
  • Bend-radius requirements 
  • Installation effort 

For that reason, armor should be applied selectively rather than automatically to every fiber run. For protected rack-to-rack routes inside a controlled pathway, a conventional fiber optic cable assembly may be sufficient. For exposed pathways with higher mechanical risks, armored construction may provide additional protection. The objective is to match the cable construction to the environment. 

 

Selecting Bulk Cable vs. Fiber Optic Cable Assemblies 

The installation method also affects the right product format. Fiber bulk cable can be useful for engineered installations where cable lengths are determined on-site, and technicians or cable specialists will perform termination. Pre-terminated fiber optic cable assemblies, on the other hand, can simplify deployment when the required connector types and cable lengths are known in advance. For larger installations, engineers may use a combination of bulk cable for permanent infrastructure and pre-terminated assemblies for equipment or patching connections. When selecting either format, verify fiber count, mode, connector type, jacket construction, armor design, length, bend radius, and performance requirements. 

 

Common Mistakes When Specifying Armored Fiber 

One common mistake is specifying armored cable everywhere without considering its additional weight and bend-radius requirements. Another is treating all armored constructions as equivalent. Interlocking and corrugated designs can have different mechanical and installation characteristics. Engineers should also avoid overlooking metallic armor bonding requirements or assuming that an armored cable can replace every form of pathway protection. Finally, cable diameter and tray fill should be checked before deployment. A mechanically protected cable still needs to be routed and supported correctly. 

 

Building a More Resilient Data Center Fiber Pathway 

An armored fiber optic cable can be a practical solution when fiber routes face crush, impact, rodent, or high-traffic risks. Its integrated mechanical protection can reduce the need for additional pathway protection in certain applications. However, armor introduces trade-offs. The cable may be heavier, less flexible, larger in diameter, and more expensive than a comparable unarmored design. Metallic constructions also require appropriate attention to grounding and bonding. 

The best approach is to specify armor based on the actual pathway conditions. Under raised floors, overhead trays, high-traffic areas, or locations with documented physical hazards, armored construction may provide useful additional protection. In controlled pathways with adequate protection, conventional fiber may remain appropriate. By matching cable construction to the pathway, data center engineers can build fiber infrastructure that balances physical protection, installation efficiency, maintainability, and long-term scalability. 

 

How L-com Supports Data Center Fiber Infrastructure 
L-com provides connectivity products for data center and network applications. For projects that involve exposed or high-traffic pathways, L-com offers fiber optic bulk cable and pre-terminated fiber optic cable assemblies that can support a range of fiber counts, connector types, and installation requirements. 

 

Frequently Asked Questions (FAQs) 

 

1. What is an armored fiber optic cable? 
An armored fiber optic cable incorporates an additional protective layer around the fiber construction to improve resistance to mechanical damage such as crushing, impact, and, in some designs, rodent damage. The armor may be metallic or nonmetallic, depending on the cable construction. 

 

2. Is armored fiber better than regular fiber? 
Neither construction is universally better. Armored fiber is designed for environments where additional mechanical protection is needed. Standard fiber can be appropriate when the pathway already provides sufficient protection. Armor adds weight, diameter, bend-radius considerations, and potentially cost, so it should be applied selectively rather than to every run. 

 

3. What is the difference between interlocking and corrugated armored fiber? 
Interlocking armor generally uses a helically formed metallic layer, while corrugated armor uses a continuous corrugated metallic layer. The two constructions can differ in flexibility, weight, crush resistance, bend radius, and installation characteristics, so compare the manufacturer’s specifications rather than selecting by construction name alone. 

 

4. Where should I use armored fiber in a data center? 
Armored fiber is most useful where physical exposure is part of the installation environment, such as under raised floors, in overhead cable trays, in high-traffic equipment areas, and in areas with a known rodent risk. In controlled pathways with adequate protection, conventional fiber may remain appropriate. 

 

5. Can armored fiber replace innerduct? 
In some applications, yes. Armored cable may be attractive when a pathway is already established but doesn’t provide enough mechanical protection, and installing a separate innerduct would be difficult. Innerduct can make more sense when the pathway is designed for future cable additions and removals. 

 

6. Does armored fiber need to be grounded? 
Metallic armored fiber requires grounding and bonding that follow the applicable electrical, telecommunications, and facility requirements, along with the manufacturer’s installation instructions. If the installation requires a nonconductive construction, a dielectric armored cable may be considered where appropriate. 

Resources

Search Entries