The promise of the hybrid cloud lies in its flexibility—marrying the control of on-premise data centers with the scalability of public cloud platforms like AWS, Microsoft Azure and Google Cloud. But making this connection seamless is not just about software integration or multi-cloud orchestration. At the core of this transformation is the physical network—the structured cabling and connectors that ensure data flows securely, quickly and reliably between cloud and enterprise.
When building a hybrid cloud infrastructure, the stakes are high. Latency can’t compromise performance, bandwidth must support growing demands and every component must contribute to security and uptime. The physical infrastructure, often overlooked in favor of cloud-native tools, has a direct impact on data transfer speed, reliability and security. Selecting the right cabling components is crucial to building a high-performance hybrid environment.
Below are four tips that every IT leader should keep in mind when designing the network cabling backbone of a hybrid cloud deployment:
1. Single-Mode OS2 Fiber for Long-Haul Uplinks
For connecting enterprise data centers to cloud endpoints over long distances, single-mode OS2 fiber is the gold standard. With low attenuation and minimal signal loss, OS2 fiber supports transmission over many kilometers without the need for regeneration. It is optimized for 1310 nm and 1550 nm wavelengths, commonly used in data center interconnects and metro-area networks. This makes it ideal for hybrid cloud scenarios where performance consistency across long-haul connections is non-negotiable.
2. LC/MPO Connectors for Flexibility and Port Density
As data rates increase, connector technology must evolve to support more efficient, compact and scalable cabling solutions. LC connectors are widely used for single-mode and multi-mode applications due to their small form factor and high performance. MPO (multi-fiber push-on) connectors, meanwhile, offer the ability to terminate 8, 12 or even 24 fibers in a single interface, enabling rapid deployment and simplified cable management in high-density environments. Together, LC and MPO connectors provide the flexibility and port density needed to support the fiber demands of hybrid cloud infrastructures.
3. 10G/25G/40G/100G-Rated Cabling for Scalable Bandwidth
Hybrid cloud traffic is data-intensive—ranging from backup operations and application workloads to real-time analytics and machine learning tasks. Supporting this volume requires a cabling infrastructure that not only meets current needs but scales for future demand. High-speed cabling rated for 10G, 25G, 40G and 100G ensures that bandwidth bottlenecks don’t become the weak link in your hybrid environment. Matching the cabling performance to your active equipment ensures that you maximize the throughput and capabilities of your switches, servers and storage devices.
4. Shielded Cat6a+ Ethernet and Surge Protection for Internal Reliability
While fiber is essential for high-speed uplinks and backbone connectivity, copper Ethernet remains a staple within the data center. Shielded Cat6a+ cables offer enhanced protection against EMI/RFI interference, making them ideal for crowded environments with high electrical noise. These cables support 10 Gigabit Ethernet over distances up to 100 meters, ensuring internal links can match the speed of external uplinks. Pairing copper runs with robust surge protection devices adds an extra layer of defense—preventing electrical spikes from damaging critical hardware and ensuring the network stays operational during power fluctuations.
Structured cable management also plays a vital role in maintaining network performance and serviceability. Organized cable routing reduces signal crosstalk, improves airflow, and allows technicians to identify, troubleshoot and upgrade network paths more efficiently. In environments where downtime is costly, structured cabling is a reliability imperative.
As enterprises expand their digital footprint into the cloud, the importance of a solid physical network foundation cannot be overstated. Whether bridging multiple data centers or establishing secure cloud connections, the right combination of fiber, copper, connectors and protection makes the difference between a robust hybrid solution and a fragile one. By focusing on performance, scalability and structured design, IT teams can ensure their hybrid cloud infrastructure is built to last.
If you are building a hybrid cloud infrastructure, L-com has the high-performance network cabling and connectors you need. Explore our wide selection now at L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST.