A sensor drops offline, data arrives corrupted or a controller loses contact with an actuator. When the fault comes and goes, tracking it down can take time while production suffers. Signal loss in bus cables can be behind these interruptions, turning a communication problem into costly downtime and extra maintenance.
Impedance mismatch, attenuation, electromagnetic interference (EMI) and poor termination can all play a part, often in combination. Longer cable runs and weaker shielding make the network more vulnerable. So where should you look first, and how can you keep the problem from returning?
Bus cables carry the real-time data that controllers, sensors and actuators need to work together. Let's look at what weakens those signals, how the effects show up in industrial systems and which cable choices and installation checks help prevent them.
Key Takeaways
- Signal loss in bus cables is usually caused by impedance mismatch, cable attenuation, EMI or poor termination.
- Longer cable runs and lower-quality shielding both increase susceptibility to signal loss.
- Signal loss can cause intermittent faults that are hard to diagnose in industrial communication networks.
- Proper termination, correct impedance matching and quality shielding are the primary prevention methods.
What Is Signal Loss in Bus Cables?
Before diagnosing signal loss, it helps to understand what bus cables are and how they carry data. Signal loss, also known as attenuation, is the gradual reduction in a data signal's strength and clarity as it travels through a cable. Some loss happens naturally because of the cable material's resistance and electrical properties. If the signal weakens too much, the receiver may struggle to distinguish it from electrical noise, leading to data errors.
In systems such as PROFIBUS, PROFINET, Ether CAT and other bus networks, devices depend on accurate, timely data. High levels of EMI and demanding physical conditions make that harder to maintain. A deteriorating signal can cause delays, misread data or a complete communication failure. To find the source, start with the cable, its installation and the environment around it.
Main Causes of Signal Loss in Bus Cables
Electromagnetic Interference (EMI)
Motors, power lines, radio transmitters and other electronic equipment generate external fields that can introduce unwanted noise into a cable. This electromagnetic interference distorts the transmitted signal, causing data errors or a complete loss of communication.
Cable Quality
The cable's condition matters too. Inferior materials and physical damage can weaken insulation and shielding, leaving signals more exposed to attenuation and outside noise. See bus cable construction and jacket material for how construction choices affect this.
Incorrect Termination
Even a good cable can have signal problems if it isn't terminated correctly. Without proper termination at the ends of a bus line, signals reflect back along the cable and interfere with the original transmission, causing distortion and potential data loss.
Exceeding Cable Length Limits
Length is another limit to check. Each bus protocol specifies a maximum segment length, such as 100 meters for Ethernet-based PROFINET. Exceeding that distance weakens the signal and increases errors.
Inadequate Shielding or Poor Grounding
Shielding and grounding need attention as well, especially over longer runs. Inadequate shielding or poor grounding lets interference reach the cable and degrade signal quality.
Environmental Factors
Finally, consider what the cable faces day to day. Extreme temperatures, chemicals, oils, ultraviolet radiation and mechanical stress can damage it and reduce its ability to carry reliable signals.
Causes and Fixes at a Glance
Once you've identified a likely cause, use this table to connect it with a practical fix.
| Cause | Fix |
|---|---|
| Electromagnetic interference (EMI) | Route cables away from motors and power lines; use shielded twisted-pair cable. |
| Poor cable quality or physical damage | Use industrial-grade cable; replace damaged or aging cable promptly. |
| Incorrect termination | Use the correct termination resistors at both ends of the bus. |
| Exceeding cable length limits | Stay within the protocol's maximum segment length; add repeaters if needed. |
| Inadequate shielding or poor grounding | Use adequately shielded cable; ground shields correctly at one or both ends. |
| Environmental exposure (heat, UV, chemicals) | Choose a jacket rated for the environment; protect with conduit or enclosures. |
How Signal Loss Affects Industrial Communication
These faults affect more than the data traveling through a cable. In automation, transportation, oil and gas, and outdoor infrastructure, controllers, sensors and actuators rely on clear communication to keep systems running reliably. A breakdown in that communication can affect efficiency and safety.
Standard cables may fail prematurely in oil-rich areas, outdoor installations exposed to UV, or facilities with extreme temperatures and corrosive chemicals. That can interrupt operations, increase maintenance costs and introduce safety risks in mission-critical applications. The prevention steps below start with matching the cable to those conditions.
How to Prevent and Minimize Signal Loss
Start with high-quality, industrial-grade cables designed for the environment, with suitable shielding, insulation and durability. During installation, route cables away from strong EMI sources, use shielded twisted-pair designs where appropriate and ground the shields correctly. Avoid tight bends, excessive tension and physical stress to help the cables last.
Next, check the protocol's maximum segment length and keep each run within it to maintain signal integrity. Use the correct termination resistors and ground shields and connected devices properly. These steps help minimize reflections and interference.
Keep checking the installation after it's in service. Inspect cables for wear, corrosion and mechanical damage, and replace compromised cables promptly. Where needed, use conduits or enclosures to protect against chemicals, ultraviolet light and mechanical stress.
Why do length, shielding and maintenance deserve this attention? The figures below put their effect on signal reliability in perspective.
Facts About Signal Loss in Bus Cables
Signal attenuation increases approximately linearly as cable length grows, making longer runs more vulnerable to degradation. Proper shielding can reduce EMI by as much as 90 percent. Twisted-pair cables also help cancel EMI and crosstalk.
Routine maintenance and inspections can prevent as many as 80 percent of communication failures resulting from signal loss. Some industrial bus systems can also operate reliably over distances of up to 1,000 meters when repeaters and properly designed cabling are used.
When troubleshooting signal loss in bus cables, use the likely cause to guide your next step, whether that's addressing EMI, replacing a damaged cable or correcting the installation. Cable selection, installation practices and regular maintenance work together to keep communication reliable.
If your checks point to a cable replacement, L-com's TKD Kabel range is one place to explore suitable options and get help with selection.
About L-com
Explore the full range of TKD Kabel through L-com. We'll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com.
Still have questions about spotting signal loss or preventing it? Here are answers to common troubleshooting questions.
FAQs About Signal Loss in Bus Cables
What causes signal loss in bus cables?
The most common causes are electromagnetic interference (EMI), poor cable quality or physical damage, incorrect termination, exceeding the protocol's maximum cable length, and inadequate shielding or grounding. Exposure to heat, UV or chemicals can make these problems worse.
How do I know if my bus cable has signal loss?
Watch for intermittent communication faults, corrupted or dropped data packets, devices that fall offline unpredictably, or errors that appear and disappear without a clear pattern. These symptoms are often signal loss rather than a hard wiring fault, especially if they worsen with distance or near EMI sources.
Does cable length affect signal loss in bus cables?
Yes. Signal attenuation increases roughly linearly with cable length, which is why every bus protocol specifies a maximum segment length. For example, the limit is 100 meters for Ethernet-based PROFINET. Exceeding it weakens the signal and increases errors unless repeaters are used.
How can I prevent signal loss in an industrial bus cable network?
Use industrial-grade, adequately shielded cable; terminate the bus correctly at both ends with the right resistors; stay within the protocol's maximum segment length; ground shields properly; and route cables away from EMI sources like motors and power lines. Regular inspection catches wear before it causes a failure.