L-com

What Is the Maximum Length for PROFIBUS / CAN-Bus Cables?

By Eileen Harvey 

In automation and control systems, communication protocols like PROFIBUS and CAN-Bus are vital for connecting sensors, actuators, controllers and other devices. A common concern among engineers and system integrators is how long the cables can be while maintaining reliable data transmission. PROFIBUS and CAN-Bus play a critical role in ensuring seamless interaction among various components, including sensors, actuators, controllers and other devices.  

These protocols serve as the backbone of automated systems, enabling devices to exchange information efficiently and effectively. However, one of the most pressing concerns for engineers and system integrators is the optimal length of the cables used in these systems, as it directly impacts the reliability of data transmission. The maximum cable lengths specified for each protocol are not arbitrary; they are determined based on factors including signal integrity, electromagnetic interference and the data rate being utilized.  

Why Cable Length Matters 

Cable length can profoundly affect performance, impacting signal integrity, transmission speed and overall user experience. Shorter cables often provide advantages such as reduced latency and lower susceptibility to interference, which makes them well suited for high-speed data transfer in environments like data centers and server rooms. In contrast, longer cables can introduce challenges such as signal degradation and increased latency that may hinder performance in critical applications. 

The length of communication cables directly influences signal quality. As cables grow longer, the risks increase for signal attenuation or loss of strength, greater susceptibility to electromagnetic interference, a higher chance of data errors and reduced system reliability. For these reasons, adhering to industry standards and manufacturer specifications is essential to maintaining optimal system performance. 

Factors Affecting Cable Length 

Standard maximum lengths established in industry specifications and manufacturer recommendations serve as important guidelines to ensure proper performance and signal integrity. However, actual cable lengths that can be used effectively depend on real-world conditions. Environmental factors, installation practices and the specific application all play a role in determining how far a cable can reliably transmit data or power without degradation. 

Signal attenuation is one of the most critical considerations, as signal strength diminishes the farther it travels through the cable, and longer runs increase the risk of data errors. Electromagnetic interference is another major factor, especially in industrial environments with motors, transformers or radio signals, although shielded cables can help mitigate these effects. Cable quality and impedance also matter because high-quality, impedance-matched cables reduce reflections and signal loss. Proper termination and grounding are equally important, since the use of correct termination resistors, such as 120 ohms for CAN-Bus, prevents reflections, while correct grounding helps reduce noise. Finally, the required data rate has a direct effect on allowable length, with higher data rates requiring shorter cables to maintain signal integrity. 

Best Practices for Extending PROFIBUS and CAN-Bus Cables 

To maximize cable length without sacrificing communication reliability, several practices should be followed. Using high-quality cables with appropriate shielding and impedance matching is critical. Proper termination resistors should be implemented at both ends of the network. Correct grounding and shielding practices reduce electromagnetic interference, while careful installation that avoids sharp bends and physical stress ensures longer cable life and consistent performance. 

For extensive networks, segmenting long runs into smaller sections with repeaters or hubs can help maintain signal quality. Choosing industrial-grade cables from reputable brands such as TKD Kabel provides additional reliability. Examples include PROFIBUS DP FMS FIP 1 Pair 150 Ohm 22 AWG solid double-shielded cables and CAN-Bus 1 Pair 120 Ohm 24 AWG stranded double-shielded cables. 

Tips for Ensuring Reliable Long-Distance Communication 

Several practices can help ensure reliable communication over long distances. It is important to follow the maximum lengths recommended by protocol standards. Using shielded, high-quality, impedance-matched cables is a key factor, along with proper termination of the network at both ends. Cables should be kept away from sources of electromagnetic interference whenever possible. Regular inspection and maintenance of connections help prevent failures, while repeaters or network bridges can be incorporated into large systems to extend overall reach and maintain consistent performance. 

FAQs (Frequently Asked Questions) 

Q1: Can I extend my PROFIBUS or CAN-Bus network beyond the maximum length?  
A: While standards provide maximum lengths, extending beyond these limits without additional devices like repeaters or hubs can cause signal degradation. Use repeaters or segment the network to maintain reliability. 

Q2: What happens if the cable length exceeds the recommended maximum?  
A: Signal attenuation increases, leading to data errors, communication failures and potential system downtime. 

Q3: How do shielded cables improve maximum cable length?  
A: Shielding reduces EMI, which helps maintain signal integrity over longer distances, effectively allowing for longer cable runs in noisy environments. 

Q4: Are fiber optic cables a better option for long distances?  
A: Yes. Fiber optic cables are immune to EMI and support very long distances with high data rates, making them ideal for extended networks. 

Q5: How important is proper termination in CAN-Bus networks?  
A: Very important. Proper termination (typically 120 ohms at each end) prevents signal reflections, which can cause data errors. 

 

For industrial applications that demand reliable data transmission over long distances, making the right choice in cabling is critical to the success of operations. The environment in which these cables operate can vary significantly, from extreme temperatures and humidity levels to exposure to chemicals and physical wear.  

Therefore, investing in high-quality, industrial-grade cables is not just a matter of convenience, but a necessity that can safeguard against potential disruptions. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

 

Resources

Search Entries