L-com

Using Servo and VFD Cables in Harsh Environments

By Eileen Harvey 

Servo and variable frequency drive (VFD) cables play an indispensable role in the world of industrial automation, CNC machines and motion control systems. These specialized cables are designed to facilitate the precise delivery of power and the reliable transmission of signals, which are crucial for the seamless operation of automated processes. In environments where equipment operates continuously and demands high performance, the integrity of these cables is paramount.  

A well-engineered servo or VFD cable ensures that machinery responds accurately to commands, maintaining operational efficiency and product quality. However, these cables must navigate a landscape of potential hazards that can compromise their functionality and longevity. In harsh industrial environments, servo and VFD cables encounter a variety of extreme challenges that can lead to significant issues if not properly addressed. Factors such as exposure to oils, ultraviolet (UV) radiation, harsh chemicals and mechanical stress can severely degrade standard cables over time.  

Understanding Harsh Industrial Environments 

Industrial applications rarely operate in clean, controlled conditions. Instead, cables are exposed to elements that compromise their performance: 

  • Oil and lubricants – Common in automotive and machining plants, oils can penetrate cable jackets, causing swelling, cracking or insulation breakdown. 
  • UV radiation – Outdoor equipment, renewable energy systems and mining setups face constant sunlight, leading to brittleness and fading in non-UV-protected cables. 
  • Chemicals and solvents – Harsh cleaning agents, acids and industrial chemicals can corrode cables, impacting signal reliability and safety. 
  • Mechanical stress – Frequent bending, torsion and abrasion can quickly wear down cables in moving robotics and CNC machines. 

Challenges Faced by Servo and VFD Cables in Harsh Conditions 

Servo and VFD cables often operate in environments that expose them to oil, sunlight and aggressive chemicals, each of which can degrade performance over time. Oil damage is a frequent issue because oils attack PVC insulation, causing it to lose flexibility and potentially leading to short circuits. UV degradation is another challenge, as prolonged exposure to sunlight makes standard cable jackets brittle and prone to cracking. Chemical corrosion occurs when industrial solvents or cleaning solutions break down insulation and shielding, weakening the cable structure. These factors increase downtime risks since cable failure in automation or motion control systems can halt entire production lines and disrupt operations. 

Material Selection for Durability 

The longevity and performance of servo and VFD cables depend heavily on the materials used for their jackets and insulation. PUR (polyurethane) offers excellent resistance to oil, abrasion and chemicals while remaining highly flexible, making it ideal for demanding industrial settings. TPE (thermoplastic elastomer) provides strong chemical and temperature resistance for environments with harsh cleaning agents or heat exposure. XLPE (cross-linked polyethylene) delivers robust insulation capable of withstanding high heat and voltage stress. Cables made with UV stabilized compounds are designed to endure long-term outdoor sun exposure. Together, these materials help ensure cables remain flexible, safe and reliable even under extreme conditions. 

Design Considerations for Harsh Environment Cables 

Selecting cables for oil rich, UV exposed or chemically intensive environments requires attention to specific design features. Reinforced jackets made from thick PUR or TPE resist cuts and abrasions, providing essential protection in heavy duty applications. Double shielding that combines aluminum foil with braided copper helps guard against EMI. Flame-retardant and halogen-free materials support safety compliance in enclosed areas. Torsional resistance is also crucial for robotics and moving machinery where cables must twist and flex without fatigue or failure. 

Applications in Harsh Industrial Settings 

Durable servo and VFD cables are used widely across industries that demand reliable operation under severe conditions. In oil and gas environments they withstand drilling mud, lubricants and hydrocarbon exposure. Automotive manufacturing requires cables that can endure oil splashes, welding sparks and continuous flexing in assembly robots. Food and beverage facilities rely on cables resistant to strong cleaning agents, hot water and disinfectants. Renewable energy installations such as solar and wind power systems need cables that survive prolonged UV radiation and outdoor exposure. Chemical plants depend on cables capable of withstanding aggressive solvents, acids and industrial chemicals. 

Best Practices for Extending Cable Life 

Proper handling and maintenance are essential to maximizing cable life even when using high durability designs. Regular inspections help identify early signs of cracks, brittleness or swelling in cable jackets. Correct routing avoids tight bends and sharp edges that create mechanical stress. Protective conduits or cable carriers should be used in high wear areas to prevent abrasion. Replacing cables before complete failure occurs helps minimize costly downtime. It is also important to use certified cables that have been tested for oil, UV and chemical resistance to ensure reliable performance in harsh environments. 

Recommended Servo and VFD Cables for Harsh Environments 

Here are some excellent options from TKD Kabel that are engineered for reliability in harsh conditions: 

FAQs About Servo and VFD Cables in Harsh Environments 

Q1: Why do standard cables fail in oily environments? 
A: PVC jackets absorb oils, causing insulation to swell and crack. Oil-resistant PUR or TPE jackets are better suited. 

Q2: Can outdoor VFD cables survive without UV protection? 
A: No. UV exposure degrades insulation quickly. Always use UV-stabilized jackets for outdoor applications. 

Q3: Are chemical-resistant cables necessary in food plants? 
A: Yes. Cleaning agents and disinfectants corrode standard cables. Chemical-resistant cables improve hygiene compliance and reduce downtime. 

Choosing the right servo and VFD cables for harsh environments is not just a matter of durability; it’s about ensuring operational safety, reliability and cost efficiency. By selecting cables engineered for oil, UV and chemical resistance, industries can reduce downtime, extend equipment life and improve overall performance. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries