By Eileen Harvey
Shielded and unshielded industrial Ethernet cables can both deliver reliable network performance, but the right choice depends on electromagnetic interference, cable length, data speed, installation conditions and budget. Understanding UTP, FTP, STP and S/FTP designs helps engineers match cable shielding to the electrical noise and reliability requirements of each industrial application.
Key Takeaways
- Shielded Ethernet cable is generally the better choice in industrial environments with motors, welders, VFDs, high-voltage lines or other strong EMI/RFI sources.
- Unshielded UTP cable is lighter, more flexible and less expensive, making it suitable for short runs and controlled, low-interference environments.
- FTP, STP, F/UTP and S/FTP use different foil and braid shielding structures; the appropriate design depends on the severity and type of interference.
- Shielded Ethernet cabling requires compatible shielded connectors and proper grounding to maintain effective EMI protection across the connection.
- Cable selection should consider EMI exposure, run length, data rate, routing, flexibility and total cost rather than assuming shielded cable is always necessary.
When designing or upgrading an industrial network, choosing between shielded and unshielded Ethernet cables is more than a technical detail. It's a decision that can determine signal reliability, downtime risk and long-term system performance.
Industrial environments introduce unique challenges such as electromagnetic interference (EMI), mechanical stress and exposure to harsh conditions. Selecting the right cable type helps your Category 5e, Cat6 or Cat6a industrial Ethernet cables maintain optimal data transmission even in demanding settings.
Shielded vs Unshielded Ethernet Cable: Key Differences
The main difference in a shielded vs unshielded Ethernet cable comparison is the conductive shield, made of foil, braid or both, that shielded cable adds around the pairs or the whole cable. The table below summarizes how the two compare. Neither is universally superior, and a properly designed unshielded system can perform reliably in many environments.
| Factor | Shielded Ethernet Cable | Unshielded Ethernet Cable |
|---|---|---|
| EMI/RFI protection | Reduces electromagnetic coupling when correctly designed and installed | Relies on balanced twisted pairs to reduce noise |
| Flexibility | Typically thicker and less flexible | Typically lighter and more flexible |
| Installation complexity | Higher; needs compatible components and careful termination | Simpler to route and terminate |
| Shield termination | Required; shield continuity must be maintained through the channel | Not applicable |
| Cost | Typically higher cable and hardware cost | Typically lower cable and hardware cost |
| Suitable environments | Strong EMI/RFI sources and noisy industrial areas | Controlled, lower-noise environments |
This comparison also applies to STP vs UTP cable choices, covered in more detail below.
Unshielded Twisted-Pair Cable
U/UTP cable, commonly called UTP, consists of pairs of twisted conductors without an additional shield. It relies on balanced twisted pairs rather than a conductive shield to reduce noise. The twist helps cancel out some interference, which makes unshielded Ethernet cable lighter, more flexible and cost-effective. Its advantages include lower cost, light weight, easy installation and flexibility for routing through tight spaces.
Because unshielded cable has no conductive shield, it can be more susceptible to EMI and crosstalk in high-noise industrial areas. Every installed link should meet its required performance level, so the cable category, installation quality and testing all matter. When comparing FTP vs UTP cable, the key question is whether the environment's noise level calls for the added shield.
Browse industrial Ethernet cables from L-com to see UTP options for general industrial networking.
Shielded Twisted-Pair Cable
Shielded Ethernet cable may use foil, braid or both around the overall cable, around individual pairs, or both. This construction reduces electromagnetic coupling from external EMI and RFI when it is correctly designed and installed. It can also reduce crosstalk between cable pairs. Designs such as S/FTP cable combine multiple shielding layers for demanding environments.
The tradeoffs are slightly higher cost, thicker and less flexible construction compared to UTP, and the need for proper termination and grounding for the shield to work effectively. In an STP vs UTP cable decision, these installation requirements matter as much as the cable itself.
For example, L-com's shielded industrial Ethernet cables offer rugged designs for demanding automation and outdoor use.
When to Use Shielded Industrial Ethernet Cable
Shielded Ethernet cable is a strong option in environments with significant EMI/RFI sources, where unshielded cables could lead to data loss, errors or downtime. Common sources include:
- Motors and conveyors
- Variable-frequency drives (VFDs)
- Welding equipment
- High-current power conductors
For additional guidance, review how proper shielded cable selection can reduce EMI in industrial network installations.
Shielding does not replace pathway separation, bonding or surge protection. It works alongside them. Not every outdoor, data center or 10Gb Ethernet installation automatically requires shielded cable. The decision depends on the actual noise environment, the cable category and the installation. When comparing shielded vs unshielded Cat6 cable for high-speed links, evaluate the EMI exposure and channel requirements rather than the data rate alone.
When to Use Unshielded Industrial Ethernet Cable
Unshielded cable can be appropriate in controlled, lower-noise environments where the selected category and installation meet performance requirements. It offers easier handling and lower cost. Typical examples include:
- Office spaces inside industrial buildings with low EMI
- Short cable runs with limited exposure to interference sources
- Installations where budget and flexibility are important and the noise environment is well understood
Unshielded cable should not be treated as suitable only for non-critical applications. Cable balance, category, installation quality and testing all affect performance. In an STP vs UTP cable comparison, a well-installed and tested unshielded channel can meet the requirements of many applications.
Types of Ethernet Cable Shielding
Not all shielding is the same. The term "STP" is often used as a broad or ambiguous term, and the same name can describe different constructions. The standardized slash notation describes the construction more precisely, with the first letter showing the overall shield and the letters after the slash showing the pair construction:
- U/UTP: no overall shield and unshielded pairs.
- F/UTP: overall foil shield with unshielded pairs.
- S/UTP: overall braid with unshielded pairs.
- U/FTP: no overall shield, with individually foiled pairs.
- F/FTP: overall foil plus individually foiled pairs.
- S/FTP: overall braid plus individually foiled pairs.
Understanding these differences helps match the shielding type to the severity of your environment, and it clears up confusion when comparing FTP vs UTP cable, S/FTP cable and other STP vs UTP cable options.
Shield Termination, Bonding and Installation
A shielded channel requires compatible shielded connectors, patch panels and equipment interfaces. The shield must stay continuous from one end of the channel to the other, so every component in the path needs to support shielding. Follow the applicable bonding and installation requirements for your site.
Incomplete termination or a break in shield continuity can reduce the shield's effectiveness, so the cable may not deliver the EMI protection it was selected for. Correct Ethernet cable grounding and termination are what allow a shielded Ethernet cable to perform as designed.
Other installation practices include:
- Keep Ethernet cables separate from high-voltage power cables whenever possible.
- For outdoor use, make sure the cable is UV-resistant and rated for outdoor environments, such as CMX-rated cable.
- Follow standards like TIA/EIA-568 guidelines for proper cabling practices.
How to Choose the Right Industrial Ethernet Cable
The decision between shielded and unshielded industrial Ethernet cables depends on environmental conditions, network requirements and budget. Evaluate the following factors:
- Measured or expected EMI/RFI exposure. Consider proximity to high-voltage lines, motors, drives or RF sources. This is the most important factor in a shielded vs unshielded Ethernet cable decision.
- Cable category and data-rate requirements. Higher data rates place greater demands on the channel. Data-rate and environmental requirements should also guide the choice between Cat5e, Cat6 and Cat6A for industrial use.
- Pathway separation from power conductors. Keeping data and power cables apart reduces noise exposure whichever cable type you choose.
- Fixed versus continuous-flex installation. Unshielded cable is generally easier to handle in tight spaces, while shielded cable is typically thicker. Fixed installations and moving patch connections may also require different stranded and solid conductors for Ethernet.
- Indoor, outdoor, wet-location, sunlight and chemical exposure. Match the jacket and construction to the environment. For harsh environments, compare PVC, PUR and TPE cable jacket materials before selecting an industrial Ethernet cable.
- Compatible connectors and termination hardware. A shielded channel needs shielded connectors, patch panels and equipment interfaces throughout.
- Installation and testing requirements. Installation quality and testing affect the performance of both shielded and unshielded cable.
- Total installed cost rather than cable price alone. Shielded cable adds material and installation cost, but in noisy environments it can help prevent costly downtime. In controlled environments, unshielded Ethernet cable can meet requirements at lower cost.
Also look for compliance with relevant standards, including TIA/EIA-568 (U.S. structured cabling standard), ISO/IEC 11801 (international cabling standard), UL-listed safety ratings and industrial Ethernet-specific standards like EtherNet/IP and PROFINET. Selecting the right cable is an investment in network stability and operational uptime.
Choose shielded cable if you are in a high-EMI environment, need maximum reliability or run high-speed connections over long distances. Choose unshielded cable if your environment is controlled, interference is minimal and cost or flexibility is a higher priority.
Frequently Asked Questions
Can Shielded and Unshielded Cables Be Used in the Same Network?
Yes, they can coexist, but an unshielded section does not gain shielding protection from adjacent shielded components. Each channel must meet its required performance on its own.
Do Shielded Ethernet Cables Require Special Connectors?
Yes. Compatible shielded connectors and termination hardware are needed to maintain shield continuity through the channel. Proper Ethernet cable grounding depends on this continuity.
Are Shielded Ethernet Cables Always Better?
No. The correct choice depends on EMI exposure, cable design, installation requirements, flexibility and total cost. In a shielded vs unshielded Ethernet cable comparison, shielded cable offers more protection in noisy environments, while unshielded cable can be a better fit for controlled, lower-noise installations.
When Should You Use Shielded Ethernet Cable?
Use shielded Ethernet cable where strong EMI/RFI sources are present, such as motors, VFDs, welding equipment and high-current power conductors. Shielding works alongside pathway separation, bonding and surge protection.
Does Shielded Ethernet Cable Need to Be Grounded?
Yes. A shielded channel needs proper termination and bonding to maintain shield continuity and deliver its intended EMI protection. Follow the applicable installation and bonding requirements.
What Is the Difference Between UTP, FTP, STP and S/FTP Ethernet Cable?
UTP has no shield, FTP has a foil shield, and S/FTP has an overall braid plus individually foiled pairs. "STP" is often used loosely, so the slash notation (such as F/UTP, U/FTP or S/FTP) describes the construction more precisely.
Explore industrial Ethernet cables to find both shielded and unshielded options built for demanding industrial applications.