L-com

Why Do Servo Cables Fail Prematurely?

A failing servo cable can bring an entire production line to a halt. Before that happens, it may cause intermittent motor faults, unreliable feedback or repeated replacements. Understanding why servo cables fail helps you spot the warning signs and address the stresses that shorten their working life.

Repeated bending, electromagnetic interference (EMI), excess heat and poor installation are common causes of early failure. The cable's construction matters too: its conductors, shielding and jacket need to suit both the movement and the environment.

So how can you keep your servo cables working reliably for longer? Let's look at their construction, trace the causes of failure and work through warning signs, troubleshooting and prevention, with examples from TKD Kabel servo cables.

 

Key Takeaways

  • The most common causes of premature servo cable failure are repeated bending stress, EMI, excess heat and poor installation practice.
  • Early warning signs include intermittent faults, visible jacket cracking and erratic motor feedback.
  • Matching cable flex-rating and shielding to the application prevents most premature failures.
  • TKD Kabel servo cables through L-com are built for continuous-motion and harsh-environment use.

 

Understanding Servo Cable Construction

Unlike standard power cables, servo cables are engineered for continuous motion. Their conductors carry motor current and control signals, while shielding protects against electromagnetic interference (EMI) that can cause motor errors. Insulation and jackets withstand flexing, chemicals and temperature fluctuations. Some hybrid configurations combine power, feedback and brake control in a single jacket.

The more demanding the application, whether it's a robot, drag chain or CNC machine, the more specialized the design needs to be. When the cable or installation doesn't match those demands, several types of stress can lead to failure.

 

Common Causes of Premature Servo Cable Failure

Start by looking at the stresses the cable faces during everyday operation:

  • Mechanical stress and flexing are major contributors, as repeated bending in robotic arms and drag chains wears out conductors. Failure also occurs when the bend radius is tighter than manufacturer recommendations or when non-flex-rated cables are used in continuous-motion applications.
  • Electrical stress is another factor and can result from voltage surges or overloads that damage insulation. Poor servo cable shielding leads to EMI and signal loss and grounding issues accelerate wear.
  • Heat is another source of stress. High current flow, poor ventilation in control cabinets and jackets that aren't designed for high temperatures can all contribute to thermal problems.
  • The surrounding environment matters too. Oils, solvents and coolants can degrade PVC jackets, while UV radiation and outdoor exposure can crack insulation. Moisture entering the cable can also cause short circuits.
  • Installation can create stress points before a cable starts moving. Sharp routing edges can damage the jacket, incorrect clamping or inadequate strain relief can add stress, and overcrowded trays can leave cables without enough spacing.
  • Manufacturing and quality issues are another source of failure particularly when substandard cables not intended for servo use are chosen or when cheap insulation and shielding break down quickly. This is why brands like TKD Kabel are trusted worldwide for long life, high flexibility and resistance to harsh environments.

These stresses don't always cause an immediate breakdown. Knowing what to watch for can help you catch a problem while there's still time to act.

 

Signs of Servo Cable Failure

Intermittent motor faults or alarms are often the first sign of trouble, followed by inconsistent encoder feedback or EMI-related errors. Check for visible jacket cracks, exposed conductors and increased heat along the cable run too. Catching these changes early can help you avoid costly downtime.

Once you've spotted a warning sign, the next step is to narrow down what's causing it.

 

Troubleshooting Servo Cable Issues

When servo performance drops, start with a visual inspection for cuts, cracks or kinks. A continuity test with a multimeter checks conductor health, while insulation resistance testing checks for leakage current. Shielding tests help identify breakdowns in EMI protection, and a bending simulation or flex test can reveal weak spots in the cable.

Symptom, Cause and Fix at a Glance

Use the table below to connect what you're seeing with likely causes and the checks or fixes to consider.

SymptomLikely CauseFix
Intermittent motor faults or alarms Loose connection, damaged conductor, or EMI ingress Visual inspection, continuity test, check shield termination
Visible jacket cracks or conductor exposure Chemical/UV exposure or bend radius tighter than rated Replace cable; switch jacket material or correct routing
Erratic encoder or feedback signals EMI ingress, poor shielding, or grounding issue Shielding test, verify grounding, separate power/signal runs
Increased heat along the cable run Overloaded conductor or poor cabinet ventilation Check current rating, improve airflow, re-size conductor

Once you've identified the cause, look beyond the immediate repair. These selection, installation and maintenance practices help reduce the chance of the same problem returning.

 

Best Practices to Prevent Premature Failures

1. Use Motion-Rated Servo Cables

Always choose cables designed for continuous flexing.

Choosing a motion-rated cable is the first step. How you route and secure it matters just as much.

2. Follow Correct Installation Guidelines

Maintaining proper bending radius and flex-life is the single biggest factor here:

  • Maintain a minimum bend radius as per the manufacturer.
  • Avoid sharp edges; use protective conduits.
  • Proper clamping and strain relief reduce stress.

After checking the routing, make sure the jacket and shielding suit the conditions around the cable.

3. Protect Against Environmental Factors

  • Select oil-resistant and chemical-resistant jackets.
  • For outdoor setups, use UV-resistant designs.
  • Consider EMI-optimized shielded cables.

Those protections need regular checks as the cable ages. Build the following tasks into your maintenance routine.

4. Perform Regular Maintenance and Monitoring

  • Schedule periodic inspections.
  • Replace cables showing early wear before total failure.
  • Keep spare lengths of servo-rated cables in inventory.

With those basics covered, a few broader choices can help you plan for reliable operation over the long term.

 

Expert Recommendations

Invest in industrial-grade cables such as TKD Kabel, since low-cost generic options often fail early. Plan the routing carefully and keep power and signal cables separated to minimize EMI. Pay attention to grounding too: proper grounding extends shield life and reduces interference.

The figures below highlight why cable selection and installation deserve that attention.

 

Useful Facts About Servo Cable Lifespan

  • High flex servo cables can withstand up to 10 million bending cycles.
  • Poor installation can cut cable lifespan by up to 70%.
  • Servo failures account for 30% to 40% of industrial downtime costs in automation.

Still have questions about service life, warning signs or choosing a cable? Here are the ones that come up most often.

 

FAQs About Servo Cables

How long should a servo cable last?

With proper installation and maintenance, a high-quality servo cable can last 5 to 10 years in industrial use.

Are TKD Kabel products suitable for harsh environments?

Yes. TKD Kabel servo cables are designed to resist oil, chemicals, UV and continuous motion stress, ensuring long operational life.

How can I tell if EMI is damaging my servo cable?

Frequent motor errors, encoder faults or inconsistent signals are typical indicators of EMI issues.

What type of servo cables are best for robotic arms?

High-flex, drag-chain rated, EMC-optimized servo cables are ideal for robotic and automation applications.

What are the signs of a failing servo cable?

Watch for intermittent motor faults or alarms, inconsistent encoder feedback, visible jacket cracks or exposed conductors, EMI-related errors and rising heat along the cable run. Any of these signs is worth investigating before it causes a full failure.

Keeping servo cables reliable starts with matching them to the movement and environment. Choose motion-rated cables such as TKD Kabel's Kaweflex range, follow the installation guidance and inspect them regularly. Together, those steps help extend cable life, reduce downtime and lower replacement costs.

Explore the full range of TKD Kabel through L-com. We'll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com.

 

Read Next

Resources

Search Entries