L-com

Overcoming Insertion Loss in Long Payload Cable Runs

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

As UAV platforms scale in size and capability, internal RF cable runs grow longer—and with that comes a critical challenge: insertion loss. In large ISR drones, long coaxial runs between antennas, sensors and processing systems can introduce significant signal attenuation, especially at frequencies above 2 GHz. 

Without proper design, this loss reduces link margin, degrades signal-to-noise ratio and ultimately limits system performance. In extreme cases, signals arriving at the receiver may fall below usable thresholds, resulting in dropped data or loss of functionality. 

Managing insertion loss requires a combination of low-loss materials, proper signal conditioning and disciplined system architecture. Components like LCCA30011 coaxial cable and LCAT1000-03 attenuators play a key role in maintaining signal integrity across extended distances within the airframe. 

 

Key Takeaways 

  • Insertion loss increases rapidly with frequency and cable length, especially above 2 GHz 
  • Low-loss coaxial designs reduce attenuation without adding excessive weight 
  • Long cable runs require careful gain and attenuation balancing to maintain dynamic range 
  • Shielding becomes more critical as cable length increases and EMI exposure grows 
  • Link margin validation is essential for reliable ISR and RF system performance 

 

The Physics of Attenuation in Large Airframes 

Insertion loss occurs as RF energy is dissipated as heat within the conductor and dielectric of a cable. This loss increases logarithmically with both frequency and distance. 

In large UAVs, cable runs can exceed 10 meters, creating substantial cumulative loss. At high frequencies, even a few additional feet of standard coax can introduce several decibels of attenuation. 

Maintaining sufficient link margin becomes a primary design constraint. Systems must ensure that the received signal remains well above the noise floor under all operating conditions, including temperature extremes and dynamic flight environments. 

 

High-Performance Interconnects: LCCA30011 (LL142 Equivalent) 

Cable selection is the first line of defense against insertion loss. 

The LCCA30011, an LL142-equivalent design, uses a low-density PTFE dielectric and optimized conductor geometry to minimize attenuation at high frequencies. This reduces both dielectric and skin-effect losses compared to standard RG-series cables. 

Equally important is phase stability. In systems such as phased-array radar or synchronized sensor arrays, maintaining consistent electrical length across long runs is critical. Variations in phase can degrade system performance or introduce alignment errors. 

By combining low loss with stable electrical characteristics, high-performance coaxial cables preserve both amplitude and phase integrity across extended distances. 

 

Balancing the Link: LCAT1000-03 Attenuators 

Managing signal amplitude across long cable runs requires more than simply minimizing loss. 

In many designs, Low Noise Amplifiers (LNAs) are used to boost signals before or during transmission through long cables. However, this can result in excessive signal levels at the receiver, leading to compression or distortion. 

Inline attenuators such as the LCAT1000-03 provide controlled signal reduction, allowing engineers to maintain optimal dynamic range at the receiver. 

Attenuators also help stabilize impedance and reduce reflections within long cable assemblies. A fixed attenuation value—such as 3 dB—can improve return loss and reduce standing wave effects that degrade signal quality. 

 

How do you design an RF backbone for large UAVs? 

Effective RF backbone design requires both electrical and mechanical considerations. 

Segmented routing strategies use bulkhead interfaces to break long cable runs into manageable sections. This simplifies maintenance and reduces the risk of large-scale failure, while minimizing impedance discontinuities when properly implemented. 

Thermal variation must also be accounted for. As UAVs transition from ground-level heat to high-altitude cold, cable characteristics shift. High-performance cables with stable materials help minimize performance drift across temperature extremes. 

Proper routing is equally critical. Long cables should be isolated from power systems and high-current wiring to prevent EMI coupling, which becomes more significant as cable length increases. 

 

Validation: Measuring the Link Margin 

System validation ensures that theoretical performance translates into operational reliability. 

Vector Network Analyzer (VNA) testing allows engineers to measure insertion loss across the full operating frequency range. This provides a detailed profile of signal attenuation throughout the system. 

Power budgeting then verifies that the received signal maintains adequate margin—typically at least 10 dB above the noise floor—under worst-case conditions. 

By combining accurate measurement with disciplined design, UAV systems can maintain consistent RF performance even across long internal cable runs. 

L-com’s broad selection of RF interconnects and cable assemblies supports reliable signal transmission in large UAV platforms. For minimal downtime and rapid deployment, we ship quickly, with same-day shipping on qualified in-stock online orders placed Monday through Friday before 5 p.m. EST. 

View L-com UAV solutions 

 

Frequently Asked Questions (FAQ) 

Why not just use thicker coaxial cable to reduce insertion loss? 
Increasing cable diameter does reduce attenuation, but it introduces significant weight and routing challenges. In long-endurance UAVs, added mass directly impacts flight time and payload capacity. Cables like LCCA30011 are engineered to deliver low-loss performance with reduced weight, providing a more practical balance for airborne systems. 

Why add an attenuator if the system is already losing signal over distance? 
Attenuators are used to control signal levels after amplification. When LNAs are used to compensate for long cable runs, the signal at the receiver can exceed its linear operating range. The LCAT1000-03 allows precise adjustment of signal amplitude while also improving impedance matching and reducing reflections. 

Does temperature variation impact insertion loss in UAV cable runs? 
Yes. Conductor resistance and dielectric properties change with temperature. As a UAV climbs to high altitude and temperatures drop, insertion loss typically decreases. However, these changes can shift system behavior by several decibels, which is why thermally stable cable designs are critical for predictable performance. 

How do you calculate total insertion loss in a UAV RF system? 
Total insertion loss is the sum of cable attenuation per unit length at the operating frequency plus losses from connectors, adapters and inline components. Each connector typically adds 0.1 to 0.2 dB. For long runs at high frequencies, total loss can exceed 15 dB if not properly managed, making cable selection and system design essential for maintaining link margin. 

Resources

Search Entries