L-com

Integrating Phased Array Radars via Right-Angle Adapters

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

Active Electronically Scanned Array (AESA) radars are pushing UAV design into extreme territory—higher frequencies, denser interconnects and tighter mechanical envelopes. Nowhere is this more apparent than in the drone nosecone, where engineers must integrate dozens or even hundreds of RF channels into a highly constrained volume. 

The challenge is not just electrical—it is geometric. Traditional straight-out connector designs quickly consume available depth, introduce mechanical stress and complicate thermal management. As phased array systems scale, interconnect strategy becomes a limiting factor in overall radar performance. 

Right-angle bulkhead connectors and hybrid fiber architectures provide a practical path forward, enabling dense RF integration without compromising signal integrity or structural reliability. 

 

Key Takeaways 

  • Right-angle bulkheads like LCCN3208 reduce required clearance depth and improve packaging density 
  • Phase consistency across all RF paths is critical for beamforming accuracy 
  • Fiber optic backhauls eliminate EMI issues in high-density radar environments 
  • Mechanical layout directly impacts thermal performance and long-term reliability 

 

The Packaging Paradox of AESA Radars 

Phased array radars require a high number of individual RF channels—often 128 or more—within a compact aperture. Each channel must maintain consistent electrical length and impedance to preserve beamforming accuracy. 

Straight connector geometries create immediate problems. Coaxial cables require minimum bend radii, which translates into significant clearance depth behind the array. In a confined nosecone, this quickly becomes unmanageable. 

Additionally, straight cable exits act as mechanical levers. Under high-G maneuvering or vibration, these cables apply stress directly to PCB-mounted connectors, increasing the risk of pad failure or solder joint fatigue. 

 

Space-Saving Geometry with LCCN3208 

Right-angle bulkhead connectors address both spatial and mechanical constraints. 

By redirecting the cable path immediately at the interface, components like the LCCN3208 allow cables to run parallel to the radar backplane. This can reduce required clearance depth by tens of millimeters, enabling more compact nosecone designs or freeing space for cooling and power systems. 

Equally important is mechanical stability. Solder-style bulkhead integration creates a fixed interface between the connector and the structure, eliminating the micro-movement that leads to long-term fatigue failures. 

In high-density arrays, this stability is critical to maintaining consistent RF performance over time. 

 

Maintaining Phase Consistency Across the Array 

In phased array systems, small electrical differences translate directly into performance degradation. 

Every interconnect—cable, connector and transition—must maintain consistent impedance and electrical length. Variations introduced by poorly designed right-angle connectors can create phase errors, resulting in beam distortion or reduced gain. 

Precision-engineered components ensure that the 90-degree transition does not introduce impedance discontinuities or measurable phase shift. This is essential when scaling arrays where cumulative error across many channels becomes significant. 

Lightening the Load with Fiber Optic Backhauls 

While RF signals must remain in coaxial form at the antenna interface, the processed data generated by the radar can be handled differently. 

Fiber optics provide a high-bandwidth, EMI-immune solution for moving radar data from the array to onboard processing systems. This reduces the need for large bundles of copper cabling, which would otherwise create both weight and interference challenges. 

In dense radar installations, fiber eliminates the risk of RF energy coupling into adjacent data lines, preserving signal integrity across both analog and digital domains. 

 

Designing a High-Density Radar Manifold 

Effective integration requires careful physical layout. 

Staggered connector placement allows engineers to maximize port density without interfering with adjacent cables. Right-angle connectors can be arranged in stepped configurations to maintain access and spacing while minimizing footprint. 

Thermal management must also be considered. Dense RF systems generate significant heat, particularly at the transmit/receive (T/R) modules. Routing cables parallel to the backplane creates airflow channels that support passive or active cooling strategies. 

These mechanical decisions directly influence both performance and reliability. 

 

Validation: Phase Matching and Structural Integrity 

Verification of a phased array system goes beyond basic continuity checks. 

Time Domain Reflectometry (TDR) is used to confirm that each RF path maintains consistent electrical length and impedance. Even small deviations can introduce phase mismatch across the array. 

Mechanical validation is equally important. Vibration and shock testing ensure that soldered bulkhead connections maintain integrity under operational conditions, including sustained rotor-induced harmonics and transient loads. 

Together, these tests confirm that the system performs as intended both electrically and mechanically. 

 

Optimizing Radar Integration for UAV Platforms 

As UAV radar systems continue to scale, interconnect design becomes a core engineering discipline rather than an afterthought. 

Right-angle bulkhead connectors, combined with fiber-based data backhauls, provide a scalable approach to managing density, maintaining signal integrity and ensuring long-term durability. 

By addressing both the electrical and mechanical challenges of phased array integration, engineers can build radar systems that meet the demands of next-generation UAV missions. 

L-com’s broad selection of wireless connectivity and networking solutions supports reliable UAV communications in demanding environments. For minimal downtime and rapid deployment, we ship quickly, with same-day shipping on qualified in-stock online orders placed Monday through Friday before 5 p.m. EST. 

View L-com UAV solutions 

 

Frequently Asked Questions (FAQ) 

Will using a right-angle connector like the LCCN3208 cause signal reflection or VSWR issues? 
Not if it is properly designed. The LCCN3208 maintains a constant 50-ohm impedance through the 90-degree transition, minimizing reflections. In phased arrays, even small impedance mismatches can degrade beamforming performance, so using precision RF connectors is critical to avoid introducing phase or amplitude errors. 

Why choose soldered bulkhead connectors instead of push-on types for phased array systems? 
Push-on connectors can loosen over time due to vibration and thermal cycling, especially in high-RPM UAV environments. Soldered bulkhead connections create a fixed mechanical and electrical interface, eliminating micro-movement and improving long-term reliability. This is particularly important in arrays where any intermittent connection can impact overall system performance. 

How much physical space can right-angle connectors realistically save in a UAV nosecone? 
Straight connectors typically require 50 mm to 70 mm of clearance to accommodate cable bend radius. Right-angle bulkheads reduce that requirement to roughly 10 mm to 15 mm by redirecting the cable immediately. This can significantly reduce overall system depth or free space for cooling, batteries or additional payload components. 

Can fiber optics and RF bulkhead connectors be used together in the same radar system? 
Yes, and this is a common architecture. RF coaxial connections are used at the antenna interface where analog signals must be preserved. Once the signal is processed, fiber optics can carry high-bandwidth digital data to the rest of the system. This hybrid approach reduces EMI risk and minimizes cable bulk while maintaining RF performance at the front end. 

Resources

Search Entries