L-com

Insertion Loss and Return Loss in Data Center Fiber Links

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics 

 

Insertion loss is the optical power a fiber link loses between transmitter and receiver, measured in decibels (dB), and lower is better. Return loss is the light reflected back toward the source at a connector or splice, also in dB, and higher is better. A data center link is ready for service when its insertion loss sits under the application budget and no connection reflects enough light to bother the transceiver. 

This guide covers typical allowances per connector, splice and kilometer, a worked loss budget, how a power meter and an OTDR measure each value, and what to check when a link fails. If you are specifying the cabling, optics and connectivity for these runs, start with L-com data center fiber solutions. 

 

Key Takeaways 

  • TIA-568.3-D allows up to 0.75 dB per mated connector pair and 0.3 dB per splice; low-loss parts land well below both. 
  • Short-reach optics leave very little room: 100GBASE-SR4 over OM4 allows only about 1.9 dB of channel insertion loss across 100 m. 
  • Return loss is a positive number where higher is better. TIA minimums are 20 dB for multimode connectors, 35 dB for single-mode UPC and 55 dB for single-mode APC. 
  • A light source and power meter gives the pass/fail insertion loss figure; OTDR testing shows where each loss and reflection sits. 
  • Dirty end faces are the most common reason a new link fails its loss test, so inspect and clean before you measure. 

What Is Insertion Loss? 

Insertion loss is the total drop in optical power from one end of a link to the other: attenuation in the glass, which grows with length, plus loss at every mated connector pair and splice. 

Because the scale is logarithmic, small numbers matter. A 3 dB loss halves the power, and a 1.0 dB link delivers about 79% of the launched light. On data center runs of tens of meters, the connectors usually account for most of the loss, not the fiber. 

At a connector, light escapes when the cores do not line up perfectly, when there is a gap between the end faces, or when dust or oil sits in the light path. Mating different core sizes, such as 62.5 micron to 50 micron, adds loss even with a perfect connector. 

What Is Return Loss? 

Return loss is the ratio of light arriving at a connection to light reflected back from it, in dB. At 20 dB, 1% of the power reflects; at 50 dB, one part in 100,000 comes back. 

Reflections happen wherever light crosses a change in refractive index, usually a small air gap between end faces. UPC polishes press the cores together to shrink that gap. APC connectors are polished at 8 degrees, so reflected light is steered out of the core instead of back to the laser. 

Return Loss vs Reflectance 

Reflectance describes the same event with the opposite sign: 50 dB return loss equals -50 dB reflectance. OTDRs usually report reflectance per event, while some test sets report optical return loss (ORL) for the whole link. Check which one your tester shows before comparing results to a spec. 

Why Do Both Numbers Matter in a Data Center? 

Insertion loss decides whether enough light reaches the receiver. IEEE 802.3 sets a maximum channel insertion loss for each application, and the limits are tight for short-reach multimode optics because part of the power budget goes to dispersion penalties: 

  • 10GBASE-SR: 2.6 dB over 300 m of OM3, or 2.9 dB over 400 m of OM4. 
  • 40GBASE-SR4: 1.9 dB over 100 m of OM3, or 1.5 dB over 150 m of OM4. 
  • 100GBASE-SR4: 1.8 dB over 70 m of OM3, or 1.9 dB over 100 m of OM4. 

Extended-reach optics use different numbers, so check the datasheet. If you are still choosing a fiber grade, our guide to OM3 vs OM4 vs OM5 compares reach by speed. 

Return loss matters more on single-mode and at higher speeds. Reflected light can destabilize a laser, and two reflective connectors on one link can bounce light back and forth and add noise. PAM4 optics at 100G per lane are more sensitive to this than older NRZ links. Our comparison of single-mode vs multimode fiber explains where each type fits. 

Typical Loss Allowances per Connector, Splice and Kilometer 

The standard values below are the design maximums in TIA-568.3-D. Quality components normally do much better, and that difference is your headroom. 

Component 

TIA-568.3-D maximum 

What to expect in practice 

Mated connector pair (LC, SC) 

0.75 dB 

About 0.15-0.3 dB for low-loss, factory-terminated parts 

Mated MPO/MTP pair 

0.75 dB 

Low-loss MPO is commonly rated 0.35 dB max 

Fusion splice 

0.3 dB 

Usually under 0.1 dB 

Multimode fiber, 850 nm 

3.0 dB/km 

About 0.3 dB on a 100 m run 

Multimode fiber, 1300 nm 

1.5 dB/km 

Rarely a factor inside a building 

Single-mode fiber, inside plant 

1.0 dB/km 

0.5 dB/km for outside plant cable 

 

Older TIA documents and the IEEE channel calculations use 3.5 dB/km for multimode at 850 nm, a slightly more conservative figure used in the example below. 

Tip: Build the budget from maximum values: the TIA limit, or the manufacturer's guaranteed maximum for low-loss parts. Typical values on a datasheet are averages, and some of the parts you install will be worse than average. 

How Do You Build a Loss Budget? 

A loss budget is the worst-case insertion loss of a link, calculated before installation. Multiply fiber length in km by attenuation per km, add mated connector pairs times loss per pair, then add splices times loss per splice. Compare the total to the application limit to see your margin. 

Take a 100GBASE-SR4 leaf-to-spine link over 80 m of OM4 with MPO trunks. The application limit is 1.9 dB. Three designs show how fast connectors use it up: 

Item 

A: 2 low-loss MPO pairs 

B: 4 low-loss MPO pairs (cross-connect) 

C: 4 standard MPO pairs 

Fiber (0.08 km x 3.5 dB/km) 

0.28 dB 

0.28 dB 

0.28 dB 

Mated MPO pairs 

2 x 0.35 = 0.70 dB 

4 x 0.35 = 1.40 dB 

4 x 0.75 = 3.00 dB 

Total budget 

0.98 dB 

1.68 dB 

3.28 dB 

Margin vs 1.9 dB limit 

0.92 dB 

0.22 dB 

-1.38 dB (fails) 

 

Design A has room to spare. Design B passes, but with only 0.22 dB of margin, one dirty connector during a future move would push it over. Design C fails on paper, and careful installation will not save it; you need fewer connections or lower-loss parts. 

If Design A measures 1.2 dB after installation, it passes the application limit but is 0.2 dB worse than your worst case. That gap points to a problem, usually contamination, worth finding before the link carries traffic. 

Recommendation: Leave some headroom beyond the bare pass. Many designers aim for 0.5 dB or more on short-reach multimode links to absorb connector wear and future moves, adds and changes. 

Measuring Insertion Loss with a Light Source and Power Meter 

A light source and power meter, often sold together as an optical loss test set (OLTS), is the reference method for insertion loss and the basis of Tier 1 certification. It gives one end-to-end number per fiber per wavelength: 

  1. Inspect and clean the test reference cords and every connector on the link under test. 
  1. Set the reference with the one-cord method (Method B in TIA terms), so the measurement includes both end connections of the link. 
  1. Connect the link and measure at both wavelengths: 850 and 1300 nm for multimode, 1310 and 1550 nm for single-mode. 
  1. Compare each result to your calculated budget and the application limit, then save the record. 

For multimode, use a launch that meets the encircled flux requirements of IEC 61280-4-1, or two testers can disagree by several tenths of a dB on the same link. For MPO trunks, an MPO-native tester avoids the extra connections a fan-out adds. 

When Is OTDR Testing the Right Tool? 

OTDR testing is the right tool when you need to know where the loss is. An optical time domain reflectometer sends light pulses down the fiber and reads the backscatter and reflections, showing each connector and splice by distance with its loss and reflectance. 

Use a launch cable at the near end and a receive cable at the far end so the first and last connectors are measured. Test splices from both directions and average the results. On short data center links, pick an OTDR with a short dead zone, or closely spaced connectors blur into one event. 

Factor 

Light source and power meter 

OTDR 

Measures 

End-to-end insertion loss 

Loss and reflectance per event, plus distance 

Return loss 

Not measured, unless the set adds ORL 

Reflectance per event and total ORL 

Finds the fault 

No 

Yes, by distance along the link 

Access needed 

Both ends 

One end, with launch and receive cables 

Best use 

Acceptance pass/fail (Tier 1) 

Troubleshooting and documentation (Tier 2) 

 

Troubleshooting a Link That Fails Its Loss Budget 

Work from the cheapest fix to the most expensive; most failures turn up in the first two steps. 

  1. Inspect every end face with a fiber scope, clean it, and inspect again. Grade it against IEC 61300-3-35 before you mate anything. 
  1. Check the test reference. A negative or suspiciously low reading usually means a bad reference or a worn test cord. 
  1. Compare wavelengths. On single-mode, clearly higher loss at 1550 nm than at 1310 nm suggests a tight bend, often at a cable tie. 
  1. Shoot the link with an OTDR from both ends to find the event that is out of line. 
  1. Look for mismatches: an OM1 or OM2 patch cord in an OM3 or OM4 channel, an APC connector mated to a UPC connector, or pinned MPO mated to pinned MPO. 
  1. Replace the failed component. A factory-terminated assembly is usually faster to swap than re-terminating in the field. 

A polarity mistake usually shows no light at all rather than high loss, so check polarity first when a fiber reads dark. 

Tip: When the OTDR shows one connector at 0.9 dB and the rest under 0.3 dB, clean that connector before replacing anything. One dust particle on the core can explain the whole difference. 

Acceptance Criteria for Commissioning 

Agree on these criteria before testing starts so installer and owner judge results the same way. 

Check 

Pass condition 

Reference 

Link insertion loss 

At or below the calculated budget and the application limit, at both wavelengths 

TIA-568.3-D, IEEE 802.3 

Mated connector pair 

0.75 dB max, or the manufacturer's max for low-loss parts 

TIA-568.3-D 

Fusion splice 

0.3 dB max, bidirectional average 

TIA-568.3-D 

Connector return loss 

20 dB min multimode; 35 dB min single-mode UPC; 55 dB min APC 

TIA-568.3-D 

End-face condition 

Passes inspection before every mating 

IEC 61300-3-35 

Test records 

Saved per fiber, with reference method, wavelength and launch condition 

Project spec 

 

Staying Inside the Budget with Quality Components 

Most of a data center loss budget is spent at the connections, so the parts you choose decide your margin. Factory-terminated fiber optic cable assemblies with low-loss connectors and a test report for each assembly remove the variability of field polishing. When you terminate on site, use fiber connectors rated for the end-face geometry and loss your budget assumes. Then pick fiber transceivers whose reach and power budget match your fiber type and calculated insertion loss. 

For cabling, connectivity and optics that support low insertion loss across the whole channel, browse L-com's data center fiber portfolio. 

 

Frequently Asked Questions (FAQs) 

1. What is a good insertion loss value for a fiber patch cord? 

A short LC or SC patch cord with low-loss connectors typically measures under 0.3 dB per mated pair, and good ones often come in around 0.15 dB. Nearly all of that loss is at the connectors, since a few meters of glass adds almost nothing. 

2. Is higher or lower return loss better? 

Higher return loss is better, because it means less light is reflected back toward the transmitter. A single-mode UPC connector should be at least 35 dB, and APC connectors at least 55 dB. 

3. Can insertion loss be negative? 

A link cannot create light, so a negative reading usually means a bad reference or a worn test cord. Check the test reference and the condition of the test cords, then measure again. 

4. Do I need OTDR testing on short data center links? 

Not for basic acceptance. TIA treats light source and power meter testing as Tier 1 certification, and OTDR testing as an optional Tier 2 step. It is worth doing when a link fails, when the specification calls for it, or when you want a per-connector record. 

5. What is the difference between insertion loss and attenuation? 

Attenuation is the loss of the fiber itself per unit length, usually given in dB/km. Insertion loss is the total for a link, including fiber attenuation plus every connector and splice. 

6. What should I do when a fiber link fails its loss test? 

Work from the cheapest fix to the most expensive. Start by inspecting every end face with a fiber scope, cleaning it, and inspecting again. Then check the test reference, compare results at both wavelengths, and use an OTDR from both ends to find the event that is out of line. Also check for mismatches, such as an OM1 or OM2 patch cord in an OM3 or OM4 channel, or an APC connector mated to a UPC connector. A factory-terminated assembly is usually faster to swap than re-terminating in the field. 

Resources

Search Entries