L-com

Industrial Wireless Gateways: Connecting the IIoT in Harsh EnvironmentsIndustrial Wireless Gateways: Connecting the IIoT in Harsh Environments

By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

  

Key Takeaways 

• An industrial wireless gateway bridges OT field devices — PLCs, RTUs, sensors using Modbus, PROFINET, EtherNet/IP, and similar protocols — to IP networks, cloud platforms, and edge systems without replacing the devices themselves. 

• Wireless standard selection (Wi-Fi 6, 4G/5G cellular, LoRaWAN, WirelessHART) depends on data rate, range, latency, and power constraints — not all IIoT applications need the same radio technology. 

• Consumer and commercial gateways fail in industrial environments because of temperature, ingress, vibration, and EMI — not because of missing features. Hardware rated for the installation environment is the baseline requirement. 

• A gateway installed inside a metal enclosure without an external antenna will have unreliable RF performance regardless of the radio standard. Antenna placement is a design decision, not an afterthought. 

• For most brownfield IIoT deployments, the right architecture is a gateway that supports serial-to-IP protocol translation, wide-range DC power, DIN-rail mounting, and external antenna ports — not the cheapest device with a Wi-Fi chip. 

  

There's a specific problem that comes up constantly in brownfield IIoT projects: you have a Modbus RTU device on an RS-485 bus that's been running reliably for 15 years, you need its data on a cloud platform for predictive maintenance, and nobody wants to replace the device. The field device works. The protocol works. What's missing is the bridge between the OT world it speaks and the IP world everything else expects. 

That's what an industrial wireless gateway does. It sits between the legacy field device and the IP network — translating protocols, managing connectivity, and surviving the physical environment in between.  

 

What Does an Industrial Wireless Gateway Do? 

An industrial wireless gateway performs two functions simultaneously: protocol translation and wireless connectivity. Strip away the marketing language, and that's the product. 

 

Protocol Translation: Bridging OT and IP 

Most OT field devices speak protocols that predate modern IP networks. Modbus RTU, developed in 1979, runs over serial RS-485 or RS-232 links. PROFINET and EtherNet/IP are Ethernet-based but use application-layer protocols that don't map natively to standard IT infrastructure. A SCADA server or cloud platform expecting JSON over MQTT or RESTful API calls can't talk directly to a Modbus RTU device. 

The gateway handles this translation. On one side, it speaks the OT protocol — polling Modbus registers, consuming PROFINET I/O data, reading EtherNet/IP tags. On the other side, it publishes that data in a format the IP network understands: OPC-UA, MQTT, HTTP, or a direct database write. The field device doesn't need to change. The gateway does the conversion. 

 

Wireless Connectivity: Replacing or Supplementing Cable Runs 

Wireless connectivity solves the cable problem. Some installation points are genuinely impractical to cable: a sensor on a rotating assembly, a meter in a utility vault with no conduit path, and a remote pumping station 10 kilometers from the nearest wired infrastructure. Others are theoretically capable, but the installation cost — trenching, conduit, and pull-through a busy production facility — is prohibitive relative to the monitoring value. 

A wireless gateway at those locations provides network connectivity without requiring a cable run. The gateway connects to the field device (often by a short local cable or serial connection) and transmits data wirelessly to a local access point, a cellular network, or a long-range IoT radio network. 

 

 Edge Processing: Optional but Increasingly Common 

Higher-end industrial gateways add a third function: local computation before data is transmitted. Rather than streaming every raw sensor reading to the cloud, the gateway applies filtering, aggregation, or anomaly detection locally — forwarding only significant events or summarized data. This reduces bandwidth costs, lowers cloud storage requirements, and maintains basic operation when the WAN link is unavailable. 

Edge processing capability varies significantly across gateway products. For simple data forwarding, it's not needed. For applications where the cloud is the primary processing platform but WAN reliability is uncertain, local buffering and pre-processing are worth the added cost. 

 

How Does a Gateway Translate OT Protocols to IP Networks? 

The protocol translation layer is where gateways earn their keep in brownfield IIoT deployments. Here's how the most common OT protocols map to IP network targets: 

  

OT Protocol 

Layer / Type 

Typical Devices 

Gateway Translation Target 

Modbus RTU / ASCII 

Serial (RS-232 / RS-485) 

PLCs, RTUs, drives, meters, sensors 

Modbus TCP over Ethernet/IP 

Modbus TCP 

Ethernet application layer 

PLCs, SCADA systems, HMIs 

Direct IP forwarding; OPC-UA encapsulation 

PROFINET 

Ethernet (IEC 61158) 

Siemens PLCs, distributed I/O, drives 

OPC-UA, MQTT, cloud platform APIs 

EtherNet/IP 

Ethernet (CIP over TCP/UDP) 

Allen-Bradley PLCs, Rockwell I/O modules 

OPC-UA, MQTT, REST API 

BACnet MS/TP 

Serial (RS-485) 

Building HVAC controllers, energy meters 

BACnet/IP over Ethernet 

DNP3 

Serial or Ethernet 

RTUs in power/water utilities 

DNP3 IP; OPC-UA encapsulation 

CANopen / DeviceNet 

CAN bus 

Motion controllers, sensors, actuators 

EtherNet/IP or OPC-UA bridge 

4–20 mA / Pulse 

Analog/digital I/O 

Legacy sensors, transmitters, flow meters 

Modbus TCP via I/O gateway 

  

A few practical notes on protocol translation: 

•       Modbus RTU to Modbus TCP is the most common gateway translation in manufacturing. It's well-supported across gateway products and the conversion is straightforward. If this is your only requirement, gateway selection is primarily a hardware and connectivity decision. 

•       OPC-UA is the preferred target protocol for most modern IIoT platforms and cloud integrations. A gateway that outputs OPC-UA gives you a standard interface that works with virtually any upstream system — SCADA, historian, cloud IoT platform, digital twin software. 

•       MQTT is the right target for high-frequency telemetry to cloud platforms (AWS IoT, Azure IoT Hub, Google Cloud IoT). It's lightweight, efficient over constrained bandwidth, and supported by most industrial IoT platforms. 

•       4–20 mA analog signals require a gateway with analog input hardware — not all gateways have this. A gateway that handles Modbus TCP but lacks analog inputs can't connect a 4–20 mA pressure transmitter directly. 

  

Which Wireless Standard Should You Use? 

Wireless standard selection is a requirements question. There's no universal right answer — the correct standard depends on your data rate, range, latency, power availability, and existing infrastructure. Here's how they compare: 

  

Standard 

Typical Range 

Bandwidth 

Best For 

Tradeoffs 

Wi-Fi 6 (802.11ax) 

Up to ~100m indoors (depends on environment) 

Up to 9.6 Gbps (theoretical); 600+ Mbps real-world 

High-bandwidth, short-range IIoT: real-time sensor data, video, SCADA polling over existing Wi-Fi infrastructure 

Requires AP infrastructure; 2.4/5 GHz bands can be congested in dense environments 

4G LTE Cellular 

Wide area — no range constraint at site level 

10–50 Mbps typical download 

Remote sites without wired WAN; primary or failover connectivity; distributed assets across large facilities 

Per-device SIM and data plan cost; latency unsuitable for hard real-time control loops 

5G Cellular 

Wide area: private 5G mmWave enables dense factory coverage 

100 Mbps – 1 Gbps; sub-10 ms latency (private 5G) 

High-speed mobile IIoT, private campus networks, latency-sensitive applications 

Private 5G infrastructure investment is high; public 5G coverage is geographic 

LoRaWAN 

Up to 10km line-of-sight; 1–5km urban/industrial 

0.3–50 kbps 

Low-power, infrequent data: temperature, vibration, tank level, asset tracking over large areas or outdoor sites 

Very low bandwidth — not suitable for real-time or high-frequency data; base station required 

WirelessHART 

Up to 250m per hop; mesh extends coverage 

250 kbps (raw); lower effective throughput 

Process industry sensor networks: pressure, flow, temperature on HART-compatible instruments 

HART ecosystem specific: mesh latency unsuitable for fast control 

Zigbee / 802.15.4 

10–100m per node; mesh network 

250 kbps 

Dense low-power sensor networks; building automation; asset tracking 

Low throughput; mesh complexity, and not common in heavy industrial 

  

 

When Wi-Fi 6 Is the Right Choice 

Wi-Fi 6 makes sense when you have existing wireless infrastructure in the facility and your IIoT devices are within coverage range of access points. It's the highest-bandwidth option at short range, which matters for applications sending large data volumes — video from a vision camera, high-frequency vibration data from an accelerometer, or image data from a process inspection system. 

The constraint is infrastructure dependency. A Wi-Fi 6 gateway needs a nearby access point with good signal quality. In facilities with variable RF environments – lots of metal, moving equipment, interference from welding or VFDs — Wi-Fi 6 reliability depends heavily on a proper RF site survey and AP placement. Don't install a Wi-Fi 6 gateway and assume coverage exists. 

  

When Cellular (4G LTE or 5G) Is the Right Choice 

Cellular is the standard for remote sites without existing wireless infrastructure and for applications requiring wide-area coverage across large facilities or between facilities. A cellular gateway with a SIM card provides WAN connectivity wherever the carrier network has coverage — no AP infrastructure, no campus network planning. 

4G LTE is sufficient for most IIoT monitoring applications. 5G adds lower latency and higher throughput — relevant for video-intensive applications or private campus networks where latency approaches those of wired connections. For simple sensor telemetry over cellular, 4G LTE is usually the cost-effective choice. 

Cellular gateways for remote or unattended sites should have dual-SIM capability (failover to a secondary carrier if the primary loses signal) and a hardware watchdog that restores connectivity automatically after power events or cellular drops. 

 

When LoRaWAN Is the Right ChoiceLoRaWAN Is the Right Choice 

LoRaWAN is purpose-built for the problem nobody else solves well: sensors that need to transmit small amounts of data infrequently, over long distances, running on battery power. A tank level sensor at the far end of a storage yard, a temperature sensor in a cold storage facility, a vibration sensor on outdoor rotating equipment — these are LoRaWAN applications. 

The bandwidth limitation is real: LoRaWAN is not suitable for streaming data, video, or any application requiring more than a few hundred bits per second. What it offers instead is range (several kilometres in open environments), very low power consumption (battery life of years on AA cells for infrequent sensors), and the ability to cover large physical areas with a single gateway serving hundreds of end nodes. 

 

What Environmental Specifications Actually Matter for Industrial Installations? 

This is the section that determines whether the gateway you've specified is still working 18 months after installation. Consumer and commercial gateways fail in industrial environments — not because they're missing features, but because they're not built for the conditions. Here's what to check and why each spec matters at specific installation points: 

  

Environment Factor 

What to Specify 

Common Mistakes 

Operating temperature 

Wide-temp rating: −20°C to 60°C minimum for most industrial and −40°C to 70°C for outdoor or extreme environments 

Specifying office-rated hardware (0–40°C) for enclosures or outdoor mounting points that exceed the range 

Ingress protection (IP rating) 

IP67 minimum for environments with wash-down, coolant mist, or outdoor exposure; IP54 for light dust/splash in enclosed plant areas 

Using IP20 (no ingress protection) hardware near wash-down zones or outdoor cable entries 

Vibration and shock 

IEC 60068-2-6 vibration testing; DIN-rail or panel mount with vibration-resistant fasteners 

Rack-mount hardware near presses, compressors, or conveyor drives without vibration isolation 

Power input 

Wide-range DC input (9–60V typical) for compatibility with industrial DC buses; redundant power inputs for critical applications 

Specifying AC-only power when the installation point has only a 24V DC bus 

EMI / EMC 

CE/FCC certified; IEC 61000-4 series compliance for industrial EMI environments 

Installing near VFDs, arc welders, or large motor contactors without verifying EMI rating 

Enclosure and mounting 

DIN-rail for panel/cabinet installation; wall-mount or pole-mount brackets for field locations; NEMA 4/4X for outdoor metal enclosures 

Using desktop or rack-mount form factors that don't fit standard industrial panel layouts 

Antenna placement 

External antenna ports with N-type or SMA connectors for placement outside metal enclosures; RF site survey before installation 

Mounting the gateway inside a steel cabinet and expecting the internal antenna to maintain reliable RF coverage 

  

 

The Antenna Problem Most Installations Get Wrong 

A gateway specified with good RF performance, installed in a steel enclosure, with the internal antenna enclosed in metal, will have poor RF performance. This sounds obvious, but it's one of the most common installation errors in industrial wireless deployments. Metal enclosures block radio signals. The solution is external antenna connectors (N-type or SMA) with the antenna mounted outside the enclosure on a bracket or mast, connected by a short RF cable. The antenna location — its height, clearance from metal structures, and line-of-sight to the access point or cell tower — determines the signal quality the gateway sees in actual operation. For challenging RF environments (large metal structures, mobile equipment, dense machinery), a site survey with a spectrum analyzer before installation is not optional. The few hours it takes to survey and plan antenna placement prevents weeks of troubleshooting after installation. 

 

What Does an Industrial Wireless Gateway Installation Look Like in Practice? 

A mid-size food processing facility needs predictive maintenance data from 40 motors spread across a production floor and a refrigerated warehouse. The motors have vibration and temperature sensors communicating over Modbus RTU on RS-485 buses. The existing plant network doesn't reach the warehouse. 

  

•       Eight industrial wireless gateways are mounted on DIN-rail inside NEMA 4 enclosures at distribution points across the facility. Each gateway handles five sensors via Modbus RTU polling on the local serial bus. 

•       The gateways use Wi-Fi 6 in the main production area, where existing AP infrastructure provides coverage. In the refrigerated warehouse — where running new AP cabling was impractical — two gateways use cellular LTE for WAN connectivity. 

•       All gateways are specified with IP67 ratings (the warehouse reaches 0°C and has condensation), wide-temperature DC power inputs (fed from the 24V DC bus in each panel), and external antenna ports with roof-mounted antennas for the cellular units. 

•       Data is published via MQTT to an edge server, which runs anomaly detection before forwarding alerts to the cloud platform. The gateways buffer locally if the WAN link drops — the maintenance team gets data gaps flagged rather than silent failures. 

  

The project took six weeks from specification to operational. The main delays were antenna placement planning for the cellular units and validating the Modbus RTU polling configuration against the sensor firmware. The gateways themselves installed in a day per location. 

 

How Do You Connect Legacy OT Equipment Without Replacing It? 

The concern that comes up most often in brownfield IIoT projects is whether existing equipment has to be replaced to gain connectivity. It usually doesn't. 

A gateway with the right serial ports can read Modbus RTU data from a PLC installed in 2001 with no modification to the PLC. The gateway polls the PLC's registers on the existing RS-485 bus, translates the data to MQTT or OPC-UA, and forwards it to a cloud platform. From the PLC's perspective, it's just another device on the bus asking for data. 

Where equipment does need modification – adding sensors to machines that have none or enabling data from instruments that weren't wired to the controls network – the right addition is often a sensor, not a controller replacement. 

Industrial IoT sensors for vibration, temperature, and pressure can be retrofitted to existing equipment and connected to a gateway's analogue or digital inputs, or directly over a local wireless sensor protocol. The gateway becomes the aggregation point for both legacy Modbus devices and new sensors at the same location. 

Industrial Ethernet switches handle the wired backbone where gateways are too far apart for reliable wireless or where latency requirements favor a wired segment. A hybrid architecture — a wired backbone to distribution points, wireless from the gateway to field devices at those points — is common in large facilities. 

 

Building Resilient Industrial Networks 

Reliable industrial security depends on more than firewall rules and network segmentation. The underlying physical infrastructure must be designed to support continuous operation in demanding environments. From industrial Ethernet and fiber connectivity to wireless networking and ruggedized connectivity solutions, L-com helps organizations build resilient industrial networks that support security, reliability, and long-term operational performance. 

 

Frequently Asked Questions (FAQs) 

What is an industrial wireless gateway? 
An industrial wireless gateway connects field devices, sensors, PLCs, and other operational technology (OT) equipment to IP-based networks, cloud platforms, and edge systems. It acts as a bridge between industrial protocols and modern networking infrastructure. 

How do industrial wireless gateways support IIoT deployments? 
Industrial wireless gateways collect data from field devices, translate industrial protocols, and transmit information to monitoring, analytics, and control systems. This allows organizations to connect legacy equipment and expand Industrial Internet of Things (IIoT) initiatives without replacing existing assets. 

Which wireless technology is best for industrial applications? 
The right wireless technology depends on the application. Wi-Fi is often used for high-bandwidth connectivity, cellular supports remote and distributed assets, and technologies such as LoRaWAN are well suited for low-power, long-range sensor deployments. 

Can industrial wireless gateways connect legacy equipment? 
Yes. Many industrial wireless gateways are designed to connect legacy devices that use protocols such as Modbus RTU, BACnet, DNP3, or other industrial communications standards, allowing existing equipment to participate in modern IIoT architectures. 

What should I look for when selecting an industrial wireless gateway? 
Key considerations include protocol support, wireless connectivity options, environmental ratings, power requirements, mounting options, security features, and the ability to operate reliably in the temperature, vibration, moisture, and EMI conditions present at the installation site.

Resources

Search Entries