L-com

How to Choose the Right Bus Cable for Your Network

By Eileen Harvey 

In modern industrial and commercial systems, bus cables form the backbone of communication between devices. Whether in factory automation, process control or automotive applications, the right bus cable ensures seamless data transmission, minimal signal loss and long-term reliability These cables are essential for ensuring that information flows smoothly between machines, sensors and control systems, enabling efficient operations across diverse applications such as factory automation, process control and automotive systems. 

The choice of bus cable can significantly impact the overall performance of the network, affecting everything from data transmission speeds to signal integrity. A high-quality bus cable can provide seamless data transmission while minimizing signal loss, which is crucial in environments where precision and reliability are paramount.  

Selecting the appropriate bus cable for your industrial automation or process control network is crucial for ensuring reliable communication, system efficiency and long-term durability.  

Why Is Choosing the Right Bus Cable Important? 

In industrial environments, communication failures or signal degradation can result in costly downtime, safety hazards and compromised data integrity. Selecting the right bus cable ensures reliable data transfer by supporting uninterrupted real-time communication. It also provides durability, withstanding challenging conditions such as temperature shifts, humidity and electromagnetic interference. The right choice allows for scalability, enabling future expansion and system upgrades, while also delivering cost-effectiveness by reducing maintenance and installation costs. 

Factors to Consider When Selecting Bus Cables 

Network Type Compatibility 

Each fieldbus system has its own electrical specifications. For example, PROFIBUS requires cables with 150 Ω impedance, CAN-Bus typically uses twisted-pair cables with 120 Ω impedance and DeviceNet demands thicker gauge conductors to carry both power and data. It is essential to verify that the cable’s electrical properties match the requirements of the chosen protocol. 

Electrical Properties: Impedance and Attenuation 

Impedance-matching is critical to avoid signal reflections. A mismatched impedance can cause unstable communication, while the correct impedance ensures seamless high-speed transmission. Attenuation, or signal loss over distance, is another factor to consider. For long cable runs, low-attenuation designs are essential. 

Shielding Options 

Shielding protects communication lines from electromagnetic noise, which is common in industrial environments. Foil shielding is lightweight and effective against high-frequency noise. Braided shielding is more durable and protects against low-frequency interference. Some cables combine foil and braid to deliver maximum protection in harsh conditions. 

Mechanical and Environmental Durability 

Bus cables must withstand physical and environmental stress. In machine shops or lubrication-heavy environments, oil resistance is vital. For outdoor installations, UV-resistant jackets prevent sunlight degradation. Cables exposed to high or low temperatures must have temperature resistance, and in plants where acids or solvents are present, chemical resistance is required. 

Flexibility and Installation Needs 

In robotics and automated machinery, bus cables may undergo continuous motion and bending. High-flex bus cables are designed for drag chains and robotic arms, while standard bus cables are more suitable for fixed installations where movement is limited and cost savings are preferred. 

Compliance with Industry Standards 

Industrial networks depend on cables that meet strict standards. Look for certifications such as UL, CSA and CE approvals, as well as ISO/IEC standards for industrial networking. It is also important to ensure that the cable is certified for the specific bus system, such as PROFIBUS-certified options. 

Common Mistakes to Avoid 

Several errors can compromise bus cable performance. Using non-certified cables for specific fieldbus systems is a frequent mistake. Another is overlooking attenuation in long-distance installations. Some users choose cables based solely on cost rather than durability and performance, which can lead to long-term issues. Ignoring scalability is another risk—selecting a cable that cannot support future bandwidth needs limits the network’s growth. 

Consider the Operating Environment 

The durability of a bus cable is closely tied to the conditions in which it is used. For high-heat machinery, outdoor setups or furnaces, temperature-resistant cables are required. UV resistance is essential for cables exposed to sunlight. In chemical-heavy or lubrication-rich facilities, cables must be resistant to oils and chemicals. For robotics and other dynamic applications, high-flex cables prevent breakage during constant movement. 

Shielding and Signal Integrity 

Shielding plays a vital role in maintaining signal integrity and preventing EMI. Foil shielding offers complete coverage against high-frequency interference. Braided shielding provides excellent low-frequency protection along with mechanical strength. Many industrial-grade bus cables combine both foil and braid for maximum shielding performance. 

Flexibility and Mechanical Properties 

Bus cables are often routed through conduits, machines and moving parts, making flexibility an important factor. Standard bus cables are sufficient for fixed installations, while high-flex designs are needed for dynamic applications such as robotic arms and drag chains. For rugged conditions, abrasion-resistant outer jackets extend service life. 

Compliance and Standards 

Industrial bus cables must comply with safety and environmental regulations. UL and CSA ratings ensure safety compliance in North America, while RoHS and REACH compliance demonstrate environmental responsibility. Each protocol, such as PROFIBUS, CAN-Bus or DeviceNet, also has its own defined electrical and physical requirements that must be met. 

Cost vs. Performance Balance 

While it may be tempting to cut costs with low-grade cables, this often leads to performance problems, downtime and higher replacement costs. High-quality industrial-grade bus cables ensure reliable performance, reducing maintenance demands and minimizing operational risks. 

Future-Proofing Your Network 

Industrial communication needs are evolving quickly, making future-proofing an essential consideration. Choosing cables that can support higher data rates prepares the system for future demands. Investing in cables compatible with multiple protocols adds flexibility. Hybrid bus cables, which combine power and data transmission, offer another way to prepare for next-generation systems. 

Choosing the right bus cable for your network involves analyzing your protocol requirements, environmental conditions, shielding needs and compliance standards. Investing in high-quality, properly rated bus cables ensures reliable performance, minimizes downtime and supports future network expansions. 

If you’re planning a new installation or upgrading an existing system, take the time to match your cable choice to both your technical and environmental needs. The right decision today ensures seamless communication for years to come. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

 

Resources

Search Entries