L-com

Edge Computing in Manufacturing: Enabling Real-Time Industrial Intelligence

 By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics  

 

 

Key Takeaway 

• Edge computing moves compute and data processing from the cloud to hardware located at or near the production floor—reducing latency from hundreds of milliseconds to single-digit milliseconds for time-critical industrial decisions. 

• Cloud-only architectures fail for real-time manufacturing applications because the round-trip time to a cloud data center (50–500 ms typical) is too slow for closed-loop process control, vision-based reject systems, and safety-adjacent decisions. 

• The industrial edge stack has five layers: field sensors, access switches, edge gateways, edge compute servers, and WAN uplinks — each with specific hardware requirements for the industrial environment. 

• Most manufacturers don't choose between edge and cloud — they use both. Edge handles real-time local decisions; the cloud handles historical analytics, model training, and multi-site dashboards. 

• The physical networking infrastructure — industrial switches, wireless gateways, and fiber backbone — is what determines whether the edge architecture is reliable in practice. Undersized or non-ruggedized networking hardware is the most common reason edge deployments underperform their design specification. 

  

Cloud computing changed what's possible for manufacturing analytics. Centralizing data from hundreds of machines, training machine learning models on years of production history, building dashboards that compare OEE across six facilities — none of that worked well before cloud platforms made it practical. 

But there's a category of manufacturing problem that cloud computing handles badly, and it comes down to one number: latency. A vision system that detects a defect and needs to trigger a divert mechanism has roughly 10 milliseconds to do before the part is past the reject gate. The round-trip time to a cloud data center and back is 50–500 milliseconds, depending on geography and network conditions. 

 

What Is Edge Computing in Manufacturing? 

Edge computing in manufacturing means running data processing, analytics, and decision logic on hardware physically located at or near the production floor — rather than transmitting raw data to a cloud data center for processing and waiting for a response. 

'Edge' is relative to the network topology. In manufacturing, the edge is typically: 

•       On the machine itself (edge gateway mounted in the machine cabinet, processing sensor data locally) 

•       At the cell or line level (edge server in a local panel room serving a production cell) 

•       At the facility level (edge data center serving a plant, with a WAN connection to cloud) 

Each of these is 'edge' relative to the cloud infrastructure above it. A machine-mounted gateway is the edge relative to a line-level server. A plant-level edge data center is the edge relative to a corporate cloud platform. 

The defining characteristic is not where the hardware sits — it's that processing happens locally, close to the data source, before (or instead of) transmitting to a central system. That locality is what enables low latency and continued operation during WAN outages. 

 

Why Does Cloud-Only Architecture Fail for Real-Time Manufacturing? 

Cloud-only fails for real-time manufacturing applications for two reasons: latency and resilience. Both are fundamental, not incidental. 

  

The Latency Problem 

Cloud computing adds network round-trip time to every decision. A sensor reading that triggers an alarm or a control action has to travel from the sensor to the gateway, from the gateway across the WAN to a cloud data center, through the cloud application, back across the WAN, and to the actuator or control system. The total round-trip is typically 50–500ms in real-world conditions — and that's for a facility with good WAN connectivity. Remote sites, congested networks, and inter-regional cloud routes push this higher. 

  

Application 

Required Latency 

Cloud Round-Trip 

Edge Decision 

Conveyor vision reject (defect → divert trigger) 

<10ms 

50–200ms (fail) 

<5ms (pass) 

Vibration anomaly alert to maintenance team 

<1 second 

100–500ms (marginal) 

<100ms (pass) 

PLC safety interlock (OT network only) 

<4ms 

Not applicable 

<1ms (pass) 

Predictive maintenance model scoring 

Minutes acceptable 

1–30 seconds (pass) 

Seconds (pass — both work) 

Energy consumption dashboard update 

Minutes to hours 

Seconds (pass) 

Seconds (pass — both work) 

Historical trend analysis (30-day) 

No real-time requirement 

Seconds (pass — cloud preferred) 

N/A — cloud is better 

  

The table above shows where cloud latency is and isn't a problem. For anything requiring a decision in under 10ms — which describes most closed-loop process control and production line response systems — cloud is architecturally unsuitable, not just slow. The physics of signal propagation over WAN links means the cloud can never meet sub-10ms requirements, regardless of compute speed. 

  

The Resilience Problem 

WAN connections fail. Cellular links drop. ISP outages happen at inconvenient times. A manufacturing facility running a cloud-only architecture loses its analytics capability, its predictive maintenance system, and potentially its production monitoring every time the WAN goes down. 

For non-critical monitoring, this is tolerable — you get a data gap and catch up when connectivity restores. For facilities where the edge system is integrated into production decisions (quality holds, process adjustments, alarm management), a WAN outage means operating blind. 

Edge architecture addresses this directly: local compute and storage continue operating regardless of WAN status. The edge system buffers data, maintains local dashboards, and continues making autonomous decisions during outages. When connectivity restores, it syncs the accumulated data to the cloud. 

 

The Bandwidth Problem 

High-resolution sensor data is voluminous. A single vibration sensor sampling at 10 kHz produces 20 MB per minute of raw data. A production line with 50 sensors produces 1 GB per minute. Streaming that to the cloud in real time requires 133 Mbps of sustained upload bandwidth — for one line. 

Edge processing reduces this by orders of magnitude. Rather than streaming raw samples, the edge gateway computes derived values (RMS, peak frequency, kurtosis) locally and transmits only those features — perhaps 1 KB per minute per sensor instead of 400 KB. The cloud receives actionable data; the WAN carries a fraction of the load. 

 

 What Does the Industrial Edge Stack Look Like? 

An industrial edge computing architecture has five hardware layers. Each layer has specific requirements that differ from IT or commercial hardware — the plant-floor environment doesn't forgive spec mismatches. 

  

Layer 

Component 

Primary Function 

Typical Hardware Specs 

Failure Mode if Wrong 

Layer 1 — Field 

Industrial sensors & actuators 

Generate process data: temperature, pressure, vibration, position, flow 

IP67+, wide-temp, appropriate protocol (4–20 mA, Modbus RTU, IO-Link, HART) 

Wrong sensor type or rating → missing data or sensor failure in environment 

Layer 2 — Access 

Industrial Ethernet switches (access layer) 

Connect field devices to the edge network and enforce access-layer VLANs and PoE for powered devices 

DIN-rail, −40°C to 70°C, DC 24V, fanless, managed (RSTP/MRP), M12 or RJ45 ports 

A commercial switch at this layer fails from temperature and vibration within months 

Layer 3 — Edge Gateway 

Industrial wireless gateway / edge gateway 

Protocol translation (Modbus → MQTT/OPC-UA); local buffering; edge analytics; WAN uplink management 

DIN-rail, wide-temp DC, dual WAN (wired + cellular failover), OT protocol support, local compute for pre-processing 

A gateway without local buffering drops data during WAN outages; wrong protocol support can't connect legacy field devices 

Layer 4 — Edge Compute 

Industrial edge server / rugged PC 

Runs ML inference, anomaly detection, vision processing, real-time analytics locally; manages edge-to-cloud sync 

Rugged fanless PC or edge server; wide-temp; SSD (no spinning disk); sufficient RAM/GPU for local workload; redundant power 

Undersized compute creates processing bottleneck; non-rugged hardware fails in thermal/vibration environment 

Layer 5 — WAN / Uplink 

Fiber backbone + WAN router / cellular router 

Connects edge infrastructure to cloud, enterprise, or remote operations centers; failover between primary and backup WAN 

Fibre optics for inter-building runs; industrial cellular router for primary or backup WAN; firewall capability at WAN boundary 

Copper backbone in EMI-heavy environment → data corruption; single WAN without failover → complete isolation on link failure 

  

 

Layer 1: Field Sensors and Actuators 

The data source. Industrial sensors for temperature, pressure, vibration, position, flow, and current generate the raw process data that the edge stack processes. The sensor selection determines data quality — wrong range, wrong accuracy, or wrong environmental rating, and the data is either missing or unreliable regardless of how good the compute above it is. 

In brownfield deployments, existing sensors typically communicate over legacy protocols: 4–20mA analogue, Modbus RTU, HART, and IO-Link. The edge gateway at Layer 3 needs to support whatever protocols the field devices speak. This is a hardware selection constraint, not a software configuration — gateways without the right serial ports or protocol stacks can't connect to specific field devices. 

  

Layer 2: Access-Layer Industrial Ethernet Switches 

Access switches aggregate connections from field devices and carry them to the edge gateway. In machine-level edge deployments, the access switch is typically DIN-rail mounted inside the machine cabinet – wide-temperature, DC-powered, fanless, with RSTP or MRP ring redundancy. 

Industrial Ethernet switches at the access layer need to handle the physical conditions of their installation point: temperature swings if the cabinet isn't climate-controlled, vibration from nearby drives and motors, DC power from the panel bus, and EMC from the VFDs and contactors that share the cabinet. A commercial switch at this layer fails from temperature and vibration within months in a typical machine cabinet environment. 

 

Layer 3: Industrial Wireless Gateways and Edge Gateways 

The gateway layer is where the OT-to-IT translation happens. An industrial wireless gateway reads data from field devices using OT protocols (Modbus, EtherNet/IP, and PROFINET), translates it to IP-friendly formats (MQTT, OPC-UA, and REST), and forwards it to the edge compute layer above — or directly to the cloud if local processing isn't needed. 

For edge deployments, the gateway also handles local buffering: storing data locally when the WAN or uplink is unavailable, then syncing when connectivity restores. Without this capability, WAN outages create data gaps that break time-series analysis and make predictive maintenance models less reliable. 

Industrial wireless gateways handle the additional function of wireless connectivity for field devices that can't be cabled — sensors on rotating equipment, instruments in locations without conduit paths, or assets spread across large outdoor areas. The wireless and protocol translation functions can be in the same device or separate, depending on the deployment architecture. 

 

Layer 4: Edge Compute Hardware 

The edge compute layer runs the actual analytics: machine learning inference models for predictive maintenance, vision processing algorithms for quality inspection, anomaly detection logic, and real-time control decision engines. This is where the 'intelligence' in industrial intelligence lives. 

Hardware at this layer needs to be ruggedised for the industrial environment while providing enough compute for the local workload. The requirements vary significantly: 

•       Simple anomaly detection on a handful of sensors: a gateway with local compute (4-core ARM processor, 4GB RAM) is sufficient 

•       Multi-sensor predictive maintenance with ML inference: an industrial PC with a 6–8 core x86 processor and 16GB+ RAM 

•       Computer vision at production line speeds: a rugged system with a dedicated GPU (NVIDIA Jetson or similar) 

Fanless designs are required for most plant floor deployments — fan failure in dirty environments is the primary cause of edge compute hardware failure. SSDs over spinning disks for the same reason. Industrial temperature ratings and wide-range DC power inputs apply. 

 

Layer 5: WAN Uplink and Fiber Backbone 

The WAN uplink connects the edge infrastructure to cloud platforms, enterprise systems, and remote operations centers. The physical medium for inter-building runs and long-distance connections within the facility is typically fiber optic — not copper. 

Fiber optic connectivity solutions eliminate the ground loop and EMI issues that copper introduces in industrial environments with large motor loads, switching equipment, and welding. For runs between buildings or across large facilities, fiber is the right call on both performance and reliability grounds. Single-mode fiber for distances over 500m or where future bandwidth upgrades are likely; multi-mode for shorter runs within a building. 

Cellular failover (4G LTE or 5G) provides backup WAN connectivity when the primary link fails. For facilities where WAN uptime is operationally critical  remote plants, facilities with unreliable primary connectivity — dual-WAN with automatic failover is standard architecture. The edge gateway or a dedicated industrial router handles the failover logic. 

 

Cloud vs. Edge vs. Hybrid: Which Architecture Do You Need? 

The honest answer for most manufacturing facilities is hybrid. Pure edge is limiting — you lose the long-term storage, multi-site analytics, and model training capabilities that cloud provides. Pure cloud is inadequate — you can't meet real-time latency requirements for production-floor decisions. Hybrid uses each where it fits. 

  

Requirement 

Cloud-Only 

Edge-Only 

Hybrid (Edge + Cloud) 

Latency tolerance 

High: 50–500ms round trip acceptable 

Low: <10 ms at the edge for local decisions 

Mixed: edge for real-time, cloud for historical/analytics 

WAN dependency 

Fully dependent — loses capability on WAN failure 

Independent — fully operational without WAN 

Resilient — degrades gracefully on WAN failure; edge keeps running 

Data volume 

Efficient for processed/summarized data; expensive for raw streams 

No WAN bandwidth cost; limited by local storage 

Optimal: raw data processed at edge; summaries/events sent to cloud 

ML model updates 

Centrally managed; easy model deployment 

Requires manual or scripted local updates 

Cloud trains and pushes model updates to edge automatically 

Storage / retention 

Unlimited cloud storage; access from anywhere 

Limited by local hardware; local access only 

Edge buffers locally; cloud provides long-term storage and remote access 

Hardware cost 

Low upfront (no edge HW); cloud compute costs at scale 

Higher upfront edge hardware and minimal ongoing cloud cost 

Moderate hardware + reduced cloud compute (edge pre-filters data) 

Security boundary 

All data traverses WAN; OT/IT boundary must be enforced at each site 

Data stays on-premise: smaller external attack surface 

Edge enforces OT/IT boundary; only processed data crosses to the cloud. 

Best for 

Non-time-critical analytics; historical trending; multi-site dashboards 

Hard real-time control, safety-adjacent decisions, sites with poor WAN 

Most production manufacturing: real-time local decisions + cloud analytics 

  

A few observations from the table that aren't obvious from reading the spec sheets: 

 

Hybrid Is Not 'Cloud With an Edge Box Bolted On' 

A well-designed hybrid architecture decides at design time which decisions happen at the edge and which happen in the cloud — and architects the data flow accordingly. It's not streaming everything to the cloud and calling it hybrid because there's a gateway in the middle. 

The decision boundary is latency and autonomy. If the decision needs to happen in under 1 second, it happens at the edge, and the cloud doesn't need to be in the loop. If the decision can wait for cloud round-trip time and benefits from cloud compute (multi-week historical data, cross-facility comparison), it goes to the cloud. 

 

Edge-Only Is Rarer Than It Sounds 

Pure edge architectures make sense for specific scenarios: facilities with no reliable WAN, safety-critical systems that must be isolated from cloud connectivity for compliance reasons, or applications where all relevant context is local. For most manufacturing facilities, some cloud connectivity is available and useful — historical trending, remote monitoring, and model updates all benefit from cloud access. 

The edge-only scenario worth planning for is not 'we chose not to connect to the cloud' but 'WAN is down and production continues.' The edge architecture should be designed to operate autonomously during WAN outages, even if the normal operating mode uses cloud connectivity. 

  

The cost math favours hybrid at scale 

Cloud compute and storage at scale is expensive when you're sending raw data. A facility generating 10 GB per hour of raw sensor data costs substantially more in cloud ingestion and storage than a facility that processes locally and sends 100 MB per hour of derived features. Edge preprocessing reduces cloud cost by an order of magnitude or more for data-intensive applications, often paying for the edge hardware within 12–18 months. 

 

How Does Edge Computing Fit With OT/IT Convergence? 

Edge computing is often the physical expression of OT/IT convergence — the place where the OT data generated by field devices becomes accessible to IT systems, cloud platforms, and analytics tools. Done right, it's also where OT/IT security boundaries are enforced. 

The edge gateway sits at the OT/IT boundary. It connects to OT devices using OT protocols and translates data to IP-native formats for the IT side. It also enforces the security boundary: OT devices communicate with the gateway using their native protocols, but they don't get routable IP connectivity to the enterprise network or the internet. The gateway is the firewall, protocol translator, and data broker simultaneously. 

This matters for security: an OT network where field devices have direct routable IP connectivity to the cloud is an OT network where those field devices are exposed to internet-sourced threats. An OT network where field devices communicate only to a local gateway — which in turn communicates selectively to cloud endpoints — has a much smaller external attack surface. 

Network segmentation at the access layer reinforces this. VLANs on industrial access switches isolate OT device traffic from IT traffic at Layer 2, even when both traverse the same physical infrastructure. The combination of gateway-level enforcement and switch-level segmentation creates the defence-in-depth that OT/IT convergence requires. 

  

What Does an Edge Computing Deployment Look Like in Practice? 

An automotive components manufacturer runs two injection moulding lines. Each press has temperature sensors, hydraulic pressure sensors, and a cycle counter. The plant currently has no real-time process visibility — process engineers use end-of-shift data to diagnose quality issues. 

  

 
Edge architecture deployed: 

•       Layer 1: 12 sensors per press (temperature, pressure, position) communicating over Modbus RTU on an RS-485 bus. Existing sensors retained — no hardware replacement needed. 

•       Layer 2: Industrial DIN-rail managed switches in each press panel, powered from the 24V DC bus. Fanless, wide-temp rated. RSTP ring topology between presses. 

•       Layer 3: Two industrial wireless gateways (one per line) poll Modbus RTU sensors at 1-second intervals, translate data to MQTT, and publish to the edge compute layer. Gateways have local 4GB flash buffers — if the edge server goes offline, sensor data buffers locally. 

•       Layer 4: One industrial edge server per line (8-core, 32GB RAM, fanless, DIN-rail mounted in the line's control panel room). Runs an anomaly detection model trained on 3 months of historical process data. Detects process drift in real time and alerts process engineers via SMS before a quality excursion occurs. 

•       Layer 5: Fiber backbone from each panel room to the plant's main switch. WAN uplink to the corporate cloud platform sends hourly summaries and anomaly events. The cloud runs the model retraining pipeline on accumulated historical data. 

  

Result: process engineers get real-time anomaly alerts rather than end-of-shift reports. Average response time to process drift dropped from hours to under 10 minutes. Scrap rate on the first line reduced measurably in the first quarter after deployment.  

 

Building Resilient Industrial Networks 

Reliable industrial security depends on more than firewall rules and network segmentation. The underlying physical infrastructure must be designed to support continuous operation in demanding environments. From industrial Ethernet and fiber connectivity to wireless networking and ruggedized connectivity solutions, L-com helps organizations build resilient industrial networks that support security, reliability, and long-term operational performance. 

 

 

Frequently Asked Questions (FAQs) 

What is edge computing in manufacturing? 
Edge computing is the practice of processing data close to where it is generated—on the machine, production line, or facility floor—rather than sending all data to a cloud platform for analysis. This reduces latency and allows manufacturers to make faster operational decisions. 

Why is edge computing important for industrial applications? 
Many industrial processes require near real-time responses. By processing data locally, edge computing helps support machine monitoring, quality inspection, predictive maintenance, and other applications where cloud latency may be too slow. 

What is the difference between an edge gateway and an edge server? 
An edge gateway primarily collects, translates, and forwards data between field devices and higher-level systems. An edge server provides the local computing resources needed to run analytics, machine learning models, visualization tools, and other processing workloads. 

Should manufacturers choose edge computing or cloud computing? 
Most manufacturers benefit from a hybrid approach. Edge computing handles time-sensitive local decisions, while cloud platforms support long-term storage, enterprise-wide analytics, model training, and multi-site visibility.

Resources

Search Entries