By Dustin Guttadauro, Product Line Manager – Telecom & Fiber, Infinite Electronics
Cyber-physical systems (CPS) are the foundation of many Industry 4.0 initiatives, connecting physical equipment with digital intelligence to create continuous feedback loops between machines, sensors, networks, and software. While the concept sounds complex, CPS is already embedded in modern manufacturing environments through predictive maintenance systems, adaptive automation, machine vision platforms, and real-time process control. Understanding how cyber-physical systems work helps manufacturers evaluate smart factory technologies, improve operational efficiency, and build the infrastructure required for more autonomous industrial operations.
Key Takeaways
- A cyber-physical system (CPS) is any system where digital computation and physical processes are tightly coupled the software continuously monitors and controls the physical process, and the physical process provides real-time feedback to the software.
- In manufacturing, CPS examples include CNC machines with in-process measurement and automatic compensation, adaptive robotics that adjust grip force based on part geometry, and production lines that adjust conveyor speed based on downstream queue depth.
- CPS differ from simple automation in that they close the loop — the physical outcome feeds back into the digital control system in real time, not just as a log entry.
- Reliable low-latency networking is a fundamental CPS requirement — if the feedback loop is slow, the control system can't respond accurately.
- CPS implementations underpin Industry 4.0's most advanced capabilities: adaptive manufacturing, autonomous quality control, and machine-to-machine coordination.
What is a cyber-physical system?
A cyber-physical system is an engineered system where physical hardware and computational software are so tightly coupled that neither function properly without the other. The physical side — machines, motors, valves, conveyors — generates real-world data. The cyber side — sensors, edge computers, control software, AI reads that data, processes it, and sends instructions back to the physical side. That loop runs continuously.
The term was coined by Helen Gill at the National Science Foundation in 2006, but the concept predates the label. SCADA systems and PLCs were doing versions of this for decades. What's changed is the scale, the speed, and the sophistication of the analysis in the middle. A CNC machine that adjusts its feed rate based on real-time torque readings is a simple CPS. A factory floor where 400 sensors feed a predictive maintenance AI that schedules maintenance orders automatically is a more complex one. The architecture is the same — physical process, sensor, network, computation, actuator, physical process again — just operating at different scales.
How do cyber-physical systems work?
A CPS operates through three layers that interact continuously. Understanding the layers helps explain why the physical hardware choices matter as much as the software choices.
The physical layer
This is the factory floor: machines, conveyors, presses, robots, HVAC, and coolant systems. Every physical process generates signals: temperature, pressure, vibration, position, current draw, and flow rate. The physical layer also includes actuators, the components that receive instructions and do something physical in response, like adjusting a valve or changing a motor speed.
The network layer
Data doesn't move on its own. The network layer is the infrastructure that carries signals from physical devices to computing systems and returns instructions to actuators. This includes wired industrial Ethernet, fibre optic backbones, wireless protocols like WirelessHART and ISA-100, and the gateways that translate between them. The network layer is where most CPS projects run into trouble. A factory floor is electrically hostile — drives, welding equipment, and motors generate interference that corrupts data on unshielded cables and degrades wireless signals. The software layer can only act on the data it receives. If that data is noisy, delayed, or incomplete, the system makes bad decisions.
The cyber layer
Edge computing nodes, cloud platforms, and AI systems live in the cyber layer. They receive the sensor data, run it through analytics models, and generate responses: maintenance alerts, process adjustments, quality flags, and production schedule changes. The output feeds back into the physical layer through actuators or operator dashboards. The speed of this loop matters. For time-critical control applications, like a press stopping before a collision or a temperature controller preventing a furnace overshoot, the loop needs to close in milliseconds. Edge computing exists specifically to handle those cases without the round-trip latency of a cloud server.
What are the core components of a CPS?
Every cyber-physical system, regardless of scale or industry, is built from the same set of components.
|
Component |
Function |
Manufacturing Example |
|
Sensors |
Convert physical phenomena into digital signals |
Vibration sensor on a motor bearing; thermocouple on a furnace |
|
Actuators |
Convert digital instructions into physical action |
Servo motor adjusting feed rate; solenoid valve controlling flow |
|
Edge computing nodes |
Process data locally with low latency |
Industrial PC running anomaly detection at the machine level |
|
Industrial network |
Move data between physical and cyber layers |
Shielded Ethernet from sensor to edge node; fiber between cells |
|
Wireless gateways |
Connect mobile or hard-to-wire assets |
Gateway aggregating readings from 30 wireless vibration sensors |
|
Cloud / analytics platform |
Store, correlate, and model data at scale |
Predictive maintenance model running across 200 machines |
|
Control software / AI |
Generate instructions from data |
AI scheduling maintenance when bearing signature shifts |
|
Human interface (HMI/SCADA) |
Give operators real-time visibility and override control |
Dashboard showing live OEE, alerts, and process trends |
The components that directly touch L-com's product lines are the sensor and network layers.Industrial IoT sensors need to be rated for the specific environmental conditions — temperature range, ingress protection, EMI tolerance — of the installation. Industrial wireless gateways need to handle the device counts and data throughput the application actually generates, not just what it generates today.
How are cyber-physical systems used in manufacturing?
Manufacturing is the industry where CPS has the clearest return on investment, because the feedback loops are direct: better data in, fewer unplanned stoppages and defects out. Here are the primary applications.
Predictive maintenance
A motor bearing failing on a production line can cost tens of thousands of dollars in unplanned downtime. A CPS puts vibration and temperature sensors on the bearing, feeds their readings to an edge computer running a failure signature model, and alerts maintenance before the signature crosses a threshold associated with imminent failure. The line gets a scheduled maintenance window instead of an unscheduled collapse.
Inline quality inspection
Traditional quality control is sampling at the end of a line. By the time an inspector catches a defect pattern, hundreds of bad parts have already been produced. A CPS with vision sensors and AI can inspect every part during production, flag the defect, trace it to a process parameter, and trigger an automatic adjustment or at minimum a maintenance alert — within seconds.
Closed-loop process control
A CPS can close the control loop entirely for well-understood processes. In injection molding, for example, cavity pressure sensors feed real-time readings to a controller that adjusts injection speed and hold pressure on each shot based on the actual conditions of that shot, not a fixed program. The result is fewer short shots, sink marks, and warped parts — without an operator making manual adjustments.
Energy management
Factory energy costs are rarely optimized because real-time energy consumption at the machine level is rarely visible. A CPS puts current sensors on individual machines and production cells, identifies the highest consumers, spots patterns (machines running at full power during idle states, compressed air leaks detectable through pressure drop signatures), and gives energy managers the data to act.
Remote monitoring and autonomous response
CPS enables facilities to be monitored and — within defined limits — managed remotely. Overnight runs without full staffing, remote expert guidance using live equipment data, automatic safe-state responses to out-of-spec conditions. These capabilities become especially relevant for multi-site manufacturers who can't put a full engineering team at every location.
What is the difference between CPS, IIoT, and a smart factory?
These three terms overlap, and people use them interchangeably — which causes confusion when you're trying to plan an actual deployment. Here's how they relate.
|
Term |
What it actually means |
|
Cyber-Physical System (CPS) |
The architectural concept — physical processes and digital systems integrated into a feedback loop. CPS is the framework. |
|
IIoT (Industrial Internet of Things) |
The connected device layer within a CPS — sensors, actuators, gateways, and the protocols they use to communicate. IIoT is a component of CPS. |
|
Smart Factory |
A manufacturing facility built on CPS and IIoT principles, combined with AI analytics, cloud platforms, and operational workflows. A smart factory is a CPS implementation at facility scale. |
|
SCADA |
Supervisory Control and Data Acquisition — a control system architecture that predates CPS terminology but shares the same physical-cyber integration concept. Modern SCADA systems are a form of CPS. |
|
Industry 4.0 |
The broader industrial transformation movement that CPS, IIoT, AI, and digital twins are all part of. Industry 4.0 is the context; CPS is one of the enabling architectures. |
If you're a plant manager deciding what to implement: CPS is how engineers describe what you're building. Smart factory is how executives describe the outcome. IIoT is what you're buying from vendors.
Why does physical connectivity determine CPS performance?
This is the part that gets left out of most CPS explainers, and it's where real deployments succeed or fail. The feedback loop in a CPS is only as good as its weakest physical link. Software and AI can compensate for a lot, but they can't compensate for data that isn't arriving, is corrupted in transit, or is delayed past the point where it's actionable. Every layer of the stack depends on the one below it.
Sensor selection
The sensor specification determines what the system can actually know about the physical process. A vibration sensor with inadequate frequency response misses the early-stage bearing fault signatures that predict failure three to six weeks out. A temperature sensor with poor thermal response time misses fast thermal events. Getting the spec right requires knowing the process — not just picking the cheapest unit that reads the right parameter. L-com's industrial IoT sensors are rated for industrial environments where off-the-shelf sensors fail—wide temperature ranges, IP-rated enclosures, and EMI tolerance built in.
Cable and shielding
Industrial environments generate electromagnetic interference from drives, motors, welding equipment, and power distribution. Unshielded cables pick up that interference as noise on the signal line. At low data rates this causes occasional bit errors. At high data rates — IIoT systems generating thousands of readings per second — it causes packet loss, retransmissions, and latency spikes that degrade system response.
For long runs or high-EMI environments,fiber optic connectivity eliminates the interference problem entirely. Fiber is immune to electromagnetic noise, supports the data rates industrial applications generate, and handles the run lengths that span large facilities.
Gateway capacity and reliability
Gateways aggregate data from multiple field devices and pass it to edge computing or cloud systems. An undersized gateway, too few connections, insufficient throughput, or consumer-grade components become the bottleneck. In a CPS, a gateway that drops connections or falls behind on throughput causes the feedback loop to fail at the exact moments when it's most needed. Industrial wireless gateways rated for wide temperature ranges and high device counts keep the data flowing in the conditions that factory floors actually produce, not just in lab conditions.
What are the security risks in cyber-physical systems?
CPS security is harder than IT security because the stakes are different. A compromised database server costs money. A compromised CPS controlling a high-pressure system, a chemical process, or a robotic cell can cause physical harm.
The risks fall into three categories.
- OT/IT convergence exposure: Connecting operational technology to IT networks — which is what CPS requires creates attack paths that didn't exist when OT was isolated. A phishing email that compromises an IT workstation can now potentially reach the control network.
• Legacy equipment vulnerabilities: Many production environments run PLCs and SCADA systems designed in an era when network connectivity wasn't expected. These systems often lack authentication, encryption, or the ability to receive security patches.
• Supply chain risk: The physical hardware in a CPS — sensors, gateways, edge nodes — comes from third-party manufacturers. Compromised firmware or hardware backdoors in components are a known attack vector.
Mitigating these risks requires network segmentation between OT and IT environments (separate VLANs at minimum, hardware-enforced zones for higher-risk installations), encrypted communications on all data transfers, strict access controls on remote connections, and continuous monitoring of OT network traffic for anomalous patterns. Cybersecurity can't be added to a CPS after the fact. The network architecture decisions made at deployment determine what's possible to defend. This is another reason to get the connectivity infrastructure right at the start segmented industrial networking is the foundation that security controls are built on.
Building Resilient Industrial Networks
Reliable industrial security depends on more than firewall rules and network segmentation. The underlying physical infrastructure must be designed to support continuous operation in demanding environments. From industrial Ethernet and fiber connectivity to wireless networking and ruggedized connectivity solutions, L-com helps organizations build resilient industrial networks that support security, reliability, and long-term operational performance.
Frequently Asked Questions (FAQs)
What is a cyber-physical system?
A cyber-physical system (CPS) combines physical equipment with digital computing, networking, and control systems that continuously monitor and influence real-world processes through closed-loop feedback.
How is a cyber-physical system different from IIoT?
IIoT refers to the connected sensors, devices, and communications infrastructure that collect and transmit data. A cyber-physical system uses that data within a feedback loop to monitor conditions, make decisions, and influence physical operations.
How are cyber-physical systems used in manufacturing?
Manufacturers use CPS for predictive maintenance, machine monitoring, adaptive process control, quality inspection, energy management, robotics, and other applications that require real-time interaction between digital systems and physical equipment.
Why is network infrastructure important to a cyber-physical system?
Cyber-physical systems depend on reliable data movement between sensors, controllers, computing platforms, and machines. Network latency, packet loss, or communication failures can limit the system's ability to respond accurately and in real time.