L-com

The Complete Guide to Industrial Bus Cables

By Eileen Harvey 

Industrial bus cables serve as the backbone of these communication networks, facilitating seamless data transfer and ensuring the smooth operation of various machinery and equipment. These specialized cables are designed to withstand the unique challenges posed by harsh industrial environments, including temperature fluctuations, electromagnetic interference (EMI) and mechanical stress.  

As industries increasingly turn towards automation and smart technologies, understanding the intricacies of industrial bus cables becomes paramount for engineers, technicians and decision-makers. Additionally, best practices for installation and maintenance will be discussed to ensure optimal performance and longevity. For robust and certified industrial bus cables, TKD Kabel is a trusted name in the industry.  

What Are Industrial Bus Cables? 

Industrial bus cables are specialized communication cables that play a crucial role in fieldbus and industrial networking systems. They are engineered to facilitate seamless communication between devices and systems within industrial environments such as factories, manufacturing plants, and automation setups. Unlike ordinary cables, bus cables must ensure precise signal transmission without interference, withstand harsh conditions that may include exposure to oil, UV radiation, and chemicals, and endure mechanical stress, particularly in robotics and automated systems. These cables are essential for connecting programmable logic controllers (PLCs), sensors, actuators and controllers while maintaining reliable and synchronized communication. 

Why Bus Cables Matter in Industrial Applications 

The importance of bus cables in industrial environments lies in several key factors. Data integrity is crucial because poor-quality cables can cause data loss, downtime, or miscommunication between devices. Durability is equally vital, as industrial systems require cables that resist abrasion, oil, and extreme temperatures. Compliance with international standards such as PROFIBUS International and the CiA for CAN-Bus ensures compatibility and quality. Cost efficiency is another benefit, since using the right cable reduces maintenance and downtime, leading to long-term savings. 

Types of Industrial Bus Cables 

PROFIBUS cables are standard in process automation and factory communication. They typically have 150-ohm impedance with double shielding for EMI resistance and are easily recognized by their violet jacket. 

CAN-Bus cables are widely used in automotive, robotics, and motion control systems. They feature standard 120-ohm impedance and are often designed with one or two pairs of conductors. Options with stranded conductors provide greater flexibility. 

DeviceNet cables are based on CAN-Bus technology but optimized for industrial networks. They combine power and signal transmission in a single cable and are used in applications such as sensors, actuators, conveyors, and assembly lines. 

AS-Interface (ASI) bus cables simplify connections between sensors and actuators. These are flat, two-conductor cables that use easy piercing technology. They follow a color-coded scheme: yellow for standard communication and black for auxiliary power. 

Ethernet-based bus cables include PROFINET, EtherCAT, and Modbus TCP/IP. They are designed for high-speed, real-time communication and feature industrial-grade shielding to resist EMI. Unlike standard office Ethernet cables, they offer oil resistance, UV stability, and rugged jackets for industrial use. 

Construction and Design Features of Bus Cables 

The construction of bus cables varies depending on the application. Conductors may be solid, which are better for long distances, or stranded, which are more flexible for moving machinery. Insulation materials include PVC for basic use, PE for low-loss transmission, and TPE for oil and UV resistance. Shielding options include foil, braid, or double shielding to protect against electrical noise. Jackets are designed with flame-retardant, UV-stable, and oil-resistant materials to withstand harsh conditions. Standardized color codes help with identification, such as violet for PROFIBUS and CAN, and yellow for ASI. 

Shielding and Interference Protection 

In industrial environments, electrical noise from motors, variable frequency drives (VFDs), and welding machines can disrupt communication signals. Shielding prevents interference by using foil layers to protect against high-frequency noise, braided shields to counter low-frequency EMI, and double shielding that combines both foil and braid for maximum protection. 

Standards and Compliance 

Industrial bus cables are governed by established standards to ensure reliability and safety. PROFIBUS and PROFINET are defined by international standards, while CAN-Bus follows guidelines set by CAN in Automation (CiA). Certifications such as UL, IEC, and EN further validate cable safety and quality. Using certified cables ensures compatibility, reliability, and compliance with automation systems. 

Key Applications of Industrial Bus Cables 

These cables are used across a wide range of industries and applications. In factory automation, they connect sensors, actuators, and PLCs. In robotics and motion control, they enable real-time communication for precision operations. In process industries such as oil and gas, pharmaceuticals, and food processing, bus cables ensure efficient monitoring and control. They also support automotive CAN-Bus systems in transportation, as well as utilities and energy sectors, including power plants and smart grids. 

How to Choose the Right Bus Cable 

Selecting the right bus cable is a critical decision that affects both the performance and reliability of networked systems. Bus cables serve as the backbone of communication between devices in environments ranging from industrial automation to vehicle systems and data centers. With a variety of options available—including twisted pairs, coaxial, and fiber optic cables—it is essential to match the cable to the application’s specific requirements. 

When choosing a bus cable, protocol compatibility is the first consideration, whether the system uses PROFIBUS, CAN-Bus, ASI, or Ethernet. Distance and data rate must also be evaluated, since long distances may require specific impedance. Environmental factors such as UV exposure, oil, and chemical resistance play a major role in selection, as does the required flexibility, with fixed installations differing from drag chain applications. Finally, certification is essential—cables with UL, IEC, or EN approvals provide assurance of safety, reliability, and compliance. 

Expert Tips and Recommendations 

  • Use double-shielded cables in high-EMI environments. 
  • For robotics, pick stranded conductor cables for flexibility. 
  • Always check temperature ratings for process industry applications. 
  • Invest in certified cables—they reduce downtime and increase system life. 

FAQs: Industrial Bus Cables 

Q1: Can I use standard Ethernet cables for PROFINET or Ether CAT? 
A: No. Industrial Ethernet cables are specially designed for durability, shielding and resistance to oil/UV, unlike office-grade Ethernet. 

Q2: What happens if I use the wrong impedance cable (e.g., 100-ohm instead of 150-ohm)? 
A: Mismatched impedance can cause signal reflection, data loss and unreliable communication. Always match cable specs to system requirements. 

Q3: Do all bus cables need shielding? 
A: Most do, especially in noisy environments. ASI cables may be unshielded since they are designed for simpler actuator/sensor networks. 

Industrial bus cables are the lifelines of automation systems, ensuring reliable, interference-free communication across industries. From PROFIBUS to CAN-Bus, ASI, and Ethernet-based solutions, selecting the right cable depends on your protocol, environment and performance needs. 

About L-com 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

 

Resources

Search Entries