By Dustin Guttadauro, Product Line Manager - Telecom & Fiber, Infinite Electronics
As data center networks move toward higher speeds, the physical layer has to support increasing bandwidth without making rack layouts unnecessarily difficult to manage. For short- and medium-reach connections, an active optical cable (AOC) can provide a practical alternative to separate optical transceivers and fiber patch cables. An AOC combines optical fiber with active electronics integrated into the cable ends. Instead of installing a separate transceiver at each switch port and connecting those modules with a fiber cable, an AOC provides an integrated cable assembly with compatible interfaces at both ends.
This plug-and-play design can simplify high-density deployments where large numbers of connections must be routed through racks, servers, and switches. AOCs are commonly available for data rates ranging from 25G and 40G to 100G and 400G, depending on the product family and application. They can be particularly useful in high-performance computing (HPC), GPU clusters, storage networks, and top-of-rack (ToR) connections.
However, an AOC is not automatically the right choice for every link. Engineers need to consider distance, port compatibility, cable routing, serviceability, future changes, and whether separate optics and structured fiber provide greater flexibility.
Key Takeaways
- An active optical cable (AOC) combines optical fiber and active electronics into one integrated cable assembly.
- AOCs simplify point-to-point high-speed connections by eliminating separate optical transceivers and patch cables.
- They are commonly used for 25G, 40G, 100G, and 400G applications, depending on the product and system.
- AOCs can provide lower cable weight and easier routing than comparable copper connections.
- GPU/HPC fabrics, ToR-to-server connections, storage networks, and short switch-to-switch links are common application areas.
- DACs are generally better suited to very short copper connections.
- Separate transceivers and fiber assemblies provide greater flexibility for structured cabling and changing network topologies.
- QSFP28 is an important form factor for 100G AOC applications.
- Always verify speed, port compatibility, cable length, reach, connector, and equipment interoperability before ordering.
What Is an Active Optical Cable?
An active optical cable, or AOC, is a cable assembly that combines optical fiber with active optical components at the ends of the cable. The basic architecture is:
Network Port → Integrated Optical Electronics → Fiber Cable → Integrated Optical Electronics → Network Port
Unlike a traditional fiber connection, where the transceivers and cable are separate components, the optical interfaces are integrated into the AOC assembly. AOCs typically use multimode fiber for short- and medium-reach data center applications, although the exact construction depends on the specific product.
The result is a cable that can be connected directly between compatible equipment without separately selecting and installing two optical transceivers and a fiber patch cable. This makes AOCs particularly attractive when the endpoints are known, the cable length can be predetermined, and a simple point-to-point connection is preferred.
How Does an AOC Work?
An AOC converts the electrical signal from a network port into an optical signal within the integrated electronics at one end of the cable. The optical signal travels through the fiber portion of the assembly. At the opposite end, integrated electronics convert the optical signal back into an electrical signal for the receiving network port. The user does not normally need to manage these optical conversion components independently.
This differs from a conventional pluggable optical architecture:
Switch → Transceiver → Fiber Cable → Transceiver → Switch
An AOC instead provides:
Switch → AOC → Switch
The integrated construction reduces the number of individual components that must be specified and installed.
Why Choose an AOC Over DAC?
One of the most common reasons to consider an AOC is when a copper DAC becomes less practical because of distance, weight, or cable routing requirements. Copper cables can become relatively heavy and difficult to manage as cable lengths and quantities increase. An optical cable can provide a lighter physical connection, which can be valuable in high-density racks containing many network, storage, and compute connections. AOCs can also support higher data rates where the selected platform and cable are designed for those speeds.
For example, an organization deploying a high-density GPU cluster may need large numbers of high-speed connections between servers and switches. Using optical cable assemblies can simplify cable routing compared with large bundles of copper cables. The correct choice still depends on the actual distance and equipment specifications.
AOC Cable Management Benefits
Cable management becomes increasingly important as port counts and network speeds increase. An AOC can provide several physical-layer advantages.
Lower cable weight: Fiber is generally lighter than copper for comparable high-speed applications. This can reduce the load created by large cable bundles.
Improved bendability: Optical cable constructions can be easier to route through dense rack environments than heavier copper assemblies.
However, every fiber cable still has a minimum bend radius. Engineers should follow the manufacturer's installation specifications rather than assuming fiber can be bent without limitation.
Reduced cable bulk: High-density deployments can involve hundreds or thousands of connections.
Reducing cable bulk can make it easier to maintain:
- Rack airflow
- Cable pathways
- Vertical managers
- Horizontal managers
- Patch areas
- Service access
Simplified installation
Because the optical components are integrated into the cable assembly, engineers do not have to separately install and manage a pair of optical transceivers and a patch cable for every AOC connection.
Common AOC Data Rates
AOCs are available across multiple generations of data center networking. Depending on the equipment and application, AOC families can support data rates such as:
- 25G
- 40G
- 100G
- 400G
The specific electrical interface and connector configuration depend on the application. For example, QSFP28 is commonly associated with 100G applications, while newer high-speed platforms can use higher-bandwidth form factors and architectures. The important point is that the AOC's advertised speed must match the switch or server port. A 100G AOC does not simply turn any physical QSFP-style port into a 100G interface. The host port, cable, and system firmware must support the intended configuration.
AOC Use Case: GPU and HPC Fabrics
High-performance computing and GPU clusters can create demanding physical-layer requirements. AI and HPC environments often use large numbers of servers or GPU nodes connected through high-speed network fabrics.
In these environments, AOCs can be attractive because they provide:
- High-speed optical connectivity
- Integrated endpoints
- Lower cable weight than comparable copper solutions
- Simplified point-to-point deployment
- Cleaner high-density cable routing
For example:
GPU Server → High-Speed AOC → Switch
can provide a straightforward point-to-point connection when the distance falls within the AOC's specified reach. Cable routing is particularly important in GPU environments because dense compute configurations can generate significant cable congestion around the rear of server racks.
AOC Use Case: Top-of-Rack to Server
Top-of-rack switching is another common AOC application. A ToR switch may connect to multiple servers within the same rack using high-speed network links. When the required distance is appropriate for the selected AOC, an integrated cable can simplify deployment:
Server NIC → AOC → ToR Switch
This avoids separately installing a transceiver at each endpoint and a fiber patch cable between them. For large racks with many servers, reducing the number of individually managed components can simplify installation and troubleshooting.
AOC Use Case: Storage Networks
High-speed storage environments can also benefit from optical connectivity.
Storage traffic can place significant bandwidth demands on network infrastructure, particularly in environments using high-performance shared storage, distributed storage, or virtualization. AOCs can provide direct high-speed connections between compatible storage equipment and network switches where the cable length and interface specifications are appropriate.
AOC Use Case: Switch-to-Switch Connections
AOCs can also be used between switches when the distance is within the specified reach.
For example:
Leaf Switch → AOC → Spine Switch
may be appropriate for a short connection inside a data hall. However, if the connection needs to pass through structured cabling, patch panels, or longer pathways, separate optical transceivers and fiber assemblies may provide greater flexibility.
When Should You Use an AOC?
An AOC is generally worth considering when several conditions are true:
- The endpoints have compatible high-speed ports.
- The required distance falls within the AOC's rated reach.
- A fixed cable length is acceptable.
- A point-to-point connection is preferred.
- Integrated optics are desirable.
- Cable weight and routing are important considerations.
- Separate transceiver replacement is not a primary requirement.
AOCs are particularly well suited to controlled rack environments where the endpoints and cable path are known in advance.
When Should You Use Separate Optical Transceivers?
Separate transceivers and fiber cable assemblies can be more appropriate when infrastructure needs to remain flexible. Consider separate optics when:
- Cable lengths vary significantly
- Links pass through patch panels
- Structured cabling is required
- The fiber plant will be reused for different equipment
- Transceivers may need to be replaced independently
- Different optical reaches may be required
- Future network changes are expected
A separate optical architecture can also make it easier to change the transceiver without replacing the entire cable.
AOC vs. DAC: A Practical Decision
For short links, the choice often comes down to AOC versus DAC.
Choose DAC when:
- The link is very short
- Equipment is in the same rack or nearby
- Copper cabling is acceptable
- Cost and simplicity are priorities
- Cable weight is manageable
Choose AOC when:
- The link is longer than a typical DAC application
- Optical transmission is preferred
- Cable weight matters
- High-density cable management is important
- An integrated optical cable is convenient
- A fixed point-to-point connection is acceptable
Choose separate optics and fiber when:
- The link requires greater flexibility
- Structured cabling is part of the design
- Cable lengths vary
- Patch panels are involved
- Transceivers need to be independently replaceable
- The infrastructure must support future topology changes
Common AOC Deployment Mistakes
- Selecting an AOC only by speed: A 100G rating does not guarantee compatibility with every 100G-capable port.
- Ignoring cable length: Excess cable can create unnecessary rack congestion, while an undersized cable can make installation impossible.
- Treating AOCs like ordinary patch cables: AOCs contain active electronics and should be selected and handled according to the manufacturer's specifications.
- Using an AOC where structured cabling is needed: AOCs are excellent for point-to-point connections, but they may not be the right solution for a facility-wide structured cabling architecture.
- Forgetting future changes: An integrated cable is convenient but less modular than separate optics and fiber. Consider how often the equipment or rack layout is likely to change.
How L-com Supports Data Center Connectivity
L-com provides connectivity products for data center and network applications. For projects that involve high-speed point-to-point connections, L-com offers active optical cables and fiber transceivers that can support a range of switch platforms, form factors, and data center architectures.
Frequently Asked Questions (FAQs)
1. What is an active optical cable (AOC)?
An active optical cable is an integrated cable assembly that combines optical fiber with active electronics at the cable ends. It provides optical connectivity between compatible network ports without requiring separate pluggable transceivers and a separate fiber patch cable.
2. What is the difference between an AOC and a DAC?
A DAC uses copper conductors, while an AOC uses optical fiber with integrated active electronics. DACs are generally intended for very short connections, while AOCs can provide longer reach and lower cable weight for appropriate applications.
3. Is an AOC the same as a fiber optic cable?
An AOC uses optical fiber to transmit the signal, but unlike a passive fiber cable, it also contains active electronic components at both ends. Those components convert the electrical signal to optical and back, so the AOC connects directly between compatible equipment.
4. When should I use an AOC instead of separate transceivers and fiber?
Use an AOC when the endpoints have compatible high-speed ports, the distance is within the AOC’s rated reach, and a fixed-length, point-to-point connection is acceptable. Use separate transceivers and fiber when cable lengths vary, links pass through patch panels, structured cabling is required, or future network changes are expected.
5. What data rates are AOCs available in?
AOCs are commonly available for 25G, 40G, 100G, and 400G applications, depending on the product family and system. The AOC’s rated speed must match the switch or server port, and the host port, cable, and system firmware must support the intended configuration.
6. Where are AOCs commonly used in data centers?
Common applications include GPU and HPC fabrics, top-of-rack-to-server connections, storage networks, and short switch-to-switch links such as leaf-to-spine connections within a data hall. They work best in controlled rack environments where the endpoints and cable path are known in advance.