L-com

What Is the Maximum Voltage Rating of Tray Cables?

By Eileen Harvey

Key Takeaways

  • A tray cable’s voltage rating is the maximum voltage its insulation can safely withstand during normal operation.
  • 300 V ratings are used for power-limited (PLTC) and instrumentation (ITC) tray cables; 600 V is the standard rating for general-purpose TC cable.
  • Specialized tray cables rated 1,000 V, 2,000 V or higher are available for high-power industrial, utility and renewable energy applications.
  • NEC Article 336, NEC Article 392 and UL 1277 govern tray cable voltage ratings, markings and installation.
  • Cables of different voltage ratings can share a tray only with proper separation, such as barriers or separate tray sections.

Tray cables are an integral part of electrical systems in industrial, commercial and utility environments. These cables are designed to provide power, control and signal transmission safely and effectively, often housed within cable trays for organized routing and support. A fundamental specification to understand when selecting tray cables is their voltage rating, which is the maximum voltage the cable insulation can safely withstand during normal operation. Choosing the proper voltage rating is essential for safety, regulatory compliance and optimal system performance.

Below we discuss the maximum voltage rating of tray cables, industry standards, code requirements and best practices for proper cable selection and installation. For a broader overview, see the ultimate guide to tray cables.

 

Understanding Voltage Ratings for Tray Cables

The voltage rating of a cable indicates the maximum alternating or direct voltage the cable insulation can safely handle. It ensures the conductor insulation remains intact and prevents dielectric breakdown, arcing or safety hazards that could arise from voltage stresses exceeding design limits.

Voltage ratings impact safety, performance and compliance. Using cables with the correct voltage rating ensures insulation integrity, protecting workers and systems from electrical faults and shock. It also helps prevent premature cable failure and potential damage to connected equipment. Additionally, adherence to voltage ratings is required by Authorities Having Jurisdiction (AHJs) and insurance providers to maintain legal and regulatory compliance. So which ratings are available?

 

Common Voltage Ratings for Tray Cables

Tray cables are available in several standardized voltage ratings, each designed to meet specific system requirements. The 300-volt cables, often labeled as PLTC (power limited tray cable), are commonly used for power-limited circuits such as alarm systems, fire alarms and intercoms. Their lower voltage rating limits the allowable current and distance, making them well suited for low-power, low-voltage control and signaling applications. Instrumentation tray cable (ITC) is also rated 300 volts and is used for instrumentation and control circuits operating at 150 volts or less.

The 600-volt rating is the most widespread for general-purpose tray cable (TC). These cables are rated to safely carry up to 600 volts AC or DC and are extensively used for power distribution and control in industrial plants, commercial buildings and data centers. They are compatible with a wide range of equipment, including motors, lighting systems and industrial controls, making them a versatile choice for many installations.

Higher-voltage tray cables, rated at 1,000 volts or more, are manufactured with enhanced insulation to handle medium-voltage power distribution or specialized industrial processes. These cables require more stringent installation practices, protective barriers and clear markings to ensure safety and compliance. Some cables carry more than one rating; for example, a cable may be marked 600 V as TC-ER and 1,000 V as WTTC (wind turbine tray cable).

The maximum voltage rating for any tray cable depends on factors such as cable construction, insulation type—whether PVC or XLPE—and testing in accordance with UL (Underwriters Laboratories) and ANSI standards. These ratings ensure that the cables perform reliably under the intended electrical and environmental conditions. Learn how the two insulation types compare in PVC vs. XLPE insulation for tray cables.

These ratings are backed by specific code requirements.

 

NEC and UL Code Requirements on Tray Cable Voltage Ratings

The National Electrical Code (NEC) and UL standards prescribe voltage classifications and installation parameters critical to safety. These standards include NEC Article 336, which defines permissible voltage ratings and application environments for tray cables. NEC Article 392 covers cable tray construction and installation, including segregation of cables by voltage. UL 1277 governs the construction and testing of tray cables, including maximum voltage ratings and thermal properties.

Voltage ratings must be clearly marked on the cable jacket, and cables must be used within their rated limits. When installing cables rated over 600 volts in cable trays, protective barriers and clear signage are typically required to alert maintenance personnel of potential hazards. Beyond code, several practical factors shape the right choice.

 

Factors Affecting Appropriate Voltage Selection

Several factors influence the selection of the appropriate voltage rating for tray cables. The function of the circuit is a primary consideration: power circuits typically require cables rated at 600 volts or higher, while control and signaling circuits may only need 300-volt-rated cables. Choosing the correct voltage ensures that the cable can safely handle the electrical load without risk of overheating or failure. Keep in mind that current capacity depends on conductor size rather than voltage rating; see our tray cable size chart.

The operational environment also plays a key role. In outdoor settings or areas with exposure to chemicals, higher-voltage cables are often preferred because their enhanced insulation provides greater robustness and durability under challenging conditions. Additionally, compliance with code and safety requirements is essential, as certain installations—such as hazardous locations or high-capacity motors—demand specific voltage ratings to meet regulatory standards. For more on motor and machinery applications, read why tray cables are essential for powering and controlling heavy equipment.

The co-location of cables within a tray is another important factor. Mixing cables of different voltage ratings is strictly regulated to prevent electrical interference and minimize potential safety risks. Careful planning of voltage selection, alongside consideration of environment and regulatory requirements, helps ensure both reliable performance and safe operation.

 

Maximum Voltage in Industrial and Utility Installations

In industrial and utility environments, 600-volt tray cables dominate performance and cost-effective distribution systems. However, specialized tray cables and cable tray-rated cables with voltage ratings up to 2,000 volts or more are available and used for medium voltage power systems, including factory high-power drives, substations and renewable energy systems.

Such higher voltage cables require enhanced insulation materials like cross-linked polyethylene (XLPE), segregated tray sections or barriers per NEC, proper labeling and warning signage, and additional grounding and bonding measures. That raises a common question: can cables of different ratings share the same tray?

 

Mixing Cables of Different Voltage Ratings in One Tray

Mixing cables with differing voltage ratings inside the same tray is permitted under NEC, provided appropriate physical and electrical separation is maintained. It is wise to follow some separation rules to enhance electrical safety and system reliability.

For instance, solid fixed barriers may be required between low-voltage and high-voltage cables. Also, installing protective shields or individual trays can prevent induced interference or arcing. A third safety practice is the clear marking of trays and cables, which helps maintenance staff identify hazards. Still have questions? Here are the ones we hear most often.

 

Frequently Asked Questions (FAQs)

What is the highest voltage rating commonly available for tray cable?

Standard tray cables typically max out at 600 volts. Specialized cables rated for 1,000 volts, 2,000 volts or higher are available for industrial medium-voltage applications.

Can 300-volt and 600-volt tray cables be installed in the same tray?

Yes, but physical separation and barriers are often required by code to maintain safety and reduce interference.

What happens if a cable is used above its rated voltage?

Using cables beyond their voltage rating can cause insulation breakdown, short circuits, fire risks and equipment damage.

Can 600V tray cable be used on a 480V system?

Yes. A 600-volt rating covers common industrial systems such as 480 V three-phase, as long as the system voltage does not exceed the cable’s rating.

Does a higher voltage rating mean a tray cable can carry more current?

No. Voltage rating describes what the insulation can withstand, while current capacity (ampacity) depends on conductor size, insulation temperature rating and installation conditions.

 

Conclusion

Selecting the proper voltage rating for tray cables is fundamental for safe and reliable electrical installations. For higher voltage needs, specialized tray cables with higher ratings exist but require strict installation controls and adherence to NEC and UL standards.

Always consult local codes, manufacturer datasheets and electrical experts to ensure your tray cable voltage rating matches your application’s demands.

By understanding and applying the correct voltage rating for tray cables, you safeguard personnel, equipment and operations while complying with industry regulations—setting your project up for success now and in the future.

 

Explore L-com’s range of TKD tray cables, with same-day shipping on all qualified, in-stock, online orders received Monday through Friday before 5 p.m. EST.

Related Products:

Resources

Search Entries