L-com

Understanding Shielding in Flexible Control Cables (Foil, Braid, Combination)

By Eileen Harvey 

Flexible control cables play a pivotal role in modern automation, robotics and many industrial applications where precise control, reliability and noise reduction are critical. These cables are built to withstand bending, twisting and constant movement while maintaining signal integrity. Their flexibility makes them suitable for intricate machinery and robotic systems where rigid cables would fail. They are also engineered to perform in harsh environments with exposure to chemicals, extreme temperatures and mechanical stress, which makes them indispensable in manufacturing plants, assembly lines and automated processes.

One of the most important design features of flexible control cables is shielding. Shielding protects the cables from electromagnetic interference (EMI) and radio-frequency interference (RFI), both of which can cause signal degradation and failures. This article explains the role of shielding in flexible control cables, why it matters, the main types available, how to choose the right option, practical usage tips and recommendations for buyers and installers.

Introduction to Shielding in Control Cables

Electromagnetic interference is a challenge in industries that operate heavy machinery, motors and advanced communication systems. EMI can cause signal degradation, noise interference and in some cases serious system failures. For example, in manufacturing environments with large motors running continuously, electromagnetic fields can disrupt signals in nearby unshielded cables. This disruption may result in faulty readings, delayed responses or complete outages, all of which impact safety and productivity. As industries increasingly rely on electronics for automation and data transfer, addressing EMI has become essential.

Shielding in flexible control cables provides protection against EMI and RFI, improves signal quality and extends cable life in demanding conditions.

Why Shielding Matters in Flexible Control Cables

Shielding ensures noise reduction by preventing cross-talk between cables, which helps maintain signal clarity. It also protects sensitive electronic systems from interference caused by nearby equipment, which increases system reliability. The shield serves as an additional barrier against mechanical stress and exposure to harsh environments, improving durability. Finally, shielding supports compliance with international safety standards that mandate its use in certain industrial applications.

Types of Shielding

1. Foil Shielding: Foil shielding relies on a thin layer of aluminum or polyester-aluminum laminate wrapped around the conductor or cable. It provides complete coverage of the conductors, is lightweight and cost-effective and works well against high-frequency EMI. However, foil shielding is less flexible than a braid and can be damaged by repetitive bending. It is best suited for low-frequency data transmission, office automation systems and electronics. An example is double-shielded Cat5e bulk cable, which provides reliable noise protection.

2. Braid Shielding: Braid shielding is made of woven strands of tinned copper or aluminum. It offers strong mechanical protection and high flexibility, making it ideal for applications with frequent motion. It provides excellent resistance to low-frequency interference. Its coverage typically ranges from 70% to 95%, which leaves small gaps. It is heavier and more expensive than foil shielding but works best in robotics, automation and other environments that require durable shielding in moving cables.

3. Combination Shielding (Foil + Braid): Combination shielding uses both foil and braid to maximize protection. A foil layer is wrapped around the conductor with a braided shield placed on top. This design offers near-complete EMI protection across both low and high frequencies, while also adding strength and flexibility. It is suitable for long-distance transmission and high-noise environments. The tradeoffs are higher cost and additional cable bulk. Combination shielding is best for heavy industrial applications, data centers and environments with high EMI exposure. An example is double-shielded Cat5e cable.

Choosing the Right Shielding for Your Application

The right shielding depends on the conditions of use. High-noise environments benefit from combination shielding, while robotics and machinery that require constant cable movement are better suited to braid shielding. Foil shielding is economical but less durable in moving systems. For frequency considerations, foil is more effective at blocking high-frequency interference while braid works better for low frequencies.

Tips for Using Shielded Control Cables

Shielded cables should always be properly grounded to ensure full EMI protection. Excessive bending can damage foil shielding, so it is best to avoid sharp bends. Using strain relief helps protect the cable at connection points. Choosing the correct jacket material, whether PVC, PUR or TPE, ensures compatibility with the operating environment.

Recommendations for Buyers and Installers

For stationary installations, foil shielding is a cost-effective solution that provides reliable EMI protection. For applications that require flexibility, braid shielding is the better option due to its durability. In critical systems where maximum signal integrity is needed, combination shielding delivers the highest level of performance. Always consult industry standards such as UL, IEC or NEC before selecting cables, and work with trusted suppliers who provide testing and compliance certifications.

Frequently Asked Questions (FAQ)

Q1: What is the purpose of shielding in flexible control cables?
A: Shielding protects cables from external electromagnetic interference, ensuring signal clarity and reliable performance.

Q2: Which shielding is best for robotics?
A:
Braided shielding is the most suitable for robotics due to its flexibility and durability under constant movement.

Q3: Is foil shielding enough for industrial environments?
A:
Foil shielding provides excellent EMI protection but may not withstand mechanical stress in dynamic environments. Combination shielding is recommended for heavy industries.

Shielded flexible control cables play a crucial role in ensuring reliable performance, especially in environments with high electromagnetic interference. Whether you choose foil shielding for cost efficiency, braided shielding for flexibility or combination shielding for maximum protection, the right choice depends on your application and operating environment.

Resources

Search Entries