L-com

Types of PROFINET Cables: Type A (Fixed), Type B (Flexible), Type C (Continuous Flex), Type D (Wireless Infrastructure)

By Eileen Harvey 

Industrial automation is a cornerstone of modern manufacturing and production processes and at the heart of this evolution lies the importance of reliable communication networks. These networks serve as the vital arteries through which data flows, connecting various components of an automated system. Among the essential elements facilitating this seamless communication are PROFINET cables, specifically engineered to meet the rigorous demands of Industrial Ethernet.  

These cables are designed to withstand harsh environments, deliver high-speed data transfer and ensure minimal downtime, all of which are crucial for maintaining the efficiency and productivity of industrial operations. 

Overview of PROFINET Cable Types 

PROFINET cables fall into four categories. Type A is fixed installation, Type B is flexible installation, Type C is continuous flex for dynamic motion and Type D is wireless infrastructure support. Each type is tailored for specific mechanical stresses and environments. By standardizing these, PI ensures seamless deployment across industries and vendors. 

Type A: Fixed Installation Cables 

Type A PROFINET cables are designed for stationary setups where movement is minimal. They feature solid copper conductors that provide excellent signal integrity and long-term stability. The cables are built with robust insulation and shielded twisted pairs to ensure strong electromagnetic compatibility (EMC) protection in environments where interference could disrupt data transmission. These cables are typically used in control cabinets, permanently mounted devices, and other static production environments. Their main advantages include affordability and reliable performance in fixed installations. However, Type A cables are not suited for situations requiring frequent bending or mechanical movement, as their solid conductors can fatigue under repetitive stress. 

Type B: Flexible Installation Cables 

Type B cables use stranded copper conductors to achieve greater mechanical flexibility compared to Type A designs. They are constructed with durable PUR or PVC jackets that provide resistance to oil, chemicals, and moderate mechanical stress. These features make them well-suited for machines that move occasionally, adjustable production lines, and environments where cables may need to be repositioned during maintenance or reconfiguration. Type B cables are more adaptable and resilient than their fixed counterparts, yet they are not intended for continuous flexing or constant motion. Their moderate flexibility provides a balanced solution for semi-dynamic applications without incurring the higher costs of continuous flex-rated cables. 

Type C: Continuous Flex Cables 

Type C PROFINET cables are engineered for environments involving constant movement and high mechanical stress. They contain extra-fine stranded conductors paired with high-flex insulation and shielding materials to maintain electrical performance through millions of bending cycles. The reinforced outer jacket offers exceptional durability, allowing these cables to function reliably within drag chains, robotic arms, and conveyor systems. Commonly used in robotics, automotive assembly lines, and other automation-heavy industries, Type C cables excel in applications demanding continuous motion. Their primary limitation is higher cost, which results from their specialized construction and materials designed to withstand extreme wear over long service life. 

Type D: Wireless Infrastructure 

Type D cables are designed to support modern wireless architectures that integrate both copper and fiber elements to enhance network adaptability. These cables are often used to connect wireless access points within smart factories, forming the backbone for IoT-enabled and mobile systems. Their design enables the deployment of hybrid infrastructures that support both wired and wireless connectivity, crucial for Industry 4.0 environments focused on flexibility and real-time communication. The main advantages of Type D cables include improved mobility, scalability, and compatibility with advanced automation networks. However, successful implementation requires careful network design and planning to ensure consistent wireless coverage and avoid signal disruptions across complex industrial spaces. 

How to Select the Right PROFINET Cable 

When selecting a PROFINET cable, there are four main considerations. The first is installation type: fixed, flexible or continuous motion. The second is environment: exposure to oil, chemicals or UV. The third consideration in selecting the right cable is EMC requirements: shielding in noisy environments. And the fourth consideration is future-proofing: higher categories (Cat6/7) for bandwidth demands. 

Applications Across Industries 

PROFINET cable is particularly useful in manufacturing, robotics, process industries and logistics. In manufacturing, Type A is used for control panels and Type B for semi-flex systems. In robotics, Type C ensures reliability in repetitive motion. For process industries, Type A and Type B are used for stable connections in chemical and food processing. In logistics, Type D supports wireless for AGVs and smart warehouses. 

Tips for Engineers 

We offer four useful tips. First, use Type A for static wiring to reduce costs. Second, select Type C in robotics to avoid frequent replacements. Third, opt for PUR jackets in environments with oil or chemicals. And fourth, combine copper and fiber where long-distance high-speed links are needed. 

Recommendations 

Trusted suppliers like TKD Kabel Industrial Cables and L-com PROFINET Cable Solutions provide certified cable options tailored for each type (A–D). Choosing certified cables ensures compliance with PROFINET International (PI) guidelines and reduces downtime. 

Facts Worth Knowing 

  • Over 37 million PROFINET devices were installed worldwide by 2022 (source: PI). 
  • Type C cables are tested for up to 10 million bending cycles in drag chains. 
  • Wireless (Type D) is becoming essential in smart factories with mobile robotics. 

 

 

 

FAQs About PROFINET Cable Types 

Q1: What is the main difference between PROFINET cable types? 
A: The difference lies in their mechanical flexibility: Type A is fixed, Type B is flexible, Type C is high-flex and Type D supports wireless infrastructure. 

Q2: Can I use Type A cables in moving applications? 
A: No, Type A is designed for fixed installations. For moving parts, use Type B or Type C. 

Q3: Which type of cable is best for robotics? 
A: Type C is ideal for robotics because it withstands continuous flexing. 

Q4: Do PROFINET cable types affect data speed? 
A: No. Data speed is defined by cable category (Cat5e, 6, 7). Cable types (A–D) mainly relate to mechanical stress and installation environment. 

Selecting the right PROFINET cable type isn’t just a technical detail—it’s a strategic decision that impacts system performance, maintenance costs and long-term reliability. Remember that Type A is best for fixed installations, Type B is flexible for moderate movement, Type C is high flex for robotics and automation, and Type D is wireless for Industry 4.0 mobility. 

By aligning cable type with application, engineers ensure networks remain robust, efficient and future-ready. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries