L-com

The Role of Shielding in Servo and VFD Cables

Electrical noise can turn a precise motor movement into a positioning error or an unexpected drive fault. In a busy automation system, that can mean disrupted production and costly downtime. Servo and VFD cable shielding helps protect the signals that keep motors and nearby equipment working reliably.

Foil shielding tackles high-frequency interference, while braid shielding adds mechanical durability and protection at lower frequencies. Many industrial cables combine the two. Choosing between them means looking at the electrical noise, movement and installation conditions your cable will face.

So what protection do your Servo cables and variable frequency drive (VFD) cables need? Let's compare the shielding options, look at their roles in each application and work through the selection and grounding considerations that help you get the most from them.

 

Key Takeaways

  • VFD cables generate high-frequency switching noise that can interfere with nearby signal cables without adequate shielding.
  • Foil shielding blocks high-frequency EMI; braid shielding adds mechanical durability and lower-frequency protection; many industrial cables combine both.
  • Servo cables carry sensitive feedback signals that are especially vulnerable to EMI-induced errors.
  • Improper grounding of a shielded cable can be as damaging as using no shield at all.

 

Understanding Shielding in Industrial Cables

Shielding is a conductive layer around the insulated conductors inside a cable. Usually made from copper braid, aluminum foil or a combination of the two, it blocks external electromagnetic noise and helps prevent internal signals from leaking out.

Each material brings something different. Copper braid is flexible and strong, with excellent EMI protection. Aluminum foil is lightweight and effective at high frequencies. Combining them offers stronger overall protection.

The shield's arrangement matters too. Overall shielding encloses all the conductors in the cable, while individual pair shielding protects each conductor pair. The latter is particularly useful for sensitive feedback and encoder signals.

 

Foil vs. Braid Shielding at a Glance

Here's how the material options compare before we look at what VFD and servo applications need from them.

Shielding TypeFrequency Range ProtectedFlexibilityCost
Foil High-frequency EMI Thin, less flexible Lower
Braid Low-to-mid-frequency EMI, strong mechanical durability More flexible, thicker Moderate
Foil + Braid combination Broad range (high and low frequency) Balanced Highest

With those differences in mind, start with VFD cables, where shielding helps contain the noise generated by the drive.

 

Shielding in VFD Cables

Variable frequency drives adjust motor speed and torque by varying frequency and voltage, but this process generates high-frequency switching noise and harmonics that can affect both the motor and nearby equipment.

Shielding is essential because it prevents EMI from radiating into surrounding electronics, reduces common mode currents that can damage motor bearings, helps facilities comply with Electromagnetic Compatibility regulations and protects nearby communication lines and sensors from interference. Without proper shielding, a VFD cable can create radiated noise that causes a nearby PLC to malfunction, whereas a shielded VFD cable preserves motor efficiency and supports overall plant reliability.

For servo cables, the concern shifts to the feedback signals that make precise movement possible.

 

Shielding in Servo Cables

Servo cables carry both power and feedback signals that enable precise motor control, and any interference in the feedback line can lead to incorrect positioning, jerky movements or complete system failure.

Shielding prevents EMI and crosstalk from disrupting encoder signals, ensures accurate speed and position feedback to controllers and supports dependable operation in robotics, CNC machines and automated assembly lines. By maintaining signal integrity, shielding also reduces downtime caused by feedback errors. In a robotic arm, even a slight EMI related disruption in encoder feedback can produce misaligned components, while a properly shielded servo cable maintains pinpoint accuracy for smooth, uninterrupted production.

Although VFD and servo cables face different signal challenges, shielding delivers several benefits across both applications.

 

Benefits of Shielding in Both Servo and VFD Cables

  • Reduces EMI and RFI: Protects sensitive signals and equipment.
  • Enhances Safety: Minimizes fire and shock hazards from stray currents.
  • Boosts Motor Performance: Stable voltage and current improve efficiency.
  • Extends Equipment Lifespan: Prevents premature wear in motors and bearings.
  • Ensures Standards Compliance: Meets UL, CSA, CE and IEC regulations.

Skipping or under-speccing shielding is also one of the more common contributors to premature servo cable failure, since unprotected feedback lines are far more prone to EMI-driven faults and wear.

To get those benefits, the shield needs to suit the system. The next step is to check the conditions that will guide your cable choice.

 

When Selecting a Shielded Cable

Start with the environment: areas with high EMI often need double shielding. Motor size and operating frequency matter too, since larger motors generate more electrical noise and can benefit from heavier shielding. Check the routing as well, especially where power cables run close to data or communication lines. Finally, plan the termination and grounding, because a shield is only effective when it's correctly grounded.

For a full walkthrough of matching voltage, shielding and insulation to your drive system, see choosing the right VFD cable.

Once you've narrowed down the cable, these practical checks help you avoid problems during installation and operation.

 

Tips and Recommendations

Shielding should always match the needs of the application, and there is no benefit in paying for double shielding unless the system requires it. Proper grounding must be maintained to prevent floating noise that can undermine cable performance. VFD and servo cables should be routed separately from low voltage communication lines to reduce the chance of interference. Using high quality shielded options such as TKD Kabel's Kaweflex series helps ensure long term reliability in demanding industrial environments.

Still have questions about shielding types, cable choice or grounding? Here are the ones that come up most often.

 

FAQs About Shielding in Servo and VFD Cables

Do all VFD cables need shielding?

Yes. Without shielding, VFDs generate EMI that can cause equipment malfunctions and safety risks.

Can I use regular power cables instead of shielded servo cables?

No. Regular power cables cannot protect sensitive encoder signals, leading to inaccurate motor control.

What's the difference between foil and braid shielding?

Foil is better for high-frequency noise, while braid is better for mechanical durability and low-frequency EMI.

How do I ground shielded cables properly?

The shield should be grounded at one or both ends, depending on system design, to maximize EMI suppression.

Reliable shielding starts with choosing a cable that suits the application and grounding it correctly. Together, those choices help reduce EMI, protect signal accuracy and keep the wider automation system running reliably.

 

Explore the full range of TKD Kabel through L-com. We'll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com.

 

Read Next

Resources

Search Entries