L-com

Shielding in PROFINET Cables: Foil, Braid or Combination

By Eileen Harvey 

In modern industrial environments, cables face more than just physical stress. They battle electromagnetic interference (EMI) from motors, drives, welding equipment and high-voltage lines. This interference can significantly impact the performance of communication networks, particularly in systems like PROFINET, where real-time data exchange is crucial for operational efficiency. Delays in data transmission, erroneous data packets or even complete network outages can occur if EMI is not adequately mitigated. Such disruptions not only hinder productivity but can also lead to costly downtime and potential safety hazards in a factory setting. 

To combat these challenges, effective shielding in PROFINET cables plays an essential role. Shielding is not merely an additional layer; rather, it serves as a robust defense mechanism designed to protect sensitive data signals from external disturbances. By incorporating high-quality shielding materials, manufacturers can create cables that maintain signal integrity even in the most demanding environments 

What Is Shielding in PROFINET Cables? 

Shielding is a protective conductive layer built into a cable to block external interference and prevent internal signal leakage. Let’s look at four key functions of shielding. First, it prevents EMI and RFI (radio frequency interference) disruptions. Second, it reduces crosstalk between pairs within the same cable. Third, shielding maintains signal integrity for real-time PROFINET communication. And fourth, it ensures compliance with industrial cabling standards 

Standards like ISO/IEC 11801 and TIA/EIA require shielding in industrial Ethernet cables used for automation. For PROFINET, shielding is non-negotiable due to the high data transmission demands of Industry 4.0 and IIoT applications. 

Types of Shielding in PROFINET Cables 

Foil Shielding (F/UTP, F/FTP): Foil shielding uses a thin layer of aluminum foil wrapped either around individual pairs, as in F/FTP designs, or around the entire cable bundle, as in F/UTP types. This construction provides a lightweight and flexible option that is cost-effective while offering solid protection against high-frequency interference. However, the foil can tear under mechanical stress and does not hold up well in environments with strong vibration, making it less durable for heavy-duty applications. Foil shielding is best suited for office-level automation systems, industrial environments with moderate EMI, and fixed installations where flexibility and affordability are priorities. 

Braid Shielding (S/UTP, S/FTP): Braid shielding employs a woven mesh of copper or tinned copper that envelops either the entire cable bundle or each individual pair. This design delivers strong mechanical durability, excellent protection against low-frequency EMI, and an effective grounding path for electrical stability. The trade-offs are greater weight, reduced flexibility, and higher cost compared to foil shielding. Because of its ruggedness, braid shielding is ideal for industrial robots, motion control systems, and other areas exposed to high levels of mechanical stress or vibration. 

Combination Shielding (SF/UTP, SF/FTP): Combination shielding merges the strengths of both foil and braid, using foil to block high-frequency EMI and braid to counter low-frequency interference while providing mechanical reinforcement. This hybrid configuration offers comprehensive EMI protection and durability suitable for harsh industrial conditions and high-speed PROFINET applications. The main drawbacks are its higher cost and reduced flexibility relative to single-shield designs. Combination shielding is the preferred choice for demanding environments such as automotive plants with welding robots, pharmaceutical and food production facilities where downtime is unacceptable, and advanced Industry 4.0 or IIoT systems requiring high bandwidth and superior EMI performance. 

Choosing the Right Shielding Type 

Selecting the appropriate shielding for a PROFINET cable depends on several key factors, including EMI exposure, mechanical stress, budget, and long-term scalability. In environments with low electromagnetic interference, foil shielding provides adequate protection at minimal cost. For areas with moderate EMI, braid shielding delivers stronger performance and better durability. When interference levels are high, combination shielding offers the most comprehensive protection across both high- and low-frequency ranges. 

Mechanical stress also influences the decision. Foil shielding works well for fixed installations where the cable remains stationary. Braid shielding is better suited for flexible or robotic systems that require repeated motion without compromising signal integrity. In harsh environments that involve continuous flexing, combination shielding ensures both resilience and signal reliability. 

Budget considerations play a role as well. Foil shielding represents the most economical choice, braid sits in the mid-tier range, and combination shielding is the premium option due to its enhanced protection and mechanical strength. For those planning long-term or scalable industrial networks, combination shielding provides the best future-proofing, ensuring consistent performance as system demands evolve. 

Standards and Compliance 

The performance of a cable’s shielding is closely linked to its adherence to recognized industry standards. ISO/IEC 11801 defines global requirements for structured cabling systems, while EN 50173 serves as the European equivalent. In the United States, TIA/EIA-568 outlines best practices for network cabling installation and performance. Additionally, PROFINET cabling guidelines provide detailed specifications tailored specifically to industrial Ethernet applications. A key factor in meeting these standards is proper termination and grounding of shielded cables, since poor grounding can completely negate the benefits of shielding and lead to increased susceptibility to interference. 

Tips for Installation and Performance 

For reliable performance, maintaining continuous shielding throughout the cable’s length is essential. The shield should never be cut during termination, as even small interruptions can create EMI vulnerabilities. Always use shielded connectors, such as RJ45 or M12 industrial types, to preserve continuity. Avoid tight bends that may crack the foil or loosen the braid, and maintain a minimum separation of 20 centimeters between shielded network cables and power lines to minimize electrical noise. Once installation is complete, test all cables using Fluke or equivalent certification tools to verify proper shielding, continuity, and signal integrity. 

Practical Recommendations 

Foil shielding offers a cost-effective solution for light automation or fixed installations where EMI exposure is minimal. Braid shielding is a better option for systems exposed to regular motion, vibration, or mechanical stress, providing greater durability and grounding capability. Combination shielding should be selected for harsh environments with heavy EMI or for systems expected to scale over time, as it combines superior protection with long-term resilience. For Industry 4.0 or other advanced automation applications, Cat6 or Cat7 cables featuring SF/FTP shielding ensure the highest performance and future compatibility with demanding industrial networks. 

FAQs About Shielding in PROFINET Cables 

Q1: What’s the difference between foil and braid shielding in PROFINET cables? 
A: Foil blocks high-frequency EMI, while braid provides better mechanical strength and low-frequency EMI protection. 

Q2: Is combination shielding necessary for all PROFINET applications? 
A: Not always. It’s essential in high-EMI environments but may be overkill for small, low-interference networks. 

Q3: Can unshielded Ethernet cables be used for PROFINET? 
A: No. PROFINET networks demand shielded cables to ensure real-time data integrity. 

Q4: How do I ensure shielding works properly? 
A: By ensuring correct termination and grounding at both ends. Improper grounding reduces shielding effectiveness. 

Shielding in PROFINET cables—foil, braid or combination—is the first line of defense against EMI and crosstalk in industrial networks. Foil shielding offers a cost-effective solution for light to moderate EMI. Braid shielding provides durability and protection in mechanically demanding setups. And combination shielding delivers the ultimate reliability in harsh, interference-heavy environments. 

The right choice depends on environmental conditions, application criticality and future scalability. Investing in proper shielding ensures network reliability, system uptime and Industry 4.0 readiness. 

Explore the full range of TKD Kabel through L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. For TKD-related inquiries, connect with our U.S-based TKD expert Eileen Harvey at eharvey@infiniteelectronics.com. 

Resources

Search Entries